/* * ======== main.c ======== */ /* System header files */ #include #include #include /*---------------------------------------- * BIOS header files *----------------------------------------*/ #include /* mandatory - if you call APIs like BIOS_start() */ /* Portable data types */ #include #include #include "components/fil.h" #include "components/sys.h" /* Global System Configuration Structure */ sysConfig_t sysConfig = { SYS_MICS_MAX, /* #microphones */ SYS_VMICS_MAX, /* #virtual microphones */ FALSE, /* Do not use file I/O to load files (must use GEL to load into memory) */ TRUE /* Use default angles for microphone configurations */ }; /* Global FILE I/O Configuration Structure (must be configured even when file I/O not used */ filConfig_t filConfig = { FIL_LENGTH_MAX, /* number of samples to load from a file */ SYS_MICS_MAX, /* number of files to use */ TRUE, /* big endian */ FALSE, /* do not wrap around */ 40*SYS_FS_HZ /* Process 40s of the signal (current mic input file length */ }; /* Miocrophone input files names (in case we want to use FILE I/O to load into memory */ char *filNames[FIL_MAX] = { "../t8/y16L8g3m7090_1.pcm", "../t8/y16L8g3m7090_2.pcm", "../t8/y16L8g3m7090_3.pcm", "../t8/y16L8g3m7090_4.pcm", "../t8/y16L8g3m7090_5.pcm", "../t8/y16L8g3m7090_6.pcm", "../t8/y16L8g3m7090_7.pcm", "../t8/y16L8g3m7090_8.pcm" }; /* Acoustic environment */ /* Room Size (X,Y,Z) in meters */ /* 5.2000 4.3000 2.7000 */ /* Table size (X,Y,Z) in meters */ /* 3.0000 2.4000 0.7600 */ /* "Echo" generating speaker position (X,Y,Z) in meters */ /* 0 2.1500 1.2172 180 -90 VM-9 */ /* People positions (X,Y,Z) in meters and angles relative to the table and array */ /* 1.8200 0.6452 1.2172 position#1 (person#1) -123.6056 -146.3944 VM-7 2.8200 0.6452 1.2172 -not used- -90.0000 180.0000 VM-6 3.8200 0.6452 1.2172 (person#2) -56.3944 146.3944 VM-5 1.8200 3.6548 1.2172 (person#3) 123.6056 -33.6056 VM-11 2.8200 3.6548 1.2172 -not used- 90.0000 0.0000 VM-0 3.8200 3.6548 1.2172 position#6 (person#4) 56.3944 33.6056 VM-1 */ /* Microphone array mic positions (X,Y,Z) in meters */ /* 2.7922 2.1500 0.7600 mic#1 ("left" most) 180 2.8004 2.1304 0.7600 -135 2.8200 2.1222 0.7600 ("lower" most) -90 2.8396 2.1304 0.7600 -45 2.8478 2.1500 0.7600 ("right" most) 0 2.8396 2.1696 0.7600 45 2.8200 2.1778 0.7600 ("upper" most) 90 2.8004 2.1696 0.7600 mic#8 135 */ /* Array Center = (2.82, 2.15, 0.76) (same as table center) */ /* Noise source position (X,Y,Z) in meters */ /* 2.6000 2.1500 2.3000 */ /* Initialize FILE I/O, system context */ static void system_init(void) { int k, err; tlong n; void *fid; fid = (void*)0xBABA; /* Just to test if we're providing fid correctly */ err = filCreate(&fid, &filConfig); /* Create FILE I/O context */ SYS_CHECK_ERROR(err); err = sysCreate(&sysConfig); /* Create system context */ SYS_CHECK_ERROR(err); err = sysPrintConfig(SYSM_SCOPE_STATIC|SYSM_SCOPE_DYNAMIC); SYS_CHECK_ERROR(err); if (sysContext.use_fileio) { /* In case we want to read directly from file (slow) */ for (k = 0; k < filConfig.nfiles; k++) { n = filLoad(filNames[k], filConfig.length, k); System_printf("Read %ld samples from %s\n", n, filNames[k]); } } ///System_flush(); /* If we are not using FILE I/O to load mic files, we need to use GEL to load into memory. */ } /* system_init */ /* * =============== main ============== */ int main(void) { system_init(); /* initialize system context, etc. */ sysBfCreate(); /* Create beamformers */ sysAsnrCreate(); /* Create ASNR's */ sysMssCreate(); /* Create MSS */ sysVauCreate(); /* Create VAU */ BIOS_start(); return(0); /* Never to return here */ } /* main */ /* nothing past this point */