/* * sample_cs.c * * Sample functions showing the implementation of critical section entry/exit * routines and various semaphore related routines (all BIOS6 depenedent). * These implementations MUST be provided by the user / application, using the * EDMA3 driver, for its correct functioning. * * Copyright (C) 2009-2012 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include #include #include #include #include #include #include extern unsigned int ccXferCompInt[][EDMA3_MAX_REGIONS]; extern unsigned int ccErrorInt[]; extern unsigned int tcErrorInt[][EDMA3_MAX_TC]; /** * Shadow Region on which the executable is running. Its value is * populated with the DSP Instance Number here in this case. */ extern unsigned int region_id; /** * \brief EDMA3 OS Protect Entry * * This function saves the current state of protection in 'intState' * variable passed by caller, if the protection level is * EDMA3_OS_PROTECT_INTERRUPT. It then applies the requested level of * protection. * For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and * EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored, * and the requested interrupt is disabled. * For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, '*intState' specifies the * Transfer Controller number whose interrupt needs to be disabled. * * \param level is numeric identifier of the desired degree of protection. * \param intState is memory location where current state of protection is * saved for future use while restoring it via edma3OsProtectExit() (Only * for EDMA3_OS_PROTECT_INTERRUPT protection level). * \return None */ void edma3OsProtectEntry (unsigned int edma3InstanceId, int level, unsigned int *intState) { if (((level == EDMA3_OS_PROTECT_INTERRUPT) || (level == EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR)) && (intState == NULL)) { return; } else { switch (level) { /* Disable all (global) interrupts */ case EDMA3_OS_PROTECT_INTERRUPT : *intState = Hwi_disable(); break; /* Disable scheduler */ case EDMA3_OS_PROTECT_SCHEDULER : Task_disable(); break; /* Disable EDMA3 transfer completion interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION : EventCombiner_disableEvent(ccXferCompInt[edma3InstanceId][region_id]); break; /* Disable EDMA3 CC error interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR : EventCombiner_disableEvent(ccErrorInt[edma3InstanceId]); break; /* Disable EDMA3 TC error interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR : switch (*intState) { case 0: case 1: case 2: case 3: case 4: case 5: case 6: case 7: /* Fall through... */ /* Disable the corresponding interrupt */ EventCombiner_disableEvent(tcErrorInt[edma3InstanceId][*intState]); break; default: break; } break; default: break; } } } /** * \brief EDMA3 OS Protect Exit * * This function undoes the protection enforced to original state * as is specified by the variable 'intState' passed, if the protection * level is EDMA3_OS_PROTECT_INTERRUPT. * For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and * EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored, * and the requested interrupt is enabled. * For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, 'intState' specifies the * Transfer Controller number whose interrupt needs to be enabled. * \param level is numeric identifier of the desired degree of protection. * \param intState is original state of protection at time when the * corresponding edma3OsProtectEntry() was called (Only * for EDMA3_OS_PROTECT_INTERRUPT protection level). * \return None */ void edma3OsProtectExit (unsigned int edma3InstanceId, int level, unsigned int intState) { switch (level) { /* Enable all (global) interrupts */ case EDMA3_OS_PROTECT_INTERRUPT : Hwi_restore(intState); break; /* Enable scheduler */ case EDMA3_OS_PROTECT_SCHEDULER : Task_enable(); break; /* Enable EDMA3 transfer completion interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION : EventCombiner_enableEvent(ccXferCompInt[edma3InstanceId][region_id]); break; /* Enable EDMA3 CC error interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR : EventCombiner_enableEvent(ccErrorInt[edma3InstanceId]); break; /* Enable EDMA3 TC error interrupt only */ case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR : switch (intState) { case 0: case 1: case 2: case 3: case 4: case 5: case 6: case 7: /* Fall through... */ /* Enable the corresponding interrupt */ EventCombiner_enableEvent(tcErrorInt[edma3InstanceId][intState]); break; default: break; } break; default: break; } } /** * \brief EDMA3 Cache Invalidate * * This function invalidates the D cache. * * \param mem_start_ptr [IN] Starting address of memory. * Please note that this should be * aligned according to the cache line size. * \param num_bytes [IN] length of buffer * \return EDMA3_DRV_SOK if success, else error code in case of error * or non-alignment of buffers. * * Note: This function is required if the buffer is in DDR. * For other cases, where buffer is NOT in DDR, user * may or may not require the below implementation and * should modify it according to her need. */ EDMA3_DRV_Result Edma3_CacheInvalidate(unsigned int mem_start_ptr, unsigned int num_bytes) { EDMA3_DRV_Result cacheInvResult = EDMA3_DRV_SOK; /* Verify whether the start address is cache aligned or not */ if((mem_start_ptr & (EDMA3_CACHE_LINE_SIZE_IN_BYTES-1u)) != 0) { #ifdef EDMA3_DRV_DEBUG EDMA3_DRV_PRINTF("\r\n Cache : Memory is not %d bytes alinged\r\n", EDMA3_CACHE_LINE_SIZE_IN_BYTES); #endif cacheInvResult = EDMA3_NON_ALIGNED_BUFFERS_ERROR; } else { Cache_inv((Ptr)mem_start_ptr, num_bytes, Cache_Type_ALL, TRUE); } return cacheInvResult; } /** * \brief EDMA3 Cache Flush * * This function flushes (cleans) the Cache * * \param mem_start_ptr [IN] Starting address of memory. * Please note that this should be * aligned according to the cache line size. * \param num_bytes [IN] length of buffer * \return EDMA3_DRV_SOK if success, else error code in case of error * or non-alignment of buffers. * * Note: This function is required if the buffer is in DDR. * For other cases, where buffer is NOT in DDR, user * may or may not require the below implementation and * should modify it according to her need. */ EDMA3_DRV_Result Edma3_CacheFlush(unsigned int mem_start_ptr, unsigned int num_bytes) { EDMA3_DRV_Result cacheFlushResult = EDMA3_DRV_SOK; /* Verify whether the start address is cache aligned or not */ if((mem_start_ptr & (EDMA3_CACHE_LINE_SIZE_IN_BYTES-1u)) != 0) { #ifdef EDMA3_DRV_DEBUG EDMA3_DRV_PRINTF("\r\n Cache : Memory is not %d bytes alinged\r\n", EDMA3_CACHE_LINE_SIZE_IN_BYTES); #endif cacheFlushResult = EDMA3_NON_ALIGNED_BUFFERS_ERROR; } else { Cache_wb((Ptr)mem_start_ptr, num_bytes, Cache_Type_ALL, TRUE); } return cacheFlushResult; } /** * Counting Semaphore related functions (OS dependent) should be * called/implemented by the application. A handle to the semaphore * is required while opening the driver/resource manager instance. */ /** * \brief EDMA3 OS Semaphore Create * * This function creates a counting semaphore with specified * attributes and initial value. It should be used to create a semaphore * with initial value as '1'. The semaphore is then passed by the user * to the EDMA3 driver/RM for proper sharing of resources. * \param initVal [IN] is initial value for semaphore * \param semParams [IN] is the semaphore attributes. * \param hSem [OUT] is location to recieve the handle to just created * semaphore * \return EDMA3_DRV_SOK if succesful, else a suitable error code. */ EDMA3_DRV_Result edma3OsSemCreate(int initVal, const Semaphore_Params *semParams, EDMA3_OS_Sem_Handle *hSem) { EDMA3_DRV_Result semCreateResult = EDMA3_DRV_SOK; if(NULL == hSem) { semCreateResult = EDMA3_DRV_E_INVALID_PARAM; } else { *hSem = (EDMA3_OS_Sem_Handle)Semaphore_create(initVal, semParams, NULL); if ( (*hSem) == NULL ) { semCreateResult = EDMA3_DRV_E_SEMAPHORE; } } return semCreateResult; } /** * \brief EDMA3 OS Semaphore Delete * * This function deletes or removes the specified semaphore * from the system. Associated dynamically allocated memory * if any is also freed up. * \param hSem [IN] handle to the semaphore to be deleted * \return EDMA3_DRV_SOK if succesful else a suitable error code */ EDMA3_DRV_Result edma3OsSemDelete(EDMA3_OS_Sem_Handle hSem) { EDMA3_DRV_Result semDeleteResult = EDMA3_DRV_SOK; if(NULL == hSem) { semDeleteResult = EDMA3_DRV_E_INVALID_PARAM; } else { Semaphore_delete((Semaphore_Handle *)&hSem); } return semDeleteResult; } /** * \brief EDMA3 OS Semaphore Take * * This function takes a semaphore token if available. * If a semaphore is unavailable, it blocks currently * running thread in wait (for specified duration) for * a free semaphore. * \param hSem [IN] is the handle of the specified semaphore * \param mSecTimeout [IN] is wait time in milliseconds * \return EDMA3_DRV_Result if successful else a suitable error code */ EDMA3_DRV_Result edma3OsSemTake(EDMA3_OS_Sem_Handle hSem, int mSecTimeout) { EDMA3_DRV_Result semTakeResult = EDMA3_DRV_SOK; unsigned short semPendResult; if(NULL == hSem) { semTakeResult = EDMA3_DRV_E_INVALID_PARAM; } else { semPendResult = Semaphore_pend(hSem, mSecTimeout); if (semPendResult == FALSE) { semTakeResult = EDMA3_DRV_E_SEMAPHORE; } } return semTakeResult; } /** * \brief EDMA3 OS Semaphore Give * * This function gives or relinquishes an already * acquired semaphore token * \param hSem [IN] is the handle of the specified semaphore * \return EDMA3_DRV_Result if successful else a suitable error code */ EDMA3_DRV_Result edma3OsSemGive(EDMA3_OS_Sem_Handle hSem) { EDMA3_DRV_Result semGiveResult = EDMA3_DRV_SOK; if(NULL == hSem) { semGiveResult = EDMA3_DRV_E_INVALID_PARAM; } else { Semaphore_post(hSem); } return semGiveResult; } /* End of File */