VPE 3.6.0.0 Release Notes
June 28, 2013
Introduction
Documentation
What's New
Upgrade and Compatibility Information
Host Support
Device Support
Validation Information
Known Issues
Version Information
Technical Support
Introduction
The Voice Processing Elements (VPE) component is a collection of voice processing modules that each perform specific functionality for a voice channel.
back to top
Documentation
The following documentation is available:
Release notes from previous releases are also available in the Release Notes Archive directory.
back to top
What's New
The following new features were added:
- Added Adaptive Spectral Noise Reduction (ASNR) module
back to top
Upgrade and Compatibility Information
This ti.mas.vpe version is compatible with the last released ti.mas.vpe version.
Please note that the package compatibility keys are independent of XDC product release numbers.
Package compatibility keys are intended to:
- Enable tooling to identify incompatibilities between components, and
- Convey a level of compatibility between different releases to set end user expectations.
Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:
- M = Major - A difference in M indicates a break in compatibility. The package consumer is required to re-write its source code in order to use the package.
- S = Source - A difference in S indicates source compatibility. The package consumer’s source code doesn't require change, but does require a recompile.
- R = Radix - A difference in R indicates an introduction of new features, but compatibility with previous interfaces is not broken. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.
- P = Patch - A difference in P indicates that only bugs have been fixed in the latest package and no new features have been introduced. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.
back to top
Host Support
The current XDC toolset can be used to build components on the following hosts:
back to top
Device Support
This release supports the following device families:
back to top
Validation Information
This release was built and validated using the following components and tools:
Component Dependencies
- ti.mas.types 5.5.5 (Common data type definitions)
- ti.mas.swtools 5.0.4 (Internally used s/w tools)
- ti.mas.util 4.7.6 (Common utilities)
- ti.mas.fract 2.4.6 (Common Fractional utilities)
Component Test Dependencies
- ti.mas.sdk 3.3.9 (Signal Generators)
- CCS Version 5.2
Tool Dependencies for Source Release
- XDC Tools version 3.20.05.76
- RTSC Packaging Standard version 2.00.00
- C55x Code Generation Tools version 4.4.1
- C6x Code Generation Tools version 7.4.2
back to top
Known Issues
back to top
Versioning
This product's version follows a version format, M.m.p.b, where:
- M is a single digit Major number
- m is a single digit minor number
- p is a single digit patch number
- b is an unrestricted set of digits used as an incrementing build counter.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
back to top
Technical Support
Questions regarding VPE should be directed to the Texas Instruments BIOS E2E Forum. Please include the text "VoLIB" in the title.
back to top
Copyright 2013, Texas Instruments Incorporated