readme: Update readme with host linux details 01.01.00.00
authorSam Nelson <sam.nelson@ti.com>
Tue, 20 Jun 2017 15:53:29 +0000 (11:53 -0400)
committerSam Nelson <sam.nelson@ti.com>
Tue, 20 Jun 2017 15:53:29 +0000 (11:53 -0400)
Signed-off-by: Sam Nelson <sam.nelson@ti.com>
readme.txt

index b854d246fa687a7afc5d364cffa09ced230927a0..388987e54c1d7e7e8db360e45646f81b45838aad 100644 (file)
@@ -7,14 +7,18 @@ BigdataIPC examples
 These examples are created to show case how to share big data buffers
 between cores in a multicore system
 
 These examples are created to show case how to share big data buffers
 between cores in a multicore system
 
+host_liux: Examples here assume host running Linux
 host_bios: Examples here assume host running TI RTOS
 
 simple_buffer_example: This example demonstrates simple buffer exchange
        between cores
 
 host_bios: Examples here assume host running TI RTOS
 
 simple_buffer_example: This example demonstrates simple buffer exchange
        between cores
 
+Build procedure: host_bios
+===========================
+The examples are integrated into the top level make of the SDK for ease of use.
+
+But in case of building this example separately:
 
 
-Build procedure
-==============
 The following commandline can be used to build the example
 with the appropriate paths set from the top directory.
 
 The following commandline can be used to build the example
 with the appropriate paths set from the top directory.
 
@@ -32,3 +36,24 @@ or
 The corresponding example products.mak can be updated with the paths
 for the various components and the individual examples can be built
 separately.
 The corresponding example products.mak can be updated with the paths
 for the various components and the individual examples can be built
 separately.
+
+
+Build procedure: host_linux
+============================
+
+The examples are integrated into the top level make of the Linux SDK for ease of use.
+
+But in case of building this example separately:
+
+The following commandline can be used to build the example
+with the appropriate paths set from the top directory.
+
+PLATFORM=<platform_name> \
+XDC_INSTALL_DIR="<xdc_install_dir>" \
+BIOS_INSTALL_DIR="<bios_install_dir>" \
+IPC_INSTALL_DIR="<ipc_install_dir>" \
+TOOLCHAIN_PREFIX="<tool_chain_prefix>" \
+env gnu.targets.arm.A15F="<A15_tools_dir>" \
+env ti.targets.elf.C66="<c66_tools_dir>"\
+BOARD_NAME=<board_name> \
+make host_linux