1 /*
2 * GStreamer
3 * Copyright (c) 2010, Texas Instruments Incorporated
4 *
5 * This library is free software; you can redistribute it and/or
6 * modify it under the terms of the GNU Lesser General Public
7 * License as published by the Free Software Foundation
8 * version 2.1 of the License.
9 *
10 * This library is distributed in the hope that it will be useful,
11 * but WITHOUT ANY WARRANTY; without even the implied warranty of
12 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13 * Lesser General Public License for more details.
14 *
15 * You should have received a copy of the GNU Lesser General Public
16 * License along with this library; if not, write to the Free Software
17 * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA
18 */
20 #ifdef HAVE_CONFIG_H
21 # include <config.h>
22 #endif
24 #include "gstdsp66.h"
25 #include "gstdsp66videokernel.h"
27 GST_DEBUG_CATEGORY (gst_dsp66_debug);
29 static gboolean
30 plugin_init (GstPlugin * plugin)
31 {
32 GST_DEBUG_CATEGORY_INIT (gst_dsp66_debug, "dsp66", 0, "dsp66");
33 return (gst_element_register (plugin, "dsp66videokernel", GST_RANK_NONE, GST_TYPE_DSP66_VIDEO_KERNEL));
34 }
36 /* PACKAGE: this is usually set by autotools depending on some _INIT macro
37 * in configure.ac and then written into and defined in config.h, but we can
38 * just set it ourselves here in case someone doesn't use autotools to
39 * compile this code. GST_PLUGIN_DEFINE needs PACKAGE to be defined.
40 */
41 #ifndef PACKAGE
42 # define PACKAGE "dsp66"
43 #endif
45 GST_PLUGIN_DEFINE (GST_VERSION_MAJOR, GST_VERSION_MINOR, dsp66 ,
46 "DSP66 accelerated filters",
47 plugin_init, VERSION, "LGPL", "GStreamer", "http://gstreamer.net/")