index fb230d88e0b4667910b0cc03ee37a7ad5cb573e4..510c9bca90590f1f083d239cf57b9a100b2b62ed 100644 (file)
else # Platform not supported
$(error Dynamic libraries not supported on this platform. Run configure with --static flag.)
endif
+ XDEPENDS =
else
ifdef LIBNAME
LIBFILE = $(LIBNAME).a
$(AR) -cru $(LIBNAME).a $(OBJFILES)
$(RANLIB) $(LIBNAME).a
ifeq ($(KALDI_FLAVOR), dynamic)
-ifeq ($(shell uname), Darwin)
+ ifeq ($(shell uname), Darwin)
$(CXX) -dynamiclib -o $@ -install_name @rpath/$@ $(LDFLAGS) $(OBJFILES) $(LDLIBS)
rm -f $(KALDILIBDIR)/$@; ln -s $(shell pwd)/$@ $(KALDILIBDIR)/$@
-else ifeq ($(shell uname), Linux)
- # Building shared library from static (static was compiled with -fPIC)
+ else ifeq ($(shell uname), Linux)
+ # Building shared library from static (static was compiled with -fPIC)
$(CXX) -shared -o $@ -Wl,--no-undefined -Wl,--as-needed -Wl,-soname=$@,--whole-archive $(LIBNAME).a -Wl,--no-whole-archive $(LDFLAGS) $(LDLIBS)
rm -f $(KALDILIBDIR)/$@; ln -s $(shell pwd)/$@ $(KALDILIBDIR)/$@
-else # Platform not supported
+ else # Platform not supported
$(error Dynamic libraries not supported on this platform. Run configure with --static flag.)
-endif
+ endif
endif
# By default (GNU) make uses the C compiler $(CC) for linking object files even
# use the C++ compiler $(CXX) instead.
LINK.o = $(CXX) $(LDFLAGS) $(TARGET_ARCH)
-ifeq ($(KALDI_FLAVOR), dynamic)
-$(BINFILES): $(LIBFILE)
-else
$(BINFILES): $(LIBFILE) $(XDEPENDS)
+
+# When building under CI, CI_NOLINKBINARIES is set to skip linking of binaries.
+ifdef CI_NOLINKBINARIES
+$(BINFILES): %: %.o
+ touch $@
endif
# Rule below would expand to, e.g.:
# ../base/kaldi-base.a:
-# make -c ../base kaldi-base.a
-# -c option to make is same as changing directory.
+# make -C ../base kaldi-base.a
+# -C option to make is same as changing directory.
%.a:
$(MAKE) -C ${@D} ${@F}
distclean: clean
-rm -f .depend.mk
-ifeq ($(KALDI_FLAVOR), dynamic)
-$(TESTFILES): $(LIBFILE)
-else
$(TESTFILES): $(LIBFILE) $(XDEPENDS)
-endif
test_compile: $(TESTFILES)