index 09020ed0af2340d3d1c4a8ec47f5b30697e54e6c..2a9095a0471c7e0ad8b872147937a01aac8881ef 100644 (file)
// 2014-2015 Vijayaditya Peddinti
// 2014-2015 Guoguo Chen
// 2015 Daniel Galvez
+// 2015 Tom Ko
// See ../../COPYING for clarification regarding multiple authors
//
namespace kaldi {
namespace nnet3 {
-/// @file This file contains declarations of components that are "simple", meaning
+/// @file nnet-simple-component.h
+/// This file contains declarations of components that are "simple", meaning
/// they don't care about the indexes they are operating on, produce one
/// output for one input, and return the kSimpleComponent flag in their
/// Properties(): for example, tanh and affine components. In
virtual void InitFromConfig(ConfigLine *cfl);
virtual int32 InputDim() const { return input_dim_; }
virtual int32 OutputDim() const { return output_dim_; }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual Component* Copy() const { return new PnormComponent(input_dim_,
int32 output_dim_;
};
+// This component randomly zeros dropout_proportion of the input
+// and the derivatives are backpropagated through the nonzero inputs.
+// Typically this component used during training but not in test time.
+// The idea is described under the name Dropout, in the paper
+// "Dropout: A Simple Way to Prevent Neural Networks from Overfitting".
+class DropoutComponent : public RandomComponent {
+ public:
+ void Init(int32 dim, BaseFloat dropout_proportion = 0.0,
+ bool dropout_per_frame = false);
+
+ DropoutComponent(int32 dim, BaseFloat dropout = 0.0,
+ bool dropout_per_frame = false) {
+ Init(dim, dropout, dropout_per_frame);
+ }
+
+ DropoutComponent(): dim_(0), dropout_proportion_(0.0),
+ dropout_per_frame_(false) { }
+
+ virtual int32 Properties() const {
+ return kLinearInInput|kBackpropInPlace|kSimpleComponent|kBackpropNeedsInput|
+ kBackpropNeedsOutput|kRandomComponent;
+ }
+ virtual std::string Type() const { return "DropoutComponent"; }
+
+ virtual void InitFromConfig(ConfigLine *cfl);
+
+ virtual int32 InputDim() const { return dim_; }
+
+ virtual int32 OutputDim() const { return dim_; }
+
+ virtual void Read(std::istream &is, bool binary);
+
+ // Write component to stream
+ virtual void Write(std::ostream &os, bool binary) const;
+
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
+ virtual void Backprop(const std::string &debug_info,
+ const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
+ Component *to_update,
+ CuMatrixBase<BaseFloat> *in_deriv) const;
+ virtual Component* Copy() const { return new DropoutComponent(dim_,
+ dropout_proportion_,
+ dropout_per_frame_); }
+ virtual std::string Info() const;
+
+ void SetDropoutProportion(BaseFloat dropout_proportion) {
+ dropout_proportion_ = dropout_proportion;
+ }
+
+ BaseFloat DropoutProportion() const { return dropout_proportion_; }
+ private:
+ int32 dim_;
+ /// dropout-proportion is the proportion that is dropped out,
+ /// e.g. if 0.1, we set 10% to zero value.
+ BaseFloat dropout_proportion_;
+ bool dropout_per_frame_;
+};
+
class ElementwiseProductComponent: public Component {
public:
void Init(int32 input_dim, int32 output_dim);
virtual void InitFromConfig(ConfigLine *cfl);
virtual int32 InputDim() const { return input_dim_; }
virtual int32 OutputDim() const { return output_dim_; }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual Component* Copy() const { return new ElementwiseProductComponent(input_dim_,
Init(input_dim, target_rms, add_log_stddev);
}
explicit NormalizeComponent(const NormalizeComponent &other);
+ // note: there is some special code in NonlinerComponent::Info() that
+ // specifically caters to this class.
virtual int32 Properties() const {
return (add_log_stddev_ ?
kSimpleComponent|kBackpropNeedsInput|kBackpropAdds :
virtual std::string Type() const { return "NormalizeComponent"; }
virtual void InitFromConfig(ConfigLine *cfl);
virtual Component* Copy() const { return new NormalizeComponent(*this); }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
};
+/*
+ Implements the sigmoid nonlinearity, i.e. the function y = exp(-x).
+
+ Configuration values accepted:
+ dim Dimension of this component, e.g. 1024
+
+ Configuration values inherited from NonlinearComponent, and their
+ local meanings:
+ self-repair-lower-threshold e.g. self-repair-lower-threshold=0.05. This
+ controls the self-repair mechanism, which for sigmoid units
+ consists of identifying units which are oversaturated (i.e.
+ usually close to -1 or +1) and nudging the inputs to be
+ closer to zero. It gates on the average derivative of the
+ nonlinearity, which for sigmoid is a value between 0 and
+ 0.25. For units where the average function-derivative
+ accumulated during this iteration (job) of training is less
+ than this threshold, we activate self-repair, which consists
+ of adding (-self-repair-scale * (2*the output of the
+ nonlinearity - 1.0)) to the backpropagated derivatives.
+ This just happens to be a convenient-to-compute function
+ that's +1 for large negative inputs, and -1 for large positive
+ inputs, and smooth in between.
+ The default value of this is -1000, which the code internally
+ maps to 0.05 which is suitable for sigmoid units; if you do set it,
+ you can set it to a value like 0.025 or 0.075.
+ self-repair-scale Scale for the self-repair mechanism; see comments above.
+ default=0, but we usually set this to 1.0e-05 (or
+ occasionally 1.0e-04) in the scripts.
+
+ */
class SigmoidComponent: public NonlinearComponent {
public:
- explicit SigmoidComponent(int32 dim): NonlinearComponent(dim) { }
explicit SigmoidComponent(const SigmoidComponent &other): NonlinearComponent(other) { }
SigmoidComponent() { }
virtual std::string Type() const { return "SigmoidComponent"; }
return kSimpleComponent|kBackpropNeedsOutput|kPropagateInPlace|kStoresStats;
}
virtual Component* Copy() const { return new SigmoidComponent(*this); }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &, //in_value
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
- virtual void StoreStats(const CuMatrixBase<BaseFloat> &out_value);
+ virtual void StoreStats(const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ void *memo);
private:
+ // this function is called from Backprop code and only does something if the
+ // self-repair-scale config value is set.
+ void RepairGradients(const CuMatrixBase<BaseFloat> &out_value,
+ CuMatrixBase<BaseFloat> *in_deriv,
+ SigmoidComponent *to_update) const;
+
SigmoidComponent &operator = (const SigmoidComponent &other); // Disallow.
};
+/*
+ Implements the tanh nonlinearity, i.e. the function y = tanh(x).
+
+ Configuration values accepted:
+ dim Dimension of this component, e.g. 1024
+
+ Configuration values inherited from NonlinearComponent, and their
+ local meanings:
+ self-repair-lower-threshold e.g. self-repair-lower-threshold=0.2. This
+ controls the self-repair mechanism, which for tanh units
+ consists of identifying units which are oversaturated (i.e.
+ usually close to -1 or +1) and nudging the inputs to be
+ closer to zero. It gates on the average derivative of
+ the nonlinearity, which for tanh is a value between 0 and 1.
+ For units where the average function-derivative accumulated
+ during this iteration (job) of training is less than
+ this threshold, we activate self-repair, which consists of
+ adding (-self-repair-scale * the output of the nonlinearity),
+ i.e. (-self-repair-scale * tanh(x)) to the backpropagated
+ derivatives.
+ The default value of this is -1000, which the code internally
+ maps to 0.2 which is suitable for tanh units; if you do set it,
+ you can set it to a value like 0.1 or 0.3.
+ self-repair-scale Scale for the self-repair mechanism; see comments above.
+ default=0, but we usually set this to 1.0e-05 (or
+ occasionally 1.0e-04) in the scripts.
+ */
class TanhComponent: public NonlinearComponent {
public:
- explicit TanhComponent(int32 dim): NonlinearComponent(dim) { }
explicit TanhComponent(const TanhComponent &other): NonlinearComponent(other) { }
TanhComponent() { }
virtual std::string Type() const { return "TanhComponent"; }
virtual int32 Properties() const {
return kSimpleComponent|kBackpropNeedsOutput|kPropagateInPlace|kStoresStats;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, //in_value
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
- virtual void StoreStats(const CuMatrixBase<BaseFloat> &out_value);
+ virtual void StoreStats(const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ void *memo);
private:
+ // this function is called from Backprop code and only does something if the
+ // self-repair-scale config value is set.
+ void RepairGradients(const CuMatrixBase<BaseFloat> &out_value,
+ CuMatrixBase<BaseFloat> *in_deriv,
+ TanhComponent *to_update) const;
+
TanhComponent &operator = (const TanhComponent &other); // Disallow.
};
+/*
+ Implements the Rectified Linear Unit nonlinearity, a.k.a. ReLU.
+
+ Configuration values accepted:
+ dim Dimension of this component, e.g. 1024
+
+ Configuration values inherited from NonlinearComponent, and their
+ local meanings:
+ self-repair-lower-threshold e.g. self-repair-lower-threshold=0.05. (Lower
+ threshold for self-repair, if set; in this case acts on
+ the average function-derivative, which is the proportion
+ of the time the output is > 0. For any unit where the
+ average function-derivative is lower than this threshold,
+ we add 'self-repair-scale' to the backpropagated
+ derivatives in backprop. There is no default
+ (default=-1000, which is interpreted specially).
+ self-repair-upper-threshold e.g. self-repair-upper-threshold=0.95.
+ Like self-repair-lower-threshold, but controls self-repair
+ for units that are active *too* much of the time. Units
+ whose average function-derivative exceeds this threshold
+ will have the negative of 'self-repair-scale' added to their
+ input derivatives in backprop. There is no default
+ (default=-1000, which is interpreted specially).
+ self-repair-scale Scale for the self-repair mechanism; see comments for
+ self-repair-lower-threshold and self-repair-upper-threshold
+ for details. default=0, but we usually set this to 1.0e-05
+ (or occasionally 1.0e-04) in the scripts.
+ */
class RectifiedLinearComponent: public NonlinearComponent {
public:
- explicit RectifiedLinearComponent(int32 dim): NonlinearComponent(dim) { }
- explicit RectifiedLinearComponent(const RectifiedLinearComponent &other): NonlinearComponent(other) { }
+ explicit RectifiedLinearComponent(const RectifiedLinearComponent &other):
+ NonlinearComponent(other) { }
RectifiedLinearComponent() { }
virtual std::string Type() const { return "RectifiedLinearComponent"; }
virtual Component* Copy() const { return new RectifiedLinearComponent(*this); }
return kSimpleComponent|kLinearInInput|kBackpropNeedsOutput|kPropagateInPlace|
kStoresStats;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, //in_value
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
- virtual void StoreStats(const CuMatrixBase<BaseFloat> &out_value);
+ virtual void StoreStats(const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ void *memo);
private:
- RectifiedLinearComponent &operator = (const RectifiedLinearComponent &other); // Disallow.
-};
-
-/**
- This component is a fixed (non-trainable) nonlinearity that sums its inputs
- to produce outputs. Currently the only supported configuration is that its
- input-dim is interpreted as consisting of n blocks, and the output is just a
- summation over the n blocks, where n = input-dim / output-dim, so for instance
- output[n] = input[n] + input[block-size + n] + .... .
- Later if needed we can add a configuration variable that allows you to sum
- over 'interleaved' input.
- */
-class SumReduceComponent: public Component {
- public:
- void Init(int32 input_dim, int32 output_dim);
- explicit SumReduceComponent(int32 input_dim, int32 output_dim) {
- Init(input_dim, output_dim);
- }
- virtual int32 Properties() const {
- return kSimpleComponent|kLinearInInput;
- }
- SumReduceComponent(): input_dim_(0), output_dim_(0) { }
- virtual std::string Type() const { return "SumReduceComponent"; }
- virtual void InitFromConfig(ConfigLine *cfl);
- virtual int32 InputDim() const { return input_dim_; }
- virtual int32 OutputDim() const { return output_dim_; }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
- virtual void Backprop(const std::string &debug_info,
- const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &, // in_value
- const CuMatrixBase<BaseFloat> &, // out_value,
- const CuMatrixBase<BaseFloat> &out_deriv,
- Component *, // to_update
- CuMatrixBase<BaseFloat> *in_deriv) const;
- virtual Component* Copy() const { return new SumReduceComponent(input_dim_,
- output_dim_); }
+ // this function is called from Backprop code and only does something if the
+ // self-repair-scale config value is set.
+ void RepairGradients(CuMatrixBase<BaseFloat> *in_deriv,
+ RectifiedLinearComponent *to_update) const;
- virtual void Read(std::istream &is, bool binary); // This Read function
- // requires that the Component has the correct type.
-
- /// Write component to stream
- virtual void Write(std::ostream &os, bool binary) const;
-
- protected:
- int32 input_dim_;
- int32 output_dim_;
+ RectifiedLinearComponent &operator = (const RectifiedLinearComponent &other); // Disallow.
};
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
// Some functions that are specific to this class.
- // This new function is used when mixing up:
- virtual void SetParams(const VectorBase<BaseFloat> &bias,
- const MatrixBase<BaseFloat> &linear);
- const CuVector<BaseFloat> &BiasParams() { return bias_params_; }
- const CuMatrix<BaseFloat> &LinearParams() { return linear_params_; }
+ virtual void SetParams(const CuVectorBase<BaseFloat> &bias,
+ const CuMatrixBase<BaseFloat> &linear);
+ const CuVector<BaseFloat> &BiasParams() const { return bias_params_; }
+ const CuMatrix<BaseFloat> &LinearParams() const { return linear_params_; }
explicit AffineComponent(const AffineComponent &other);
// The next constructor is used in converting from nnet1.
AffineComponent(const CuMatrixBase<BaseFloat> &linear_params,
// parameters to zero, while leaving any other configuration values the same.
virtual void Resize(int32 input_dim, int32 output_dim);
- // The following functions are used for collapsing multiple layers
- // together. They return a pointer to a new Component equivalent to
- // the sequence of two components. We haven't implemented this for
- // FixedLinearComponent yet.
- Component *CollapseWithNext(const AffineComponent &next) const ;
- Component *CollapseWithNext(const FixedAffineComponent &next) const;
- Component *CollapseWithNext(const FixedScaleComponent &next) const;
- Component *CollapseWithPrevious(const FixedAffineComponent &prev) const;
-
protected:
friend class NaturalGradientAffineComponent;
// This function Update() is for extensibility; child classes may override
kBackpropNeedsInput|kBackpropAdds;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
return kSimpleComponent|kUpdatableComponent|kLinearInParameters|
kBackpropNeedsInput|kBackpropAdds|kInputContiguous|kOutputContiguous;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
virtual void UnVectorize(const VectorBase<BaseFloat> ¶ms);
// Some functions that are specific to this class.
- const CuVector<BaseFloat> &BiasParams() { return bias_params_; }
- const CuMatrix<BaseFloat> &LinearParams() { return linear_params_; }
+ const CuVector<BaseFloat> &BiasParams() const { return bias_params_; }
+ const CuMatrix<BaseFloat> &LinearParams() const { return linear_params_; }
explicit RepeatedAffineComponent(const RepeatedAffineComponent &other);
void Init(int32 input_dim, int32 output_dim, int32 num_repeats,
class SoftmaxComponent: public NonlinearComponent {
public:
- explicit SoftmaxComponent(int32 dim): NonlinearComponent(dim) { }
explicit SoftmaxComponent(const SoftmaxComponent &other):
NonlinearComponent(other) { }
SoftmaxComponent() { }
virtual int32 Properties() const {
return kSimpleComponent|kBackpropNeedsOutput|kStoresStats;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
- virtual void StoreStats(const CuMatrixBase<BaseFloat> &out_value);
-
+ virtual void StoreStats(const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ void *memo);
virtual Component* Copy() const { return new SoftmaxComponent(*this); }
private:
SoftmaxComponent &operator = (const SoftmaxComponent &other); // Disallow.
};
+
+/*
+ Implements the log of a softmax nonlinearity, so it's the same
+ as shifting each input vector by a constant offset so that, when
+ exponentiated, it would sum to one.
+
+ We usually use this in place of softmax because the log-scale
+ output will not saturate.
+
+ Configuration values accepted:
+ dim e.g. dim=8061. Usually this is the last component
+ in a network, so 'dim' is the number of classes.
+ */
class LogSoftmaxComponent: public NonlinearComponent {
public:
- explicit LogSoftmaxComponent(int32 dim): NonlinearComponent(dim) { }
explicit LogSoftmaxComponent(const LogSoftmaxComponent &other):
NonlinearComponent(other) { }
LogSoftmaxComponent() { }
virtual int32 Properties() const {
return kSimpleComponent|kBackpropNeedsOutput|kStoresStats;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
LogSoftmaxComponent &operator = (const LogSoftmaxComponent &other); // Disallow.
};
-/// Keywords: natural gradient descent, NG-SGD, naturalgradient. For
-/// the top-level of the natural gradient code look here, and also in
-/// nnet-precondition-online.h.
-/// NaturalGradientAffineComponent is
-/// a version of AffineComponent that has a non-(multiple of unit) learning-rate
-/// matrix. See nnet-precondition-online.h for a description of the technique.
-/// It is described, under the name Online NG-SGD, in the paper "Parallel
-/// training of DNNs with Natural Gradient and Parameter Averaging" (ICLR
-/// workshop, 2015) by Daniel Povey, Xiaohui Zhang and Sanjeev Khudanpur.
+/*
+ Keywords: natural gradient descent, NG-SGD, naturalgradient. For
+ the top-level of the natural gradient code look here, and also in
+ nnet-precondition-online.h.
+ NaturalGradientAffineComponent is
+ a version of AffineComponent that has a non-(multiple of unit) learning-rate
+ matrix. See nnet-precondition-online.h for a description of the technique.
+ It is described, under the name Online NG-SGD, in the paper "Parallel
+ training of DNNs with Natural Gradient and Parameter Averaging" (ICLR
+ workshop, 2015) by Daniel Povey, Xiaohui Zhang and Sanjeev Khudanpur.
+
+ Configuration values accepted by this component:
+
+ Values inherited from UpdatableComponent (see its declaration in
+ nnet-component-itf for details):
+ learning-rate
+ learning-rate-factor
+ max-change
+
+ Values used in initializing the component's parameters:
+ input-dim e.g. input-dim=1024. The input dimension.
+ output-dim e.g. output-dim=1024. The output dimension.
+ param-stddev e.g. param-stddev=0.025. The standard deviation
+ used to randomly initialize the linear parameters
+ (as Gaussian random values * param-stddev).
+ Defaults to 1/sqrt(input-dim), which is Glorot
+ initialization.
+ bias-stddev e.g. bias-stddev=0.0. The standard deviation
+ used to randomly initialize the bias parameters.
+ Defaults to 1.0 but we usually set it to 0.0
+ in the config.
+ bias-mean e.g. bias-mean=1.0. Allows you to ininialize the
+ bias parameters with an offset. Default is 0.0
+ which is normally suitable
+
+ matrix e.g. matrix=foo/bar/init.mat May be used as an
+ alternative to (input-dim, output-dim, param-stddev,
+ bias-stddev, bias-mean) to initialize the parameters.
+ Dimension is output-dim by (input-dim + 1), last
+ column is interpreted as the bias.
+
+ Options to the natural gradient (you won't normally have to set these,
+ the defaults are suitable):
+
+ num-samples-history Number of frames used as the time-constant to
+ determine how 'up-to-date' the Fisher-matrix
+ estimates are. Smaller -> more up-to-date, but more
+ noisy. default=2000.
+ alpha Constant that determines how much we smooth the
+ Fisher-matrix estimates with the unit matrix.
+ Larger means more smoothing. default=4.0
+ rank-in Rank used in low-rank-plus-unit estimate of Fisher
+ matrix in the input space. default=20.
+ rank-out Rank used in low-rank-plus-unit estimate of Fisher
+ matrix in the output-derivative space. default=80.
+ update-period Determines after with what frequency (in
+ minibatches) we update the Fisher-matrix estimates;
+ making this > 1 saves a little time in training.
+ default=4.
+*/
class NaturalGradientAffineComponent: public AffineComponent {
public:
virtual std::string Type() const { return "NaturalGradientAffineComponent"; }
void Init(int32 input_dim, int32 output_dim,
BaseFloat param_stddev, BaseFloat bias_stddev, BaseFloat bias_mean,
int32 rank_in, int32 rank_out, int32 update_period,
- BaseFloat num_samples_history, BaseFloat alpha,
- BaseFloat max_change_per_sample);
+ BaseFloat num_samples_history, BaseFloat alpha);
void Init(int32 rank_in, int32 rank_out, int32 update_period,
BaseFloat num_samples_history,
- BaseFloat alpha, BaseFloat max_change_per_sample,
- std::string matrix_filename);
+ BaseFloat alpha, std::string matrix_filename);
// this constructor does not really initialize, use Init() or Read().
NaturalGradientAffineComponent();
- virtual void Resize(int32 input_dim, int32 output_dim);
- virtual void InitFromConfig(ConfigLine *cfl);
+ void Resize(int32 input_dim, int32 output_dim);
+ void InitFromConfig(ConfigLine *cfl);
virtual std::string Info() const;
virtual Component* Copy() const;
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
+ virtual void FreezeNaturalGradient(bool freeze);
// copy constructor
explicit NaturalGradientAffineComponent(
const NaturalGradientAffineComponent &other);
- virtual void ZeroStats();
-
private:
// disallow assignment operator.
NaturalGradientAffineComponent &operator= (
OnlineNaturalGradient preconditioner_out_;
- // If > 0, max_change_per_sample_ is the maximum amount of parameter
- // change (in L2 norm) that we allow per sample, averaged over the minibatch.
- // This was introduced in order to control instability.
- // Instead of the exact L2 parameter change, for
- // efficiency purposes we limit a bound on the exact
- // change. The limit is applied via a constant <= 1.0
- // for each minibatch, A suitable value might be, for
- // example, 10 or so; larger if there are more
- // parameters.
- BaseFloat max_change_per_sample_;
-
- // update_count_ records how many updates we have done.
- double update_count_;
-
- // active_scaling_count_ records how many updates we have done,
- // where the scaling factor is active (not 1.0).
- double active_scaling_count_;
-
- // max_change_scale_stats_ records the sum of scaling factors
- // in each update, so we can compute the averaged scaling factor
- // in Info().
- double max_change_scale_stats_;
-
// Sets the configs rank, alpha and eta in the preconditioner objects,
// from the class variables.
void SetNaturalGradientConfigs();
virtual std::string Type() const { return "FixedAffineComponent"; }
virtual std::string Info() const;
+ // Copy constructor from AffineComponent-- can be used when we're done
+ // training a particular part of the model and want to efficiently disable
+ // further training.
+ FixedAffineComponent(const AffineComponent &c);
+
/// matrix should be of size input-dim+1 to output-dim, last col is offset
void Init(const CuMatrixBase<BaseFloat> &matrix);
virtual int32 InputDim() const { return linear_params_.NumCols(); }
virtual int32 OutputDim() const { return linear_params_.NumRows(); }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual void Read(std::istream &is, bool binary);
virtual void Write(std::ostream &os, bool binary) const;
- // Function to provide access to linear_params_.
const CuMatrix<BaseFloat> &LinearParams() const { return linear_params_; }
+ const CuVector<BaseFloat> &BiasParams() const { return bias_params_; }
protected:
friend class AffineComponent;
CuMatrix<BaseFloat> linear_params_;
SumGroupComponent() { }
virtual std::string Type() const { return "SumGroupComponent"; }
virtual int32 Properties() const { return kSimpleComponent|kLinearInInput; }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual Component* Copy() const;
virtual int32 InputDim() const { return scales_.Dim(); }
virtual int32 OutputDim() const { return scales_.Dim(); }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, // in_value
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *, // to_update
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual Component* Copy() const;
virtual void Read(std::istream &is, bool binary);
virtual void Write(std::ostream &os, bool binary) const;
+ const CuVector<BaseFloat> &Scales() const { return scales_; }
protected:
- friend class AffineComponent; // necessary for collapse
CuVector<BaseFloat> scales_;
KALDI_DISALLOW_COPY_AND_ASSIGN(FixedScaleComponent);
};
virtual int32 InputDim() const { return bias_.Dim(); }
virtual int32 OutputDim() const { return bias_.Dim(); }
using Component::Propagate; // to avoid name hiding
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, // in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *, // to_update
CuMatrixBase<BaseFloat> *in_deriv) const;
virtual Component* Copy() const;
KALDI_DISALLOW_COPY_AND_ASSIGN(FixedBiasComponent);
};
-// NoOpComponent just duplicates its input. We don't anticipate this being used
-// very often, but it may sometimes make your life easier
+/** NoOpComponent just duplicates its input. We don't anticipate this being used
+ very often, but it may sometimes make your life easier
+ The only config parameter it accepts is 'dim', e.g. 'dim=400'.
+*/
class NoOpComponent: public NonlinearComponent {
public:
- explicit NoOpComponent(int32 dim): NonlinearComponent(dim) { }
explicit NoOpComponent(const NoOpComponent &other): NonlinearComponent(other) { }
NoOpComponent() { }
virtual std::string Type() const { return "NoOpComponent"; }
return kSimpleComponent|kLinearInInput|kPropagateInPlace;
}
virtual Component* Copy() const { return new NoOpComponent(*this); }
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &in,
- CuMatrixBase<BaseFloat> *out) const;
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &, //in_value
const CuMatrixBase<BaseFloat> &, // out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
private:
NoOpComponent &operator = (const NoOpComponent &other); // Disallow.
};
+/** SumBlockComponent sums over blocks of its input: for instance, if
+ you create one with the config "input-dim=400 output-dim=100",
+ its output will be the sum over the 4 100-dimensional blocks of
+ the input.
+
+ The "scale" config parameter may be used if you want to do averaging
+ instead of summing, e.g. "input-dim=400 output-dim=100 scale=0.25"
+ will accomplish averaging.
+
+ Accepted values on its config-file line are:
+ input-dim The input dimension. Required.
+ output-dim The block dimension. Required. Must divide input-dim.
+ scale A scaling factor on the output. Defaults to 1.0.
+ */
+class SumBlockComponent: public Component {
+ public:
+ explicit SumBlockComponent(const SumBlockComponent &other);
+ SumBlockComponent() { }
+ virtual std::string Type() const { return "SumBlockComponent"; }
+ virtual int32 Properties() const {
+ return kSimpleComponent|kLinearInInput|kPropagateAdds|kBackpropAdds;
+ }
+ virtual void InitFromConfig(ConfigLine *cfl);
+ virtual int32 InputDim() const { return input_dim_; }
+ virtual int32 OutputDim() const { return output_dim_; }
+ virtual void Read(std::istream &is, bool binary);
+ virtual void Write(std::ostream &os, bool binary) const;
+ virtual std::string Info() const;
+ virtual Component* Copy() const { return new SumBlockComponent(*this); }
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
+ virtual void Backprop(const std::string &debug_info,
+ const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &, //in_value
+ const CuMatrixBase<BaseFloat> &, // out_value,
+ const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
+ Component *to_update,
+ CuMatrixBase<BaseFloat> *in_deriv) const;
+ private:
+ int32 input_dim_;
+ int32 output_dim_;
+ BaseFloat scale_;
+ SumBlockComponent &operator = (const SumBlockComponent &other); // Disallow.
+};
+
+
// ClipGradientComponent just duplicates its input, but clips gradients
// during backpropagation if they cross a predetermined threshold.
// This component will be used to prevent gradient explosion problem in
class ClipGradientComponent: public Component {
public:
ClipGradientComponent(int32 dim, BaseFloat clipping_threshold,
- bool norm_based_clipping, int32 num_clipped,
- int32 count) {
- Init(dim, clipping_threshold, norm_based_clipping, num_clipped, count);}
+ bool norm_based_clipping,
+ BaseFloat self_repair_clipped_proportion_threshold,
+ BaseFloat self_repair_target,
+ BaseFloat self_repair_scale,
+ int32 num_clipped,
+ int32 count,
+ int32 num_self_repaired,
+ int32 num_backpropped) {
+ Init(dim, clipping_threshold, norm_based_clipping,
+ self_repair_clipped_proportion_threshold,
+ self_repair_target,
+ self_repair_scale,
+ num_clipped, count,
+ num_self_repaired, num_backpropped);}
ClipGradientComponent(): dim_(0), clipping_threshold_(-1),
- norm_based_clipping_(false), num_clipped_(0), count_(0) { }
+ norm_based_clipping_(false),
+ self_repair_clipped_proportion_threshold_(1.0),
+ self_repair_target_(0.0),
+ self_repair_scale_(0.0),
+ num_clipped_(0), count_(0),
+ num_self_repaired_(0), num_backpropped_(0) { }
virtual int32 InputDim() const { return dim_; }
virtual int32 OutputDim() const { return dim_; }
virtual void InitFromConfig(ConfigLine *cfl);
void Init(int32 dim, BaseFloat clipping_threshold, bool norm_based_clipping,
- int32 num_clipped, int32 count);
+ BaseFloat self_repair_clipped_proportion_threshold,
+ BaseFloat self_repair_target,
+ BaseFloat self_repair_scale,
+ int32 num_clipped, int32 count,
+ int32 num_self_repaired, int32 num_backpropped);
virtual std::string Type() const { return "ClipGradientComponent"; }
virtual int32 Properties() const {
- return kSimpleComponent|kLinearInInput|kPropagateInPlace|kBackpropInPlace;
+ return kSimpleComponent|kLinearInInput|kPropagateInPlace|kBackpropInPlace|
+ kBackpropNeedsInput;
}
virtual void ZeroStats();
return new ClipGradientComponent(dim_,
clipping_threshold_,
norm_based_clipping_,
+ self_repair_clipped_proportion_threshold_,
+ self_repair_target_,
+ self_repair_scale_,
num_clipped_,
- count_);}
+ count_,
+ num_self_repaired_,
+ num_backpropped_);}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const ComponentPrecomputedIndexes *indexes,
- const CuMatrixBase<BaseFloat> &, //in_value
+ const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
/// Write component to stream
virtual void Write(std::ostream &os, bool binary) const;
virtual std::string Info() const;
+ virtual ~ClipGradientComponent() {
+ if (num_self_repaired_ > 0)
+ KALDI_LOG << "ClipGradientComponent(node_name=" << debug_info_
+ << ")'s self-repair was activated " << num_self_repaired_
+ << " time(s) out of " << num_backpropped_
+ << " times of calling Backprop() in this training job.";
+ }
private:
int32 dim_; // input/output dimension
BaseFloat clipping_threshold_; // threshold to be used for clipping
// else element-wise absolute value clipping is
// done
+ // some configuration values relating to self-repairing.
+ BaseFloat self_repair_clipped_proportion_threshold_; // the threshold of
+ // clipped-proportion
+ // for self-repair to be
+ // activated
+ BaseFloat self_repair_target_; // the target value towards which self-repair
+ // is trying to set for in-deriv
+ BaseFloat self_repair_scale_; // constant scaling the self-repair vector
+ std::string debug_info_; // component-node name, used in the destructor to
+ // print out stats of self-repair
+
+ // this function is called from Backprop code, and only does something if the
+ // self-repair-scale config value is set and the current clipped proportion
+ // exceeds the threshold. What it does is to add a term to in-deriv that
+ // forces the input to the ClipGradientComponent to be close to some small
+ // value (e.g., 0.0 or 0.5, depending on what the input is, e.g.,
+ // Sigmoid or Tanh or Affine). The hope is that if the input is forced to be
+ // small, the parameters on the path will also tend to be small, which may
+ // help tamp down the divergence caused by gradient explosion.
+ void RepairGradients(const std::string &debug_info,
+ const CuMatrixBase<BaseFloat> &in_value,
+ CuMatrixBase<BaseFloat> *in_deriv,
+ ClipGradientComponent *to_update) const;
ClipGradientComponent &operator =
(const ClipGradientComponent &other); // Disallow.
// Note: no stats are stored when norm_based_clipping_ is false
int32 num_clipped_; // number of elements which were clipped
int32 count_; // number of elements which were processed
+ int32 num_self_repaired_; // number of times self-repair is activated
+ int32 num_backpropped_; //number of times backprop is called
};
virtual Component* Copy() const;
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, //in_value
const CuMatrixBase<BaseFloat> &, // out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
kLinearInParameters|kBackpropNeedsInput|kPropagateInPlace;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
void Init(std::string vector_filename);
protected:
- friend class AffineComponent; // necessary for collapse
// This function Update() is for extensibility; child classes may override
// this, e.g. for natural gradient update.
virtual void Update(
CuVector<BaseFloat> scales_;
};
+/*
+ PerElementOffsetComponent offsets each dimension of its input with a separate
+ trainable bias; it's like an affine component with fixed weight matrix which
+ is always equal to I.
+
+ Accepted values on its config line, with defaults if applicable.
+
+ vector If specified, the offsets will be read from this file ('vector'
+ is interpreted as an rxfilename).
+
+ dim If 'vector' is not specified, you should specify the
+ dimension 'dim', and will be randomly initialized according
+ to 'param-mean' and 'param-stddev'.
+ param-mean=0.0 Mean of randomly initialized offset parameters.
+ param-stddev=0.0 Standard deviation of randomly initialized offset parameters.
-// PerElementOffsetComponent offsets each dimension of its input with a separate
-// trainable bias; it's like an affine component with fixed weight matrix which is always equal to I.
+*/
class PerElementOffsetComponent: public UpdatableComponent {
public:
virtual int32 InputDim() const { return offsets_.Dim(); }
kBackpropInPlace|kPropagateInPlace;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, // in_value
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
// i.e. its output does not depend on its input. It is the same as
// an affine component with the linear term fixed at zero.
// It is optionally trainable, and optionally you can use natural
-// gradient. The input is required only because the framework
-// requires components to have an input.
+// gradient. The input is required only because it's more convenient
+// to make SimpleComponents [but see ConstantComponent, which requires
+// no inputs].
class ConstantFunctionComponent: public UpdatableComponent {
public:
virtual int32 InputDim() const { return input_dim_; }
virtual int32 Properties() const {
return kSimpleComponent|
(is_updatable_ ? kUpdatableComponent|kLinearInParameters : 0) |
- (InputDim() == OutputDim() ? kPropagateInPlace|kBackpropInPlace: 0) |
+ (InputDim() == OutputDim() ? kPropagateInPlace: 0) |
kBackpropAdds;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &, // in_value
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
@@ -1273,6 +1568,7 @@ class NaturalGradientPerElementScaleComponent: public PerElementScaleComponent {
virtual void Read(std::istream &is, bool binary);
virtual void Write(std::ostream &os, bool binary) const;
+ virtual void FreezeNaturalGradient(bool freeze);
virtual Component* Copy() const;
@@ -1282,16 +1578,12 @@ class NaturalGradientPerElementScaleComponent: public PerElementScaleComponent {
void Init(int32 dim, BaseFloat param_mean,
BaseFloat param_stddev, int32 rank, int32 update_period,
- BaseFloat num_samples_history, BaseFloat alpha,
- BaseFloat max_change_per_minibatch);
+ BaseFloat num_samples_history, BaseFloat alpha);
void Init(std::string vector_filename,
int32 rank, int32 update_period, BaseFloat num_samples_history,
- BaseFloat alpha, BaseFloat max_change_per_minibatch);
+ BaseFloat alpha);
private:
- // configuration value for imposing max-change...
- BaseFloat max_change_per_minibatch_;
-
// unlike the NaturalGradientAffineComponent, there is only one dimension to
// consider as the parameters are a vector not a matrix, so we only need one
// preconditioner.
@@ -1312,6 +1604,8 @@ class NaturalGradientPerElementScaleComponent: public PerElementScaleComponent {
};
/**
+ * WARNING, this component is deprecated in favor of
+ * TimeHeightConvolutionComponent, and will be deleted.
* ConvolutionalComponent implements 2d-convolution.
* It uses 3D filters on 3D inputs, but the 3D filters hop only over
* 2 dimensions as it has same size as the input along the 3rd dimension.
virtual std::string Type() const { return "ConvolutionComponent"; }
virtual int32 Properties() const {
return kSimpleComponent|kUpdatableComponent|kBackpropNeedsInput|
- kBackpropAdds|kPropagateAdds;
+ kBackpropAdds|kPropagateAdds;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update_in,
CuMatrixBase<BaseFloat> *in_deriv) const;
void Update(const std::string &debug_info,
const std::vector<CuSubMatrix<BaseFloat> *>& out_deriv_batch);
-
virtual void Read(std::istream &is, bool binary);
virtual void Write(std::ostream &os, bool binary) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
// Some functions that are specific to this class.
void SetParams(const VectorBase<BaseFloat> &bias,
const MatrixBase<BaseFloat> &filter);
- const CuVector<BaseFloat> &BiasParams() { return bias_params_; }
- const CuMatrix<BaseFloat> &LinearParams() { return filter_params_; }
+ const CuVector<BaseFloat> &BiasParams() const { return bias_params_; }
+ const CuMatrix<BaseFloat> &LinearParams() const { return filter_params_; }
void Init(int32 input_x_dim, int32 input_y_dim, int32 input_z_dim,
int32 filt_x_dim, int32 filt_y_dim,
int32 filt_x_step, int32 filt_y_step, int32 num_filters,
void Resize(int32 input_dim, int32 output_dim);
void Update(const std::string &debug_info,
- const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_deriv);
const ConvolutionComponent &operator = (const ConvolutionComponent &other); // Disallow.
};
-/**
- * Convolutional1dComponent implements convolution over frequency axis.
- * We assume the input featrues are spliced, i.e. each frame is in
- * fact a set of stacked frames, where we can form patches which span
- * over several frequency bands and whole time axis. A patch is the
- * instance of a filter on a group of frequency bands and whole time
- * axis. Shifts of the filter generate patches.
- *
- * The convolution is done over whole axis with same filter
- * coefficients, i.e. we don't use separate filters for different
- * 'regions' of frequency axis. Due to convolution, same weights are
- * used repeateadly, the final gradient is a sum of all
- * position-specific gradients (the sum was found better than
- * averaging).
- *
- * In order to have a fast implementations, the filters are
- * represented in vectorized form, where each rectangular filter
- * corresponds to a row in a matrix, where all the filters are
- * stored. The features are then re-shaped to a set of matrices, where
- * one matrix corresponds to single patch-position, where all the
- * filters get applied.
- *
- * The type of convolution is controled by hyperparameters:
- * patch_dim_ ... frequency axis size of the patch
- * patch_step_ ... size of shift in the convolution
- * patch_stride_ ... shift for 2nd dim of a patch
- * (i.e. frame length before splicing)
- * For instance, for a convolutional component after raw input,
- * if the input is 36-dim fbank feature with delta of order 2
- * and spliced using +/- 5 frames of contexts, the convolutional
- * component takes the input as a 36 x 33 image. The patch_stride_
- * should be configured 36. If patch_step_ and patch_dim_ are
- * configured 1 and 7, the Convolutional1dComponent creates a
- * 2D filter of 7 x 33, such that the convolution is actually done
- * only along the frequency axis. Specifically, the convolutional
- * output along the frequency axis is (36 - 7) / 1 + 1 = 30, and
- * the convolutional output along the temporal axis is 33 - 33 + 1 = 1,
- * resulting in an output image of 30 x 1, which is called a feature map
- * in ConvNet. Then if the output-dim is set 3840, the constructor
- * would know there should be 3840 / 30 = 128 distinct filters,
- * which will create 128 feature maps of 30 x 1 for one frame of
- * input. The feature maps are vectorized as a 3840-dim row vector
- * in the output matrix of this component. For details on progatation
- * of Convolutional1dComponent, check the function definition.
- *
- */
-class Convolutional1dComponent: public UpdatableComponent {
+
+/*
+ LstmNonlinearityComponent is a component that implements part of an LSTM, by
+ combining together the sigmoids and tanh's, plus some diagonal terms, into
+ a single block.
+ We will refer to the LSTM formulation used in
+
+ Long Short-Term Memory Recurrent Neural Network Architectures for Large Scale Acoustic Modeling"
+ by H. Sak et al,
+ http://static.googleusercontent.com/media/research.google.com/en//pubs/archive/43905.pdf.
+
+ Suppose the cell dimension is C. Then outside this component, we compute
+ the 4 * C-dimensional quantity consisting of 4 blocks as follows, by a single
+ matrix multiplication:
+
+ i_part = W_{ix} x_t + W_{im} m_{t-1} + b_i
+ f_part = W_{fx} x_t + W_{fm} m_{t-1} + b_f
+ c_part = W_{cx} x_t + W_{cm} m_{t-1} + b_c
+ o_part = W_{cx} x_t + W_{om} m_{t-1} + b_o
+
+ The part of the computation that takes place in this component is as follows.
+ Its input is of dimension 5C [however, search for 'dropout' below],
+ consisting of 5 blocks: (i_part, f_part, c_part, o_part, and c_{t-1}). Its
+ output is of dimension 2C, consisting of 2 blocks: c_t and m_t.
+
+ To recap: the input is (i_part, f_part, c_part, o_part, c_{t-1}); the output is (c_t, m_t).
+
+ This component has parameters, 3C of them in total: the diagonal matrices w_i, w_f
+ and w_o.
+
+
+ In the forward pass (Propagate), this component computes the following:
+
+ i_t = Sigmoid(i_part + w_{ic}*c_{t-1}) (1)
+ f_t = Sigmoid(f_part + w_{fc}*c_{t-1}) (2)
+ c_t = f_t*c_{t-1} + i_t * Tanh(c_part) (3)
+ o_t = Sigmoid(o_part + w_{oc}*c_t) (4)
+ m_t = o_t * Tanh(c_t) (5)
+ # note: the outputs are just c_t and m_t.
+
+ [Note regarding dropout: optionally the input-dimension may be 5C + 3 instead
+ of 5C in this case, the last three input dimensions will be interpreted as
+ per-frame dropout masks on i_t, f_t and o_t respectively, so that on the RHS of
+ (3), i_t is replaced by i_t * i_t_scale, and likewise for f_t and o_t.]
+
+ The backprop is as you would think, but for the "self-repair" we need to pass
+ in additional vectors (of the same dim as the parameters of the layer) that
+ dictate whether or not we add an additional term to the backpropagated
+ derivatives. (This term helps force the input to the nonlinearities into the
+ range where the derivatives are not too small).
+
+ This component stores stats of the same form as are normally stored by the
+ StoreStats() functions for the sigmoid and tanh units, i.e. averages of the
+ activations and derivatives, but this is done inside the Backprop() functions.
+ [the StoreStats() functions don't take the input data as an argument, so
+ storing this data that way is impossible, and anyway it's more efficient to
+ do it as part of backprop.]
+
+ Configuration values accepted:
+ cell-dim e.g. cell-dim=1024 Cell dimension. The input
+ dimension of this component is cell-dim * 5, and the
+ output dimension is cell-dim * 2. Note: this
+ component implements only part of the LSTM layer,
+ see comments above.
+ param-stddev Standard deviation for random initialization of
+ the diagonal matrices (AKA peephole connections).
+ default=1.0, which is probably too high but
+ we couldn't see any reliable gain from decreasing it.
+ tanh-self-repair-threshold Equivalent to the self-repair-lower-threshold
+ in a TanhComponent; applies to both the tanh nonlinearities.
+ default=0.2, you probably won't want to changethis.
+ sigmoid-self-repair-threshold Equivalent to self-repair-lower-threshold
+ in a SigmoidComponent; applies to all three of the sigmoid
+ nonlinearities. default=0.05, you probably won't want to
+ change this.
+ self-repair-scale Equivalent to the self-repair-scale in a SigmoidComponent
+ or TanhComponent; applies to both the sigmoid and tanh
+ nonlinearities. default=1.0e-05, which you probably won't
+ want to change unless dealing with an objective function
+ that has smaller or larger dynamic range than normal, in
+ which case you might want to make it smaller or larger.
+*/
+class LstmNonlinearityComponent: public UpdatableComponent {
public:
- Convolutional1dComponent();
- // constructor using another component
- Convolutional1dComponent(const Convolutional1dComponent &component);
- // constructor using parameters
- Convolutional1dComponent(const CuMatrixBase<BaseFloat> &filter_params,
- const CuVectorBase<BaseFloat> &bias_params,
- BaseFloat learning_rate);
virtual int32 InputDim() const;
virtual int32 OutputDim() const;
-
virtual std::string Info() const;
virtual void InitFromConfig(ConfigLine *cfl);
- virtual std::string Type() const { return "Convolutional1dComponent"; }
+ LstmNonlinearityComponent(): use_dropout_(false) { }
+ virtual std::string Type() const { return "LstmNonlinearityComponent"; }
virtual int32 Properties() const {
- return kSimpleComponent|kUpdatableComponent|kBackpropNeedsInput|
- kBackpropAdds|kPropagateAdds;
+ return kSimpleComponent|kUpdatableComponent|kBackpropNeedsInput;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update_in,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Some functions from base-class UpdatableComponent.
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
virtual void Vectorize(VectorBase<BaseFloat> *params) const;
virtual void UnVectorize(const VectorBase<BaseFloat> ¶ms);
+ virtual void ZeroStats();
+ virtual void FreezeNaturalGradient(bool freeze);
- // Some functions that are specific to this class.
- void SetParams(const VectorBase<BaseFloat> &bias,
- const MatrixBase<BaseFloat> &filter);
- const CuVector<BaseFloat> &BiasParams() { return bias_params_; }
- const CuMatrix<BaseFloat> &LinearParams() { return filter_params_; }
- void Init(int32 input_dim, int32 output_dim,
- int32 patch_dim, int32 patch_step, int32 patch_stride,
- BaseFloat param_stddev, BaseFloat bias_stddev);
- void Init(int32 patch_dim, int32 patch_step, int32 patch_stride,
- std::string matrix_filename);
+ // Some functions that are specific to this class:
+ explicit LstmNonlinearityComponent(
+ const LstmNonlinearityComponent &other);
- // resize the component, setting the parameters to zero, while
- // leaving any other configuration values the same
- void Resize(int32 input_dim, int32 output_dim);
-
- void Update(const std::string &debug_info,
- const CuMatrixBase<BaseFloat> &in_value,
- const CuMatrixBase<BaseFloat> &out_deriv);
+ void Init(int32 cell_dim, bool use_dropout,
+ BaseFloat param_stddev,
+ BaseFloat tanh_self_repair_threshold,
+ BaseFloat sigmoid_self_repair_threshold,
+ BaseFloat self_repair_scale);
private:
- int32 patch_dim_;
- int32 patch_step_;
- int32 patch_stride_;
- static void ReverseIndexes(const std::vector<int32> &forward_indexes,
- int32 input_dim,
- std::vector<std::vector<int32> > *backward_indexes);
- static void RearrangeIndexes(const std::vector<std::vector<int32> > &in,
- std::vector<std::vector<int32> > *out);
+ // Initializes the natural-gradient object with the configuration we
+ // use for this object, which for now is hardcoded at the C++ level.
+ void InitNaturalGradient();
+
+ // Notation: C is the cell dimension; it equals params_.NumCols().
+
+ // The dimension of the parameter matrix is (3 x C);
+ // it contains the 3 diagonal parameter matrices w_i, w_f and w_o.
+ CuMatrix<BaseFloat> params_;
+
+ // If true, we expect an extra 2 dimensions on the input, for dropout masks
+ // for i_t and f_t.
+ bool use_dropout_;
+
+ // Of dimension 5 * C, with a row for each of the Sigmoid/Tanh functions in
+ // equations (1) through (5), this is the sum of the values of the nonliearities
+ // (used for diagnostics only). It is comparable to value_sum_ vector
+ // in base-class NonlinearComponent.
+ CuMatrix<double> value_sum_;
+
+ // Of dimension 5 * C, with a row for each of the Sigmoid/Tanh functions in
+ // equations (1) through (5), this is the sum of the derivatives of the
+ // nonliearities (used for diagnostics and to control self-repair). It is
+ // comparable to the deriv_sum_ vector in base-class
+ // NonlinearComponent.
+ CuMatrix<double> deriv_sum_;
+
+ // This matrix has dimension 10. The contents are a block of 5 self-repair
+ // thresholds (typically "0.05 0.05 0.2 0.05 0.2"), then a block of 5
+ // self-repair scales (typically all 0.00001). These are for each of the 5
+ // nonlinearities in the LSTM component in turn (see comments in cu-math.h for
+ // more info).
+ CuVector<BaseFloat> self_repair_config_;
+
+ // This matrix has dimension 5. For each of the 5 nonlinearities in the LSTM
+ // component (see comments in cu-math.h for more info), it contains the total,
+ // over all frames represented in count_, of the number of dimensions that
+ // were subject to self_repair. To get the self-repair proportion you should
+ // divide by (count_ times cell_dim_).
+ CuVector<double> self_repair_total_;
+
+ // The total count (number of frames) corresponding to the stats in value_sum_
+ // and deriv_sum_.
+ double count_;
+
+ // Preconditioner for the parameters of this component [operates in the space
+ // of dimension C].
+ // The preconditioner stores its own configuration values; we write and read
+ // these, but not the preconditioner object itself.
+ OnlineNaturalGradient preconditioner_;
- const Convolutional1dComponent &operator = (const Convolutional1dComponent &other); // Disallow.
- CuMatrix<BaseFloat> filter_params_;
- CuVector<BaseFloat> bias_params_;
- bool is_gradient_;
+ const LstmNonlinearityComponent &operator
+ = (const LstmNonlinearityComponent &other); // Disallow.
};
-/**
- * MaxPoolingComponent : Maxpooling component was firstly used in ConvNet for
- * selecting an representative activation in an area. Its output is the maximum
- * of the a range of the inputs along a particular convolutional dimension.
- * This implementation doesn't support overlaps, i.e. any input element only
- * appears in the max() expression for one output element.
+
+
+
+/*
+ * WARNING, this component is deprecated as it's not compatible with
+ * TimeHeightConvolutionComponent, and it will eventually be deleted.
+ * MaxPoolingComponent :
+ * Maxpooling component was firstly used in ConvNet for selecting an
+ * representative activation in an area. It inspired Maxout nonlinearity.
+ * Each output element of this component is the maximum of a block of
+ * input elements where the block has a 3D dimension (pool_x_size_,
+ * pool_y_size_, pool_z_size_).
+ * Blocks could overlap if the shift value on any axis is smaller
+ * than its corresponding pool size (e.g. pool_x_step_ < pool_x_size_).
+ * If the shift values are euqal to their pool size, there is no
+ * overlap; while if they all equal 1, the blocks overlap to
+ * the greatest possible extent.
+ *
+ * This component is designed to be used after a ConvolutionComponent
+ * so that the input matrix is propagated from a 2d-convolutional layer.
+ * This component implements 3d-maxpooling which performs
+ * max pooling along the three axes.
+ * Input : A matrix where each row is a vectorized 3D-tensor.
+ * The 3D tensor has dimensions
+ * x: (e.g. time)
+ * y: (e.g. frequency)
+ * z: (e.g. channels like number of filters in the ConvolutionComponent)
*
- * This is a simple component, so the num-rows on the input and output are the
- * same.
+ * The component assumes input vectorizations of type zyx
+ * which is the default output vectorization type of a ConvolutionComponent.
+ * e.g. for input vectorization of type zyx the input is vectorized by
+ * spanning axes z, y and x of the tensor in that order.
+ * Given 3d tensor A with sizes (2, 2, 2) along the three dimensions
+ * the zyx vectorized input looks like
+ * A(0,0,0) A(0,0,1) A(0,1,0) A(0,1,1) A(1,0,0) A(1,0,1) A(1,1,0) A(1,1,1)
+ *
+ * Output : The output is also a 3D tensor vectorized in the zyx format.
+ *
+ * For information on the hyperparameters and parameters of this component see
+ * the variable declarations.
*
- * The InputDim() and OutputDim() [i.e. the num-cols of the input and output]
- * must both be multiples of pool_stride_. Consider one row of the input
- * and one row of the output, written as x and y respectively.
- * We view x and y as made up of sub-vectors of dimension pool_stride_, so
- * x = [ x1 x2 x3 .. ] and y = [ y1 y2 y3 ... ],
*
- * Each sub-vector y is the elementwise maximum of several successive sub-vectors x,
- * so for instance if pool_size_ == 2 then
- * y1 = elementwise-max(x1, x2)
- * y2 = elementwise-max(x3, x4)
- * and so on.
*/
class MaxpoolingComponent: public Component {
public:
- explicit MaxpoolingComponent(int32 input_dim, int32 output_dim,
- int32 pool_size, int32 pool_stride) {
- Init(input_dim, output_dim, pool_size, pool_stride);
- }
- MaxpoolingComponent(): input_dim_(0), output_dim_(0),
- pool_size_(0), pool_stride_(0) { }
- virtual int32 InputDim() const { return input_dim_; }
- virtual int32 OutputDim() const { return output_dim_; }
+
+ MaxpoolingComponent(): input_x_dim_(0), input_y_dim_(0), input_z_dim_(0),
+ pool_x_size_(0), pool_y_size_(0), pool_z_size_(0),
+ pool_x_step_(0), pool_y_step_(0), pool_z_step_(0) { }
+ // constructor using another component
+ MaxpoolingComponent(const MaxpoolingComponent &component);
+
+ virtual int32 InputDim() const;
+ virtual int32 OutputDim() const;
virtual std::string Info() const;
virtual void InitFromConfig(ConfigLine *cfl);
virtual std::string Type() const { return "MaxpoolingComponent"; }
virtual int32 Properties() const {
return kSimpleComponent|kBackpropNeedsInput|kBackpropNeedsOutput|
- kBackpropAdds;
+ kBackpropAdds;
}
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &out_value,
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *, // to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
/// Write component to stream
virtual void Write(std::ostream &os, bool binary) const;
- // We don't implement InitFromConfig() at this level: child-class should do
- // it.
- virtual Component* Copy() const {
- return new MaxpoolingComponent(input_dim_, output_dim_,
- pool_size_, pool_stride_); }
+ virtual Component* Copy() const { return new MaxpoolingComponent(*this); }
- // Some functions that are specific to this class
- void Init(int32 input_dim, int32 output_dim,
- int32 pool_size, int32 pool_stride);
protected:
- int32 input_dim_;
- int32 output_dim_;
- int32 pool_size_;
- int32 pool_stride_;
+ void InputToInputPatches(const CuMatrixBase<BaseFloat>& in,
+ CuMatrix<BaseFloat> *patches) const;
+ void InderivPatchesToInderiv(const CuMatrix<BaseFloat>& in_deriv_patches,
+ CuMatrixBase<BaseFloat> *in_deriv) const;
+ virtual void Check() const;
+
+
+ int32 input_x_dim_; // size of the input along x-axis
+ // (e.g. number of time steps)
+ int32 input_y_dim_; // size of input along y-axis
+ // (e.g. number of mel-frequency bins)
+ int32 input_z_dim_; // size of input along z-axis
+ // (e.g. number of filters in the ConvolutionComponent)
+
+ int32 pool_x_size_; // size of the pooling window along x-axis
+ int32 pool_y_size_; // size of the pooling window along y-axis
+ int32 pool_z_size_; // size of the pooling window along z-axis
+
+ int32 pool_x_step_; // the number of steps taken along x-axis of input
+ // before computing the next pool
+ int32 pool_y_step_; // the number of steps taken along y-axis of input
+ // before computing the next pool
+ int32 pool_z_step_; // the number of steps taken along z-axis of input
+ // before computing the next pool
+
};
+
+/*
+ BatchNormComponent
+
+ This implements batch normalization; for each dimension of the
+ input it normalizes the data to be zero-mean, unit-variance. You
+ can set the block-dim configuration value to implement spatial
+ batch normalization, see the comment for the variable.
+
+ It's a simple component (uses the kSimpleComponent flag), but it is unusual in
+ that it will give different results if you call it on half the matrix at a
+ time. Most of the time this would be pretty harmless, so we still return the
+ kSimpleComponent flag. We may have to modify the test code a little to
+ account for this, or possibly remove the kSimpleComponent flag. In some sense
+ each output Index depends on every input Index, but putting those dependencies
+ explicitly into the dependency-tracking framework as a GeneralComponent
+ would be very impractical and might lead to a lot of unnecessary things being
+ computed. You have to be a bit careful where you put this component, and understand
+ what you're doing e.g. putting it in the path of a recurrence is a bit problematic
+ if the minibatch size were small.
+ */
+class BatchNormComponent: public Component {
+ public:
+
+ BatchNormComponent(): dim_(0), block_dim_(0),
+ epsilon_(1.0e-03), target_rms_(1.0),
+ test_mode_(false), count_(0) { }
+
+ // call this with 'true' to set 'test mode' where the batch normalization is
+ // done with stored stats. There won't normally be any need to specially
+ // accumulate these stats; they are stored as a matter of course on each
+ // iteration of training, as for NonlinearComponents, and we'll use the stats
+ // from the most recent [script-level] iteration.
+ void SetTestMode(bool test_mode);
+
+ // constructor using another component
+ BatchNormComponent(const BatchNormComponent &other);
+
+ virtual int32 InputDim() const { return dim_; }
+ virtual int32 OutputDim() const { return dim_; }
+
+ virtual std::string Info() const;
+ // supports the config variables dim, block-dim (which defaults to dim),
+ // epsilon (which defaults to 1.0e-3), and target-rms (which defaults to 1.0,
+ // and is a scaling on the output; it's comparable to the target-rms of
+ // NormalizeComponent). it also accepts a boolean 'test-mode' config which is
+ // only intended for use in testing code, and not in real situations. (note:
+ // test-mode is a real thing that's used during 'inference' given a previously
+ // computed model, and we do set test mode in real situations; we just don't
+ // do so from the config, we use the function SetTestMode().
+ virtual void InitFromConfig(ConfigLine *cfl);
+ virtual std::string Type() const { return "BatchNormComponent"; }
+ virtual int32 Properties() const {
+ // If the block-dim is less than the dim, we need the input and output
+ // matrices to be contiguous (stride==num-cols), as we'll be reshaping
+ // internally. This is not much of a cost, because this will be used
+ // in convnets where we have to do this anyway.
+ return kSimpleComponent|kBackpropNeedsOutput|kPropagateInPlace|
+ kBackpropInPlace|
+ (block_dim_ < dim_ ? kInputContiguous|kOutputContiguous : 0)|
+ (test_mode_ ? 0 : kUsesMemo|kStoresStats);
+ }
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in,
+ CuMatrixBase<BaseFloat> *out) const;
+ virtual void Backprop(const std::string &debug_info,
+ const ComponentPrecomputedIndexes *indexes,
+ const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
+ Component *, // to_update,
+ CuMatrixBase<BaseFloat> *in_deriv) const;
+
+ virtual void Read(std::istream &is, bool binary); // This Read function
+ // requires that the Component has the correct type.
+
+ /// Write component to stream
+ virtual void Write(std::ostream &os, bool binary) const;
+ virtual Component* Copy() const { return new BatchNormComponent(*this); }
+
+ virtual void Scale(BaseFloat scale);
+ virtual void Add(BaseFloat alpha, const Component &other);
+ virtual void ZeroStats();
+
+
+ virtual void DeleteMemo(void *memo) const { delete static_cast<Memo*>(memo); }
+
+ virtual void StoreStats(const CuMatrixBase<BaseFloat> &in_value,
+ const CuMatrixBase<BaseFloat> &out_value,
+ void *memo);
+
+ // Members specific to this component type.
+ // Note: the offset and scale will only be nonempty in 'test mode'.
+ const CuVector<BaseFloat> &Offset() const { return offset_; }
+ const CuVector<BaseFloat> &Scale() const { return scale_; }
+
+ private:
+
+ struct Memo {
+ // number of frames (after any reshaping).
+ int32 num_frames;
+ // 'sum_sumsq_scale' is of dimension 4 by block_dim_:
+ // Row 0 = mean = the mean of the rows of the input
+ // Row 1 = uvar = the uncentered variance of the input (= sumsq / num_frames).
+ // Row 2 = scale = the scale of the renormalization, which is
+ // Row 3 is used as a temporary in Backprop.
+ // the inverse stddev of the input (modified by epsilon_,
+ // see the Propagate function.
+ CuMatrix<BaseFloat> mean_uvar_scale;
+ };
+
+ void Check() const;
+
+ // this function is used in a couple of places; it turns the raw stats into
+ // the offset/scale term of a normalizing transform.
+ static void ComputeOffsetAndScale(double count,
+ BaseFloat epsilon,
+ const Vector<double> &stats_sum,
+ const Vector<double> &stats_sumsq,
+ Vector<BaseFloat> *offset,
+ Vector<BaseFloat> *scale);
+ // computes derived parameters offset_ and scale_.
+ void ComputeDerived();
+
+ // Dimension of the input and output.
+ int32 dim_;
+ // This would normally be the same as dim_, but if it's less (and it must be >
+ // 0 and must divide dim_), then each separate block of the input of dimension
+ // 'block_dim_' is treated like a separate frame for the purposes of
+ // normalization. This can be used to implement spatial batch normalization
+ // for convolutional setups-- assuming the filter-dim has stride 1, which it
+ // always will in the new code in nnet-convolutional-component.h, when it's
+ // finished.
+ int32 block_dim_;
+
+ // Used to avoid exact-zero variances, epsilon has the dimension of a
+ // covariance; in this work it is applied as a floor, not as an additive term
+ // (this is safer in the presence of numerical roundoff).
+ BaseFloat epsilon_;
+
+ // This value will normally be 1.0, which is the default, but you can set it
+ // to other values as a way to control how fast the following layer learns
+ // (smaller -> slower). The same config exists in NormalizeComponent.
+ BaseFloat target_rms_;
+
+ // This is true if we want the batch normalization to operate in 'test mode'
+ // meaning the data mean and stddev used for the normalziation are fixed
+ // quantities based on previously accumulated stats. Note: the stats we use
+ // for this are based on the same 'StoreStats' mechanism as we use for
+ // components like SigmoidComponent and ReluComponent; we'll be using
+ // the stats from the most recent [script-level] iteration of training.
+ bool test_mode_;
+
+
+ // total count of stats stored by StoreStats().
+ double count_;
+ // sum-of-data component of stats of input data.
+ CuVector<double> stats_sum_;
+ // sum-of-squared component of stats of input data.
+ CuVector<double> stats_sumsq_;
+
+ // offset_ and scale_ are derived from stats_sum_ and stats_sumsq_; they
+ // dictate the transform that is done in 'test mode'. They are set only when
+ // reading the model from disk and when calling SetTestMode(true); they are
+ // resized to empty when the stats are updated, to ensure that out-of-date
+ // values are not kept around.
+ CuVector<BaseFloat> offset_;
+ CuVector<BaseFloat> scale_;
+};
+
+
+
/**
CompositeComponent is a component representing a sequence of
[simple] components. The config line would be something like the following
// call would involve propagating the internals.
virtual int32 Properties() const;
- virtual void Propagate(const ComponentPrecomputedIndexes *indexes,
+ virtual void* Propagate(const ComponentPrecomputedIndexes *indexes,
const CuMatrixBase<BaseFloat> &in,
CuMatrixBase<BaseFloat> *out) const;
virtual void Backprop(const std::string &debug_info,
const CuMatrixBase<BaseFloat> &in_value,
const CuMatrixBase<BaseFloat> &, // out_value
const CuMatrixBase<BaseFloat> &out_deriv,
+ void *memo,
Component *to_update,
CuMatrixBase<BaseFloat> *in_deriv) const;
// Don't implement Copy() at this level: implement it in the child class.
// Some functions from base-class UpdatableComponent.
- virtual void SetLearningRate(BaseFloat lrate);
+ virtual void SetUnderlyingLearningRate(BaseFloat lrate);
+ virtual void SetActualLearningRate(BaseFloat lrate);
+ virtual void SetAsGradient();
virtual void Scale(BaseFloat scale);
virtual void Add(BaseFloat alpha, const Component &other);
- virtual void SetZero(bool treat_as_gradient);
virtual void PerturbParams(BaseFloat stddev);
virtual BaseFloat DotProduct(const UpdatableComponent &other) const;
virtual int32 NumParameters() const;
virtual void Vectorize(VectorBase<BaseFloat> *params) const;
virtual void UnVectorize(const VectorBase<BaseFloat> ¶ms);
+ virtual void FreezeNaturalGradient(bool freeze);
// note: we dont implement the StoreStats function as it would be quite
// expensive; instead, by default we call StoreStats() for any components that