[src] Fix bug in fstrmymbols RE recent const-fst changes (thanks: Jon Nichols); other...
authorDaniel Povey <dpovey@gmail.com>
Thu, 22 Jun 2017 18:01:29 +0000 (14:01 -0400)
committerDaniel Povey <dpovey@gmail.com>
Thu, 22 Jun 2017 18:01:29 +0000 (14:01 -0400)
src/doc/get_version_info.sh
src/fstbin/fstrmsymbols.cc
src/nnet3/nnet-simple-component.h

index d800d9115333df4aa761913012d83b7ca04a76df..8c8a218c1f1736a6522932468e477bcd40e331d1 100755 (executable)
@@ -53,8 +53,8 @@ for tuple in "5.0 5.0 c160a9883" "5.1 5.1 2145519961" "5.2 master 393ef73caa93";
   echo "$0: for version=$major_minor_number, writing git output to $tempfile"
 
   patch_number=0
-  # git rev-list --reverse $first_commit..$branch  lists the revisions from
-  # $first_commit to $branch... --boundary causes it to include $first_commit
+  # git rev-list --reverse $first_commit..upstream/$branch  lists the revisions from
+  # $first_commit to upstream/$branch... --boundary causes it to include $first_commit
   # in the range, but with a dash (-) included for the first commit, so we
   # use a sed command to get rid of that.
   for rev in $(git rev-list --reverse $first_commit..upstream/$branch --boundary | sed s/-//); do
index e713d9e149f46917024e931aac39bd71182be8ed..a365b016e5815bc76c88ecb0e487d24d92511f91 100644 (file)
@@ -136,7 +136,8 @@ int main(int argc, char *argv[]) {
         fst_rxfilename = po.GetOptArg(2),
         fst_wxfilename = po.GetOptArg(3);
 
-    VectorFst<StdArc> *fst = ReadFstKaldi(fst_rxfilename);
+    VectorFst<StdArc> *fst = CastOrConvertToVectorFst(
+        ReadFstKaldiGeneric(fst_rxfilename));
 
     std::vector<int32> disambig_in;
     if (!ReadIntegerVectorSimple(disambig_rxfilename, &disambig_in))
index d19be76461aa33699384e6121aac2d280cef7519..2a9095a0471c7e0ad8b872147937a01aac8881ef 100644 (file)
@@ -1604,6 +1604,8 @@ class NaturalGradientPerElementScaleComponent: public PerElementScaleComponent {
 };
 
 /**
+ * WARNING, this component is deprecated in favor of
+ *  TimeHeightConvolutionComponent, and will be deleted.
  * ConvolutionalComponent implements 2d-convolution.
  * It uses 3D filters on 3D inputs, but the 3D filters hop only over
  * 2 dimensions as it has same size as the input along the 3rd dimension.
@@ -2008,6 +2010,8 @@ class LstmNonlinearityComponent: public UpdatableComponent {
 
 
 /*
+ * WARNING, this component is deprecated as it's not compatible with
+ *   TimeHeightConvolutionComponent, and it will eventually be deleted.
  * MaxPoolingComponent :
  * Maxpooling component was firstly used in ConvNet for selecting an
  * representative activation in an area. It inspired Maxout nonlinearity.