summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1307803)
raw | patch | inline | side by side (parent: 1307803)
author | qin <yinfeng.qin@foxmail.com> | |
Wed, 7 Jun 2017 23:07:30 +0000 (07:07 +0800) | ||
committer | Daniel Povey <dpovey@gmail.com> | |
Wed, 7 Jun 2017 23:07:30 +0000 (19:07 -0400) |
src/doc/tutorial_running.dox | patch | blob | history |
index 1f3cb4ee82afa3b6496bd725e3ba35db9e655938..f977348a3cb5c7817396d76ef38562cba06607b0 100644 (file)
You can see the acoustic likelihods on each iteration. Next look at one of the files
exp/mono/log/update.*.log to see what kind of information is in the update log.
-When the monophone training is finished, we can test the monophone decoding. Before decoding, we have to creat the decode graph. Type:
+When the monophone training is finished, we can test the monophone decoding. Before decoding, we have to create the decode graph. Type:
\verbatim
utils/mkgraph.sh --mono data/lang exp/mono exp/mono/graph
\endverbatim
try to understand it (this one has spaces inside, so Kaldi prints it out with single quotes
around it so that you could paste it into the shell and the program would run as intended).
-The moniphone system is now finished and we will do triphone training and decoding in the
+The monophone system is now finished and we will do triphone training and decoding in the
next step of tutorial.
\ref tutorial "Up: Kaldi tutorial" <BR>