summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d3c7778)
raw | patch | inline | side by side (parent: d3c7778)
author | Tim Hutt <tim.hutt@dyson.com> | |
Mon, 11 Jan 2016 10:49:01 +0000 (10:49 +0000) | ||
committer | Tim Hutt <tim.hutt@dyson.com> | |
Mon, 11 Jan 2016 10:49:01 +0000 (10:49 +0000) |
There were some stray tabs in the Windows INSTALL file.
windows/INSTALL | patch | blob | history |
diff --git a/windows/INSTALL b/windows/INSTALL
index d743129498b9b64a54ac8d3da709fef226290ca4..58955ca60a577fe8aa40bbe5e3bb98c5ac28735e 100644 (file)
--- a/windows/INSTALL
+++ b/windows/INSTALL
be taken in the tools dir
Example:
$ cd (kaldi)/tools
- (kaldi)/tools$ pwd
+ (kaldi)/tools$ pwd
2a) Use git to clone the OpenFST(win) from
2b) Download pthread-win32 (or wget or curl)
https://sourceforge.net/projects/pthreads4w/
(kaldi)/tools$ wget http://downloads.sourceforge.net/project/pthreads4w/pthreads-w32-2-9-1-release.zip
- (kaldi)/tools$ mkdir pthreads; cd pthreads
- (kaldi)/tools/pthreads$ unzip ../pthreads-w32-2-9-1-release.zip
+ (kaldi)/tools$ mkdir pthreads; cd pthreads
+ (kaldi)/tools/pthreads$ unzip ../pthreads-w32-2-9-1-release.zip
2c) Use patch (or you can use git patch) to patch the OpenFST(win)
patch location tools/extras/openfstwin-1.3.4.patch,
Example:
(kaldi)/tools$ cd openfst
- (kaldi)/tools/openfst$ patch -p1 <../extras/openfstwin-1.3.4.patch
+ (kaldi)/tools/openfst$ patch -p1 <../extras/openfstwin-1.3.4.patch
2d-1) Download the OpenBLAS binary packages
https://sourceforge.net/projects/openblas
- (kaldi)/tools$ wget http://sourceforge.net/projects/openblas/files/v0.2.14/OpenBLAS-v0.2.14-Win64-int32.zip
- (kaldi)/tools$ wget http://sourceforge.net/projects/openblas/files/v0.2.14/mingw64_dll.zip
- (kaldi)/tools$ unzip OpenBLAS-v0.2.14-Win64-int32.zip
- (kaldi)/tools$ unzip mingw64_dll.zip
-
- NOTE: Be carefull to download "Win64-int32" and not "Win64-int64"!
-
+ (kaldi)/tools$ wget http://sourceforge.net/projects/openblas/files/v0.2.14/OpenBLAS-v0.2.14-Win64-int32.zip
+ (kaldi)/tools$ wget http://sourceforge.net/projects/openblas/files/v0.2.14/mingw64_dll.zip
+ (kaldi)/tools$ unzip OpenBLAS-v0.2.14-Win64-int32.zip
+ (kaldi)/tools$ unzip mingw64_dll.zip
+
+ NOTE: Be carefull to download "Win64-int32" and not "Win64-int64"!
+
2d-2) Install MKL
2e) If you want enabled CUDA support, download and install NVidia CUDA SDK.
Be careful and strive for as standard install as possible. The installer
- set certain environment variables on which the MSVC Build rules rely.
- If you call "set" in the command line, you should see:
+ set certain environment variables on which the MSVC Build rules rely.
+ If you call "set" in the command line, you should see:
- (kaldi)/tools $ set | grep CUDA
+ (kaldi)/tools $ set | grep CUDA
CUDA_PATH='C:\Users\Yenda\Downloads\cuda'
CUDA_PATH_V7_0='C:\Users\Yenda\Downloads\cuda'
NVCUDASAMPLES7_0_ROOT='C:\Users\Yenda\Downloads\cuda'
NVCUDASAMPLES_ROOT='C:\Users\Yenda\Downloads\cuda'
-
+
The first one (CUDA_PATH) is particulary important.
-
+
3) Open the OpenFST solution in VS --
for VS 2013, the correct solution is in VS2012 directory
for VS 2014, the correct solution is in VS2014 directory
4) Enter the (kaldi)/windows directory
Example:
- (kaldi)/tools/openfst$ cd ../../windows
- (kaldi)/windows $ pwd
-
+ (kaldi)/tools/openfst$ cd ../../windows
+ (kaldi)/windows $ pwd
+
4a) modify the file variables.props to reflect
the correct paths, using your favorite text editor.
- Don't worry, it's a text file, even though you have to be
- careful to keep the structure itself intact
- (kaldi)/windows $ vim variables.props
-
- If you plan to use MKL, you can ignore the OPENBLASDIR path
- If you plan to use OpenBLAS, you can ignore the MKLDIR path
- No matter what you plan to use, set both the OPENFST* and PTHREADW
- variables correctly
-
+ Don't worry, it's a text file, even though you have to be
+ careful to keep the structure itself intact
+ (kaldi)/windows $ vim variables.props
+
+ If you plan to use MKL, you can ignore the OPENBLASDIR path
+ If you plan to use OpenBLAS, you can ignore the MKLDIR path
+ No matter what you plan to use, set both the OPENFST* and PTHREADW
+ variables correctly
+
4b-1) For OpenBLAS support, copy the file "kaldiwin_openblas.props" to "kaldiwin.props"
4b-2) For MKL support, you don't have to do anything, it should work out of the box.
When you need to switch from OpenBLAS to MKL, copy the "kaldiwin_mkl.props"
- to "kaldiwin.props"
+ to "kaldiwin.props"
4c) call the script that generates the MSVC solution
- i.e.
- generate_solution.pl --vsver <default|vs2013|vs2015>
- i.e. for example
- generate_solution.pl --vsver vs2013
-
- For CUDA support, add switch --enable-cuda to the command line,
- i.e. for example
- generate_solution.pl --vsver vs2013 --enable-cuda
-
+ i.e.
+ generate_solution.pl --vsver <default|vs2013|vs2015>
+ i.e. for example
+ generate_solution.pl --vsver vs2013
+
+ For CUDA support, add switch --enable-cuda to the command line,
+ i.e. for example
+ generate_solution.pl --vsver vs2013 --enable-cuda
+
5) Open the generated solution in the visual studio and switch to Debug|x64 (or Release|x64) and build
Expect 10 projects to fail, majority of them will fail because of missing include "portaudio.h"
-------
+------
NOTE: I'm leaving the information about ATLAS here, for reference (also do not forget to consult the README.ATLAS)
(B) either
(i) compile ATLAS under cygwin [see INSTALL.atlas] and copy