[build] dependency-check: that python2.7 and python3 exist and 2.7 is default (#1876)
[processor-sdk/kaldi.git] / src /
2017-09-08 Daniel Povey[doc] Keep tutorial code up to date (thanks: Luwei...
2017-09-05 Daniel Povey[build] Cosmetic fix in Makefile
2017-09-02 Daniel GalvezRemove memory leaks and unused variables (when CUDA...
2017-08-31 Daniel Povey[doc] Fix to how documentation is built (thanks: David...
2017-08-30 Vimal Manohar[src] Adding documentation for lattice discriminative...
2017-08-30 Daniel Galvez[src] Typo fixes in documenation. (#1857)
2017-08-29 Daniel Galvez[src] Remove repeated parameter documentation. (#1849)
2017-08-25 Ashish Arora[scripts,src,egs] simplify by removing --leftmost-quest...
2017-08-25 pegahgh[src] fixed copy-constructor bug RE test_mode option...
2017-08-25 Aswin Shanmugam... [src] fix #include directive in compressed-matrix.h...
2017-08-21 Daniel Povey[doc] Add some terms to glossary
2017-08-20 Adam Zahran[doc] Fix typos (#1833)
2017-08-15 Kirill Katsnelson[build] Enable Travis cache for faster Travis builds...
2017-08-15 Daniel Povey[src] Inconsequential bug-fixes to problems found when...
2017-08-15 Xiaohui Zhang[scripts,src] Check that symbol '#0' is not in the...
2017-08-15 hainan-xv[build] fix compilation problem of tfrnnlm and tfrnnlmb...
2017-08-11 hainan-xv[src,scripts,egs,build] Enable RNNLM lattice rescoring...
2017-08-11 Daniel Povey[build,scripts] Fix to fast-lstm xconfig layer which...
2017-08-09 pegahgh[src] modify feature-extraction binaries to support...
2017-08-09 Daniel Povey[src] Small test-code fix
2017-08-09 Daniel Povey[src] Fix bug in model-update consolidation code (thank...
2017-08-07 Daniel Galvez[src] Cosmetic fix to usage message (#1800)
2017-08-03 Vimal Manohar[src,egs,scripts] Cosmetic and other minor fixes, some...
2017-07-31 Jan "yenda" Trmal[src] Circumvent Visual Studio 2017 bug regarding name...
2017-07-26 Daniel Povey[src] make dithering in feature processing more efficie...
2017-07-16 LvHang[src] Change to arpa-reading code to accept blank lines...
2017-07-15 Jan "yenda" Trmal[src] Add support for row/column ranges when reading...
2017-07-15 Daniel Povey[src] Change name of option --norm-mean->--norm-means...
2017-07-11 Alex Hung[src] Fix indexing error in nnet1::Convolutional2DCompo...
2017-07-11 Daniel Povey[src] Fix usage message of program (thanks:jubang0219...
2017-07-09 Dogan Can[build] Add configuration check for incompatible g...
2017-07-06 Daniel Povey[src] remove remap-leaves.h (thanks: @kkm000)
2017-07-03 Daniel Povey[src] Make sure softmax-related functions can work...
2017-06-30 Daniel Povey[src] Bug-fix in model-collapsing code (thanks: aarora8)
2017-06-28 Eduardo Silva[src] Fix bug in lattice string-pushing, affecting...
2017-06-28 Tanel Alumäe[src] Fix for threaded nnet2 decoding: check if threads...
2017-06-22 Daniel Povey[src] Fix bug in fstrmymbols RE recent const-fst change...
2017-06-21 Daniel Povey[src] nnet3: fix assertion that shouldn't have been...
2017-06-20 Kirill Katsnelson[src] Fix compiler warnings and work around bug on...
2017-06-20 Karel Vesely[src] Adding options to MBR/confidence code (#1696)
2017-06-17 Daniel Povey[src] nnet3 model-collapsing code, for slight decoding...
2017-06-15 Benoit BESSET[src] Fix to multiple-fst case of latgen-faster-mapped...
2017-06-14 Yiming Wang[src,scripts,egs] Backstitch code+scripts, and one...
2017-06-13 Daniel Povey[egs,scripts,src] Tune image recognition examples;...
2017-06-13 Daniel Povey[src] Fix bug in looped computation (#1673)
2017-06-13 guangxu[src] fix to gst-plugin/Makefile (remove -lkaldi-thread...
2017-06-11 Daniel Povey[src] Cosmetic fixes to usage messages
2017-06-08 Daniel Povey[build] Fix small bug in configure
2017-06-07 qin[doc] Fix typo (#1669)
2017-06-07 Daniel Povey[src] nnet3: fix small bug in checking code. Thanks...
2017-06-02 Daniel Povey[src] Add #include missing from previous commit
2017-06-02 Daniel Povey[src] Fix bug in online2-nnet3 decoding RE dropout...
2017-06-02 LvHang[src,scripts] Use ConstFst or decoding (half the memory...
2017-06-01 Jan "yenda" Trmal[src] keyword search tools: fix Minimize() call, necess...
2017-05-31 Daniel Povey[build,scripts] Update scripts that make version info...
2017-05-31 Daniel Povey[src] minor bugfix in convolutional component (doesn...
2017-05-29 Daniel PoveyMerge pull request #1547 from kaldi-asr/kaldi_52
2017-05-29 Daniel Povey[build] Upgrade .version (this is official start of...
2017-05-29 Daniel PoveyMerge pull request #1656 from danpovey/kaldi_52_merge_m...
2017-05-29 Daniel PoveyMerge remote-tracking branch 'upstream/master' into...
2017-05-27 Daniel Povey[src] Fix bug in newly refactored threading code
2017-05-27 Jan "yenda" Trmal[src] keyword search: fix invalid assumption about...
2017-05-26 Dogan Can[src] Use STL thread support library instead of pthread...
2017-05-25 Daniel Povey[src] Add extra diagnostic in nnet3-show-progress
2017-05-24 Daniel Povey[src,scripts,egs] Merge master into kaldi_52 (#1628)
2017-05-21 Hossein Hadian[src] fix regarding first/last chunk's right-context...
2017-05-20 Daniel Povey[src] Make parsing error-msg more informative (thanks...
2017-05-18 Daniel Povey[doc] small fix RE queue configuration.
2017-05-18 Daniel Povey[src,egs,scripts] Add SVHN example; fix asymmetry in...
2017-05-17 pegahgh[src,scripts,egs] Add capability for multilingual...
2017-05-15 LvHang[src] fix a small bug: logging cuda elapsed time (...
2017-05-13 Daniel PoveyMerging master into kaldi_52 (#1621)
2017-05-13 Daniel Povey[src] Fix template instantiation bug causing failure...
2017-05-13 Daniel Povey[src] Change to GPU synchronization, for speed (disable...
2017-05-13 Daniel Povey[src,scripts,egs] Implement and tune resnets. (#1620)
2017-05-11 Daniel Povey[src] Fix bug found by Hainan and Yiming regarding...
2017-05-09 Vimal Manohar[src,scripts,egs] Segmenting long erroneous recordings...
2017-05-07 hainan-xv[src] cosmetic change to const-arpa-lm-building code...
2017-05-07 Daniel Povey[src] Minor fixes to nnet3-egs-augment-image.cc
2017-05-05 Daniel PoveyMerge remote-tracking branch 'upstream/master' into...
2017-05-05 Xingyu Na[src] Add --write-per-frame-acoustic-loglikes options...
2017-05-05 YiwenShaoStephen[src] Add --fill-mode option in nnet3-egs-augment-image...
2017-05-05 Daniel Povey[src] Fix bug that can cause crash for for kernel-sizes...
2017-05-04 Daniel PoveyMerge remote-tracking branch 'upstream/master' into...
2017-05-04 Daniel Povey[src] bug-fix for memory bug in nnet computation cache...
2017-05-03 Kirill Katsnelson[src] Refactor wave-reading code, un-support non-16...
2017-05-01 Hossein Hadian[src,egs] Changes to image augmentation code; example...
2017-05-01 Daniel PoveyMerge remote-tracking branch 'upstream/master' into...
2017-05-01 Daniel PoveyMerge remote-tracking branch 'upstream/master' into...
2017-04-29 Daniel Povey[src] Small fix to how combination+batch-norm works...
2017-04-29 Vassil Panayotov[src] Remove the GetLinearSymbolSequences() function...
2017-04-29 Daniel Povey[src] Changing how batch-norm stats are recomputed...
2017-04-28 Daniel Povey[src,scripts,egs] Change how combination works with...
2017-04-26 Yiming Wang[src,scripts] Add 'test mode' to dropout component...
2017-04-26 Daniel Povey[src] Possible fix for bug found by Gaofeng Cheng
2017-04-26 Daniel Povey[src] Fix test failure in nnet-derivative-test.cc
2017-04-25 Jan "yenda" Trmal[src] Minor bug-fixes in compute-wer-bootci and WSJ...
2017-04-25 Daniel Povey[src,egs,scripts] Minor fixes; new example script with...
2017-04-25 Daniel Povey[src,scripts] Some convolution-related fixes: now learn...
2017-04-24 Daniel Povey[src,egs,scripts] Some partially completed work relatin...
next