remoteproc: resource table: add fw checksum rsc Add firmware checksum resource type to resource table. It can be used for the master to check if the remote runs on the expected firmware if it is still running before it tries to boot the remote. Signed-off-by: Wendy Liang <jliang@xilinx.com>
rproc: add rproc_mem resource entry Add fw_rsc_rproc_mem resource entry to tell the host the remote processor's memory which can be used as shared memory. Signed-off-by: Wendy Liang <jliang@xilinx.com>
Use lib/ for source files for OpenAMP library Move OpenAMP source files into lib/ directory. Porting/ is not necessary, move porting/system/ to system/ Signed-off-by: Wendy Liang <jliang@xilinx.com>