08f8cbd5ac609358369ca202939ce05209973f62
1 open-amp
2 ========
3 This repository is the home for the Open Asymmetric Multi Processing (OpenAMP) framework project. The OpenAMP framework provides software components that enable development of software applications for Asymmetric Multiprocessing (AMP) systems. The framework provides the following key capabilities.
5 1. Provides Life Cycle Management, and Inter Processor Communication capabilities for management of remote compute resources and their associated software contexts
6 2. Provides a stand alone library usable with RTOS and Baremetal software environments
7 3. Compatibility with upstream Linux remoteproc and rpmsg components
8 4. Following AMP configurations supported
9 a. Linux master/Baremetal remote
10 b. Baremetal master/Linux remote
11 5. Proxy infrastructure and supplied demos showcase ability of proxy on master to handle printf, scanf, open, close, read, write calls from Bare metal based remote contexts.
13 Following are the known limitations:
15 1. In rpc_demo.c(the remote demonstration application that showcases usage of rpmsg retargetting infrastructure), the bindings for the flag input parameter in open() system call has been redefined. The GCC tool library bindings for this input argument is different between arm-xilinx/none-eabi, and arm-linux-eabi toolchains. For this reason, redefinition is required for compatibility with proxy on Linux master.
18 For using the framework please refer to the documents present in the /docs folder.