223e3cce59109fe44eff20469337262a12d35299
1 /*
2 * Copyright (c) 2014, Mentor Graphics Corporation
3 * All rights reserved.
4 * Copyright (c) 2015 Xilinx, Inc. All rights reserved.
5 * Copyright (c) 2016 Freescale Semiconductor, Inc. All rights reserved.
6 *
7 * Redistribution and use in source and binary forms, with or without
8 * modification, are permitted provided that the following conditions are met:
9 *
10 * 1. Redistributions of source code must retain the above copyright notice,
11 * this list of conditions and the following disclaimer.
12 * 2. Redistributions in binary form must reproduce the above copyright notice,
13 * this list of conditions and the following disclaimer in the documentation
14 * and/or other materials provided with the distribution.
15 * 3. Neither the name of Mentor Graphics Corporation nor the names of its
16 * contributors may be used to endorse or promote products derived from this
17 * software without specific prior written permission.
18 *
19 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
20 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
21 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
22 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
23 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
24 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
25 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
26 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
27 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
28 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
29 * POSSIBILITY OF SUCH DAMAGE.
30 */
32 /**************************************************************************
33 * FILE NAME
34 *
35 * remote_device.c
36 *
37 * COMPONENT
38 *
39 * OpenAMP Stack
40 *
41 * DESCRIPTION
42 *
43 * This file provides services to manage the remote devices.It also implements
44 * the interface defined by the virtio and provides few other utility functions.
45 *
46 *
47 **************************************************************************/
49 #include <string.h>
50 #include "openamp/rpmsg.h"
51 #include "openamp/remoteproc.h"
52 #include "metal/utilities.h"
53 #include "metal/alloc.h"
54 #include "metal/atomic.h"
55 #include "metal/cpu.h"
57 /* Macro to initialize vring HW info */
58 #define INIT_VRING_ALLOC_INFO(ring_info,vring_hw) \
59 (ring_info).vaddr = (vring_hw).vaddr; \
60 (ring_info).align = (vring_hw).align; \
61 (ring_info).num_descs = (vring_hw).num_descs
63 /* Local functions */
64 static int rpmsg_rdev_init_channels(struct remote_device *rdev);
66 /* Ops table for virtio device */
67 virtio_dispatch rpmsg_rdev_config_ops = {
68 rpmsg_rdev_create_virtqueues,
69 rpmsg_rdev_get_status,
70 rpmsg_rdev_set_status,
71 rpmsg_rdev_get_feature,
72 rpmsg_rdev_set_feature,
73 rpmsg_rdev_negotiate_feature,
74 rpmsg_rdev_read_config,
75 rpmsg_rdev_write_config,
76 rpmsg_rdev_reset
77 };
79 /**
80 * rpmsg_rdev_init
81 *
82 * This function creates and initializes the remote device. The remote device
83 * encapsulates virtio device.
84 *
85 * @param proc - pointer to hil_proc
86 * @param rdev - pointer to newly created remote device
87 * @param role - role of the other device, Master or Remote
88 * @param channel_created - callback function for channel creation
89 * @param channel_destroyed - callback function for channel deletion
90 * @param default_cb - default callback for channel
91 *
92 * @return - status of function execution
93 *
94 */
95 int rpmsg_rdev_init(struct hil_proc *proc,
96 struct remote_device **rdev, int role,
97 rpmsg_chnl_cb_t channel_created,
98 rpmsg_chnl_cb_t channel_destroyed, rpmsg_rx_cb_t default_cb)
99 {
101 struct remote_device *rdev_loc;
102 struct virtio_device *virt_dev;
103 struct proc_shm *shm;
104 int status;
106 if (!proc)
107 return RPMSG_ERR_PARAM;
108 /* Initialize HIL data structures for given device */
109 if (hil_init_proc(proc))
110 return RPMSG_ERR_DEV_INIT;
112 /* Create software representation of remote processor. */
113 rdev_loc = (struct remote_device *)metal_allocate_memory(sizeof(struct remote_device));
115 if (!rdev_loc) {
116 return RPMSG_ERR_NO_MEM;
117 }
119 memset(rdev_loc, 0x00, sizeof(struct remote_device));
120 metal_mutex_init(&rdev_loc->lock);
122 rdev_loc->proc = proc;
123 rdev_loc->role = role;
124 rdev_loc->channel_created = channel_created;
125 rdev_loc->channel_destroyed = channel_destroyed;
126 rdev_loc->default_cb = default_cb;
128 /* Restrict the ept address - zero address can't be assigned */
129 rdev_loc->bitmap[0] = 1;
131 /* Initialize the virtio device */
132 virt_dev = &rdev_loc->virt_dev;
133 virt_dev->device = proc;
134 virt_dev->func = &rpmsg_rdev_config_ops;
135 if (virt_dev->func->set_features != RPMSG_NULL) {
136 virt_dev->func->set_features(virt_dev, proc->vdev.dfeatures);
137 }
139 if (rdev_loc->role == RPMSG_REMOTE) {
140 /*
141 * Since device is RPMSG Remote so we need to manage the
142 * shared buffers. Create shared memory pool to handle buffers.
143 */
144 shm = hil_get_shm_info(proc);
145 rdev_loc->mem_pool =
146 sh_mem_create_pool(shm->start_addr, shm->size,
147 RPMSG_BUFFER_SIZE);
149 if (!rdev_loc->mem_pool) {
150 return RPMSG_ERR_NO_MEM;
151 }
152 }
154 /* Initialize endpoints list */
155 metal_list_init(&rdev_loc->rp_endpoints);
157 /* Initialize channels for RPMSG Remote */
158 status = rpmsg_rdev_init_channels(rdev_loc);
160 if (status != RPMSG_SUCCESS) {
161 return status;
162 }
164 *rdev = rdev_loc;
166 return RPMSG_SUCCESS;
167 }
169 /**
170 * rpmsg_rdev_deinit
171 *
172 * This function un-initializes the remote device.
173 *
174 * @param rdev - pointer to remote device to deinit.
175 *
176 * @return - none
177 *
178 */
179 void rpmsg_rdev_deinit(struct remote_device *rdev)
180 {
181 struct metal_list *node;
182 struct rpmsg_channel *rp_chnl;
183 struct rpmsg_endpoint *rp_ept;
186 while(!metal_list_is_empty(&rdev->rp_channels)) {
187 node = rdev->rp_channels.next;
188 rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
190 if (rdev->channel_destroyed) {
191 rdev->channel_destroyed(rp_chnl);
192 }
194 if ((rdev->support_ns) && (rdev->role == RPMSG_MASTER)) {
195 rpmsg_send_ns_message(rdev, rp_chnl, RPMSG_NS_DESTROY);
196 }
198 /* Delete default endpoint for channel */
199 if (rp_chnl->rp_ept) {
200 rpmsg_destroy_ept(rp_chnl->rp_ept);
201 }
203 _rpmsg_delete_channel(rp_chnl);
204 }
206 /* Delete name service endpoint */
207 metal_mutex_acquire(&rdev->lock);
208 rp_ept = rpmsg_rdev_get_endpoint_from_addr(rdev, RPMSG_NS_EPT_ADDR);
209 metal_mutex_release(&rdev->lock);
210 if (rp_ept) {
211 _destroy_endpoint(rdev, rp_ept);
212 }
214 if (rdev->rvq) {
215 virtqueue_free(rdev->rvq);
216 }
217 if (rdev->tvq) {
218 virtqueue_free(rdev->tvq);
219 }
220 if (rdev->mem_pool) {
221 sh_mem_delete_pool(rdev->mem_pool);
222 }
223 metal_mutex_deinit(&rdev->lock);
224 if (rdev->proc) {
225 hil_delete_proc(rdev->proc);
226 rdev->proc = 0;
227 }
229 metal_free_memory(rdev);
230 }
232 /**
233 * rpmsg_rdev_get_chnl_from_id
234 *
235 * This function returns channel node based on channel name. It must be called
236 * with mutex locked.
237 *
238 * @param stack - pointer to remote device
239 * @param rp_chnl_id - rpmsg channel name
240 *
241 * @return - rpmsg channel
242 *
243 */
244 struct rpmsg_channel *rpmsg_rdev_get_chnl_from_id(struct remote_device *rdev,
245 char *rp_chnl_id)
246 {
247 struct rpmsg_channel *rp_chnl;
248 struct metal_list *node;
250 metal_list_for_each(&rdev->rp_channels, node) {
251 rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
252 if (strncmp
253 (rp_chnl->name, rp_chnl_id, sizeof(rp_chnl->name))
254 == 0) {
255 return rp_chnl;
256 }
257 }
259 return RPMSG_NULL;
260 }
262 /**
263 * rpmsg_rdev_get_endpoint_from_addr
264 *
265 * This function returns endpoint node based on src address. It must be called
266 * with mutex locked.
267 *
268 * @param rdev - pointer remote device control block
269 * @param addr - src address
270 *
271 * @return - rpmsg endpoint
272 *
273 */
274 struct rpmsg_endpoint *rpmsg_rdev_get_endpoint_from_addr(struct remote_device *rdev,
275 unsigned long addr)
276 {
277 struct rpmsg_endpoint *rp_ept;
278 struct metal_list *node;
280 metal_list_for_each(&rdev->rp_endpoints, node) {
281 rp_ept = metal_container_of(node,
282 struct rpmsg_endpoint, node);
283 if (rp_ept->addr == addr) {
284 return rp_ept;
285 }
286 }
288 return RPMSG_NULL;
289 }
291 /*
292 * rpmsg_rdev_notify
293 *
294 * This function checks whether remote device is up or not. If it is up then
295 * notification is sent based on device role to start IPC.
296 *
297 * @param rdev - pointer to remote device
298 *
299 * @return - status of function execution
300 *
301 */
302 int rpmsg_rdev_notify(struct remote_device *rdev)
303 {
304 int status = RPMSG_SUCCESS;
306 if (rdev->role == RPMSG_REMOTE) {
307 status = hil_get_status(rdev->proc);
309 /*
310 * Let the remote device know that Master is ready for
311 * communication.
312 */
313 if (!status)
314 virtqueue_kick(rdev->rvq);
316 } else {
317 status = hil_set_status(rdev->proc);
318 }
320 if (status == RPMSG_SUCCESS) {
321 rdev->state = RPMSG_DEV_STATE_ACTIVE;
322 }
324 return status;
325 }
327 /**
328 * rpmsg_rdev_init_channels
329 *
330 * This function is only applicable to RPMSG remote. It obtains channel IDs
331 * from the HIL and creates RPMSG channels corresponding to each ID.
332 *
333 * @param rdev - pointer to remote device
334 *
335 * @return - status of function execution
336 *
337 */
338 int rpmsg_rdev_init_channels(struct remote_device *rdev)
339 {
340 struct rpmsg_channel *rp_chnl;
341 struct proc_chnl *chnl_info;
342 int num_chnls, idx;
344 metal_list_init(&rdev->rp_channels);
345 if (rdev->role == RPMSG_MASTER) {
347 chnl_info = hil_get_chnl_info(rdev->proc, &num_chnls);
348 for (idx = 0; idx < num_chnls; idx++) {
350 rp_chnl =
351 _rpmsg_create_channel(rdev, chnl_info[idx].name,
352 0x00, RPMSG_NS_EPT_ADDR);
353 if (!rp_chnl) {
354 return RPMSG_ERR_NO_MEM;
355 }
357 rp_chnl->rp_ept =
358 rpmsg_create_ept(rp_chnl, rdev->default_cb, rdev,
359 RPMSG_ADDR_ANY);
361 if (!rp_chnl->rp_ept) {
362 return RPMSG_ERR_NO_MEM;
363 }
365 rp_chnl->src = rp_chnl->rp_ept->addr;
366 }
367 }
369 return RPMSG_SUCCESS;
370 }
372 /**
373 * check if the remote is ready to start RPMsg communication
374 */
375 int rpmsg_rdev_remote_ready(struct remote_device *rdev)
376 {
377 struct virtio_device *vdev = &rdev->virt_dev;
378 uint8_t status;
379 if (rdev->role == RPMSG_MASTER) {
380 while (1) {
381 /* Busy wait until the remote is ready */
382 status = vdev->func->get_status(vdev);
383 if (status & VIRTIO_CONFIG_STATUS_DRIVER_OK)
384 return true;
385 metal_cpu_yield();
386 }
387 } else {
388 return true;
389 }
390 /* Never come here */
391 return false;
392 }
394 static void rpmsg_memset_io(struct metal_io_region *io, void *dst, int c, size_t count)
395 {
396 if ((io->mem_flags & METAL_IO_MAPPED)) {
397 metal_memset_io(dst, c, count);
398 } else {
399 memset(dst, c, count);
400 }
401 }
403 /**
404 *------------------------------------------------------------------------
405 * The rest of the file implements the virtio device interface as defined
406 * by the virtio.h file.
407 *------------------------------------------------------------------------
408 */
409 int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
410 const char *names[], vq_callback * callbacks[],
411 struct virtqueue *vqs_[])
412 {
413 struct remote_device *rdev;
414 struct vring_alloc_info ring_info;
415 struct virtqueue *vqs[RPMSG_MAX_VQ_PER_RDEV];
416 struct proc_vring *vring_table;
417 void *buffer;
418 struct metal_sg sg;
419 int idx, num_vrings, status;
421 (void)flags;
422 (void)vqs_;
424 rdev = (struct remote_device *)dev;
426 /* Get the vring HW info for the given virtio device */
427 vring_table = hil_get_vring_info(&rdev->proc->vdev, &num_vrings);
429 if (num_vrings > nvqs) {
430 return RPMSG_ERR_MAX_VQ;
431 }
433 /* Create virtqueue for each vring. */
434 for (idx = 0; idx < num_vrings; idx++) {
436 INIT_VRING_ALLOC_INFO(ring_info, vring_table[idx]);
438 if (rdev->role == RPMSG_REMOTE) {
439 rpmsg_memset_io(vring_table[idx].io, (void *)ring_info.vaddr, 0x00,
440 vring_size(vring_table[idx].num_descs, vring_table[idx].align));
441 }
443 status =
444 virtqueue_create(dev, idx, (char *)names[idx], &ring_info,
445 callbacks[idx], hil_vring_notify,
446 rdev->proc->sh_buff.io,
447 &vqs[idx]);
449 if (status != RPMSG_SUCCESS) {
450 return status;
451 }
452 }
454 //FIXME - a better way to handle this , tx for master is rx for remote and vice versa.
455 if (rdev->role == RPMSG_MASTER) {
456 rdev->tvq = vqs[0];
457 rdev->rvq = vqs[1];
458 } else {
459 rdev->tvq = vqs[1];
460 rdev->rvq = vqs[0];
461 }
463 if (rdev->role == RPMSG_REMOTE) {
464 sg.io = rdev->proc->sh_buff.io;
465 sg.len = RPMSG_BUFFER_SIZE;
466 for (idx = 0; ((idx < rdev->rvq->vq_nentries)
467 && (idx < rdev->mem_pool->total_buffs / 2));
468 idx++) {
470 /* Initialize TX virtqueue buffers for remote device */
471 buffer = sh_mem_get_buffer(rdev->mem_pool);
473 if (!buffer) {
474 return RPMSG_ERR_NO_BUFF;
475 }
477 sg.virt = buffer;
479 rpmsg_memset_io(sg.io, buffer, 0x00, RPMSG_BUFFER_SIZE);
480 status =
481 virtqueue_add_buffer(rdev->rvq, &sg, 0, 1,
482 buffer);
484 if (status != RPMSG_SUCCESS) {
485 return status;
486 }
487 }
488 }
490 return RPMSG_SUCCESS;
491 }
493 unsigned char rpmsg_rdev_get_status(struct virtio_device *dev)
494 {
495 struct hil_proc *proc = dev->device;
496 struct proc_vdev *pvdev = &proc->vdev;
497 struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
499 if (!vdev_rsc)
500 return -1;
502 return vdev_rsc->status;
503 }
505 void rpmsg_rdev_set_status(struct virtio_device *dev, unsigned char status)
506 {
507 struct hil_proc *proc = dev->device;
508 struct proc_vdev *pvdev = &proc->vdev;
509 struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
511 if (!vdev_rsc)
512 return;
514 vdev_rsc->status = status;
516 atomic_thread_fence(memory_order_seq_cst);
517 }
519 uint32_t rpmsg_rdev_get_feature(struct virtio_device *dev)
520 {
521 return dev->features;
522 }
524 void rpmsg_rdev_set_feature(struct virtio_device *dev, uint32_t feature)
525 {
526 dev->features |= feature;
527 }
529 uint32_t rpmsg_rdev_negotiate_feature(struct virtio_device *dev,
530 uint32_t features)
531 {
532 (void)dev;
533 (void)features;
535 return 0;
536 }
538 /*
539 * Read/write a variable amount from the device specific (ie, network)
540 * configuration region. This region is encoded in the same endian as
541 * the guest.
542 */
543 void rpmsg_rdev_read_config(struct virtio_device *dev, uint32_t offset,
544 void *dst, int length)
545 {
546 (void)dev;
547 (void)offset;
548 (void)dst;
549 (void)length;
551 return;
552 }
554 void rpmsg_rdev_write_config(struct virtio_device *dev, uint32_t offset,
555 void *src, int length)
556 {
557 (void)dev;
558 (void)offset;
559 (void)src;
560 (void)length;
562 return;
563 }
565 void rpmsg_rdev_reset(struct virtio_device *dev)
566 {
567 (void)dev;
569 return;
570 }