ebb170f262190c80fc1e082eecfef24b450369c2
1 /*
2 * Copyright (c) 2014, Mentor Graphics Corporation
3 * All rights reserved.
4 * Copyright (c) 2015 Xilinx, Inc. All rights reserved.
5 * Copyright (c) 2016 Freescale Semiconductor, Inc. All rights reserved.
6 *
7 * Redistribution and use in source and binary forms, with or without
8 * modification, are permitted provided that the following conditions are met:
9 *
10 * 1. Redistributions of source code must retain the above copyright notice,
11 * this list of conditions and the following disclaimer.
12 * 2. Redistributions in binary form must reproduce the above copyright notice,
13 * this list of conditions and the following disclaimer in the documentation
14 * and/or other materials provided with the distribution.
15 * 3. Neither the name of Mentor Graphics Corporation nor the names of its
16 * contributors may be used to endorse or promote products derived from this
17 * software without specific prior written permission.
18 *
19 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
20 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
21 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
22 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
23 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
24 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
25 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
26 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
27 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
28 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
29 * POSSIBILITY OF SUCH DAMAGE.
30 */
32 /**************************************************************************
33 * FILE NAME
34 *
35 * remote_device.c
36 *
37 * COMPONENT
38 *
39 * OpenAMP Stack
40 *
41 * DESCRIPTION
42 *
43 * This file provides services to manage the remote devices.It also implements
44 * the interface defined by the virtio and provides few other utility functions.
45 *
46 *
47 **************************************************************************/
49 #include <string.h>
50 #include "openamp/rpmsg.h"
51 #include "openamp/remoteproc.h"
52 #include "metal/utilities.h"
53 #include "metal/alloc.h"
54 #include "metal/atomic.h"
55 #include "metal/cpu.h"
57 /* Macro to initialize vring HW info */
58 #define INIT_VRING_ALLOC_INFO(ring_info,vring_hw) \
59 (ring_info).vaddr = (vring_hw).vaddr; \
60 (ring_info).align = (vring_hw).align; \
61 (ring_info).num_descs = (vring_hw).num_descs
63 /* Local functions */
64 static int rpmsg_rdev_init_channels(struct remote_device *rdev);
66 /* Ops table for virtio device */
67 virtio_dispatch rpmsg_rdev_config_ops = {
68 rpmsg_rdev_create_virtqueues,
69 rpmsg_rdev_get_status,
70 rpmsg_rdev_set_status,
71 rpmsg_rdev_get_feature,
72 rpmsg_rdev_set_feature,
73 rpmsg_rdev_negotiate_feature,
74 rpmsg_rdev_read_config,
75 rpmsg_rdev_write_config,
76 rpmsg_rdev_reset
77 };
79 /**
80 * rpmsg_rdev_init
81 *
82 * This function creates and initializes the remote device. The remote device
83 * encapsulates virtio device.
84 *
85 * @param proc - pointer to hil_proc
86 * @param rdev - pointer to newly created remote device
87 * @param role - role of the other device, Master or Remote
88 * @param channel_created - callback function for channel creation
89 * @param channel_destroyed - callback function for channel deletion
90 * @param default_cb - default callback for channel
91 *
92 * @return - status of function execution
93 *
94 */
95 int rpmsg_rdev_init(struct hil_proc *proc,
96 struct remote_device **rdev, int role,
97 rpmsg_chnl_cb_t channel_created,
98 rpmsg_chnl_cb_t channel_destroyed, rpmsg_rx_cb_t default_cb)
99 {
101 struct remote_device *rdev_loc;
102 struct virtio_device *virt_dev;
103 struct proc_shm *shm;
104 int status;
106 if (!proc)
107 return RPMSG_ERR_PARAM;
108 /* Initialize HIL data structures for given device */
109 if (hil_init_proc(proc))
110 return RPMSG_ERR_DEV_INIT;
112 /* Create software representation of remote processor. */
113 rdev_loc = (struct remote_device *)metal_allocate_memory(sizeof(struct remote_device));
115 if (!rdev_loc) {
116 return RPMSG_ERR_NO_MEM;
117 }
119 memset(rdev_loc, 0x00, sizeof(struct remote_device));
120 metal_mutex_init(&rdev_loc->lock);
122 rdev_loc->proc = proc;
123 rdev_loc->role = role;
124 rdev_loc->channel_created = channel_created;
125 rdev_loc->channel_destroyed = channel_destroyed;
126 rdev_loc->default_cb = default_cb;
128 /* Restrict the ept address - zero address can't be assigned */
129 rdev_loc->bitmap[0] = 1;
131 /* Initialize the virtio device */
132 virt_dev = &rdev_loc->virt_dev;
133 virt_dev->device = proc;
134 virt_dev->func = &rpmsg_rdev_config_ops;
135 if (virt_dev->func->set_features != RPMSG_NULL) {
136 virt_dev->func->set_features(virt_dev, proc->vdev.dfeatures);
137 }
139 if (rdev_loc->role == RPMSG_REMOTE) {
140 /*
141 * Since device is RPMSG Remote so we need to manage the
142 * shared buffers. Create shared memory pool to handle buffers.
143 */
144 shm = hil_get_shm_info(proc);
145 rdev_loc->mem_pool =
146 sh_mem_create_pool(shm->start_addr, shm->size,
147 RPMSG_BUFFER_SIZE);
149 if (!rdev_loc->mem_pool) {
150 return RPMSG_ERR_NO_MEM;
151 }
152 }
154 if (!rpmsg_rdev_remote_ready(rdev_loc))
155 return RPMSG_ERR_DEV_INIT;
157 /* Initialize endpoints list */
158 metal_list_init(&rdev_loc->rp_endpoints);
160 /* Initialize channels for RPMSG Remote */
161 status = rpmsg_rdev_init_channels(rdev_loc);
163 if (status != RPMSG_SUCCESS) {
164 return status;
165 }
167 *rdev = rdev_loc;
169 return RPMSG_SUCCESS;
170 }
172 /**
173 * rpmsg_rdev_deinit
174 *
175 * This function un-initializes the remote device.
176 *
177 * @param rdev - pointer to remote device to deinit.
178 *
179 * @return - none
180 *
181 */
182 void rpmsg_rdev_deinit(struct remote_device *rdev)
183 {
184 struct metal_list *node;
185 struct rpmsg_channel *rp_chnl;
186 struct rpmsg_endpoint *rp_ept;
189 while(!metal_list_is_empty(&rdev->rp_channels)) {
190 node = rdev->rp_channels.next;
191 rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
193 if (rdev->channel_destroyed) {
194 rdev->channel_destroyed(rp_chnl);
195 }
197 if ((rdev->support_ns) && (rdev->role == RPMSG_MASTER)) {
198 rpmsg_send_ns_message(rdev, rp_chnl, RPMSG_NS_DESTROY);
199 }
201 /* Delete default endpoint for channel */
202 if (rp_chnl->rp_ept) {
203 rpmsg_destroy_ept(rp_chnl->rp_ept);
204 }
206 _rpmsg_delete_channel(rp_chnl);
207 }
209 /* Delete name service endpoint */
210 metal_mutex_acquire(&rdev->lock);
211 rp_ept = rpmsg_rdev_get_endpoint_from_addr(rdev, RPMSG_NS_EPT_ADDR);
212 metal_mutex_release(&rdev->lock);
213 if (rp_ept) {
214 _destroy_endpoint(rdev, rp_ept);
215 }
217 metal_mutex_acquire(&rdev->lock);
218 rdev->rvq = 0;
219 rdev->tvq = 0;
220 if (rdev->mem_pool) {
221 sh_mem_delete_pool(rdev->mem_pool);
222 rdev->mem_pool = 0;
223 }
224 metal_mutex_release(&rdev->lock);
225 hil_free_vqs(&rdev->virt_dev);
227 if (rdev->proc) {
228 hil_delete_proc(rdev->proc);
229 rdev->proc = 0;
230 }
231 metal_mutex_deinit(&rdev->lock);
233 metal_free_memory(rdev);
234 }
236 /**
237 * rpmsg_rdev_get_chnl_from_id
238 *
239 * This function returns channel node based on channel name. It must be called
240 * with mutex locked.
241 *
242 * @param stack - pointer to remote device
243 * @param rp_chnl_id - rpmsg channel name
244 *
245 * @return - rpmsg channel
246 *
247 */
248 struct rpmsg_channel *rpmsg_rdev_get_chnl_from_id(struct remote_device *rdev,
249 char *rp_chnl_id)
250 {
251 struct rpmsg_channel *rp_chnl;
252 struct metal_list *node;
254 metal_list_for_each(&rdev->rp_channels, node) {
255 rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
256 if (strncmp
257 (rp_chnl->name, rp_chnl_id, sizeof(rp_chnl->name))
258 == 0) {
259 return rp_chnl;
260 }
261 }
263 return RPMSG_NULL;
264 }
266 /**
267 * rpmsg_rdev_get_endpoint_from_addr
268 *
269 * This function returns endpoint node based on src address. It must be called
270 * with mutex locked.
271 *
272 * @param rdev - pointer remote device control block
273 * @param addr - src address
274 *
275 * @return - rpmsg endpoint
276 *
277 */
278 struct rpmsg_endpoint *rpmsg_rdev_get_endpoint_from_addr(struct remote_device *rdev,
279 unsigned long addr)
280 {
281 struct rpmsg_endpoint *rp_ept;
282 struct metal_list *node;
284 metal_list_for_each(&rdev->rp_endpoints, node) {
285 rp_ept = metal_container_of(node,
286 struct rpmsg_endpoint, node);
287 if (rp_ept->addr == addr) {
288 return rp_ept;
289 }
290 }
292 return RPMSG_NULL;
293 }
295 /*
296 * rpmsg_rdev_notify
297 *
298 * This function checks whether remote device is up or not. If it is up then
299 * notification is sent based on device role to start IPC.
300 *
301 * @param rdev - pointer to remote device
302 *
303 * @return - status of function execution
304 *
305 */
306 int rpmsg_rdev_notify(struct remote_device *rdev)
307 {
308 struct virtio_device *vdev = &rdev->virt_dev;
310 hil_vdev_notify(vdev);
312 return RPMSG_SUCCESS;
313 }
315 /**
316 * rpmsg_rdev_init_channels
317 *
318 * This function is only applicable to RPMSG remote. It obtains channel IDs
319 * from the HIL and creates RPMSG channels corresponding to each ID.
320 *
321 * @param rdev - pointer to remote device
322 *
323 * @return - status of function execution
324 *
325 */
326 int rpmsg_rdev_init_channels(struct remote_device *rdev)
327 {
328 struct rpmsg_channel *rp_chnl;
329 struct proc_chnl *chnl_info;
330 int num_chnls, idx;
332 metal_list_init(&rdev->rp_channels);
333 if (rdev->role == RPMSG_MASTER) {
335 chnl_info = hil_get_chnl_info(rdev->proc, &num_chnls);
336 for (idx = 0; idx < num_chnls; idx++) {
338 rp_chnl =
339 _rpmsg_create_channel(rdev, chnl_info[idx].name,
340 0x00, RPMSG_NS_EPT_ADDR);
341 if (!rp_chnl) {
342 return RPMSG_ERR_NO_MEM;
343 }
345 rp_chnl->rp_ept =
346 rpmsg_create_ept(rp_chnl, rdev->default_cb, rdev,
347 RPMSG_ADDR_ANY);
349 if (!rp_chnl->rp_ept) {
350 return RPMSG_ERR_NO_MEM;
351 }
353 rp_chnl->src = rp_chnl->rp_ept->addr;
354 }
355 }
357 return RPMSG_SUCCESS;
358 }
360 /**
361 * check if the remote is ready to start RPMsg communication
362 */
363 int rpmsg_rdev_remote_ready(struct remote_device *rdev)
364 {
365 struct virtio_device *vdev = &rdev->virt_dev;
366 uint8_t status;
367 if (rdev->role == RPMSG_MASTER) {
368 while (1) {
369 /* Busy wait until the remote is ready */
370 status = vdev->func->get_status(vdev);
371 if (status & VIRTIO_CONFIG_STATUS_DRIVER_OK)
372 return true;
373 metal_cpu_yield();
374 }
375 } else {
376 return true;
377 }
378 /* Never come here */
379 return false;
380 }
382 static void rpmsg_memset_io(struct metal_io_region *io, void *dst, int c, size_t count)
383 {
384 if ((io->mem_flags & METAL_IO_MAPPED)) {
385 metal_memset_io(dst, c, count);
386 } else {
387 memset(dst, c, count);
388 }
389 }
391 /**
392 *------------------------------------------------------------------------
393 * The rest of the file implements the virtio device interface as defined
394 * by the virtio.h file.
395 *------------------------------------------------------------------------
396 */
397 int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
398 const char *names[], vq_callback * callbacks[],
399 struct virtqueue *vqs_[])
400 {
401 struct remote_device *rdev;
402 struct vring_alloc_info ring_info;
403 struct virtqueue *vqs[RPMSG_MAX_VQ_PER_RDEV];
404 struct proc_vring *vring_table;
405 void *buffer;
406 struct metal_sg sg;
407 int idx, num_vrings, status;
409 (void)flags;
410 (void)vqs_;
412 rdev = (struct remote_device *)dev;
414 /* Get the vring HW info for the given virtio device */
415 vring_table = hil_get_vring_info(&rdev->proc->vdev, &num_vrings);
417 if (num_vrings > nvqs) {
418 return RPMSG_ERR_MAX_VQ;
419 }
421 /* Create virtqueue for each vring. */
422 for (idx = 0; idx < num_vrings; idx++) {
424 INIT_VRING_ALLOC_INFO(ring_info, vring_table[idx]);
426 if (rdev->role == RPMSG_REMOTE) {
427 rpmsg_memset_io(vring_table[idx].io, (void *)ring_info.vaddr, 0x00,
428 vring_size(vring_table[idx].num_descs, vring_table[idx].align));
429 }
431 status =
432 virtqueue_create(dev, idx, (char *)names[idx], &ring_info,
433 callbacks[idx], hil_vring_notify,
434 rdev->proc->sh_buff.io,
435 &vqs[idx]);
437 if (status != RPMSG_SUCCESS) {
438 return status;
439 }
440 }
442 //FIXME - a better way to handle this , tx for master is rx for remote and vice versa.
443 if (rdev->role == RPMSG_MASTER) {
444 rdev->tvq = vqs[0];
445 rdev->rvq = vqs[1];
446 } else {
447 rdev->tvq = vqs[1];
448 rdev->rvq = vqs[0];
449 }
451 if (rdev->role == RPMSG_REMOTE) {
452 sg.io = rdev->proc->sh_buff.io;
453 sg.len = RPMSG_BUFFER_SIZE;
454 for (idx = 0; ((idx < rdev->rvq->vq_nentries)
455 && (idx < rdev->mem_pool->total_buffs / 2));
456 idx++) {
458 /* Initialize TX virtqueue buffers for remote device */
459 buffer = sh_mem_get_buffer(rdev->mem_pool);
461 if (!buffer) {
462 return RPMSG_ERR_NO_BUFF;
463 }
465 sg.virt = buffer;
467 rpmsg_memset_io(sg.io, buffer, 0x00, RPMSG_BUFFER_SIZE);
468 status =
469 virtqueue_add_buffer(rdev->rvq, &sg, 0, 1,
470 buffer);
472 if (status != RPMSG_SUCCESS) {
473 return status;
474 }
475 }
476 }
478 return RPMSG_SUCCESS;
479 }
481 unsigned char rpmsg_rdev_get_status(struct virtio_device *dev)
482 {
483 struct hil_proc *proc = dev->device;
484 struct proc_vdev *pvdev = &proc->vdev;
485 struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
487 if (!vdev_rsc)
488 return -1;
490 return vdev_rsc->status;
491 }
493 void rpmsg_rdev_set_status(struct virtio_device *dev, unsigned char status)
494 {
495 struct hil_proc *proc = dev->device;
496 struct proc_vdev *pvdev = &proc->vdev;
497 struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
499 if (!vdev_rsc)
500 return;
502 vdev_rsc->status = status;
504 atomic_thread_fence(memory_order_seq_cst);
505 }
507 uint32_t rpmsg_rdev_get_feature(struct virtio_device *dev)
508 {
509 return dev->features;
510 }
512 void rpmsg_rdev_set_feature(struct virtio_device *dev, uint32_t feature)
513 {
514 dev->features |= feature;
515 }
517 uint32_t rpmsg_rdev_negotiate_feature(struct virtio_device *dev,
518 uint32_t features)
519 {
520 (void)dev;
521 (void)features;
523 return 0;
524 }
526 /*
527 * Read/write a variable amount from the device specific (ie, network)
528 * configuration region. This region is encoded in the same endian as
529 * the guest.
530 */
531 void rpmsg_rdev_read_config(struct virtio_device *dev, uint32_t offset,
532 void *dst, int length)
533 {
534 (void)dev;
535 (void)offset;
536 (void)dst;
537 (void)length;
539 return;
540 }
542 void rpmsg_rdev_write_config(struct virtio_device *dev, uint32_t offset,
543 void *src, int length)
544 {
545 (void)dev;
546 (void)offset;
547 (void)src;
548 (void)length;
550 return;
551 }
553 void rpmsg_rdev_reset(struct virtio_device *dev)
554 {
555 (void)dev;
557 return;
558 }