]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - processor-sdk/open-amp.git/blob - obsolete/system/generic/machine/zynq7/linux-firmware/zlib/inftrees.h
Restruct obsolete directory
[processor-sdk/open-amp.git] / obsolete / system / generic / machine / zynq7 / linux-firmware / zlib / inftrees.h
1 /* inftrees.h -- header to use inftrees.c
2  * Copyright (C) 1995-2005, 2010 Mark Adler
3  * For conditions of distribution and use, see copyright notice in zlib.h
4  */
6 /* WARNING: this file should *not* be used by applications. It is
7    part of the implementation of the compression library and is
8    subject to change. Applications should only use zlib.h.
9  */
11 /* Structure for decoding tables.  Each entry provides either the
12    information needed to do the operation requested by the code that
13    indexed that table entry, or it provides a pointer to another
14    table that indexes more bits of the code.  op indicates whether
15    the entry is a pointer to another table, a literal, a length or
16    distance, an end-of-block, or an invalid code.  For a table
17    pointer, the low four bits of op is the number of index bits of
18    that table.  For a length or distance, the low four bits of op
19    is the number of extra bits to get after the code.  bits is
20    the number of bits in this code or part of the code to drop off
21    of the bit buffer.  val is the actual byte to output in the case
22    of a literal, the base length or distance, or the offset from
23    the current table to the next table.  Each entry is four bytes. */
24 typedef struct {
25         unsigned char op;       /* operation, extra bits, table bits */
26         unsigned char bits;     /* bits in this part of the code */
27         unsigned short val;     /* offset in table or code value */
28 } code;
30 /* op values as set by inflate_table():
31     00000000 - literal
32     0000tttt - table link, tttt != 0 is the number of table index bits
33     0001eeee - length or distance, eeee is the number of extra bits
34     01100000 - end of block
35     01000000 - invalid code
36  */
38 /* Maximum size of the dynamic table.  The maximum number of code structures is
39    1444, which is the sum of 852 for literal/length codes and 592 for distance
40    codes.  These values were found by exhaustive searches using the program
41    examples/enough.c found in the zlib distribtution.  The arguments to that
42    program are the number of symbols, the initial root table size, and the
43    maximum bit length of a code.  "enough 286 9 15" for literal/length codes
44    returns returns 852, and "enough 30 6 15" for distance codes returns 592.
45    The initial root table size (9 or 6) is found in the fifth argument of the
46    inflate_table() calls in inflate.c and infback.c.  If the root table size is
47    changed, then these maximum sizes would be need to be recalculated and
48    updated. */
49 #define ENOUGH_LENS 852
50 #define ENOUGH_DISTS 592
51 #define ENOUGH (ENOUGH_LENS+ENOUGH_DISTS)
53 /* Type of code to build for inflate_table() */
54 typedef enum {
55         CODES,
56         LENS,
57         DISTS
58 } codetype;
60 int ZLIB_INTERNAL inflate_table OF((codetype type, unsigned short FAR * lens,
61                                     unsigned codes, code FAR * FAR * table,
62                                     unsigned FAR * bits,
63                                     unsigned short FAR * work));