/* * Copyright (c) 2014, Mentor Graphics Corporation * All rights reserved. * Copyright (c) 2015 Xilinx, Inc. All rights reserved. * Copyright (c) 2016 Freescale Semiconductor, Inc. All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * 1. Redistributions of source code must retain the above copyright notice, * this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright notice, * this list of conditions and the following disclaimer in the documentation * and/or other materials provided with the distribution. * 3. Neither the name of Mentor Graphics Corporation nor the names of its * contributors may be used to endorse or promote products derived from this * software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE * POSSIBILITY OF SUCH DAMAGE. */ /************************************************************************** * FILE NAME * * rpmsg_core.c * * COMPONENT * * OpenAMP * * DESCRIPTION * * This file provides the core functionality of RPMSG messaging part like * message parsing ,Rx/Tx callbacks handling , channel creation/deletion * and address management. * * **************************************************************************/ #include #include "openamp/rpmsg.h" #include "metal/utilities.h" #include "metal/io.h" #include "metal/cache.h" #include "metal/alloc.h" /* Internal functions */ static void rpmsg_rx_callback(struct virtqueue *vq); static void rpmsg_tx_callback(struct virtqueue *vq); /** * rpmsg_start_ipc * * This function creates communication links(virtqueues) for remote device * and notifies it to start IPC. * * @param rdev - remote device handle * * @return - status of function execution * */ int rpmsg_start_ipc(struct remote_device *rdev) { struct virtio_device *virt_dev; struct rpmsg_endpoint *ns_ept; void (*callback[2]) (struct virtqueue * vq); const char *vq_names[2]; unsigned long dev_features; int status; struct virtqueue *vqs[2]; int i; virt_dev = &rdev->virt_dev; /* Initialize names and callbacks based on the device role */ if (rdev->role == RPMSG_MASTER) { vq_names[0] = "tx_vq"; vq_names[1] = "rx_vq"; callback[0] = rpmsg_tx_callback; callback[1] = rpmsg_rx_callback; } else { vq_names[0] = "rx_vq"; vq_names[1] = "tx_vq"; callback[0] = rpmsg_rx_callback; callback[1] = rpmsg_tx_callback; } /* Create virtqueues for remote device */ status = virt_dev->func->create_virtqueues(virt_dev, 0, RPMSG_MAX_VQ_PER_RDEV, vq_names, callback, RPMSG_NULL); if (status != RPMSG_SUCCESS) { return status; } dev_features = virt_dev->func->get_features(virt_dev); /* * Create name service announcement endpoint if device supports name * service announcement feature. */ if ((dev_features & (1 << VIRTIO_RPMSG_F_NS))) { rdev->support_ns = RPMSG_TRUE; ns_ept = _create_endpoint(rdev, rpmsg_ns_callback, rdev, RPMSG_NS_EPT_ADDR); if (!ns_ept) { return RPMSG_ERR_NO_MEM; } } /* Initialize notifications for vring. */ if (rdev->role == RPMSG_MASTER) { vqs[0] = rdev->tvq; vqs[1] = rdev->rvq; } else { vqs[0] = rdev->rvq; vqs[1] = rdev->tvq; } for (i = 0; i <= 1; i++) { status = hil_enable_vring_notifications(i, vqs[i]); if (status != RPMSG_SUCCESS) { return status; } } status = rpmsg_rdev_notify(rdev); return status; } /** * _rpmsg_create_channel * * Creates new rpmsg channel with the given parameters. * * @param rdev - pointer to remote device which contains the channel * @param name - name of the device * @param src - source address for the rpmsg channel * @param dst - destination address for the rpmsg channel * * @return - pointer to new rpmsg channel * */ struct rpmsg_channel *_rpmsg_create_channel(struct remote_device *rdev, char *name, unsigned long src, unsigned long dst) { struct rpmsg_channel *rp_chnl; rp_chnl = metal_allocate_memory(sizeof(struct rpmsg_channel)); if (rp_chnl) { memset(rp_chnl, 0x00, sizeof(struct rpmsg_channel)); strncpy(rp_chnl->name, name, sizeof(rp_chnl->name)); rp_chnl->src = src; rp_chnl->dst = dst; rp_chnl->rdev = rdev; /* Place channel on channels list */ metal_mutex_acquire(&rdev->lock); metal_list_add_tail(&rdev->rp_channels, &rp_chnl->node); metal_mutex_release(&rdev->lock); } return rp_chnl; } /** * _rpmsg_delete_channel * * Deletes given rpmsg channel. * * @param rp_chnl - pointer to rpmsg channel to delete * * return - none */ void _rpmsg_delete_channel(struct rpmsg_channel *rp_chnl) { if (rp_chnl) { metal_mutex_acquire(&rp_chnl->rdev->lock); metal_list_del(&rp_chnl->node); metal_mutex_release(&rp_chnl->rdev->lock); metal_free_memory(rp_chnl); } } /** * _create_endpoint * * This function creates rpmsg endpoint. * * @param rdev - pointer to remote device * @param cb - Rx completion call back * @param priv - private data * @param addr - endpoint src address * * @return - pointer to endpoint control block * */ struct rpmsg_endpoint *_create_endpoint(struct remote_device *rdev, rpmsg_rx_cb_t cb, void *priv, unsigned long addr) { struct rpmsg_endpoint *rp_ept; int status = RPMSG_SUCCESS; rp_ept = metal_allocate_memory(sizeof(struct rpmsg_endpoint)); if (!rp_ept) { return RPMSG_NULL; } memset(rp_ept, 0x00, sizeof(struct rpmsg_endpoint)); metal_mutex_acquire(&rdev->lock); if (addr != RPMSG_ADDR_ANY) { /* * Application has requested a particular src address for endpoint, * first check if address is available. */ if (!rpmsg_is_address_set (rdev->bitmap, RPMSG_ADDR_BMP_SIZE, addr)) { /* Mark the address as used in the address bitmap. */ rpmsg_set_address(rdev->bitmap, RPMSG_ADDR_BMP_SIZE, addr); } else { status = RPMSG_ERR_DEV_ADDR; } } else { addr = rpmsg_get_address(rdev->bitmap, RPMSG_ADDR_BMP_SIZE); if ((int)addr < 0) { status = RPMSG_ERR_DEV_ADDR; } } /* Do cleanup in case of error and return */ if (RPMSG_SUCCESS != status) { metal_free_memory(rp_ept); metal_mutex_release(&rdev->lock); return RPMSG_NULL; } rp_ept->addr = addr; rp_ept->cb = cb; rp_ept->priv = priv; metal_list_add_tail(&rdev->rp_endpoints, &rp_ept->node); metal_mutex_release(&rdev->lock); return rp_ept; } /** * rpmsg_destroy_ept * * This function deletes rpmsg endpoint and performs cleanup. * * @param rdev - pointer to remote device * @param rp_ept - pointer to endpoint to destroy * */ void _destroy_endpoint(struct remote_device *rdev, struct rpmsg_endpoint *rp_ept) { metal_mutex_acquire(&rdev->lock); rpmsg_release_address(rdev->bitmap, RPMSG_ADDR_BMP_SIZE, rp_ept->addr); metal_list_del(&rp_ept->node); metal_mutex_release(&rdev->lock); /* free node and rp_ept */ metal_free_memory(rp_ept); } /** * rpmsg_send_ns_message * * Sends name service announcement to remote device * * @param rdev - pointer to remote device * @param rp_chnl - pointer to rpmsg channel * @param flags - Channel creation/deletion flags * */ void rpmsg_send_ns_message(struct remote_device *rdev, struct rpmsg_channel *rp_chnl, unsigned long flags) { struct rpmsg_hdr *rp_hdr; struct rpmsg_ns_msg *ns_msg; unsigned short idx; unsigned long len; metal_mutex_acquire(&rdev->lock); /* Get Tx buffer. */ rp_hdr = (struct rpmsg_hdr *)rpmsg_get_tx_buffer(rdev, &len, &idx); if (!rp_hdr) { metal_mutex_release(&rdev->lock); return; } /* Fill out name service data. */ rp_hdr->dst = RPMSG_NS_EPT_ADDR; rp_hdr->len = sizeof(struct rpmsg_ns_msg); ns_msg = (struct rpmsg_ns_msg *) RPMSG_LOCATE_DATA(rp_hdr); strncpy(ns_msg->name, rp_chnl->name, sizeof(rp_chnl->name)); ns_msg->flags = flags; ns_msg->addr = rp_chnl->src; /* Place the buffer on virtqueue. */ rpmsg_enqueue_buffer(rdev, rp_hdr, len, idx); /* Notify the other side that it has data to process. */ virtqueue_kick(rdev->tvq); metal_mutex_release(&rdev->lock); } /** * rpmsg_enqueue_buffers * * Places buffer on the virtqueue for consumption by the other side. * * @param rdev - pointer to remote core * @param buffer - buffer pointer * @param len - buffer length * @idx - buffer index * * @return - status of function execution * */ int rpmsg_enqueue_buffer(struct remote_device *rdev, void *buffer, unsigned long len, unsigned short idx) { int status; struct metal_sg sg; struct metal_io_region *io; io = rdev->proc->sh_buff.io; if (io) { if (! (io->mem_flags & METAL_UNCACHED)) metal_cache_flush(buffer, (unsigned int)len); } if (rdev->role == RPMSG_REMOTE) { /* Initialize buffer node */ sg.virt = buffer; sg.len = len; sg.io = io; status = virtqueue_add_buffer(rdev->tvq, &sg, 0, 1, buffer); } else { (void)sg; status = virtqueue_add_consumed_buffer(rdev->tvq, idx, len); } return status; } /** * rpmsg_return_buffer * * Places the used buffer back on the virtqueue. * * @param rdev - pointer to remote core * @param buffer - buffer pointer * @param len - buffer length * @param idx - buffer index * */ void rpmsg_return_buffer(struct remote_device *rdev, void *buffer, unsigned long len, unsigned short idx) { struct metal_sg sg; if (rdev->role == RPMSG_REMOTE) { /* Initialize buffer node */ sg.virt = buffer; sg.len = len; sg.io = rdev->proc->sh_buff.io; virtqueue_add_buffer(rdev->rvq, &sg, 0, 1, buffer); } else { (void)sg; virtqueue_add_consumed_buffer(rdev->rvq, idx, len); } } /** * rpmsg_get_tx_buffer * * Provides buffer to transmit messages. * * @param rdev - pointer to remote device * @param len - length of returned buffer * @param idx - buffer index * * return - pointer to buffer. */ void *rpmsg_get_tx_buffer(struct remote_device *rdev, unsigned long *len, unsigned short *idx) { void *data; if (rdev->role == RPMSG_REMOTE) { data = virtqueue_get_buffer(rdev->tvq, (uint32_t *) len, idx); if (data == RPMSG_NULL) { data = sh_mem_get_buffer(rdev->mem_pool); *len = RPMSG_BUFFER_SIZE; } } else { data = virtqueue_get_available_buffer(rdev->tvq, idx, (uint32_t *) len); } return data; } /** * rpmsg_get_rx_buffer * * Retrieves the received buffer from the virtqueue. * * @param rdev - pointer to remote device * @param len - size of received buffer * @param idx - index of buffer * * @return - pointer to received buffer * */ void *rpmsg_get_rx_buffer(struct remote_device *rdev, unsigned long *len, unsigned short *idx) { void *data; if (rdev->role == RPMSG_REMOTE) { data = virtqueue_get_buffer(rdev->rvq, (uint32_t *) len, idx); } else { data = virtqueue_get_available_buffer(rdev->rvq, idx, (uint32_t *) len); } if (data) { struct metal_io_region *io; io = rdev->proc->sh_buff.io; if (io) { if (! (io->mem_flags & METAL_UNCACHED)) metal_cache_invalidate(data, (unsigned int)(*len)); } } return data; } /** * rpmsg_free_buffer * * Frees the allocated buffers. * * @param rdev - pointer to remote device * @param buffer - pointer to buffer to free * */ void rpmsg_free_buffer(struct remote_device *rdev, void *buffer) { if (rdev->role == RPMSG_REMOTE) { sh_mem_free_buffer(buffer, rdev->mem_pool); } } /** * rpmsg_tx_callback * * Tx callback function. * * @param vq - pointer to virtqueue on which Tx is has been * completed. * */ static void rpmsg_tx_callback(struct virtqueue *vq) { struct remote_device *rdev; struct virtio_device *vdev; struct rpmsg_channel *rp_chnl; struct metal_list *node; vdev = (struct virtio_device *)vq->vq_dev; rdev = (struct remote_device *)vdev; /* Check if the remote device is master. */ if (rdev->role == RPMSG_MASTER) { /* Notification is received from the master. Now the remote(us) can * performs one of two operations; * * a. If name service announcement is supported then it will send NS message. * else * b. It will update the channel state to active so that further communication * can take place. */ metal_list_for_each(&rdev->rp_channels, node) { rp_chnl = metal_container_of(node, struct rpmsg_channel, node); if (rp_chnl->state == RPMSG_CHNL_STATE_IDLE) { if (rdev->support_ns) { rp_chnl->state = RPMSG_CHNL_STATE_NS; } else { rp_chnl->state = RPMSG_CHNL_STATE_ACTIVE; } if (rp_chnl->state == RPMSG_CHNL_STATE_NS) { rpmsg_send_ns_message(rdev, rp_chnl, RPMSG_NS_CREATE); } } } } } /** * rpmsg_rx_callback * * Rx callback function. * * @param vq - pointer to virtqueue on which messages is received * */ void rpmsg_rx_callback(struct virtqueue *vq) { struct remote_device *rdev; struct virtio_device *vdev; struct rpmsg_channel *rp_chnl; struct rpmsg_endpoint *rp_ept; struct rpmsg_hdr *rp_hdr; struct rpmsg_hdr_reserved *reserved; struct metal_list *node; unsigned long len; unsigned short idx; vdev = (struct virtio_device *)vq->vq_dev; rdev = (struct remote_device *)vdev; if (rdev->role == RPMSG_MASTER) { metal_list_for_each(&rdev->rp_channels, node) { rp_chnl = metal_container_of(node, struct rpmsg_channel, node); if (rp_chnl->state == RPMSG_CHNL_STATE_IDLE) { if (rdev->support_ns) { rp_chnl->state = RPMSG_CHNL_STATE_NS; rpmsg_send_ns_message(rdev, rp_chnl, RPMSG_NS_CREATE); } else { rp_chnl->state = RPMSG_CHNL_STATE_ACTIVE; } return; } } } metal_mutex_acquire(&rdev->lock); /* Process the received data from remote node */ rp_hdr = (struct rpmsg_hdr *)rpmsg_get_rx_buffer(rdev, &len, &idx); metal_mutex_release(&rdev->lock); while (rp_hdr) { /* Get the channel node from the remote device channels list. */ metal_mutex_acquire(&rdev->lock); rp_ept = rpmsg_rdev_get_endpoint_from_addr(rdev, rp_hdr->dst); metal_mutex_release(&rdev->lock); if (!rp_ept) /* Fatal error no endpoint for the given dst addr. */ return; rp_chnl = rp_ept->rp_chnl; if ((rp_chnl) && (rp_chnl->state == RPMSG_CHNL_STATE_NS)) { /* First message from RPMSG Master, update channel * destination address and state */ rp_chnl->dst = rp_hdr->src; rp_chnl->state = RPMSG_CHNL_STATE_ACTIVE; /* Notify channel creation to application */ if (rdev->channel_created) { rdev->channel_created(rp_chnl); } } else { rp_ept->cb(rp_chnl, (void *)RPMSG_LOCATE_DATA(rp_hdr), rp_hdr->len, rp_ept->priv, rp_hdr->src); } metal_mutex_acquire(&rdev->lock); /* Check whether callback wants to hold buffer */ if (rp_hdr->reserved & RPMSG_BUF_HELD) { /* 'rp_hdr->reserved' field is now used as storage for * 'idx' to release buffer later */ reserved = (struct rpmsg_hdr_reserved*)&rp_hdr->reserved; reserved->idx = (uint16_t)idx; } else { /* Return used buffers. */ rpmsg_return_buffer(rdev, rp_hdr, len, idx); } rp_hdr = (struct rpmsg_hdr *)rpmsg_get_rx_buffer(rdev, &len, &idx); metal_mutex_release(&rdev->lock); } } /** * rpmsg_ns_callback * * This callback handles name service announcement from the remote device * and creates/deletes rpmsg channels. * * @param server_chnl - pointer to server channel control block. * @param data - pointer to received messages * @param len - length of received data * @param priv - any private data * @param src - source address * * @return - none */ void rpmsg_ns_callback(struct rpmsg_channel *server_chnl, void *data, int len, void *priv, unsigned long src) { struct remote_device *rdev; struct rpmsg_channel *rp_chnl; struct rpmsg_ns_msg *ns_msg; (void)server_chnl; (void)src; rdev = (struct remote_device *)priv; //FIXME: This assumes same name string size for channel name both on master //and remote. If this is not the case then we will have to parse the //message contents. ns_msg = (struct rpmsg_ns_msg *)data; ns_msg->name[len - 1] = '\0'; if (ns_msg->flags & RPMSG_NS_DESTROY) { metal_mutex_acquire(&rdev->lock); rp_chnl = rpmsg_rdev_get_chnl_from_id(rdev, ns_msg->name); metal_mutex_release(&rdev->lock); if (rp_chnl) { if (rdev->channel_destroyed) { rdev->channel_destroyed(rp_chnl); } rpmsg_destroy_ept(rp_chnl->rp_ept); _rpmsg_delete_channel(rp_chnl); } } else { rp_chnl = _rpmsg_create_channel(rdev, ns_msg->name, 0x00, ns_msg->addr); if (rp_chnl) { rp_chnl->state = RPMSG_CHNL_STATE_ACTIVE; /* Create default endpoint for channel */ rp_chnl->rp_ept = rpmsg_create_ept(rp_chnl, rdev->default_cb, rdev, RPMSG_ADDR_ANY); if (rp_chnl->rp_ept) { rp_chnl->src = rp_chnl->rp_ept->addr; /* * Echo back the NS message to remote in order to * complete the connection stage. Remote will know the endpoint * address from this point onward which will enable it to send * message without waiting for any application level message from * master. */ rpmsg_send(rp_chnl, data, len); if (rdev->channel_created) { rdev->channel_created(rp_chnl); } } } } } /** * rpmsg_get_address * * This function provides unique 32 bit address. * * @param bitmap - bit map for addresses * @param size - size of bitmap * * return - a unique address */ int rpmsg_get_address(unsigned long *bitmap, int size) { int addr = -1; int i, tmp32; /* Find first available buffer */ for (i = 0; i < size; i++) { tmp32 = get_first_zero_bit(bitmap[i]); if (tmp32 < 32) { addr = tmp32 + (i*32); bitmap[i] |= (1 << tmp32); break; } } return addr; } /** * rpmsg_release_address * * Frees the given address. * * @param bitmap - bit map for addresses * @param size - size of bitmap * @param addr - address to free * * return - none */ int rpmsg_release_address(unsigned long *bitmap, int size, int addr) { unsigned int i, j; unsigned long mask = 1; if (addr >= size * 32) return -1; /* Mark the addr as available */ i = addr / 32; j = addr % 32; mask = mask << j; bitmap[i] = bitmap[i] & (~mask); return RPMSG_SUCCESS; } /** * rpmsg_is_address_set * * Checks whether address is used or free. * * @param bitmap - bit map for addresses * @param size - size of bitmap * @param addr - address to free * * return - TRUE/FALSE */ int rpmsg_is_address_set(unsigned long *bitmap, int size, int addr) { int i, j; unsigned long mask = 1; if (addr >= size * 32) return -1; /* Mark the id as available */ i = addr / 32; j = addr % 32; mask = mask << j; return (bitmap[i] & mask); } /** * rpmsg_set_address * * Marks the address as consumed. * * @param bitmap - bit map for addresses * @param size - size of bitmap * @param addr - address to free * * return - none */ int rpmsg_set_address(unsigned long *bitmap, int size, int addr) { int i, j; unsigned long mask = 1; if (addr >= size * 32) return -1; /* Mark the id as available */ i = addr / 32; j = addr % 32; mask = mask << j; bitmap[i] |= mask; return RPMSG_SUCCESS; }