/*- * Copyright (c) 2011, Bryan Venteicher * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * 1. Redistributions of source code must retain the above copyright * notice unmodified, this list of conditions, and the following * disclaimer. * 2. Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * THIS SOFTWARE IS PROVIDED BY THE AUTHOR ``AS IS'' AND ANY EXPRESS OR * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. * IN NO EVENT SHALL THE AUTHOR BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT * NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF * THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ #include "openamp/virtqueue.h" /* Prototype for internal functions. */ static void vq_ring_init(struct virtqueue *); static void vq_ring_update_avail(struct virtqueue *, uint16_t); static uint16_t vq_ring_add_buffer(struct virtqueue *, struct vring_desc *, uint16_t, struct llist *, int, int); static int vq_ring_enable_interrupt(struct virtqueue *, uint16_t); static void vq_ring_free_chain(struct virtqueue *, uint16_t); static int vq_ring_must_notify_host(struct virtqueue *vq); static void vq_ring_notify_host(struct virtqueue *vq); static int virtqueue_nused(struct virtqueue *vq); /** * virtqueue_create - Creates new VirtIO queue * * @param device - Pointer to VirtIO device * @param id - VirtIO queue ID , must be unique * @param name - Name of VirtIO queue * @param ring - Pointer to vring_alloc_info control block * @param callback - Pointer to callback function, invoked * when message is available on VirtIO queue * @param notify - Pointer to notify function, used to notify * other side that there is job available for it * @param v_queue - Created VirtIO queue. * * @return - Function status */ int virtqueue_create(struct virtio_device *virt_dev, unsigned short id, char *name, struct vring_alloc_info *ring, void (*callback) (struct virtqueue * vq), void (*notify) (struct virtqueue * vq), struct virtqueue **v_queue) { struct virtqueue *vq = VQ_NULL; int status = VQUEUE_SUCCESS; uint32_t vq_size = 0; VQ_PARAM_CHK(ring == VQ_NULL, status, ERROR_VQUEUE_INVLD_PARAM); VQ_PARAM_CHK(ring->num_descs == 0, status, ERROR_VQUEUE_INVLD_PARAM); VQ_PARAM_CHK(ring->num_descs & (ring->num_descs - 1), status, ERROR_VRING_ALIGN); //TODO : Error check for indirect buffer addition if (status == VQUEUE_SUCCESS) { vq_size = sizeof(struct virtqueue) + (ring->num_descs) * sizeof(struct vq_desc_extra); vq = (struct virtqueue *)env_allocate_memory(vq_size); if (vq == VQ_NULL) { return (ERROR_NO_MEM); } env_memset(vq, 0x00, vq_size); vq->vq_dev = virt_dev; env_strncpy(vq->vq_name, name, VIRTQUEUE_MAX_NAME_SZ); vq->vq_queue_index = id; vq->vq_alignment = ring->align; vq->vq_nentries = ring->num_descs; vq->vq_free_cnt = vq->vq_nentries; vq->callback = callback; vq->notify = notify; //TODO : Whether we want to support indirect addition or not. vq->vq_ring_size = vring_size(ring->num_descs, ring->align); vq->vq_ring_mem = (void *)ring->phy_addr; /* Initialize vring control block in virtqueue. */ vq_ring_init(vq); /* Disable callbacks - will be enabled by the application * once initialization is completed. */ virtqueue_disable_cb(vq); *v_queue = vq; //TODO : Need to add cleanup in case of error used with the indirect buffer addition //TODO: do we need to save the new queue in db based on its id } return (status); } /** * virtqueue_add_buffer() - Enqueues new buffer in vring for consumption * by other side. Readable buffers are always * inserted before writable buffers * * @param vq - Pointer to VirtIO queue control block. * @param buffer - Pointer to buffer list * @param readable - Number of readable buffers * @param writable - Number of writable buffers * @param cookie - Pointer to hold call back data * * @return - Function status */ int virtqueue_add_buffer(struct virtqueue *vq, struct llist *buffer, int readable, int writable, void *cookie) { struct vq_desc_extra *dxp = VQ_NULL; int status = VQUEUE_SUCCESS; uint16_t head_idx; uint16_t idx; int needed; needed = readable + writable; VQ_PARAM_CHK(vq == VQ_NULL, status, ERROR_VQUEUE_INVLD_PARAM); VQ_PARAM_CHK(needed < 1, status, ERROR_VQUEUE_INVLD_PARAM); VQ_PARAM_CHK(vq->vq_free_cnt == 0, status, ERROR_VRING_FULL); //TODO: Add parameters validation for indirect buffer addition VQUEUE_BUSY(vq); if (status == VQUEUE_SUCCESS) { //TODO : Indirect buffer addition support VQASSERT(vq, cookie != VQ_NULL, "enqueuing with no cookie"); head_idx = vq->vq_desc_head_idx; VQ_RING_ASSERT_VALID_IDX(vq, head_idx); dxp = &vq->vq_descx[head_idx]; VQASSERT(vq, (dxp->cookie == VQ_NULL), "cookie already exists for index"); dxp->cookie = cookie; dxp->ndescs = needed; /* Enqueue buffer onto the ring. */ idx = vq_ring_add_buffer(vq, vq->vq_ring.desc, head_idx, buffer, readable, writable); vq->vq_desc_head_idx = idx; vq->vq_free_cnt -= needed; if (vq->vq_free_cnt == 0) VQ_RING_ASSERT_CHAIN_TERM(vq); else VQ_RING_ASSERT_VALID_IDX(vq, idx); /* * Update vring_avail control block fields so that other * side can get buffer using it. */ vq_ring_update_avail(vq, head_idx); } VQUEUE_IDLE(vq); return (status); } /** * virtqueue_add_single_buffer - Enqueues single buffer in vring * * @param vq - Pointer to VirtIO queue control block * @param cookie - Pointer to hold call back data * @param buffer_addr - Address of buffer * @param len - Length of buffer * @param writable - If buffer writable * @param has_next - If buffers for subsequent call are * to be chained * * @return - Function status */ int virtqueue_add_single_buffer(struct virtqueue *vq, void *cookie, void *buffer_addr, uint32_t len, int writable, boolean has_next) { struct vq_desc_extra *dxp; struct vring_desc *dp; uint16_t head_idx; uint16_t idx; int status = VQUEUE_SUCCESS; VQ_PARAM_CHK(vq == VQ_NULL, status, ERROR_VQUEUE_INVLD_PARAM); VQ_PARAM_CHK(vq->vq_free_cnt == 0, status, ERROR_VRING_FULL); VQUEUE_BUSY(vq); if (status == VQUEUE_SUCCESS) { VQASSERT(vq, cookie != VQ_NULL, "enqueuing with no cookie"); head_idx = vq->vq_desc_head_idx; dxp = &vq->vq_descx[head_idx]; dxp->cookie = cookie; dxp->ndescs = 1; idx = head_idx; dp = &vq->vq_ring.desc[idx]; dp->addr = env_map_vatopa(buffer_addr); dp->len = len; dp->flags = 0; idx = dp->next; if (has_next) dp->flags |= VRING_DESC_F_NEXT; if (writable) dp->flags |= VRING_DESC_F_WRITE; vq->vq_desc_head_idx = idx; vq->vq_free_cnt--; if (vq->vq_free_cnt == 0) VQ_RING_ASSERT_CHAIN_TERM(vq); else VQ_RING_ASSERT_VALID_IDX(vq, idx); vq_ring_update_avail(vq, head_idx); } VQUEUE_IDLE(vq); return (status); } /** * virtqueue_get_buffer - Returns used buffers from VirtIO queue * * @param vq - Pointer to VirtIO queue control block * @param len - Length of conumed buffer * * @return - Pointer to used buffer */ void *virtqueue_get_buffer(struct virtqueue *vq, uint32_t * len) { struct vring_used_elem *uep; void *cookie; uint16_t used_idx, desc_idx; if ((vq == VQ_NULL) || (vq->vq_used_cons_idx == vq->vq_ring.used->idx)) return (VQ_NULL); VQUEUE_BUSY(vq); used_idx = vq->vq_used_cons_idx++ & (vq->vq_nentries - 1); uep = &vq->vq_ring.used->ring[used_idx]; env_rmb(); desc_idx = (uint16_t) uep->id; if (len != VQ_NULL) *len = uep->len; vq_ring_free_chain(vq, desc_idx); cookie = vq->vq_descx[desc_idx].cookie; vq->vq_descx[desc_idx].cookie = VQ_NULL; VQUEUE_IDLE(vq); return (cookie); } /** * virtqueue_free - Frees VirtIO queue resources * * @param vq - Pointer to VirtIO queue control block * */ void virtqueue_free(struct virtqueue *vq) { if (vq != VQ_NULL) { if (vq->vq_free_cnt != vq->vq_nentries) { env_print ("\r\nWARNING %s: freeing non-empty virtqueue\r\n", vq->vq_name); } //TODO : Need to free indirect buffers here if (vq->vq_ring_mem != VQ_NULL) { vq->vq_ring_size = 0; vq->vq_ring_mem = VQ_NULL; } env_free_memory(vq); } } /** * virtqueue_get_available_buffer - Returns buffer available for use in the * VirtIO queue * * @param vq - Pointer to VirtIO queue control block * @param avail_idx - Pointer to index used in vring desc table * @param len - Length of buffer * * @return - Pointer to available buffer */ void *virtqueue_get_available_buffer(struct virtqueue *vq, uint16_t * avail_idx, uint32_t * len) { uint16_t head_idx = 0; void *buffer; if (vq->vq_available_idx == vq->vq_ring.avail->idx) { return (VQ_NULL); } VQUEUE_BUSY(vq); head_idx = vq->vq_available_idx++ & (vq->vq_nentries - 1); *avail_idx = vq->vq_ring.avail->ring[head_idx]; env_rmb(); buffer = env_map_patova(vq->vq_ring.desc[*avail_idx].addr); *len = vq->vq_ring.desc[*avail_idx].len; VQUEUE_IDLE(vq); return (buffer); } /** * virtqueue_add_consumed_buffer - Returns consumed buffer back to VirtIO queue * * @param vq - Pointer to VirtIO queue control block * @param head_idx - Index of vring desc containing used buffer * @param len - Length of buffer * * @return - Function status */ int virtqueue_add_consumed_buffer(struct virtqueue *vq, uint16_t head_idx, uint32_t len) { struct vring_used_elem *used_desc = VQ_NULL; uint16_t used_idx; if ((head_idx > vq->vq_nentries) || (head_idx < 0)) { return (ERROR_VRING_NO_BUFF); } VQUEUE_BUSY(vq); used_idx = vq->vq_ring.used->idx & (vq->vq_nentries - 1); used_desc = &(vq->vq_ring.used->ring[used_idx]); used_desc->id = head_idx; used_desc->len = len; env_wmb(); vq->vq_ring.used->idx++; VQUEUE_IDLE(vq); return (VQUEUE_SUCCESS); } /** * virtqueue_enable_cb - Enables callback generation * * @param vq - Pointer to VirtIO queue control block * * @return - Function status */ int virtqueue_enable_cb(struct virtqueue *vq) { return (vq_ring_enable_interrupt(vq, 0)); } /** * virtqueue_enable_cb - Disables callback generation * * @param vq - Pointer to VirtIO queue control block * */ void virtqueue_disable_cb(struct virtqueue *vq) { VQUEUE_BUSY(vq); if (vq->vq_flags & VIRTQUEUE_FLAG_EVENT_IDX) { vring_used_event(&vq->vq_ring) = vq->vq_used_cons_idx - vq->vq_nentries - 1; } else { vq->vq_ring.avail->flags |= VRING_AVAIL_F_NO_INTERRUPT; } VQUEUE_IDLE(vq); } /** * virtqueue_kick - Notifies other side that there is buffer available for it. * * @param vq - Pointer to VirtIO queue control block */ void virtqueue_kick(struct virtqueue *vq) { VQUEUE_BUSY(vq); /* Ensure updated avail->idx is visible to host. */ env_mb(); if (vq_ring_must_notify_host(vq)) vq_ring_notify_host(vq); vq->vq_queued_cnt = 0; VQUEUE_IDLE(vq); } /** * virtqueue_dump Dumps important virtqueue fields , use for debugging purposes * * @param vq - Pointer to VirtIO queue control block */ void virtqueue_dump(struct virtqueue *vq) { if (vq == VQ_NULL) return; env_print("VQ: %s - size=%d; free=%d; used=%d; queued=%d; " "desc_head_idx=%d; avail.idx=%d; used_cons_idx=%d; " "used.idx=%d; avail.flags=0x%x; used.flags=0x%x\r\n", vq->vq_name, vq->vq_nentries, vq->vq_free_cnt, virtqueue_nused(vq), vq->vq_queued_cnt, vq->vq_desc_head_idx, vq->vq_ring.avail->idx, vq->vq_used_cons_idx, vq->vq_ring.used->idx, vq->vq_ring.avail->flags, vq->vq_ring.used->flags); } /** * virtqueue_get_desc_size - Returns vring descriptor size * * @param vq - Pointer to VirtIO queue control block * * @return - Descriptor length */ uint32_t virtqueue_get_desc_size(struct virtqueue * vq) { uint16_t head_idx = 0; uint16_t avail_idx = 0; uint32_t len = 0; if (vq->vq_available_idx == vq->vq_ring.avail->idx) { return (VQ_NULL); } VQUEUE_BUSY(vq); head_idx = vq->vq_available_idx & (vq->vq_nentries - 1); avail_idx = vq->vq_ring.avail->ring[head_idx]; len = vq->vq_ring.desc[avail_idx].len; VQUEUE_IDLE(vq); return (len); } /************************************************************************** * Helper Functions * **************************************************************************/ /** * * vq_ring_add_buffer * */ static uint16_t vq_ring_add_buffer(struct virtqueue *vq, struct vring_desc *desc, uint16_t head_idx, struct llist *buffer, int readable, int writable) { struct vring_desc *dp; int i, needed; uint16_t idx; needed = readable + writable; for (i = 0, idx = head_idx; (i < needed && buffer != VQ_NULL); i++, idx = dp->next, buffer = buffer->next) { VQASSERT(vq, idx != VQ_RING_DESC_CHAIN_END, "premature end of free desc chain"); dp = &desc[idx]; dp->addr = env_map_vatopa(buffer->data); dp->len = buffer->attr; dp->flags = 0; if (i < needed - 1) dp->flags |= VRING_DESC_F_NEXT; /* Readable buffers are inserted into vring before the writable buffers. */ if (i >= readable) dp->flags |= VRING_DESC_F_WRITE; } return (idx); } /** * * vq_ring_free_chain * */ static void vq_ring_free_chain(struct virtqueue *vq, uint16_t desc_idx) { struct vring_desc *dp; struct vq_desc_extra *dxp; VQ_RING_ASSERT_VALID_IDX(vq, desc_idx); dp = &vq->vq_ring.desc[desc_idx]; dxp = &vq->vq_descx[desc_idx]; if (vq->vq_free_cnt == 0) VQ_RING_ASSERT_CHAIN_TERM(vq); vq->vq_free_cnt += dxp->ndescs; dxp->ndescs--; if ((dp->flags & VRING_DESC_F_INDIRECT) == 0) { while (dp->flags & VRING_DESC_F_NEXT) { VQ_RING_ASSERT_VALID_IDX(vq, dp->next); dp = &vq->vq_ring.desc[dp->next]; dxp->ndescs--; } } VQASSERT(vq, (dxp->ndescs == 0), "failed to free entire desc chain, remaining"); /* * We must append the existing free chain, if any, to the end of * newly freed chain. If the virtqueue was completely used, then * head would be VQ_RING_DESC_CHAIN_END (ASSERTed above). */ dp->next = vq->vq_desc_head_idx; vq->vq_desc_head_idx = desc_idx; } /** * * vq_ring_init * */ static void vq_ring_init(struct virtqueue *vq) { struct vring *vr; unsigned char *ring_mem; int i, size; ring_mem = vq->vq_ring_mem; size = vq->vq_nentries; vr = &vq->vq_ring; vring_init(vr, size, ring_mem, vq->vq_alignment); for (i = 0; i < size - 1; i++) vr->desc[i].next = i + 1; vr->desc[i].next = VQ_RING_DESC_CHAIN_END; } /** * * vq_ring_update_avail * */ static void vq_ring_update_avail(struct virtqueue *vq, uint16_t desc_idx) { uint16_t avail_idx; /* * Place the head of the descriptor chain into the next slot and make * it usable to the host. The chain is made available now rather than * deferring to virtqueue_notify() in the hopes that if the host is * currently running on another CPU, we can keep it processing the new * descriptor. */ avail_idx = vq->vq_ring.avail->idx & (vq->vq_nentries - 1); vq->vq_ring.avail->ring[avail_idx] = desc_idx; env_wmb(); vq->vq_ring.avail->idx++; /* Keep pending count until virtqueue_notify(). */ vq->vq_queued_cnt++; } /** * * vq_ring_enable_interrupt * */ static int vq_ring_enable_interrupt(struct virtqueue *vq, uint16_t ndesc) { /* * Enable interrupts, making sure we get the latest index of * what's already been consumed. */ if (vq->vq_flags & VIRTQUEUE_FLAG_EVENT_IDX) { vring_used_event(&vq->vq_ring) = vq->vq_used_cons_idx + ndesc; } else { vq->vq_ring.avail->flags &= ~VRING_AVAIL_F_NO_INTERRUPT; } env_mb(); /* * Enough items may have already been consumed to meet our threshold * since we last checked. Let our caller know so it processes the new * entries. */ if (virtqueue_nused(vq) > ndesc) { return (1); } return (0); } /** * * virtqueue_interrupt * */ void virtqueue_notification(struct virtqueue *vq) { if (vq->callback != VQ_NULL) vq->callback(vq); } /** * * vq_ring_must_notify_host * */ static int vq_ring_must_notify_host(struct virtqueue *vq) { uint16_t new_idx, prev_idx, event_idx; if (vq->vq_flags & VIRTQUEUE_FLAG_EVENT_IDX) { new_idx = vq->vq_ring.avail->idx; prev_idx = new_idx - vq->vq_queued_cnt; event_idx = vring_avail_event(&vq->vq_ring); return (vring_need_event(event_idx, new_idx, prev_idx) != 0); } return ((vq->vq_ring.used->flags & VRING_USED_F_NO_NOTIFY) == 0); } /** * * vq_ring_notify_host * */ static void vq_ring_notify_host(struct virtqueue *vq) { if (vq->notify != VQ_NULL) vq->notify(vq); } /** * * virtqueue_nused * */ static int virtqueue_nused(struct virtqueue *vq) { uint16_t used_idx, nused; used_idx = vq->vq_ring.used->idx; nused = (uint16_t) (used_idx - vq->vq_used_cons_idx); VQASSERT(vq, nused <= vq->vq_nentries, "used more than available"); return (nused); }