Rewrap README.md and add link to mailing list.
[processor-sdk/open-amp.git] / README.md
index f57cda2ef90dd070fc49bd0dca46f1fcc9d1c756..8497c0b99913c4f9c61a07bd556bd277314762f3 100644 (file)
--- a/README.md
+++ b/README.md
@@ -1,2 +1,31 @@
 open-amp
 ========
+This repository is the home for the Open Asymmetric Multi Processing (OpenAMP)
+framework project. The OpenAMP framework provides software components that
+enable development of software applications for Asymmetric Multiprocessing
+(AMP) systems. The framework provides the following key capabilities.
+
+1. Provides Life Cycle Management, and Inter Processor Communication
+   capabilities for management of remote compute resources and their associated
+   software contexts
+2. Provides a stand alone library usable with RTOS and Baremetal software
+   environments
+3. Compatibility with upstream Linux remoteproc and rpmsg components
+4. Following AMP configurations supported
+       a. Linux master/Baremetal remote
+       b. Baremetal master/Linux remote
+5. Proxy infrastructure and supplied demos showcase ability of proxy on master
+   to handle printf, scanf, open, close, read, write calls from Bare metal
+   based remote contexts.
+
+Following are the known limitations:
+
+1. In rpc_demo.c(the remote demonstration application that showcases usage of
+   rpmsg retargetting infrastructure),  the bindings for the flag input
+   parameter in open() system call has been redefined. The GCC tool library
+   bindings for this input argument is different between arm-xilinx/none-eabi, and
+   arm-linux-eabi toolchains. For this reason, redefinition is required for
+   compatibility with proxy on Linux master.
+
+For using the framework please refer to the documents present in the /docs folder.
+Subscribe to the open-amp mailing list at https://groups.google.com/group/open-amp.