diff --git a/README.md b/README.md
index 3910ba580e1b9a95dc30c55518d880a424a65927..efad7ef3b4b4e7480aaed441620e66da731f8edf 100644 (file)
--- a/README.md
+++ b/README.md
1. Provides Life Cycle Management, and Inter Processor Communication
capabilities for management of remote compute resources and their associated
- software contexts
+ software contexts.
2. Provides a stand alone library usable with RTOS and Baremetal software
environments
3. Compatibility with upstream Linux remoteproc and rpmsg components
```
|- lib/
| |- common/ # common helper functions
-| |- virtio/ # virtio implemnetation
+| |- virtio/ # virtio implementation
| |- rpmsg/ # rpmsg implementation
| |- remoteproc/ # remoteproc implementation
| | |- drivers # remoteproc drivers
| |- proxy/ # implement one processor access device on the
| | # other processor with file operations
-| |- system/ # os specific implementation
-| | | |- generic/ # E.g. generic system (that is baremetal)
-| | | | |- machine/ # machine specific implmentation for the system
-| |- include/ # header files
-| | |- machine/ # machine specific header files
-| | |- system/ # system specific header files
-|- apps/ # demontrastion/testing applicaitons
+|- apps/ # demonstration/testing applications
| |- machine/ # common files for machine can be shared by applications
| # It is up to each app to decide whether to use these files.
-| |- system/ # common files for system can be shared by applicaitons
+| |- system/ # common files for system can be shared by applications
| # It is up to each app to decide whether to use these files.
|- obsolete # It is used to build libs which may also required when
| # building the apps. It will be removed in future since
|- cmake # CMake files
```
-OpenAMP library libopen_amp is composed of the following directorys in `lib/`:
+OpenAMP library libopen_amp is composed of the following directories in `lib/`:
* `common/`
* `virtio/`
* `rpmsg/`
* `remoteproc/`
* `proxy/`
-* `system/`
+
+OpenAMP system/machine support has been moved to libmetal, the system/machine
+layer in the `apps/` directory is for system application initialization, and
+resource table definition.
+
+### libmetal APIs used in OpenAMP
+Here are the libmetal APIs used by OpenAMP, if you want to port OpenAMP for your
+system, you will need to implement the following libmetal APIs in the libmetal's
+`lib/system/<SYS>` directory:
+* alloc, for memory allocation and memory free
+* cache, for flushing cache and invalidating cache
+* io, for memory mapping. OpenAMP required memory mapping in order to access
+ vrings and carved out memory.
+* irq, for IRQ handler registration, IRQ disable/enable and global IRQ handling.
+* mutex
+* shmem (For RTOS, you can usually use the implementation from
+ `lib/system/generic/`)
+* sleep, at the moment, OpenAMP only requires microseconds sleep as when OpenAMP
+ fails to get a buffer to send messages, it will call this function to sleep and
+ then try again.
+* time, for timestamp
+* init, for libmetal initialization.
+* atomic
+
+Please refer to `lib/system/generic` when you port libmetal for your system.
+
+If you a different compiler to GNU gcc, please refer to `lib/compiler/gcc/` to
+port libmetal for your compiler. At the moment, OpenAMP needs the atomic
+operations defined in `lib/compiler/gcc/atomic.h`.
## OpenAMP Compilation
-OpenAMP uses CMake for library and demonstration applicaiton compilation.
+OpenAMP uses CMake for library and demonstration application compilation.
+OpenAMP requires libmetal library. For now, you will need to download and
+compile libmetal library separately before you compiling OpenAMP library.
+In future, we will try to make libmetal as a submodule to OpenAMP to make this
+flow easier.
-### Example to compile Zynq MP SoC R5 generic(baremetal) remote:
-```
-$ mkdir build
-$ cd build/
-$ cmake ../open-amp -DCMAKE_TOOLCHAIN_FILE=zynqmp_r5_generic -DWITH_OBSOLETE=ON -DWITH_APPS=ON
-$ make DESTDIR=$(pwd) install
-```
-The OpenAMP library will be generated to `build/usr/local/lib` directory, headers will be generated to
-`build/usr/local/include` directory, and the applications executables will be generated to
-`build/usr/local/bin` directory.
+### Example to compile OpenAMP for communication between Linux processes:
+* Install libsysfs devel and libhugetlbfs devel packages on your Linux host.
+* build libmetal library on your host as follows:
-* `-DWITH_OBSOLETE=ON` is to build the `libxil.a`.
-* `-DWITH_APPS=ON` is to build the demonstration applications.
+ ```
+ $ mkdir -p build-libmetal
+ $ cd build-libmetal
+ $ cmake <libmetal_source>
+ $ make VERBOSE=1 DESTDIR=<libmetal_install> install
+ ```
-### Example to compile Zynq A9 remote:
-```
-$ mkdir build
-$ cd build/
-$ cmake ../open-amp -DCMAKE_TOOLCHAIN_FILE=zynq7_generic -DWITH_OBSOLETE=on -DWITH_APPS=ON
-$ make DESTDIR=$(pwd) install
-```
+* build OpenAMP library on your host as follows:
+
+ $ mkdir -p build-openamp
+ $ cd build-openamp
+ $ cmake <openamp_source> -DCMAKE_INCLUDE_PATH=<libmetal_built_include_dir> \
+ -DCMAKE_LIBRARY_PATH=<libmetal_built_lib_dir> [-DWITH_APPS=ON]
+ $ make VERBOSE=1 DESTDIR=$(pwd) install
+
+The OpenAMP library will be generated to `build/usr/local/lib` directory,
+headers will be generated to `build/usr/local/include` directory, and the
+applications executable will be generated to `build/usr/local/bin`
+directory.
+* cmake option `-DWITH_APPS=ON` is to build the demonstration applications.
+
+### Example to compile Zynq UltraScale+ MPSoC R5 generic(baremetal) remote:
+* build libmetal library on your host as follows:
+ * Create your on cmake toolchain file to compile libmetal for your generic
+ (baremetal) platform. Here is the example of the toolchain file:
+
+ ```
+ set (CMAKE_SYSTEM_PROCESSOR "arm" CACHE STRING "")
+ set (MACHINE "zynqmp_r5" CACHE STRING "")
+
+ set (CROSS_PREFIX "armr5-none-eabi-" CACHE STRING "")
+ set (CMAKE_C_FLAGS "-mfloat-abi=soft -mcpu=cortex-r5 -Wall -Werror -Wextra \
+ -flto -Os -I/ws/xsdk/r5_0_bsp/psu_cortexr5_0/include" CACHE STRING "")
+
+ SET(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -flto")
+ SET(CMAKE_AR "gcc-ar" CACHE STRING "")
+ SET(CMAKE_C_ARCHIVE_CREATE "<CMAKE_AR> qcs <TARGET> <LINK_FLAGS> <OBJECTS>")
+ SET(CMAKE_C_ARCHIVE_FINISH true)
+
+ include (cross-generic-gcc)
+ ```
+
+ * Compile libmetal library:
+
+ ```
+ $ mkdir -p build-libmetal
+ $ cd build-libmetal
+ $ cmake <libmetal_source> -DCMAKE_TOOLCHAIN_FILE=<toolchain_file>
+ $ make VERBOSE=1 DESTDIR=<libmetal_install> install
+ ```
+
+* build OpenAMP library on your host as follows:
+ * Create your on cmake toolchain file to compile openamp for your generic
+ (baremetal) platform. Here is the example of the toolchain file:
+ ```
+ set (CMAKE_SYSTEM_PROCESSOR "arm" CACHE STRING "")
+ set (MACHINE "zynqmp_r5" CACHE STRING "")
+ set (CROSS_PREFIX "armr5-none-eabi-" CACHE STRING "")
+ set (CMAKE_C_FLAGS "-mfloat-abi=soft -mcpu=cortex-r5 -Os -flto \
+ -I/ws/libmetal-r5-generic/usr/local/include \
+ -I/ws/xsdk/r5_0_bsp/psu_cortexr5_0/include" CACHE STRING "")
+ set (CMAKE_ASM_FLAGS "-mfloat-abi=soft -mcpu=cortex-r5" CACHE STRING "")
+ set (PLATFORM_LIB_DEPS "-lxil -lc -lm" CACHE STRING "")
+ SET(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -flto")
+ SET(CMAKE_AR "gcc-ar" CACHE STRING "")
+ SET(CMAKE_C_ARCHIVE_CREATE "<CMAKE_AR> qcs <TARGET> <LINK_FLAGS> <OBJECTS>")
+ SET(CMAKE_C_ARCHIVE_FINISH true)
+ set (CMAKE_FIND_ROOT_PATH /ws/libmetal-r5-generic/usr/local/lib \
+ /ws/xsdk/r5_bsp/psu_cortexr5_0/lib )
+
+ include (cross_generic_gcc)
+ ```
+
+ * We use cmake `find_path` and `find_library` to check if libmetal includes
+ and libmetal library is in the includes and library search paths. However,
+ for non-linux system, it doesn't work with `CMAKE_INCLUDE_PATH` and
+ `CMAKE_LIBRARY_PATH` variables, and thus, we need to specify those paths
+ in the toolchain file with `CMAKE_C_FLAGS` and `CMAKE_FIND_ROOT_PATH`.
+* Compile the OpenAMP library:
+
+ ```
+ $ mkdir -p build-openamp
+ $ cd build-openamp
+ $ cmake <openamp_source> -DCMAKE_TOOLCHAIN_FILE=<toolchain_file>
+ $ make VERBOSE=1 DESTDIR=$(pwd) install
+ ```
+
+The OpenAMP library will be generated to `build/usr/local/lib` directory,
+headers will be generated to `build/usr/local/include` directory, and the
+applications executable will be generated to `build/usr/local/bin`
+directory.
+
+* `-DWITH_APPS=ON` is to build the demonstration applications.
+ If you have used `-DWITH_APPS=ON` to build the demos, you can try them on
+ your Linux host as follows:
+
+ ```
+ # Start echo test server to wait for message to echo
+ $ sudo LD_LIBRARY_PATH=<openamp_built>/usr/local/lib:<libmetal_built>/usr/local/lib \
+ build/usr/local/bin/echo_testd-shared
+ # Run echo test to send message to echo test server
+ $ sudo LD_LIBRARY_PATH=<openamp_built>/usr/local/lib:<libmetal_built>/usr/local/lib \
+ build/usr/local/bin/echo_test-shared 1
+ ```
+
+### Example to compile OpenAMP Linux Userspace for Zynq UltraScale+ MPSoC
+We can use yocto to build the OpenAMP Linux userspace library and application.
+open-amp and libmetal recipes are in this yocto layer:
+https://github.com/OpenAMP/meta-openamp
+* Add the `meta-openamp` layer to your layers in your yocto build project's `bblayers.conf` file.
+* Add `libmetal` and `open-amp` to your packages list. E.g. add `libmetal` and `open-amp` to the
+ `IMAGE_INSTALL_append` in the `local.conf` file.
+* You can also add OpenAMP demos Linux applications packages to your yocto packages list. OpenAMP
+ demo examples recipes are also in `meta-openamp`:
+ https://github.com/OpenAMP/meta-openamp/tree/master/recipes-openamp/openamp-examples
+
+In order to user OpenAMP(RPMsg) in Linux userspace, you will need to have put the IPI device,
+ vring memory and shared buffer memory to your Linux kernel device tree. The device tree example
+ can be found here:
+ https://github.com/OpenAMP/open-amp/blob/master/apps/machine/zynqmp/openamp-linux-userspace.dtsi
## Supported System and Machines
For now, it supports:
* Zynq generic slave
-* Zynq generic master
-* ZynqMP R5 generic slave
+* Zynq UltraScale+ MPSoC R5 generic slave
+* Linux host OpenAMP between Linux userspace processes
+* Linux userspace OpenAMP RPMsg master
+* Linux userspace OpenAMP RPMsg slave
## Known Limitations:
-1. In rpc_demo.c(the remote demonstration application that showcases usage of
- rpmsg retargetting infrastructure), the bindings for the flag input
- parameter in open() system call has been redefined. The GCC tool library
- bindings for this input argument is different between arm-xilinx/none-eabi, and
- arm-linux-eabi toolchains. For this reason, redefinition is required for
- compatibility with proxy on Linux master.
-
-For using the framework please refer to the documents present in the /docs folder.
+1. OpenAMP framework supports OpenAMP firmware running as master, however,
+ the example to show this ability is not ready yet.
+2. In case of OpenAMP on Linux userspace for inter processors communication,
+ life cycle management with remoteproc is not supported yet, that is for now,
+ it is not able to load the remote firmware with OpenAMP running on Linux
+ userspace.
+3. In case of OpenAMP on Linux userspace for inter processors communication,
+ it only supports static vrings and shared buffers.
+4. `sudo` is required to run the OpenAMP demos between Linux processes, as
+ it doesn't work on some systems if you are normal users.
+
+For using the framework please refer to the wiki of the OpenAMP repo.
Subscribe to the open-amp mailing list at https://groups.google.com/group/open-amp.