index 792c10a78a835aae28935851e2f0ad998fb4d706..ced4eef662e170e032c79123c992a8b0de4ad131 100644 (file)
#include "openamp/env.h"
#include "openamp/hil.h"
#include "metal/sys.h"
+#include "metal/alloc.h"
+#include "metal/sleep.h"
/**
* remoteproc_resource_init
*
* @param rsc_info - pointer to resource table info control
* block
- * @param pdata - platform data for remote processor
+ * @param proc - pointer to the hil_proc
* @param channel_created - callback function for channel creation
* @param channel_destroyed - callback function for channel deletion
* @param default_cb - default callback for channel I/O
* @param rproc_handle - pointer to new remoteproc instance
+ * @param rpmsg_role - 1 for rpmsg master, or 0 for rpmsg slave
*
* @param returns - status of function execution
*
*/
int remoteproc_resource_init(struct rsc_table_info *rsc_info,
- void *pdata,
+ struct hil_proc *proc,
rpmsg_chnl_cb_t channel_created,
rpmsg_chnl_cb_t channel_destroyed,
rpmsg_rx_cb_t default_cb,
- struct remote_proc **rproc_handle)
+ struct remote_proc **rproc_handle,
+ int rpmsg_role)
{
struct remote_proc *rproc;
int status;
+ int remote_rpmsg_role;
- if (!rsc_info) {
+ if (!rsc_info || !proc) {
return RPROC_ERR_PARAM;
}
- rproc = env_allocate_memory(sizeof(struct remote_proc));
+ rproc = metal_allocate_memory(sizeof(struct remote_proc));
if (rproc) {
memset(rproc, 0x00, sizeof(struct remote_proc));
/* There can be only one master for remote configuration so use the
* rsvd cpu id for creating hil proc */
- rproc->proc = hil_create_proc(pdata, HIL_RSVD_CPU_ID);
- if (rproc->proc) {
+ rproc->proc = proc;
+ status = hil_init_proc(proc);
+ if (!status) {
/* Parse resource table */
status =
handle_rsc_table(rproc, rsc_info->rsc_tab,
if (status == RPROC_SUCCESS) {
/* Initialize RPMSG "messaging" component */
*rproc_handle = rproc;
+ remote_rpmsg_role = (rpmsg_role == RPMSG_MASTER?
+ RPMSG_REMOTE : RPMSG_MASTER);
status =
- rpmsg_init(NULL, rproc->proc->cpu_id,
+ rpmsg_init(proc,
&rproc->rdev, channel_created,
channel_destroyed, default_cb,
- RPMSG_MASTER);
+ remote_rpmsg_role);
} else {
status = RPROC_ERR_NO_RSC_TABLE;
}
} else {
- status = RPROC_ERR_CPU_ID;
+ status = RPROC_ERR_CPU_INIT;
}
} else {
status = RPROC_ERR_NO_MEM;
int remoteproc_resource_deinit(struct remote_proc *rproc)
{
- int i = 0;
- struct proc_vring *vring_hw = 0;
if (rproc) {
if (rproc->rdev) {
- /* disable IPC interrupts */
- if (rproc->proc->ops->reg_ipi_after_deinit) {
- for (i = 0; i < 2; i++) {
- vring_hw =
- &rproc->proc->vdev.vring_info[i];
- rproc->proc->ops->
- reg_ipi_after_deinit(vring_hw);
- }
- }
rpmsg_deinit(rproc->rdev);
}
if (rproc->proc) {
hil_delete_proc(rproc->proc);
+ rproc->proc = NULL;
}
-
- env_free_memory(rproc);
+ metal_free_memory(rproc);
}
- metal_finish();
-
- /*
- * Flush and Invalidate the caches - When the application is built with
- * Xilinx Standalone BSP, caches are invalidated as part of boot process.
- * Even if the master boots firmware multiple times without hard reset on
- * same core, caches are flushed and invalidated at the end of
- * remoteproc_resource_deinit for this run and caches would be again
- * invalidated before starting the main thread of the application on next
- * run to avoid any cache inconsistencies.
- */
- env_flush_invalidate_all_caches();
-
-
return RPROC_SUCCESS;
}
* remoteproc master applications are allowed to call this function.
*
* @param fw_name - name of frimware
- * @param pdata - platform data for remote processor
+ * @param proc - pointer to hil_proc
* @param channel_created - callback function for channel creation
* @param channel_destroyed - callback function for channel deletion
* @param default_cb - default callback for channel I/O
* @param returns - status of function execution
*
*/
-int remoteproc_init(char *fw_name, void *pdata,
+int remoteproc_init(char *fw_name, struct hil_proc *proc,
rpmsg_chnl_cb_t channel_created,
rpmsg_chnl_cb_t channel_destroyed, rpmsg_rx_cb_t default_cb,
struct remote_proc **rproc_handle)
struct remote_proc *rproc;
struct resource_table *rsc_table;
- unsigned int fw_addr, fw_size, rsc_size;
- int status, cpu_id;
+ unsigned int fw_size, rsc_size;
+ uintptr_t fw_addr;
+ int status;
if (!fw_name) {
return RPROC_ERR_PARAM;
}
- rproc = env_allocate_memory(sizeof(struct remote_proc));
+ rproc = metal_allocate_memory(sizeof(struct remote_proc));
if (rproc) {
memset((void *)rproc, 0x00, sizeof(struct remote_proc));
- /* Get CPU ID for the given firmware name */
- cpu_id = hil_get_cpuforfw(fw_name);
- if (cpu_id >= 0) {
- /* Create proc instance */
- rproc->proc = hil_create_proc(pdata, cpu_id);
- if (rproc->proc) {
- /* Retrieve firmware attributes */
- status =
- hil_get_firmware(fw_name, &fw_addr,
- &fw_size);
- if (!status) {
- /* Initialize ELF loader - currently only ELF format is supported */
- rproc->loader =
- remoteproc_loader_init(ELF_LOADER);
- if (rproc->loader) {
- /* Attach the given firmware with the ELF parser/loader */
- status =
- remoteproc_loader_attach_firmware
- (rproc->loader,
- (void *)fw_addr);
- } else {
- status = RPROC_ERR_LOADER;
- }
+ /* Create proc instance */
+ status = hil_init_proc(proc);
+ if (!status) {
+ /* Retrieve firmware attributes */
+ status =
+ hil_get_firmware(fw_name, &fw_addr,
+ &fw_size);
+ if (!status) {
+ /* Initialize ELF loader - currently only ELF format is supported */
+ rproc->loader =
+ remoteproc_loader_init(ELF_LOADER);
+ if (rproc->loader) {
+ /* Attach the given firmware with the ELF parser/loader */
+ status =
+ remoteproc_loader_attach_firmware
+ (rproc->loader,
+ (void *)fw_addr);
+ } else {
+ status = RPROC_ERR_LOADER;
}
- } else {
- status = RPROC_ERR_NO_MEM;
}
} else {
- status = RPROC_ERR_INVLD_FW;
+ status = RPROC_ERR_CPU_INIT;
}
} else {
status = RPROC_ERR_NO_MEM;
hil_delete_proc(rproc->proc);
rproc->proc = RPROC_NULL;
}
- env_free_memory(rproc);
+ metal_free_memory(rproc);
}
- metal_finish();
-
return RPROC_SUCCESS;
}
if (load_addr != RPROC_ERR_PTR) {
/* Start the remote cpu */
status = hil_boot_cpu(rproc->proc,
- (unsigned int)load_addr);
+ (uintptr_t)load_addr);
if (status == RPROC_SUCCESS) {
/* Wait for remote side to come up. This delay is arbitrary and may
* need adjustment for different configuration of remote systems */
- env_sleep_msec(RPROC_BOOT_DELAY);
+ metal_sleep_usec(RPROC_BOOT_DELAY);
/* Initialize RPMSG "messaging" component */
configuration only. */
#if defined (OPENAMP_REMOTE_LINUX_ENABLE)
status =
- rpmsg_init(NULL, rproc->proc->cpu_id,
+ rpmsg_init(rproc->proc,
&rproc->rdev,
rproc->channel_created,
rproc->channel_destroyed,
rproc->default_cb, RPMSG_MASTER);
#else
status =
- rpmsg_init(NULL, rproc->proc->cpu_id,
+ rpmsg_init(rproc->proc,
&rproc->rdev,
rproc->channel_created,
rproc->channel_destroyed,
{
if (rproc) {
+ if (rproc->proc) {
+ hil_shutdown_cpu(rproc->proc);
+ }
if (rproc->rdev) {
rpmsg_deinit(rproc->rdev);
rproc->rdev = RPROC_NULL;
- }
- if (rproc->proc) {
- hil_shutdown_cpu(rproc->proc);
+ rproc->proc = RPROC_NULL;
}
}