index 03c1fe4687c619f7002188e6cefd5dc5adb84ff1..9ddfa93c0edb0718e3d254ef5e68a3de23c1492a 100644 (file)
*
**************************************************************************/
+#include <string.h>
#include "openamp/rpmsg.h"
+#include "openamp/remoteproc.h"
+#include "metal/utilities.h"
+#include "metal/alloc.h"
+#include "metal/atomic.h"
+#include "metal/cpu.h"
/* Macro to initialize vring HW info */
#define INIT_VRING_ALLOC_INFO(ring_info,vring_hw) \
- (ring_info).phy_addr = (vring_hw).phy_addr; \
+ (ring_info).vaddr = (vring_hw).vaddr; \
(ring_info).align = (vring_hw).align; \
(ring_info).num_descs = (vring_hw).num_descs
* This function creates and initializes the remote device. The remote device
* encapsulates virtio device.
*
+ * @param proc - pointer to hil_proc
* @param rdev - pointer to newly created remote device
- * @param dev-id - ID of device to create , remote cpu id
* @param role - role of the other device, Master or Remote
* @param channel_created - callback function for channel creation
* @param channel_destroyed - callback function for channel deletion
* @return - status of function execution
*
*/
-int rpmsg_rdev_init(struct remote_device **rdev, int dev_id, int role,
+int rpmsg_rdev_init(struct hil_proc *proc,
+ struct remote_device **rdev, int role,
rpmsg_chnl_cb_t channel_created,
rpmsg_chnl_cb_t channel_destroyed, rpmsg_rx_cb_t default_cb)
{
struct remote_device *rdev_loc;
struct virtio_device *virt_dev;
- struct hil_proc *proc;
struct proc_shm *shm;
int status;
+ if (!proc)
+ return RPMSG_ERR_PARAM;
/* Initialize HIL data structures for given device */
- proc = hil_create_proc(dev_id);
-
- if (!proc) {
- return RPMSG_ERR_DEV_ID;
- }
+ if (hil_init_proc(proc))
+ return RPMSG_ERR_DEV_INIT;
/* Create software representation of remote processor. */
- rdev_loc =
- (struct remote_device *)
- env_allocate_memory(sizeof(struct remote_device));
+ rdev_loc = (struct remote_device *)metal_allocate_memory(sizeof(struct remote_device));
if (!rdev_loc) {
return RPMSG_ERR_NO_MEM;
}
- env_memset(rdev_loc, 0x00, sizeof(struct remote_device));
+ memset(rdev_loc, 0x00, sizeof(struct remote_device));
metal_mutex_init(&rdev_loc->lock);
rdev_loc->proc = proc;
}
}
+ if (!rpmsg_rdev_remote_ready(rdev_loc))
+ return RPMSG_ERR_DEV_INIT;
+
+ /* Initialize endpoints list */
+ metal_list_init(&rdev_loc->rp_endpoints);
+
/* Initialize channels for RPMSG Remote */
status = rpmsg_rdev_init_channels(rdev_loc);
*/
void rpmsg_rdev_deinit(struct remote_device *rdev)
{
- struct llist *rp_chnl_head, *rp_chnl_temp, *node;
+ struct metal_list *node;
struct rpmsg_channel *rp_chnl;
+ struct rpmsg_endpoint *rp_ept;
- rp_chnl_head = rdev->rp_channels;
- while (rp_chnl_head != RPMSG_NULL) {
-
- rp_chnl_temp = rp_chnl_head->next;
- rp_chnl = (struct rpmsg_channel *)rp_chnl_head->data;
+ while(!metal_list_is_empty(&rdev->rp_channels)) {
+ node = rdev->rp_channels.next;
+ rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
if (rdev->channel_destroyed) {
rdev->channel_destroyed(rp_chnl);
}
_rpmsg_delete_channel(rp_chnl);
- rp_chnl_head = rp_chnl_temp;
}
/* Delete name service endpoint */
-
metal_mutex_acquire(&rdev->lock);
- node = rpmsg_rdev_get_endpoint_from_addr(rdev, RPMSG_NS_EPT_ADDR);
+ rp_ept = rpmsg_rdev_get_endpoint_from_addr(rdev, RPMSG_NS_EPT_ADDR);
metal_mutex_release(&rdev->lock);
- if (node) {
- _destroy_endpoint(rdev, (struct rpmsg_endpoint *)node->data);
+ if (rp_ept) {
+ _destroy_endpoint(rdev, rp_ept);
}
if (rdev->rvq) {
rdev->proc = 0;
}
- env_free_memory(rdev);
+ metal_free_memory(rdev);
}
/**
- * rpmsg_rdev_get_chnl_node_from_id
+ * rpmsg_rdev_get_chnl_from_id
*
* This function returns channel node based on channel name. It must be called
* with mutex locked.
* @param stack - pointer to remote device
* @param rp_chnl_id - rpmsg channel name
*
- * @return - channel node
+ * @return - rpmsg channel
*
*/
-struct llist *rpmsg_rdev_get_chnl_node_from_id(struct remote_device *rdev,
+struct rpmsg_channel *rpmsg_rdev_get_chnl_from_id(struct remote_device *rdev,
char *rp_chnl_id)
{
struct rpmsg_channel *rp_chnl;
- struct llist *rp_chnl_head;
+ struct metal_list *node;
- rp_chnl_head = rdev->rp_channels;
-
- while (rp_chnl_head) {
- rp_chnl = (struct rpmsg_channel *)rp_chnl_head->data;
- if (env_strncmp
+ metal_list_for_each(&rdev->rp_channels, node) {
+ rp_chnl = metal_container_of(node, struct rpmsg_channel, node);
+ if (strncmp
(rp_chnl->name, rp_chnl_id, sizeof(rp_chnl->name))
== 0) {
- return rp_chnl_head;
+ return rp_chnl;
}
- rp_chnl_head = rp_chnl_head->next;
}
return RPMSG_NULL;
* @param rdev - pointer remote device control block
* @param addr - src address
*
- * @return - endpoint node
+ * @return - rpmsg endpoint
*
*/
-struct llist *rpmsg_rdev_get_endpoint_from_addr(struct remote_device *rdev,
+struct rpmsg_endpoint *rpmsg_rdev_get_endpoint_from_addr(struct remote_device *rdev,
unsigned long addr)
{
- struct llist *rp_ept_lut_head;
-
- rp_ept_lut_head = rdev->rp_endpoints;
+ struct rpmsg_endpoint *rp_ept;
+ struct metal_list *node;
- while (rp_ept_lut_head) {
- struct rpmsg_endpoint *rp_ept =
- (struct rpmsg_endpoint *)rp_ept_lut_head->data;
+ metal_list_for_each(&rdev->rp_endpoints, node) {
+ rp_ept = metal_container_of(node,
+ struct rpmsg_endpoint, node);
if (rp_ept->addr == addr) {
- return rp_ept_lut_head;
+ return rp_ept;
}
- rp_ept_lut_head = rp_ept_lut_head->next;
}
return RPMSG_NULL;
struct proc_chnl *chnl_info;
int num_chnls, idx;
+ metal_list_init(&rdev->rp_channels);
if (rdev->role == RPMSG_MASTER) {
chnl_info = hil_get_chnl_info(rdev->proc, &num_chnls);
return RPMSG_SUCCESS;
}
+/**
+ * check if the remote is ready to start RPMsg communication
+ */
+int rpmsg_rdev_remote_ready(struct remote_device *rdev)
+{
+ struct virtio_device *vdev = &rdev->virt_dev;
+ uint8_t status;
+ if (rdev->role == RPMSG_MASTER) {
+ while (1) {
+ /* Busy wait until the remote is ready */
+ status = vdev->func->get_status(vdev);
+ if (status & VIRTIO_CONFIG_STATUS_DRIVER_OK)
+ return true;
+ metal_cpu_yield();
+ }
+ } else {
+ return true;
+ }
+ /* Never come here */
+ return false;
+}
+
+static void rpmsg_memset_io(struct metal_io_region *io, void *dst, int c, size_t count)
+{
+ if ((io->mem_flags & METAL_IO_MAPPED)) {
+ metal_memset_io(dst, c, count);
+ } else {
+ memset(dst, c, count);
+ }
+}
+
/**
*------------------------------------------------------------------------
* The rest of the file implements the virtio device interface as defined
@@ -385,7 +418,7 @@ int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
struct virtqueue *vqs[RPMSG_MAX_VQ_PER_RDEV];
struct proc_vring *vring_table;
void *buffer;
- struct llist node;
+ struct metal_sg sg;
int idx, num_vrings, status;
(void)flags;
@@ -406,14 +439,14 @@ int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
INIT_VRING_ALLOC_INFO(ring_info, vring_table[idx]);
if (rdev->role == RPMSG_REMOTE) {
- env_memset((void *)ring_info.phy_addr, 0x00,
- vring_size(vring_table[idx].num_descs,
- vring_table[idx].align));
+ rpmsg_memset_io(vring_table[idx].io, (void *)ring_info.vaddr, 0x00,
+ vring_size(vring_table[idx].num_descs, vring_table[idx].align));
}
status =
virtqueue_create(dev, idx, (char *)names[idx], &ring_info,
callbacks[idx], hil_vring_notify,
+ rdev->proc->sh_buff.io,
&vqs[idx]);
if (status != RPMSG_SUCCESS) {
@@ -431,6 +464,8 @@ int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
}
if (rdev->role == RPMSG_REMOTE) {
+ sg.io = rdev->proc->sh_buff.io;
+ sg.len = RPMSG_BUFFER_SIZE;
for (idx = 0; ((idx < rdev->rvq->vq_nentries)
&& (idx < rdev->mem_pool->total_buffs / 2));
idx++) {
@@ -442,13 +477,11 @@ int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
return RPMSG_ERR_NO_BUFF;
}
- node.data = buffer;
- node.attr = RPMSG_BUFFER_SIZE;
- node.next = RPMSG_NULL;
+ sg.virt = buffer;
- env_memset(buffer, 0x00, RPMSG_BUFFER_SIZE);
+ rpmsg_memset_io(sg.io, buffer, 0x00, RPMSG_BUFFER_SIZE);
status =
- virtqueue_add_buffer(rdev->rvq, &node, 0, 1,
+ virtqueue_add_buffer(rdev->rvq, &sg, 0, 1,
buffer);
if (status != RPMSG_SUCCESS) {
@@ -462,14 +495,28 @@ int rpmsg_rdev_create_virtqueues(struct virtio_device *dev, int flags, int nvqs,
unsigned char rpmsg_rdev_get_status(struct virtio_device *dev)
{
- (void)dev;
- return 0;
+ struct hil_proc *proc = dev->device;
+ struct proc_vdev *pvdev = &proc->vdev;
+ struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
+
+ if (!vdev_rsc)
+ return -1;
+
+ return vdev_rsc->status;
}
void rpmsg_rdev_set_status(struct virtio_device *dev, unsigned char status)
{
- (void)dev;
- (void)status;
+ struct hil_proc *proc = dev->device;
+ struct proc_vdev *pvdev = &proc->vdev;
+ struct fw_rsc_vdev *vdev_rsc = pvdev->vdev_info;
+
+ if (!vdev_rsc)
+ return;
+
+ vdev_rsc->status = status;
+
+ atomic_thread_fence(memory_order_seq_cst);
}
uint32_t rpmsg_rdev_get_feature(struct virtio_device *dev)