summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 06b8349)
raw | patch | inline | side by side (parent: 06b8349)
author | Wendy Liang <jliang@xilinx.com> | |
Thu, 22 Sep 2016 06:34:36 +0000 (23:34 -0700) | ||
committer | Wendy Liang <jliang@xilinx.com> | |
Fri, 14 Oct 2016 00:05:35 +0000 (17:05 -0700) |
As remoteproc_plat has been removed, update the ZynqMP Linux
userspace apps helper functions not to use those APIs.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
userspace apps helper functions not to use those APIs.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
apps/machine/zynqmp/platform_info.c | patch | blob | history | |
apps/system/linux/machine/zynqmp/helper.c | patch | blob | history |
index 4c955bc091e23fb85c496e1beef6be9b7b94104b..e0c5f69ec68a69df1f7aab6b21604483eedcaf7b 100755 (executable)
**************************************************************************/
#include "openamp/hil.h"
-#include "openamp/remoteproc_plat.h"
#include "metal/atomic.h"
-#include "platform_info.h"
-#define IPI_CHN_BITMASK 0x00000100 /* IPI channel bit mask APU<->RPU0 */
-#define REMOTE_CPU_ID 0
+#define RPU_CPU_ID 0 /* RPU ID */
+#define IPI_CHN_BITMASK 0x00000100 /* IPI channel bit mask APU<->RPU0 */
+#define RPMSG_CHAN_NAME "rpmsg-openamp-demo-channel"
+#define DEV_BUS_NAME "platform"
+#define IPI_DEV_NAME "ff340000.ipi"
+#define VRING_DEV_NAME "3ed40000.vring"
+#define SHM_DEV_NAME "3ed80000.shm"
/* -- FIX ME: ipi info is to be defined -- */
struct ipi_info {
- uint32_t ipi_chn_mask;
- int need_reg;
- atomic_int sync;
+ const char *name;
+ const char *bus_name;
+ struct meta_device *dev;
+ struct metal_io_region *io;
+ metal_phys_addr_t paddr;
+ uint32_t ipi_chn_mask;
+ int need_reg;
+ atomic_int sync;
};
-/* Reference implementation that show cases platform_get_cpu_info and
- platform_get_for_firmware API implementation for Bare metal environment */
extern struct hil_platform_ops zynqmp_a53_r5_proc_ops;
static struct ipi_info chn_ipi_info[] = {
- { IPI_CHN_BITMASK, 1, 0},
- { IPI_CHN_BITMASK, 0, 0},
+ {IPI_DEV_NAME, DEV_BUS_NAME, NULL, NULL, 0, IPI_CHN_BITMASK, 1, 0},
+ {IPI_DEV_NAME, DEV_BUS_NAME, NULL, NULL, 0, IPI_CHN_BITMASK, 0, 0},
};
-struct rproc_info_plat_local proc_table = {
- {
- /* CPU ID of master */
- REMOTE_CPU_ID,
-
- /* HIL platform ops table. */
- &zynqmp_a53_r5_proc_ops,
- },
- /* vring0 ipi device and vring descriptors memory device */
- {
- PLAT_RSC_VRING,
- "platform",
- "ff340000.ipi",
- &chn_ipi_info[0],
- "platform",
- "3ed40000.vring",
- },
- /* vring0 ipi device and vring descriptors memory device */
- {
- PLAT_RSC_VRING,
- "platform",
- "ff340000.ipi",
- &chn_ipi_info[1],
- "platform",
- "3ed40000.vring",
- },
- /* Shared memory device */
- {
- PLAT_RSC_SHM,
- "shm",
- 0, /* UNDEFINED, up to the I/O region size */
- },
- /* Shared memory device */
- {
- PLAT_RSC_RPMSG_CHANNEL,
- "rpmsg-openamp-demo-channel",
- },
- PLAT_RSC_LAST,
-};
const struct firmware_info fw_table[] =
{
0}
};
-int fw_table_size = sizeof(fw_table)/sizeof(struct firmware_info);
+const int fw_table_size = sizeof(fw_table)/sizeof(struct firmware_info);
+
+struct hil_proc *platform_create_proc(int proc_index)
+{
+ (void) proc_index;
+ struct hil_proc *proc;
+ proc = hil_create_proc(&zynqmp_a53_r5_proc_ops, RPU_CPU_ID, NULL);
+ if (!proc)
+ return NULL;
+
+ /* Setup IPI info */
+ hil_set_ipi(proc, 0, (unsigned int)(-1), (void *)&chn_ipi_info[0]);
+ hil_set_ipi(proc, 1, (unsigned int)(-1), (void *)&chn_ipi_info[1]);
+ /* Setup vring info */
+ hil_set_vring(proc, 0, DEV_BUS_NAME, VRING_DEV_NAME);
+ hil_set_vring(proc, 1, DEV_BUS_NAME, VRING_DEV_NAME);
+ /* Setup shared memory info */
+ hil_set_shm (proc, DEV_BUS_NAME, SHM_DEV_NAME, 0, 0x40000);
+ /* Setup RPMSG channel info */
+ hil_set_rpmsg_channel(proc, 0, RPMSG_CHAN_NAME);
+ return proc;
+}
index b19894aa5d098be70807737e798eb4d866dcd191..589835a6dc95598db04297952150ea743300af88 100644 (file)
#include <string.h>
#include <stdio.h>
#include "metal/sys.h"
-#include "metal/shmem.h"
-#include "metal/device.h"
-#include "metal/io.h"
-
-#define SHM_DEV_NAME "3ed80000.shm"
-#define SHM_BUS_NAME "platform"
-
-static struct metal_device *shm_dev;
-static struct metal_generic_shmem shm;
void init_system()
{
- int ret;
- struct metal_io_region *io;
struct metal_init_params metal_param = METAL_INIT_DEFAULTS;
metal_init(&metal_param);
- /* Register the UIO shared memory */
- /* This will be a temporary solution, we should
- * use DMA memory in fugure.
- */
- ret = metal_device_open(SHM_BUS_NAME, SHM_DEV_NAME, &shm_dev);
- if (ret) {
- fprintf(stderr, "ERROR: Failed to open shared memory device.\n");
- return;
- }
- io = metal_device_io_region(shm_dev, 0);
- if (!io) {
- fprintf(stderr, "ERROR: Failed to get the I/O region of shared memory.\n");
- return;
- }
-
- memset(&shm, 0, sizeof(struct metal_generic_shmem));
- shm.name = "shm";
- memcpy((void *)&shm.io, io, sizeof(struct metal_io_region));
- ret = metal_shmem_register_generic(&shm);
- if (ret) {
- fprintf(stderr, "ERROR: Failed to registered shared memory.\n");
- return;
- }
return;
}
void cleanup_system()
{
- if (shm_dev)
- metal_device_close(shm_dev);
metal_finish();
}