summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: edb841c)
raw | patch | inline | side by side (from parent 1: edb841c)
author | Wendy Liang <jliang@xilinx.com> | |
Mon, 15 Aug 2016 22:39:56 +0000 (15:39 -0700) | ||
committer | Wendy Liang <jliang@xilinx.com> | |
Thu, 13 Oct 2016 05:01:48 +0000 (22:01 -0700) |
This application is to generate random 6*6 matrices, send them
to the remote, and wait for the result, and then it will check
if the result is as expected.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
to the remote, and wait for the result, and then it will check
if the result is as expected.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
apps/matrix_multiply/matrix_multiply.c | [new file with mode: 0644] | patch | blob |
diff --git a/apps/matrix_multiply/matrix_multiply.c b/apps/matrix_multiply/matrix_multiply.c
--- /dev/null
@@ -0,0 +1,240 @@
+/* This is a sample demonstration application that showcases usage of remoteproc
+and rpmsg APIs on the remote core. This application is meant to run on the remote CPU
+running baremetal code. This applicationr receives two matrices from the master,
+multiplies them and returns the result to the master core. */
+
+#include <stdio.h>
+#include <stdlib.h>
+#include <string.h>
+#include <time.h>
+#include <unistd.h>
+#include "openamp/open_amp.h"
+#include "rsc_table.h"
+#include "platform_info.h"
+
+#define MAX_SIZE 6
+#define NUM_MATRIX 2
+#define SHUTDOWN_MSG 0xEF56A55A
+
+#define raw_printf(format, ...) printf(format, ##__VA_ARGS__)
+#define LPRINTF(format, ...) raw_printf("CLIENT> " format, ##__VA_ARGS__)
+#define LPERROR(format, ...) LPRINTF("ERROR: " format, ##__VA_ARGS__)
+
+typedef struct _matrix {
+ unsigned int size;
+ unsigned int elements[MAX_SIZE][MAX_SIZE];
+} matrix;
+
+/* Internal functions */
+static void rpmsg_channel_created(struct rpmsg_channel *rp_chnl);
+static void rpmsg_channel_deleted(struct rpmsg_channel *rp_chnl);
+static void rpmsg_read_cb(struct rpmsg_channel *, void *, int, void *,
+ unsigned long);
+
+/* Globals */
+static struct rpmsg_channel *app_rp_chnl;
+static struct _matrix i_matrix[2];
+static struct _matrix e_matrix;
+static unsigned int result_returned = 0;
+static int err_cnt = 0;;
+static struct rpmsg_endpoint *rp_ept;
+static struct remote_proc *proc = NULL;
+static struct rsc_table_info rsc_info;
+extern const struct remote_resource_table resources;
+extern struct rproc_info_plat_local proc_table;
+
+/* External functions */
+extern void init_system();
+extern void cleanup_system();
+
+int __attribute__((weak)) _gettimeofday(struct timeval *tv,
+ void *tz)
+{
+ (void)tv;
+ (void)tz;
+ return 0;
+}
+
+static void matrix_print(struct _matrix *m)
+{
+ unsigned int i, j;
+
+ /* Generate two random matrices */
+ LPRINTF("Printing matrix... \n");
+
+ for (i = 0; i < m->size; ++i) {
+ for (j = 0; j < m->size; ++j)
+ raw_printf(" %u ", m->elements[i][j]);
+ raw_printf("\n");
+ }
+}
+
+static void generate_matrices(int num_matrices,
+ unsigned int matrix_size, void *p_data)
+{
+ unsigned int i, j, k;
+ struct _matrix *p_matrix = p_data;
+ unsigned long value;
+
+
+ for (i = 0; i < (unsigned int)num_matrices; i++) {
+ /* Initialize workload */
+ p_matrix[i].size = matrix_size;
+
+ //LPRINTF("Input matrix %d \n", i);
+ for (j = 0; j < matrix_size; j++) {
+ //printf("\n");
+ for (k = 0; k < matrix_size; k++) {
+
+ value = (rand() & 0x7F);
+ value = value % 10;
+ p_matrix[i].elements[j][k] = value;
+ //printf(" %u ", p_matrix[i].elements[j][k]);
+ }
+ }
+ //printf("\n");
+ }
+
+}
+
+static void matrix_multiply(const matrix * m, const matrix * n, matrix * r)
+{
+ unsigned int i, j, k;
+
+ memset(r, 0x0, sizeof(matrix));
+ r->size = m->size;
+
+ for (i = 0; i < m->size; ++i) {
+ for (j = 0; j < n->size; ++j) {
+ for (k = 0; k < r->size; ++k) {
+ r->elements[i][j] +=
+ m->elements[i][k] * n->elements[k][j];
+ }
+ }
+ }
+}
+
+/* Application entry point */
+int main()
+{
+ int shutdown_msg = SHUTDOWN_MSG;
+ int c;
+ int status = 0;
+
+ /* Initialize HW system components */
+ init_system();
+
+ rsc_info.rsc_tab = (struct resource_table *)&resources;
+ rsc_info.size = sizeof(resources);
+
+ LPRINTF("Compute thread unblocked ..\n");
+ LPRINTF("It will generate two random matrices.\n");
+ LPRINTF("Send to the remote and get the computation result back.\n");
+ LPRINTF("It will then check if the result is expected.\n");
+
+ /* Initialize RPMSG framework */
+ status =
+ remoteproc_resource_init(&rsc_info, &proc_table,
+ rpmsg_channel_created,
+ rpmsg_channel_deleted, rpmsg_read_cb,
+ &proc, 1);
+ if (status) {
+ LPERROR("Failed to initialize remoteproc resource.\n");
+ return -1;
+ }
+
+ LPRINTF("Remote proc resource initialized.\n");
+ while (!app_rp_chnl) {
+ hil_poll(proc->proc, 0);
+ }
+
+ LPRINTF("RPMSG channel has created.\n");
+ err_cnt = 0;
+ srand(time(NULL));
+ for (c = 0; c < 200; c++) {
+ generate_matrices(2, MAX_SIZE, i_matrix);
+ matrix_multiply(&i_matrix[0], &i_matrix[1],
+ &e_matrix);
+ result_returned = 0;
+ status = rpmsg_send(app_rp_chnl, i_matrix, sizeof(i_matrix));
+
+ if (status) {
+ LPRINTF("Error sending data...\n");
+ break;
+ }
+ LPRINTF("Matrix multiply: sent : %u\n", sizeof(i_matrix));
+ do {
+ hil_poll(proc->proc, 0);
+ } while (!result_returned && !err_cnt && app_rp_chnl);
+
+ if (err_cnt && !app_rp_chnl)
+ break;
+ }
+
+ if (app_rp_chnl) {
+ /* Send shutdown message to remote */
+ rpmsg_send(app_rp_chnl, &shutdown_msg, sizeof(int));
+ }
+ sleep(1);
+ LPRINTF("Quitting application .. Matrix multiplication end\n");
+
+ LPRINTF("**********************************\n");
+ LPRINTF(" Test Results: Error count = %d \n", err_cnt);
+ LPRINTF("**********************************\n");
+
+ remoteproc_resource_deinit(proc);
+ cleanup_system();
+
+ return 0;
+}
+
+static void rpmsg_channel_created(struct rpmsg_channel *rp_chnl)
+{
+ app_rp_chnl = rp_chnl;
+ rp_ept = rpmsg_create_ept(rp_chnl, rpmsg_read_cb, RPMSG_NULL,
+ RPMSG_ADDR_ANY);
+}
+
+static void rpmsg_channel_deleted(struct rpmsg_channel *rp_chnl)
+{
+ (void)rp_chnl;
+ rpmsg_destroy_ept(rp_ept);
+ LPRINTF("%s\n", __func__);
+ app_rp_chnl = NULL;
+ rp_ept = NULL;
+}
+
+static void rpmsg_read_cb(struct rpmsg_channel *rp_chnl, void *data, int len,
+ void *priv, unsigned long src)
+{
+ (void)rp_chnl;
+ (void)priv;
+ (void)src;
+ struct _matrix *r_matrix = (struct _matrix *)data;
+ int i, j;
+ if (len != sizeof(struct _matrix)) {
+ LPERROR("Received matrix is of invalid len: %d:%d\n",
+ (int)sizeof(struct _matrix), len);
+ err_cnt++;
+ return;
+ }
+ for (i = 0; i < MAX_SIZE; i++) {
+ for (j = 0; j < MAX_SIZE; j++) {
+ if (r_matrix->elements[i][j] !=
+ e_matrix.elements[i][j]) {
+ err_cnt++;
+ break;
+ }
+ }
+ }
+ if (err_cnt) {
+ LPERROR("Result mismatched...\n");
+ LPERROR("Expected matrix:\n");
+ matrix_print(&e_matrix);
+ LPERROR("Actual matrix:\n");
+ matrix_print(r_matrix);
+ } else {
+ result_returned = 1;
+ }
+}
+