summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: 93bf6ac)
raw | patch | inline | side by side (from parent 1: 93bf6ac)
author | Wendy Liang <jliang@xilinx.com> | |
Mon, 15 Aug 2016 22:32:30 +0000 (15:32 -0700) | ||
committer | Wendy Liang <jliang@xilinx.com> | |
Thu, 13 Oct 2016 05:01:48 +0000 (22:01 -0700) |
This driver is used to trigger IPI if application has
a message to send, or for applicaiton to morning the IPI
and vrings to see if there was message sent from the RPU
is available.
It polls the IPI ISR to see if the other side kicks the APU.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
a message to send, or for applicaiton to morning the IPI
and vrings to see if there was message sent from the RPU
is available.
It polls the IPI ISR to see if the other side kicks the APU.
Signed-off-by: Wendy Liang <jliang@xilinx.com>
lib/remoteproc/drivers/CMakeLists.txt | patch | blob | history | |
lib/remoteproc/drivers/zynqmp_remoteproc_r5.c | [new file with mode: 0644] | patch | blob |
index bc568f9844acafbcb1e143b6df65276e019817b0..8fe435847ef7cf54190de8a90003992266ee296e 100644 (file)
collect (PROJECT_LIB_SOURCES zynq_remoteproc_a9.c)
collect (PROJECT_LIB_SOURCES zynq_a9_trampoline.S)
endif ("${MACHINE}" STREQUAL "zynq7")
+
+if ("${MACHINE}" STREQUAL "zynqmp")
+ collect (PROJECT_LIB_SOURCES zynqmp_remoteproc_r5.c)
+endif ("${MACHINE}" STREQUAL "zynqmp")
diff --git a/lib/remoteproc/drivers/zynqmp_remoteproc_r5.c b/lib/remoteproc/drivers/zynqmp_remoteproc_r5.c
--- /dev/null
@@ -0,0 +1,201 @@
+/*
+ * Copyright (c) 2014, Mentor Graphics Corporation
+ * All rights reserved.
+ * Copyright (c) 2015 Xilinx, Inc.
+ *
+ * Redistribution and use in source and binary forms, with or without
+ * modification, are permitted provided that the following conditions are met:
+ *
+ * 1. Redistributions of source code must retain the above copyright notice,
+ * this list of conditions and the following disclaimer.
+ * 2. Redistributions in binary form must reproduce the above copyright notice,
+ * this list of conditions and the following disclaimer in the documentation
+ * and/or other materials provided with the distribution.
+ * 3. Neither the name of Mentor Graphics Corporation nor the names of its
+ * contributors may be used to endorse or promote products derived from this
+ * software without specific prior written permission.
+ *
+ * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
+ * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
+ * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
+ * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
+ * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
+ * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
+ * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
+ * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
+ * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
+ * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
+ * POSSIBILITY OF SUCH DAMAGE.
+ */
+
+/**************************************************************************
+ * FILE NAME
+ *
+ * zynqmp_remoteproc_r5.c
+ *
+ * DESCRIPTION
+ *
+ * This file is the Implementation of IPC hardware layer interface
+ * for Xilinx Zynq UltraScale+ MPSoC system.
+ *
+ **************************************************************************/
+
+#include <errno.h>
+#include <string.h>
+#include <stdio.h>
+#include "metal/io.h"
+#include "metal/device.h"
+#include "metal/utilities.h"
+#include "metal/atomic.h"
+#include "metal/irq.h"
+#include "metal/cpu.h"
+#include "metal/alloc.h"
+#include "openamp/hil.h"
+#include "openamp/remoteproc_plat.h"
+#include "openamp/virtqueue.h"
+
+/* IPI REGs OFFSET */
+#define IPI_TRIG_OFFSET 0x00000000 /** IPI trigger register offset */
+#define IPI_OBS_OFFSET 0x00000004 /** IPI observation register offset */
+#define IPI_ISR_OFFSET 0x00000010 /* IPI interrupt status register offset */
+#define IPI_IMR_OFFSET 0x00000014 /* IPI interrupt mask register offset */
+#define IPI_IER_OFFSET 0x00000018 /* IPI interrupt enable register offset */
+#define IPI_IDR_OFFSET 0x0000001C /* IPI interrupt disable register offset */
+
+#define _rproc_wait() metal_cpu_yield()
+
+#define DEBUG 1
+
+/* -- FIX ME: ipi info is to be defined -- */
+struct ipi_info {
+ uint32_t ipi_chn_mask;
+ int need_reg;
+ atomic_int sync;
+};
+
+/*--------------------------- Declare Functions ------------------------ */
+static int _enable_interrupt(struct proc_vring *vring_hw);
+static void _notify(int cpu_id, struct proc_intr *intr_info);
+static int _boot_cpu(int cpu_id, unsigned int load_addr);
+static void _shutdown_cpu(int cpu_id);
+static int _poll(struct hil_proc *proc, int nonblock);
+static struct hil_proc *_initialize(void *pdata, int cpu_id);
+static void _release(struct hil_proc *proc);
+
+/*--------------------------- Globals ---------------------------------- */
+struct hil_platform_ops zynqmp_a53_r5_proc_ops = {
+ .enable_interrupt = _enable_interrupt,
+ .notify = _notify,
+ .boot_cpu = _boot_cpu,
+ .shutdown_cpu = _shutdown_cpu,
+ .poll = _poll,
+ .initialize = _initialize,
+ .release = _release,
+};
+
+static int _enable_interrupt(struct proc_vring *vring_hw)
+{
+ (void)vring_hw;
+ return 0;
+}
+
+static void _notify(int cpu_id, struct proc_intr *intr_info)
+{
+
+ (void)cpu_id;
+ struct ipi_info *ipi = (struct ipi_info *)(intr_info->data);
+ if (ipi == NULL)
+ return;
+
+ /* Trigger IPI */
+ metal_io_write32(intr_info->io, IPI_TRIG_OFFSET, ipi->ipi_chn_mask);
+}
+
+static int _boot_cpu(int cpu_id, unsigned int load_addr)
+{
+ (void)cpu_id;
+ (void)load_addr;
+ return -1;
+}
+
+static void _shutdown_cpu(int cpu_id)
+{
+ (void)cpu_id;
+ return;
+}
+
+static int _poll(struct hil_proc *proc, int nonblock)
+{
+ struct proc_vring *vring;
+ struct ipi_info *ipi;
+ struct metal_io_region *io;
+
+ vring = &proc->vdev.vring_info[0];
+ ipi = (struct ipi_info *)(vring->intr_info.data);
+ io = vring->intr_info.io;
+ while(1) {
+ unsigned int ipi_intr_status =
+ (unsigned int)metal_io_read32(io, IPI_ISR_OFFSET);
+ if (ipi_intr_status & ipi->ipi_chn_mask) {
+ metal_io_write32(io, IPI_ISR_OFFSET,
+ ipi->ipi_chn_mask);
+ virtqueue_notification(vring->vq);
+ return 0;
+ } else if (nonblock) {
+ return -EAGAIN;
+ }
+ _rproc_wait();
+ }
+}
+
+static struct hil_proc * _initialize(void *pdata, int cpu_id)
+{
+ (void) cpu_id;
+
+ struct hil_proc *proc;
+ int ret;
+ struct metal_io_region *io;
+ struct proc_intr *intr_info;
+ struct ipi_info *ipi;
+ unsigned int ipi_intr_status;
+
+ /* Allocate memory for proc instance */
+ proc = metal_allocate_memory(sizeof(struct hil_proc));
+ if (!proc) {
+ openamp_dbg("failed to allocate hil_proc mem\n");
+ return NULL;
+ }
+ memset(proc, 0, sizeof(struct hil_proc));
+
+ ret = rproc_init_plat_data(pdata, proc);
+ if (ret) {
+ openamp_dbg("failed to allocate hil_proc mem\n");
+ goto error;
+ }
+ intr_info = &(proc->vdev.vring_info[0].intr_info);
+ io = intr_info->io;
+ ipi = (struct ipi_info *)(intr_info->data);
+ ipi_intr_status =
+ (unsigned int)metal_io_read32(io, IPI_ISR_OFFSET);
+ if (ipi_intr_status & ipi->ipi_chn_mask) {
+ metal_io_write32(io, IPI_ISR_OFFSET, ipi->ipi_chn_mask);
+ }
+ metal_io_write32(io, IPI_IDR_OFFSET, ipi->ipi_chn_mask);
+ atomic_store(&ipi->sync, 1);
+ return proc;
+error:
+ if (proc) {
+ rproc_close_plat(proc);
+ metal_free_memory(proc);
+ }
+ return NULL;
+}
+
+static void _release(struct hil_proc *proc)
+{
+ if (proc) {
+ rproc_close_plat(proc);
+ metal_free_memory(proc);
+ }
+}
+