Add zynqMP APU to RPU remoteproc driver
authorWendy Liang <jliang@xilinx.com>
Mon, 15 Aug 2016 22:32:30 +0000 (15:32 -0700)
committerWendy Liang <jliang@xilinx.com>
Thu, 13 Oct 2016 05:01:48 +0000 (22:01 -0700)
This driver is used to trigger IPI if application has
a message to send, or for applicaiton to morning the IPI
and vrings to see if there was message sent from the RPU
is available.

It polls the IPI ISR to see if the other side kicks the APU.

Signed-off-by: Wendy Liang <jliang@xilinx.com>

No differences found