Rewrap README.md and add link to mailing list.
authorCyril Chemparathy <cyril.chemparathy@xilinx.com>
Tue, 8 Sep 2015 22:35:11 +0000 (15:35 -0700)
committerCyril Chemparathy <cyril.chemparathy@xilinx.com>
Tue, 8 Sep 2015 22:35:11 +0000 (15:35 -0700)
This commit rewraps the README.md content to fit within 80 columns (for
most sane editors :)).  We also add a link pointing visitors to the
mailing list hosted on googlegroups.  Please subscribe!

README.md

index 08f8cbd5ac609358369ca202939ce05209973f62..8497c0b99913c4f9c61a07bd556bd277314762f3 100644 (file)
--- a/README.md
+++ b/README.md
@@ -1,18 +1,31 @@
 open-amp
 ========
-This repository is the home for the Open Asymmetric Multi Processing (OpenAMP) framework project. The OpenAMP framework provides software components that enable development of software applications for Asymmetric Multiprocessing (AMP) systems. The framework provides the following key capabilities. 
+This repository is the home for the Open Asymmetric Multi Processing (OpenAMP)
+framework project. The OpenAMP framework provides software components that
+enable development of software applications for Asymmetric Multiprocessing
+(AMP) systems. The framework provides the following key capabilities.
 
-1. Provides Life Cycle Management, and Inter Processor Communication capabilities for management of remote compute resources and their associated software contexts   
-2. Provides a stand alone library usable with RTOS and Baremetal software environments 
+1. Provides Life Cycle Management, and Inter Processor Communication
+   capabilities for management of remote compute resources and their associated
+   software contexts
+2. Provides a stand alone library usable with RTOS and Baremetal software
+   environments
 3. Compatibility with upstream Linux remoteproc and rpmsg components
 4. Following AMP configurations supported
        a. Linux master/Baremetal remote
        b. Baremetal master/Linux remote
-5. Proxy infrastructure and supplied demos showcase ability of proxy on master to handle printf, scanf, open, close, read, write calls from Bare metal based remote contexts.
+5. Proxy infrastructure and supplied demos showcase ability of proxy on master
+   to handle printf, scanf, open, close, read, write calls from Bare metal
+   based remote contexts.
 
 Following are the known limitations:
 
-1. In rpc_demo.c(the remote demonstration application that showcases usage of rpmsg retargetting infrastructure),  the bindings for the flag input parameter in open() system call has been redefined. The GCC tool library bindings for this input argument is different between arm-xilinx/none-eabi, and arm-linux-eabi toolchains. For this reason, redefinition is required for compatibility with proxy on Linux master.
-
+1. In rpc_demo.c(the remote demonstration application that showcases usage of
+   rpmsg retargetting infrastructure),  the bindings for the flag input
+   parameter in open() system call has been redefined. The GCC tool library
+   bindings for this input argument is different between arm-xilinx/none-eabi, and
+   arm-linux-eabi toolchains. For this reason, redefinition is required for
+   compatibility with proxy on Linux master.
 
 For using the framework please refer to the documents present in the /docs folder.
+Subscribe to the open-amp mailing list at https://groups.google.com/group/open-amp.