3 module Settings
4 {
5 /*! This is the EMAC Version */
6 config string emaclldVersionString = "01.00.03.13";
8 /*! This variable is to control the device type selection.
9 * By default this variable is set to NULL.
10 *
11 * To use EMAC for the selected device, add the following lines to config
12 * file and set the socType correctly:
13 *
14 * var emacSettings = xdc.useModule ('ti.drv.emac.Settings');
15 * emacSettings.socType = "k2g";
16 *
17 */
18 metaonly config string socType = "";
19 /*! This flag is used to indicate whether or not the benchmarking code
20 * (defined in the profilingHooks class) will be used in the project.
21 * Note that a separate library has been compiled and will be used
22 * ($NAME).profiling.a($SUFFIX). This is set in the *.cfg file.
23 */
24 config Bool enableProfiling = false;
25 /*! This variable is to control the device library type selection.
26 * By default this variable is set to release.
27 *
28 * To use CSL to use the debug/release library, add the following lines to config
29 * file and set the library profile accordingly:
30 *
31 * var Uart Settings = xdc.useModule ('ti.Uart.Settings');
32 * UartSettings.libProfile = "debug";
33 *
34 */
35 metaonly config string libProfile = "release";
36 }