[processor-sdk/pdk.git] / packages / ti / drv / sciclient / soc / sysfw / binaries / system-firmware-public-documentation / _sources / 1_intro / TISCI.rst.txt
1 .. _pub_sysfw_introduction:
3 Introduction
4 ============
6 Traditional Texas Instruments SoCs implement system control functions such as
7 power management on each of the processing units (ARM/DSP etc).
8 However, the traditional approach had tremendous challenges
9 to ensure system stability. A few of the challenges include:
11 - Complex interactions between Operating Systems on heterogeneous SoCs for
12 generic features.
13 - Lack of centralized knowledge of system state.
14 - Complex implementation challenges with regards to implementation of
15 workarounds for system quirks.
16 - Equivalent system capability entitlement on all variations of operation
17 conditions.
19 K3 devices introduces the concept of a centralized Power, Resource and Security
20 Management to allow mitigating the challenges of the traditional approach to
21 system control.
23 |sysfw| is a collective term used to describe the TI Foundational Security (TIFS)
24 and Resource Management (RM)/ Power Management (PM) services.
26 |sysfw| executes on the Security Manager and Device Manager Core.
27 On K3 devices, the DMSC subsystem is the Security Manager Core in the SoC.
28 The Device Manager core can be on the DMSC itself or the MCU R5F.
29 The choice of whether this runs on the DMSC or the
30 MCU R5F is based on the kind of applications the device is targeting.
31 If the device is targetting applications, where there is a need for a dedicated
32 HSM, the Device manager core is independent of the DMSC (which is exclusively
33 kept for Security functions). For devices which do not have need for a dedicated
34 security island or HSM, the device manager runs on the DMSC.
36 The following table highlights the variations
37 of where the RM and PM execute versus the TIFS on the different K3 family of
38 devices.
40 .. _pub_sysfw_map_per_device:
42 .. table:: TI Foundational Security Software and RM/PM SCI Server Mapping
44 +----------------+-------------------------+-------------------------+---------------------+
45 | Device | TI Foundation Security | 3rd Party HSM/SHE stack | RM/PM SCI Server |
46 +================+=========================+=========================+=====================+
47 | AM65x/ DRA80x, | DMSC (M3 based) | NA | DMSC (M3 based) |
48 | AM64x | | | |
49 +----------------+-------------------------+-------------------------+---------------------+
50 | DRA82X, TDA4X | DMSC (M3 based) | DMSC (M3 based) | Library on MCU R5* |
51 | | | | |
52 +----------------+-------------------------+-------------------------+---------------------+
55 Note, the TI provided software does not allow for a given SoC to support both HSM and non
56 HSM applications. To know the mapping refer :ref:`pub_sysfw_map_per_device`.
58 The purpose of this document is to define the software interface for
59 the |sysfw|. The split up of the responsibilities are:
61 - TIFS:
62 - Responsible for Centralized Foundational Security Management. These
63 include functions like authenticated boot, JTAG unlock etc.
64 - Behaves like a forwarding agent for Resource Management and Power Management
65 requests made by Secure hosts (other CPUs) in the SoC.
66 - Behaves as a forwarding agent for Resource Management and Power Management
67 responses from the device manager to the Secure Hosts.
68 - Firewall Management for resources requested by both secure and non-secure
69 hosts.
70 - Device Manager (DMSC M3 or MCU R5F based on the device)
71 - Responsible for servicing resource management and power management messages
72 from secure and non-secure hosts.
73 - Reponsible for forwarding non-secure host requests to set the processor
74 boot control or firewall configuration for safety applications to the DMSC.
75 - Responsible for forwaring response recieved from the DMSC to non-secure
76 hosts for the above forwarded messages.
78 Centralized Device Management
79 -----------------------------
81 In the Power management domain, the centralized power management takes into account that every device has:
83 - Different power and clock domains.
84 - Derivatives have slight differences in the clocking architecture based on combination of modules.
86 It provides an OS agnostic interface for power management allowing peripherals and clocks to be
87 handled by multiple processors running different OSes (Linux, RTOS, etc.). The centralized power
88 management entity aims to provide the same control for power and clock setting across all OSes.
90 Centralized Resource management is driven by the centralized DMA architecture. Key components
91 of the centralized resource management include:
93 - Navigator Subsystem: Collection of Data movement components
94 - UDMA (Unified DMA), PKTDMA, BCDMA: DMA engine for standard parallel DMA (CBA) or PSI/stream based IP.
95 - RA (Ring Accelerator): Queue management providing abstract SW view to HW DMA queues
96 - Proxy: Allows efficient access to RA queues, also enables address containment/virtualization (access RA via separate MMU page / regions)
97 - Interrupt & events handling: Interrupt aggregators and Interrupt routers
99 Centralized Foundational Security Management
100 --------------------------------------------
102 The DMSC M3 subsystem in the K3 family of devices is responsible to run the software stack for
103 the device foundational security management. This software entity is responsible for:
105 - Foundational device security in DMSC
107 - Secure boot with secure keys/root-of-trust, Security configuration and Debug unlock
108 - RSA or ECC Root Keys, AES symmetric key
109 - Utilizes PKA, SHA2 and AES Crypto accelerators
110 - Basic security functionality to extend root of trust (optional)
111 - Authenticated Key ring to extend root-of-trust keys
112 - SYSFW and Bootloader Rollback protection via eFuse
113 - Device Unique Key / Key Derivation to support 3P stacks
115 The centralized power, resource and security management entity is henceforth
116 refered to as System Control Entity and System Firmware interchangeably.
117 Any software and hardware entity which communicates with the System Control
118 Entity is refered to as "Host".
119 The block diagram of the System Controller Entity or System firmware is as below:
121 .. figure:: ../img/blockDiagram.png
123 System Controller Entity interacting with Other Hosts
125 Architecture Change between SDK 7.0 and SDK 7.1
126 -------------------------------------------------
128 The SDK 7.1 (v2020.08 of |sysfw|) firmware is not compatible with SDK 7.0.
129 (v2020.04 of the |sysfw|) and earlier releases in terms of location of the binaries.
130 Note the TISCI interface is the same as what is available on earlier releases.
132 The following figure describes the typical software stack and highlights the
133 difference in the location of execution of centralized services from |sysfw|.
135 .. figure:: ../img/softwareStack.png
137 DMSC Firmware Change | TDA4VM, DRA829, DRA821
139 Purpose of DMSC firmware change
141 - Secure HSM functions can run on a DMSC Security Island
142 - Free a main domain R5F for general customer use.
143 - Enables MCU Only mode with HSM functions on DMSC
144 - Lockstep Safety R5F runs safety critical PM & RM functions.
146 The Memory / CPU requirement is minimal (< 150 KB, < 10 MHz) so having the RM
147 and PM execute on the MCU R5f has minimal impact to user applications.
149 The SW impact summary for the end users is as given below. Kindly note since the
150 API interface remains the same, the rest of the documentation for |sysfw| is the
151 same between SDK 7.1 and 7.0. Refer to the SDK documentation to know more about
152 the changes required for integration of the SCISERVER and RM/PM on the MCU R5F.
154 .. figure:: ../img/swimpact.png
156 SW Impact for end-users between SDK 7.0 and SDK 7.1
158 Further Reading
159 ---------------
161 - In :ref:`pub_tisci_msg_doc`, we describe how one can communicate with the system control entity and the various messages that can be used.
162 - In :ref:`pub_boardcfg_messages_index`, we desribe the format and content of the boardcfg messages that does onetime configuration of |sysfw|.
163 - In :ref:`pub_interpret_trace`, we define trace data format.
164 - In :ref:`pub_soc_family_doc`, we provide information specific to each SOC that is required using the TISCI messages described in :ref:`pub_tisci_msg_doc`.
165 - In :ref:`pub_user_guides`, we provide user guides for the more complex scenarios.
167 Glossary
168 --------
170 The following list defines the different acronyms and terms used in the rest of the document:
172 - **TIFS** (Texas Instruments Foundational Security): Foundational security software provided from TI.
173 - **TISCI** (Texas Instruments System Controller Interface) : API interface to TIFS, RM/PM services.
174 - **DM** (Device Manager) : Collective term used to refer to the Resource Management and Power Management Software.
175 - **RM** (Resource Management): Term used to refer to the Resource Management Software.
176 - **PM** (Power Management): Term used to refer to the Power Management Software.
177 - **SYSFW** (System Firmware): Collective term used to refer to the TIFS and RM/PM Software.