1 /******************************************************************************
2 * FILE PURPOSE: Build description for the osal Driver
3 ******************************************************************************
4 * FILE NAME: package.bld
5 *
6 * DESCRIPTION:
7 * This file contains the build specification and description for the osal driver
8 *
9 * The file takes the following parameters from the command line through the
10 * XDCARGS variable.
11 * XDCARGS[0] = osal Driver Install Type
12 * Valid Values are "TAR" or "SETUP"
13 * DEFAULT is "SETUP"
14 *
15 * Example for a valid command:
16 * xdc XDCARGS="SETUP" release
17 *
18 * Copyright (C) 2014-2019, Texas Instruments, Inc.
19 *****************************************************************************/
21 /* List of all subdirectories that combine to make the osal Socket Driver Package. */
22 var subDirectories = [ "src", "docs", "arch", "soc", "test"];
24 var osalDriverInstallType;
26 /* Determine if we need to create the InstallJammer Application or not?
27 * osal LLD Deliverables be either of the following formats:
28 * - TAR Ball Package
29 * - Setup Executable
30 * DEFAULT is a SETUP Executable. */
32 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
33 osalDriverInstallType = "TAR";
34 else
35 osalDriverInstallType = arguments[0];
37 /* Irrespective of the InstallType we always create a TAR Ball Package as a part
38 * of the RTSC Build. Here we determine the name of the TAR Ball Package
39 * Format is as follows:
40 * osal_<version> */
41 var osalRTSCFileName = "osal" + "_" +
42 osalDriverReleaseVersion[0] + "_" + osalDriverReleaseVersion[1] + "_" +
43 osalDriverReleaseVersion[2] + "_" + osalDriverReleaseVersion[3];
45 var package_type = java.lang.System.getenv("PDK_PACKAGE_TYPE");
47 /******************************************************************
48 ************************ Release Banner **************************
49 ******************************************************************/
51 print ("************* osal Socket Driver Build Information *************");
52 print ("osal Socket Driver Install : " + osalDriverInstallType);
53 print ("osal Socket Driver LLD Version : " + osalDriverReleaseVersion);
54 print ("C66 Tools Directory : " + c66ToolsBaseDir);
55 print ("C67 Tools Directory : " + c674ToolsBaseDir);
56 print ("M4 Tools Directory : " + m4ToolsBaseDir);
57 print ("A15 Tools Directory : " + a15ToolsBaseDir);
58 print ("A9 Tools Directory : " + a9ToolsBaseDir);
59 print ("A8 Tools Directory : " + a8ToolsBaseDir);
60 print ("RTSC File Name : " + osalRTSCFileName);
61 print ("osal Socket Driver LLD Path : " + osalDriverPath);
62 if (pOpts == 1)
63 {
64 print ("CC LE opts : " + C66LE.ccOpts.prefix);
65 print ("CC BE opts : " + C66BE.ccOpts.prefix);
66 print ("M4 LE opts : " + M4LE.ccOpts.prefix);
67 print ("A15 basic opts : " + A15LE.ccOpts.prefix);
68 print ("A9 basic opts : " + A9LE.ccOpts.prefix);
69 print ("A8 basic opts : " + A8LE.ccOpts.prefix);
70 }
71 print ("****************************************************************");
73 /* Create the release package for the osal LLD */
74 Pkg.defaultRelease = Pkg.addRelease (osalRTSCFileName, {prefix: "./packages/"});
76 /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
77 * not supported in the XDC tools being used. Currenly builds need to be done with the
78 * following options:-
79 * xdc MK_FIXLISTOPTS=-t release
80 * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
81 * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
82 //Pkg.attrs = {archiver : "zip"};
84 if (package_type != "package_type_makefile")
85 {
86 /* Cycle through all the sub-directories and build all the files */
87 for (var i = 0; i < subDirectories.length; i++)
88 {
89 /* Load the capsule in the sub directory. */
90 var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
92 print ("Building directory " + subDirectories[i]);
94 /* Build the capsule. */
95 caps.modBuild();
97 /* Package the module.xs files for building via package */
98 Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
99 }
101 /* Package the remaining files */
102 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
103 Pkg.otherFiles[Pkg.otherFiles.length++] = "config_mk.bld";
104 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
105 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
106 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs";
107 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
108 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";
109 Pkg.otherFiles[Pkg.otherFiles.length++] = "SemaphoreP.h";
110 Pkg.otherFiles[Pkg.otherFiles.length++] = "MuxIntcP.h";
111 Pkg.otherFiles[Pkg.otherFiles.length++] = "CacheP.h";
112 Pkg.otherFiles[Pkg.otherFiles.length++] = "HwiP.h";
113 Pkg.otherFiles[Pkg.otherFiles.length++] = "SwiP.h";
114 Pkg.otherFiles[Pkg.otherFiles.length++] = "osal.h";
115 Pkg.otherFiles[Pkg.otherFiles.length++] = "osalver.h";
116 Pkg.otherFiles[Pkg.otherFiles.length++] = "osalver.h.xdt";
117 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
118 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt";
119 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
120 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
121 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_nonos_indp.mk";
122 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_nonos.mk";
123 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_tirtos_indp.mk";
124 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_tirtos.mk";
125 Pkg.otherFiles[Pkg.otherFiles.length++] = "src/src_common_nonos.mk";
126 Pkg.otherFiles[Pkg.otherFiles.length++] = "src/src_common_tirtos.mk";
127 Pkg.otherFiles[Pkg.otherFiles.length++] = "osal_component.mk";
128 Pkg.otherFiles[Pkg.otherFiles.length++] = "./lib";
130 /* Generate Users Manual Doxyfile */
131 var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
132 tplt.genFile("./docs/Doxyfile",osalDriverReleaseVersion);
133 }
135 /* Generate Settings.xdc */
136 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
137 tplt.genFile("./Settings.xdc",osalDriverReleaseVersion);
139 /* Generate paver.h */
140 var tplt = xdc.loadTemplate("./osalver.h.xdt");
141 tplt.genFile("./osalver.h",osalDriverReleaseVersion);