#******************************************************************************* #* FILE PURPOSE: Top level makefile for Creating Component Libraries and example #* binaries of PDK #******************************************************************************* #* FILE NAME: makefile #* #* DESCRIPTION: Builds the PDK Drivers & Examples #* #* #******************************************************************************* #* # (Mandatory) Specify where various tools are installed. .NOTPARALLEL: # This make file is not parallel in its highest level. This is done to serialize the multiple SOCS,BOARDS,CORES. # However the subsequent makefiles invoked by this makefile have parallelism supported. i.e -j option given to this # makefile will be passed on to the subsequent makefiles resulting in parallel builds. ifeq ($(RULES_MAKE), ) include $(PDK_INSTALL_PATH)/ti/build/Rules.make else include $(RULES_MAKE) endif ifndef MAKE export MAKE = make endif ifndef ECHO export ECHO = echo endif ifndef RM export RM = rm -f endif ifndef CP export CP = cp endif ifneq ($(LIMIT_SOCS),) SOC_LIST = $(LIMIT_SOCS) else SOC_LIST = $(SOC) endif ifneq ($(LIMIT_BOARDS),) BOARD_LIST = $(LIMIT_BOARDS) else BOARD_LIST = $(BOARD) endif ifneq ($(LIMIT_CORES),) # PRU cores are not built directly CORE_LIST = $(filter-out $(PRUCORE_LIST),$(LIMIT_CORES)) else CORE_LIST = $(CORE) endif .PHONY: all all_libs all_examples clean env_check help xdc_meta \ buildinfra_all buildinfra_clean buildinfra_pdk_examples \ non-buildinfra_all non-buildinfra_clean buildinfra_pdk_libs non-buildinfra_pdk_examples \ cplusplus_build # Default BUILD profile is release BUILD_PROFILE ?= release #The top level makefile two kinds of sub modules. Ones which are supported by the 'build infrastructure' and which are not. # i.e The modules which supports 'build infrastructure' are included in ti/build/component.mk and follow a standard set of conventions and targets. # They can be built using ti/build/makefile. Many newer targets such as AM3/4/5/6/7 have their modules in this category. # Those targets in this makefile has the 'buildinfra_' prefix in them. # The non-build infrastructure modules are the ones which do not adhere to the ti/build/component.mk . They have custom makefiles which are either RTSC generated or custom written makefiles with custom targets & build options. # Many legacy components for K1/K2 follow this methodology. # Those non-build infrastructure targets in this makefile has 'non-buildinfra_' prefix in them. ### Common targets for build infra and non-build infra all: env_check buildinfra_all non-buildinfra_all all_libs: env_check buildinfra_pdk_libs non-buildinfra_pdk_libs all_examples: env_check buildinfra_pdk_examples non-buildinfra_pdk_examples clean: env_check buildinfra_clean non-buildinfra_clean ### Targets which are built by build infrastructure (ti/build/makefile # The below builds for each SOC, its applicable BOARDS and CORES, filtered by the LIMIT_SOCS/BOARDS/CORES buildinfra_all buildinfra_pdk_libs buildinfra_pdk_examples buildinfra_clean : $(foreach current_soc, $(SOC_LIST),\ $(foreach current_board, $(filter $(BOARD_LIST),$(BOARD_LIST_$(current_soc)) ), \ $(foreach current_core, $(filter $(CORE_LIST),$(CORE_LIST_$(current_soc)) ), \ $(MAKE) -C $(PDK_INSTALL_PATH)/ti/build -f makefile $(subst buildinfra_,,$@) CORE=$(current_core) BOARD=$(current_board) SOC=$(current_soc) BUILD_PROFILE=$(BUILD_PROFILE);\ ))) # echo "$@ called with CORE=$(current_core) BOARD=$(current_board) SOC=$(current_soc) BUILD_PROFILE=$(BUILD_PROFILE)";\ ### Targets which are not built by build infrastructure, (eg legacy rtsc generated makefiles,custom makefiles non-buildinfra_all non-buildinfra_pdk_libs non-buildinfra_pdk_examples: $(MAKE) -C $(PDK_INSTALL_PATH)/ti/build -f makefile_non-buildinfra $(subst non-buildinfra_,,$@) PDK_SOC=$(PDK_SOC) ### Non library/example targets env_check: ifeq ($(PDK_SOC),) $(ECHO) "Warning !! PDK_SOC is not set!!! Please run 'help' and refer to 'Optional Arguments' in the help section" endif help: env_check $(ECHO) "------------------------------------------------------" $(ECHO) "\# Top level make help" $(ECHO) "------------------------------------------------------" $(ECHO) "make [OPTIONAL ARGUMENTS]" $(ECHO) "" $(ECHO) "------------------" $(ECHO) "TARGETS " $(ECHO) "------------------" $(ECHO) " all: Builds all modules (includes library & applications). Available modules are " $(ECHO) " Example: \"make all \"" $(ECHO) "" $(ECHO) " clean: Cleans libraries & applications of all modules. Available modules are " $(ECHO) " Example: \"make clean \"" $(ECHO) "" $(ECHO) " all_libs: Builds all pdk driver libraries" $(ECHO) " Example: \"make all_libs \"" $(ECHO) "" $(ECHO) " clean: Cleans libraries & applications of all modules." $(ECHO) " Example: \"make clean \"" $(ECHO) "" $(ECHO) " xdc_meta/xdc_meta: Generates xdc meta file (used if pdk is cloned from pdk.git)." $(ECHO) " Example: \"make xdc_meta \"" $(ECHO) "" $(ECHO) "------------------" $(ECHO) "OPTIONAL ARGUMENTS " $(ECHO) "------------------" $(ECHO) "LIMIT_SOCS= This will restrict the building of libraries/apps to the particular SOC(s) specified" $(ECHO) "Valid values of LIMIT_SOCS are $(LIMIT_SOCS)" $(ECHO) "" $(ECHO) "LIMIT_BOARDS= This will restrict the building of libraries/apps to the particular BOARD(s) specified" $(ECHO) "Valid values of LIMIT_BOARDS are $(LIMIT_BOARDS)" $(ECHO) "" $(ECHO) "LIMIT_CORES= This will restrict the building of libraries/apps to the particular CORE(s) specified" $(ECHO) "Valid values of LIMIT_CORES are $(LIMIT_CORES)" $(ECHO) "" $(ECHO) "PDK_SOC= This will specify the SOC version if the pdk directory does not specify it (if git clone pdk.git is used)" $(ECHO) "If pdk is git cloned, PDK_SOC should be set to the where the original PDK directory from the installer was pdk__)" $(ECHO) "For example if the original PDK installed directory (which got replaced by pdk.git) was /pdk_am65xx_1_0_5, PDK_SOC=am65xx" $(ECHO) "" $(ECHO) "BUILD_PROFILE= This will determine the type of libraries/examples generated (release/debug friendly). Default is 'release " $(ECHO) "Valid values of LIMIT_CORES are $(LIMIT_CORES)" $(ECHO) "" $(ECHO) "SOC= CORE= BOARD= This will build libraries/examples for the specified combination of " $(ECHO) "Valid values of SOC/BOARD/CORE are found from LIMIT_SOC/BOARD/CORES above" # if PDK.git is initiated from a fresh clone, the XDC meta headers will not have been generated. (xdc meta headers are used for CCS based projects) # These headers are usually generated during the procsdk installer building process ('make release' from within a component's directory) # This xdc_meta target will help enable the user to generate the same meta files after a fresh git clone of pdk # Find all the directories with package.xdc and run xdc_meta on them to generate the rtsc meta files PACKAGE_XDC_LOC := $(wildcard */package.xdc) PACKAGE_XDC_LOC += $(wildcard */*/package.xdc) PACKAGE_XDC_LOC += $(wildcard */*/*/package.xdc) PACKAGE_XDC_LOC += $(wildcard */*/*/*/package.xdc) SUBDIRS = $(filter-out ./,$(dir $(PACKAGE_XDC_LOC))) xdc_meta: $(foreach xdcdir, $(SUBDIRS),\ $(MAKE) -C $(xdcdir) $@; \ ) cplusplus_build: $(MAKE) all BUILD_PROFILE=debug CPLUSPLUS_BUILD=yes