/****************************************************************************** * FILE PURPOSE: Build configuration Script for the board library ****************************************************************************** * FILE NAME: config.bld * * DESCRIPTION: * This file contains the build configuration script for the board library * and is responsible for configuration of the paths for the various * tools required to build the library. * * Copyright (C) 2014-2015, Texas Instruments, Inc. *****************************************************************************/ /* Get the Tools Base directory from the Environment Variable. */ var c66ToolsBaseDir = java.lang.System.getenv("C6X_GEN_INSTALL_PATH"); var c674ToolsBaseDir = java.lang.System.getenv("C6X_GEN_INSTALL_PATH"); var m4ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_M4"); var a15ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A15"); var a9ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A9"); var arm9ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_ARM9"); var a8ToolsBaseDir = java.lang.System.getenv("TOOLCHAIN_PATH_A8"); /* Do not Print the Compiler Options */ var pOpts = 0; /* List of all devices that needs to be build via XDC * As the build happens through makefile, there is nothing to build via XDC * using the below for packaging infrastructure */ var socs = []; var devices = []; var buildArguments = []; var build_devices = []; Build.useTargets = null; Build.targets = [] var boards = [];