/* * Copyright (C) 2018-2020 Texas Instruments Incorporated - http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include #include #include #include #include #include #include #include #include #include #include #if defined(SBL_ENABLE_HLOS_BOOT) #if defined(SOC_J721E) || defined(SOC_AM65XX) const uint32_t gSciclient_boardCfgLow_hlos_rm[(SCICLIENT_BOARDCFG_RM_LINUX_SIZE_IN_BYTES+3U)/4U] __attribute__(( aligned(128), section(".boardcfg_data") )) = SCICLIENT_BOARDCFG_RM_LINUX; #endif #endif #ifdef __cplusplus #pragma DATA_SECTION(".firmware") #else #pragma WEAK (SBL_ReadSysfwImage) #pragma DATA_SECTION(gSciclient_firmware, ".firmware") #endif uint32_t gSciclient_firmware[1]; #if SCICLIENT_FIRMWARE_SIZE_IN_BYTES > SBL_SYSFW_MAX_SIZE #error "SYSFW too large...update SBL_SYSFW_MAX_SIZE" #endif #if defined(SOC_AM65XX) || defined(SOC_J721E) || defined(SOC_J7200) /* Firewall ID for MCU_FSS0_S0 */ #define MCU_FSS0_S0_FWID (1036) #define MCU_FSS0_S0_FW_REGIONS (8) #if (!defined(SBL_SKIP_BRD_CFG_PM)) || (!defined(SBL_SKIP_BRD_CFG_RM)) static int32_t Sciclient_setBoardConfigHeader (); #if defined (SOC_J721E) || defined (SOC_J7200) /** \brief Aligned address at which the X509 header is placed. */ #define SCISERVER_COMMON_X509_HEADER_ADDR (0x41cffb00U) /** \brief Aligned address at which the Board Config header is placed. */ #define SCISERVER_BOARDCONFIG_HEADER_ADDR (0x41c80000U) /** \brief Aligned address at which the Board Config is placed. */ #define SCISERVER_BOARDCONFIG_DATA_ADDR (0x41c80040U) #endif #endif #endif uint32_t SBL_IsAuthReq(void) { uint32_t retVal = SBL_ALWAYS_AUTH_APP; uint32_t dev_type; uint32_t dev_subtype; SBL_ADD_PROFILE_POINT; dev_type = CSL_REG32_RD(SBL_SYS_STATUS_REG) & SBL_SYS_STATUS_DEV_TYPE_MASK; dev_subtype = CSL_REG32_RD(SBL_SYS_STATUS_REG) & SBL_SYS_STATUS_DEV_SUBTYPE_MASK; /* No auth possible, if valid SMPK/BMPK is not present */ if ((dev_subtype == SBL_SYS_STATUS_DEV_SUBTYPE_FS) || (dev_type == SBL_SYS_STATUS_DEV_TYPE_GP) || (dev_type == SBL_SYS_STATUS_DEV_TYPE_TEST)) { retVal = SBL_NEVER_AUTH_APP; } SBL_ADD_PROFILE_POINT; return retVal; } #ifndef SBL_SKIP_SYSFW_INIT Sciclient_BoardCfgPrms_t sblBoardCfgPrms = {0}; Sciclient_BoardCfgPrms_t sblBoardCfgPmPrms = {0}; Sciclient_BoardCfgPrms_t sblBoardCfgRmPrms = {0}; #ifndef SBL_SKIP_BRD_CFG_SEC Sciclient_BoardCfgPrms_t sblBoardCfgSecPrms = {0}; #endif #endif void SBL_SciClientInit(void) { int32_t status = CSL_EFAIL; void *sysfw_ptr = gSciclient_firmware; #ifndef SBL_SKIP_SYSFW_INIT /* SYSFW board configurations */ Sciclient_DefaultBoardCfgInfo_t boardCfgInfo; Sciclient_ConfigPrms_t config = { SCICLIENT_SERVICE_OPERATION_MODE_POLLED, NULL, 1, 0, TRUE }; #endif SBL_ADD_PROFILE_POINT; status = SBL_ReadSysfwImage(&sysfw_ptr, SBL_SYSFW_MAX_SIZE); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW read...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } #ifndef SBL_SKIP_SYSFW_INIT SBL_ADD_PROFILE_POINT; status = Sciclient_getDefaultBoardCfgInfo(&boardCfgInfo); #if defined(SBL_ENABLE_HLOS_BOOT) #if defined(SOC_J721E) || defined(SOC_AM65XX) /* Replace default Sciclient boardCfgLowRm with alternate version for HLOS boot */ boardCfgInfo.boardCfgLowRm = &gSciclient_boardCfgLow_hlos_rm[0U]; boardCfgInfo.boardCfgLowRmSize = SCICLIENT_BOARDCFG_RM_LINUX_SIZE_IN_BYTES; #endif #endif if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW get default board config...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } status = Sciclient_loadFirmware((const uint32_t *) sysfw_ptr); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW load...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } SBL_ADD_PROFILE_POINT; status = Sciclient_init(&config); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW init ...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } #ifndef SBL_SKIP_BRD_CFG_BOARD SBL_ADD_PROFILE_POINT; sblBoardCfgPrms.boardConfigLow = (uint32_t)boardCfgInfo.boardCfgLow; sblBoardCfgPrms.boardConfigHigh = 0; sblBoardCfgPrms.boardConfigSize = boardCfgInfo.boardCfgLowSize; sblBoardCfgPrms.devGrp = SBL_DEVGRP; status = Sciclient_boardCfg(&sblBoardCfgPrms); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW board config ...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } #endif #ifndef SBL_SKIP_BRD_CFG_PM if (SBL_LOG_LEVEL > SBL_LOG_NONE) { SBL_ADD_PROFILE_POINT; UART_stdioDeInit(); } SBL_ADD_PROFILE_POINT; sblBoardCfgPmPrms.boardConfigLow = (uint32_t)boardCfgInfo.boardCfgLowPm; sblBoardCfgPmPrms.boardConfigHigh = 0; sblBoardCfgPmPrms.boardConfigSize = boardCfgInfo.boardCfgLowPmSize; sblBoardCfgPmPrms.devGrp = SBL_DEVGRP; status = Sciclient_boardCfgPm(&sblBoardCfgPmPrms); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW board config pm...FAILED \n") SblErrLoop(__FILE__, __LINE__); } if (SBL_LOG_LEVEL > SBL_LOG_NONE) { /* Re-init UART for logging */ UART_HwAttrs uart_cfg; SBL_ADD_PROFILE_POINT; UART_socGetInitCfg(BOARD_UART_INSTANCE, &uart_cfg); uart_cfg.frequency = SBL_SYSFW_UART_MODULE_INPUT_CLK; UART_socSetInitCfg(BOARD_UART_INSTANCE, &uart_cfg); UART_stdioInit(BOARD_UART_INSTANCE); } #endif #ifndef SBL_SKIP_BRD_CFG_RM SBL_ADD_PROFILE_POINT; sblBoardCfgRmPrms.boardConfigLow = (uint32_t)boardCfgInfo.boardCfgLowRm; sblBoardCfgRmPrms.boardConfigHigh = 0; sblBoardCfgRmPrms.boardConfigSize = boardCfgInfo.boardCfgLowRmSize; sblBoardCfgRmPrms.devGrp = SBL_DEVGRP; status = Sciclient_boardCfgRm(&sblBoardCfgRmPrms); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW board config rm...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } #endif #ifndef SBL_SKIP_BRD_CFG_SEC SBL_ADD_PROFILE_POINT; sblBoardCfgSecPrms.boardConfigLow = (uint32_t)boardCfgInfo.boardCfgLowSec; sblBoardCfgSecPrms.boardConfigHigh = 0; sblBoardCfgSecPrms.boardConfigSize = boardCfgInfo.boardCfgLowSecSize; sblBoardCfgSecPrms.devGrp = SBL_DEVGRP; status = Sciclient_boardCfgSec(&sblBoardCfgSecPrms); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"SYSFW board config sec...FAILED \n"); SblErrLoop(__FILE__, __LINE__); } #if defined(SOC_AM65XX) || defined(SOC_J721E) || defined(SOC_J7200) /* Secure ROM has left firewall regions for FSS DAT0 set. Disable them for DMA usage. */ uint16_t i; struct tisci_msg_fwl_set_firewall_region_resp respFwCtrl = {0}; struct tisci_msg_fwl_set_firewall_region_req reqFwCtrl = { .fwl_id = (uint16_t) MCU_FSS0_S0_FWID, .region = (uint16_t) 0, .n_permission_regs = (uint32_t) 3, /* Set .control to zero to disable the firewall region */ .control = (uint32_t) 0, .permissions[0] = (uint32_t) 0, .permissions[1] = (uint32_t) 0, .permissions[2] = (uint32_t) 0, .start_address = 0, .end_address = 0 }; for (i = 0; i < MCU_FSS0_S0_FW_REGIONS; i++) { reqFwCtrl.region = i; status = Sciclient_firewallSetRegion(&reqFwCtrl, &respFwCtrl, SCICLIENT_SERVICE_WAIT_FOREVER); if (status != CSL_PASS) { SBL_log(SBL_LOG_ERR,"MCU FSS0_S0 firewall region # %d disable...FAILED \n", i); } } #endif #endif /* Get SYSFW version */ SBL_ADD_PROFILE_POINT; if (SBL_LOG_LEVEL > SBL_LOG_ERR) { struct tisci_msg_version_req req = {0}; const Sciclient_ReqPrm_t reqPrm = { TISCI_MSG_VERSION, TISCI_MSG_FLAG_AOP, (const uint8_t *)&req, sizeof(req), SCICLIENT_SERVICE_WAIT_FOREVER }; struct tisci_msg_version_resp response; Sciclient_RespPrm_t respPrm = { 0, (uint8_t *) &response, (uint32_t)sizeof (response) }; status = Sciclient_service(&reqPrm, &respPrm); if (CSL_PASS == status) { if (respPrm.flags == (uint32_t)TISCI_MSG_FLAG_ACK) { SBL_ADD_PROFILE_POINT; SBL_log(SBL_LOG_MIN,"SYSFW ver: %s\n", (char *) response.str); } else { SBL_log(SBL_LOG_ERR,"SYSFW Get Version failed \n"); SblErrLoop(__FILE__, __LINE__); } } } #if (!defined(SBL_SKIP_BRD_CFG_PM)) || (!defined(SBL_SKIP_BRD_CFG_RM)) status = Sciclient_setBoardConfigHeader(); if (CSL_PASS == status) { SBL_log(SBL_LOG_MAX,"Sciclient_setBoardConfigHeader... PASSED\n"); } else { SBL_log(SBL_LOG_ERR,"Sciclient_setBoardConfigHeader... FAILED\n"); SblErrLoop(__FILE__, __LINE__); } #endif #if !defined(SBL_SKIP_MCU_RESET) /* RTI seems to be turned on by ROM. Turning it off so that Power domain can transition */ Sciclient_pmSetModuleState(SBL_DEV_ID_RTI0, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); Sciclient_pmSetModuleState(SBL_DEV_ID_RTI1, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); #if defined(SOC_AM64X) Sciclient_pmSetModuleState(SBL_DEV_ID_RTI8, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); Sciclient_pmSetModuleState(SBL_DEV_ID_RTI9, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); Sciclient_pmSetModuleState(SBL_DEV_ID_RTI10, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); Sciclient_pmSetModuleState(SBL_DEV_ID_RTI11, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); Sciclient_pmSetModuleState(SBL_DEV_ID_MCU_RTI0, TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF, TISCI_MSG_FLAG_AOP, SCICLIENT_SERVICE_WAIT_FOREVER); #endif #endif #endif SBL_ADD_PROFILE_POINT; } #if (!defined(SBL_SKIP_BRD_CFG_PM)) || (!defined(SBL_SKIP_BRD_CFG_RM)) static int32_t Sciclient_setBoardConfigHeader () { int32_t status = CSL_PASS; #if defined (SOC_J7200) || defined (SOC_J721E) //uint32_t alignedOffset = ((SCICLIENT_BOARDCFG_PM_SIZE_IN_BYTES + 128U)/128U)*128U; uint32_t alignedOffset = SCICLIENT_BOARDCFG_PM_SIZE_IN_BYTES; Sciclient_BoardCfgPrms_t boardCfgPrms_pm = { .boardConfigLow = (uint32_t)SCISERVER_BOARDCONFIG_DATA_ADDR, .boardConfigHigh = 0, .boardConfigSize = SCICLIENT_BOARDCFG_PM_SIZE_IN_BYTES, .devGrp = DEVGRP_ALL }; Sciclient_BoardCfgPrms_t boardCfgPrms_rm = { .boardConfigLow = (uint32_t) SCISERVER_BOARDCONFIG_DATA_ADDR + alignedOffset, .boardConfigHigh = 0, .boardConfigSize = SCICLIENT_BOARDCFG_RM_SIZE_IN_BYTES, .devGrp = DEVGRP_ALL }; status = Sciclient_boardCfgPrepHeader ( (uint8_t *) SCISERVER_COMMON_X509_HEADER_ADDR, (uint8_t *) SCISERVER_BOARDCONFIG_HEADER_ADDR, &boardCfgPrms_pm, &boardCfgPrms_rm); if (CSL_PASS == status) { SBL_log(SBL_LOG_MAX,"SCISERVER Board Configuration header population... "); SBL_log(SBL_LOG_MAX,"PASSED\n"); } else { SBL_log(SBL_LOG_MIN,"SCISERVER Board Configuration header population... "); SBL_log(SBL_LOG_MIN,"FAILED\n"); } memcpy((void *)boardCfgPrms_pm.boardConfigLow, (void *) sblBoardCfgPmPrms.boardConfigLow, SCICLIENT_BOARDCFG_PM_SIZE_IN_BYTES); memcpy((void *)boardCfgPrms_rm.boardConfigLow, (void *) sblBoardCfgRmPrms.boardConfigLow, SCICLIENT_BOARDCFG_RM_SIZE_IN_BYTES); #endif return status; } #endif