****************************************************************************** * FILE PURPOSE: Readme File for building the baremetal test/example ****************************************************************************** * FILE NAME: Readme.txt * Copyright (C) 2015, Texas Instruments, Inc. ***************************************************************************** The baremetal test/example makefile is located under ti/drv/gpio/test/, where is "c66" or armv7, the makefile builds both the test and example. To build baremetal test/example, run the following commands: cd ti/drv/gpio gmake -f test/baremetal//makefile DEVICE= where is "c66" or armv7, and is "K2H", "K2K", "K2E", "K2L", "C6678", "C6657". Notes: 1. Currently only K2 C66 baremetal test/example is supported 2. PDK need to be installed properly to include the board/osal libs 3. The following paths need to be set/exported properly to build the test/example: * PDK_INSTALL_PATH * CGTOOLS * TOOLCHAIN_PATH_A15 * CROSS_TOOL_PRFX E.g., in windows, run the following commands before calling the makefile: set PDK_INSTALL_PATH="C:/ti//packages" set CGTOOLS="C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.0.3" set TOOLCHAIN_PATH_A15="C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8-2014q3" set CROSS_TOOL_PRFX="arm-none-eabi-"