diff --git a/packages/makefile b/packages/makefile
index 6b5c9e4ccd1b70bdfd645c4265e5a0feaa31dd30..4bf86d979e319d138d4efa0021bb73098163a6f4 100755 (executable)
--- a/packages/makefile
+++ b/packages/makefile
#*******************************************************************************
-#* FILE PURPOSE: Top level makefile for Creating Component Libraries and example
+#* FILE PURPOSE: Top level makefile for Creating Component Libraries and example
#* binaries of PDK
#*******************************************************************************
#* FILE NAME: makefile
#*
-#* DESCRIPTION: Builds the PDK Drivers & Examples
+#* DESCRIPTION: Builds the PDK Drivers & Examples
#*
#*
#*******************************************************************************
.NOTPARALLEL:
# This make file is not parallel in its highest level. This is done to serialize the multiple SOCS,BOARDS,CORES.
# However the subsequent makefiles invoked by this makefile have parallelism supported. i.e -j option given to this
-# makefile will be passed on to the subsequent makefiles resulting in parallel builds.
+# makefile will be passed on to the subsequent makefiles resulting in parallel builds.
+
+#Default when PDK env script is not run
+PDK_INSTALL_PATH ?= $(abspath .)
+SDK_INSTALL_PATH ?= $(abspath ../../)
ifeq ($(RULES_MAKE), )
include $(PDK_INSTALL_PATH)/ti/build/Rules.make
else
CORE_LIST = $(CORE)
endif
-
+
.PHONY: all all_libs all_examples clean env_check help xdc_meta \
buildinfra_all buildinfra_clean buildinfra_pdk_examples \
non-buildinfra_all non-buildinfra_clean buildinfra_pdk_libs non-buildinfra_pdk_examples \
# Default BUILD profile is release
BUILD_PROFILE ?= release
#The top level makefile two kinds of sub modules. Ones which are supported by the 'build infrastructure' and which are not.
-# i.e The modules which supports 'build infrastructure' are included in ti/build/component.mk and follow a standard set of conventions and targets.
+# i.e The modules which supports 'build infrastructure' are included in ti/build/component.mk and follow a standard set of conventions and targets.
# They can be built using ti/build/makefile. Many newer targets such as AM3/4/5/6/7 have their modules in this category.
# Those targets in this makefile has the 'buildinfra_' prefix in them.
### Non library/example targets
env_check:
-ifeq ($(PDK_SOC),)
- $(ECHO) "Warning !! PDK_SOC is not set!!! Please run 'help' and refer to 'Optional Arguments' in the help section"
+ifneq ($(PDK_SOC),$(filter $(PDK_SOC), $(PROCSDK_SUPPORTED_PDK_SOCS)))
+ $(ECHO) "Warning !! PDK_SOC is not set properly!!!"
+ $(ECHO) "PDK_SOC should be set to any of the values: $(PROCSDK_SUPPORTED_PDK_SOCS)"
endif
help: env_check
$(ECHO) "PDK_SOC=<soc> This will specify the SOC version if the pdk directory does not specify it (if git clone pdk.git is used)"
$(ECHO) "If pdk is git cloned, PDK_SOC should be set to the <soc> where the original PDK directory from the installer was pdk_<soc>_<version>)"
$(ECHO) "For example if the original PDK installed directory (which got replaced by pdk.git) was <procsdk_install_dir>/pdk_am65xx_1_0_5, PDK_SOC=am65xx"
+ $(ECHO) " PDK_SOC should be set to any of the values: $(PROCSDK_SUPPORTED_PDK_SOCS)"
$(ECHO) ""
$(ECHO) "BUILD_PROFILE=<release/debug> This will determine the type of libraries/examples generated (release/debug friendly). Default is 'release "
$(ECHO) "Valid values of LIMIT_CORES are $(LIMIT_CORES)"
$(ECHO) ""
$(ECHO) "SOC=<soc> CORE=<core> BOARD=<board> This will build libraries/examples for the specified combination of <soc,core,board>"
$(ECHO) "Valid values of SOC/BOARD/CORE are found from LIMIT_SOC/BOARD/CORES above"
-
-
+
+
# if PDK.git is initiated from a fresh clone, the XDC meta headers will not have been generated. (xdc meta headers are used for CCS based projects)