index 19bb1490f07f544b9eab6655a3911d078aa73dca..d3f04e363cc55f8f3415f3572eb1cb48d2b5252b 100644 (file)
--- a/packages/pdksetupenv.bat
+++ b/packages/pdksetupenv.bat
@REM ******************************************************************************\r
@REM * FILE NAME: pdksetupenv.bat\r
@REM *\r
-@REM * DESCRIPTION: \r
+@REM * DESCRIPTION:\r
@REM * Configures and sets up the Build Environment for PDK.\r
@REM *\r
@REM * The batch file expects an optional argument:PDK_INSTALL_PATH: Location\r
@REM ********************** GET PARAMETERS PASSED THROUGH ARGUMENT ***************\r
@REM *******************************************************************************\r
@REM Parameter Validation: Check if the argument was passed to the batch file and\r
-@REM if so we use that else we default to the working directory where the batch \r
+@REM if so we use that else we default to the working directory where the batch\r
@REM file was invoked from\r
\r
@REM PDK_INSTALL_PATH if it is passed as an argument.\r
\r
@REM When pdk folder represents a device family, set a default SOC for that family\r
if %pdksoc% == jacinto (\r
- set pdksoc=am65xx\r
-)\r
-if %pdksoc% == sitara (\r
- set pdksoc=am64x\r
+ set pdksoc=j721e\r
)\r
\r
@REM Go to the SDK install directory\r
set GMAKE_INSTALL_PATH=%SDK_INSTALL_PATH%/xdctools_%XDC_VERSION%\r
)\r
set GMAKE_INSTALL_PATH=%GMAKE_INSTALL_PATH:\=/%\r
-@REM GMAKE Tool location; Uncomment the following line to set the \r
+@REM GMAKE Tool location; Uncomment the following line to set the\r
@REM gmake install path into env PATH variable.\r
set PATH=%GMAKE_INSTALL_PATH:/=\%;%PATH%\r
\r