PDK-9098: Board: am64x_evm add MCU GPIO for sitara-apps/servo_drive_demo
[processor-sdk/pdk.git] / packages / pdksetupenv.bat
index 43ad1953fa6eced356f27073a22624696d25b02f..d3f04e363cc55f8f3415f3572eb1cb48d2b5252b 100644 (file)
@@ -3,7 +3,7 @@
 @REM ******************************************************************************\r
 @REM * FILE NAME: pdksetupenv.bat\r
 @REM *\r
-@REM * DESCRIPTION: \r
+@REM * DESCRIPTION:\r
 @REM *  Configures and sets up the Build Environment for PDK.\r
 @REM *\r
 @REM *  The batch file expects an optional argument:PDK_INSTALL_PATH: Location\r
@@ -23,7 +23,7 @@
 @REM ********************** GET PARAMETERS PASSED THROUGH ARGUMENT   ***************\r
 @REM *******************************************************************************\r
 @REM Parameter Validation: Check if the argument was passed to the batch file and\r
-@REM if so we use that else we default to the working directory where the batch \r
+@REM if so we use that else we default to the working directory where the batch\r
 @REM file was invoked from\r
 \r
 @REM PDK_INSTALL_PATH if it is passed as an argument.\r
@@ -46,6 +46,11 @@ for %%a  in (%s%) do (
 for /f "tokens=1,2,3,4,5 delims=/_" %%a in ("%pdkdir%") do set pdksoc=%%b&set v1=%%c&set v2=%%d&set v3=%%e\r
 set pdkdir_ver=%v1%_%v2%_%v3%\r
 \r
+@REM When pdk folder represents a device family, set a default SOC for that family\r
+if %pdksoc% == jacinto (\r
+    set pdksoc=j721e\r
+)\r
+\r
 @REM Go to the SDK install directory\r
 cd %PDK_INSTALL_PATH%\..\..\r
 \r
@@ -76,7 +81,7 @@ if not defined GMAKE_INSTALL_PATH (
     set GMAKE_INSTALL_PATH=%SDK_INSTALL_PATH%/xdctools_%XDC_VERSION%\r
 )\r
 set GMAKE_INSTALL_PATH=%GMAKE_INSTALL_PATH:\=/%\r
-@REM GMAKE Tool location; Uncomment the following line to set the \r
+@REM GMAKE Tool location; Uncomment the following line to set the\r
 @REM gmake install path into env PATH variable.\r
 set PATH=%GMAKE_INSTALL_PATH:/=\%;%PATH%\r
 \r