diff --git a/packages/ti/drv/cbuff/example/cbuff_manual_testapp/main.c b/packages/ti/drv/cbuff/example/cbuff_manual_testapp/main.c
index ea7cf4502be13d048611437f794e4a7a8d2d4e5d..51d5841bc597afff3ee690b612a552c594d21e58 100644 (file)
#include <string.h>
#include <stdio.h>
-/* BIOS/XDC Include Files. */
-#include <xdc/std.h>
-#include <xdc/runtime/System.h>
-#include <ti/sysbios/BIOS.h>
-#include <ti/sysbios/knl/Task.h>
+#include <ti/osal/TaskP.h>
+#include <ti/osal/DebugP.h>
+#include <ti/osal/CacheP.h>
#include <ti/board/board.h>
-#include <ti/board/src/tpr12_evm/include/board_clock.h>
-
-#include <ti/osal/DebugP.h>
#include <ti/csl/cslr.h>
-
#include <ti/drv/edma/soc/edma_soc.h>
/* Cbuff Driver: */
/* ========================================================================== */
/* Global Variables */
/* ========================================================================== */
+static uint8_t gAppTskStackMain[4 * 1024] __attribute__((aligned(32)));
uint16_t gUserBuffer0[CSL_NEXT_MULTIPLE_OF_POW2(1024,CSL_CACHE_L1D_LINESIZE)] __attribute__ ((aligned(CSL_CACHE_L1D_LINESIZE)));
uint32_t i = 0;
/* Debug Message: */
- System_printf ("---------------------------------------------------\n");
- System_printf ("Debug: Testing CBUFF interface \n");
- System_printf ("---------------------------------------------------\n");
+ DebugP_log0 ("---------------------------------------------------\n");
+ DebugP_log0 ("Debug: Testing CBUFF interface \n");
+ DebugP_log0 ("---------------------------------------------------\n");
/* Initialize the configuration: */
memset ((void*)&initCfg, 0, sizeof(CBUFF_InitCfg));
cbuffHandle = CBUFF_init (&initCfg, &errCode);
if (cbuffHandle == NULL)
{
- System_printf ("Error: CBUFF Driver initialization failed [Error code %d]\n", errCode);
+ DebugP_log1 ("Error: CBUFF Driver initialization failed [Error code %d]\n", errCode);
return -1;
}
sessionHandle = CBUFF_open (cbuffHandle, &sessionCfg, &errCode);
if (sessionHandle == NULL)
{
- System_printf ("Error: Unable to create the session [Error code %d]\n", errCode);
+ DebugP_log1 ("Error: Unable to create the session [Error code %d]\n", errCode);
return -1;
}
/* Debug Message: Display the EDMA Channel Usage for the test. */
- System_printf ("Debug: EDMA Channel Usage = %d\n", gCBUFFEDMAChannelResourceCounter);
+ DebugP_log1 ("Debug: EDMA Channel Usage = %d\n", gCBUFFEDMAChannelResourceCounter);
/* Activate the session: */
if (CBUFF_activateSession (sessionHandle, &errCode) < 0)
{
- System_printf ("Error: Unable to activate the session [Error code %d]\n", errCode);
+ DebugP_log1 ("Error: Unable to activate the session [Error code %d]\n", errCode);
return -1;
}
/* Deactivate the session: */
if (CBUFF_deactivateSession (sessionHandle, &errCode) < 0)
{
- System_printf ("Error: Unable to deactivate the session [Error code %d]\n", errCode);
+ DebugP_log1 ("Error: Unable to deactivate the session [Error code %d]\n", errCode);
return -1;
}
/* Delete the session: */
if (CBUFF_close (sessionHandle, &errCode) < 0)
{
- System_printf ("Error: Unable to delete the session [Error code %d]\n", errCode);
+ DebugP_log1 ("Error: Unable to delete the session [Error code %d]\n", errCode);
return -1;
}
/* Sanity Check: Ensure that all the EDMA resources have been cleaned up */
if (gCBUFFEDMAChannelResourceCounter != 0)
{
- System_printf ("Error: EDMA Channel Memory leak detected\n");
+ DebugP_log0 ("Error: EDMA Channel Memory leak detected\n");
return -1;
}
return 0;
}
-void Test_initTask(UArg arg0, UArg arg1)
+void Test_initTask(void* arg0, void* arg1)
{
EDMA_Handle edmaHandle;
int32_t errCode;
char instName[25];
EDMA_getInstanceName(gInstanceId, &instName[0], sizeof(instName));
- System_printf("EDMA instance #%d: %s\n", gInstanceId, instName);
+ DebugP_log2("EDMA instance #%d: %s\n", gInstanceId, (uintptr_t)instName);
EDMA3CCInitParams_init(&initParam);
initParam.initParamSet = TRUE;
edmaHandle = EDMA_open(gInstanceId, &errCode, &instanceInfo);
if (edmaHandle == NULL)
{
- System_printf("Error: Unable to open the edma Instance, erorCode = %d\n", errCode);
+ DebugP_log1("Error: Unable to open the edma Instance, erorCode = %d\n", errCode);
}
}
errCode = EDMA_configErrorMonitoring(edmaHandle, &errorConfig);
if (errCode != EDMA_NO_ERROR)
{
- System_printf("Debug: EDMA_configErrorMonitoring() failed with errorCode = %d\n", errCode);
+ DebugP_log1("Debug: EDMA_configErrorMonitoring() failed with errorCode = %d\n", errCode);
return;
}
if (Test_Cbuff (edmaHandle) < 0)
return;
- /* Exit BIOS */
- BIOS_exit(0);
+ /* Stop OS */
+ OS_stop();
return;
}
int main (void)
{
- Task_Params taskParams;
+ TaskP_Params taskParams;
MmwDemo_BoardInit();
HW_WR_REG32(CSL_TOP_CTRL_U_BASE + 4, 0x10);
/* Debug Message: */
- System_printf ("***********************************************\n");
- System_printf ("************** CBUFF Unit Tests ***************\n");
- System_printf ("***********************************************\n");
+ DebugP_log0 ("***********************************************\n");
+ DebugP_log0 ("************** CBUFF Unit Tests ***************\n");
+ DebugP_log0 ("***********************************************\n");
/* Initialize the Task Parameters. */
- Task_Params_init(&taskParams);
- taskParams.stackSize = 4*1024;
- Task_create(Test_initTask, &taskParams, NULL);
+ TaskP_Params_init(&taskParams);
+ taskParams.stack = gAppTskStackMain;
+ taskParams.stacksize = sizeof(gAppTskStackMain);
+ TaskP_create(Test_initTask, &taskParams);
- /* Start BIOS */
- BIOS_start();
+ /* Start OS */
+ OS_start();
return 0;
}