summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: 54fd330)
raw | patch | inline | side by side (from parent 1: 54fd330)
author | Sivaraj R <sivaraj@ti.com> | |
Thu, 28 May 2020 11:04:49 +0000 (16:34 +0530) | ||
committer | Sujith Shivalingappa <a0393175@ti.com> | |
Thu, 28 May 2020 11:43:10 +0000 (06:43 -0500) |
- This is because we use "jacinto" as the directory name when we package PDK now
- Due to this the PDK_SOC variable is set to jacinto when the steenv script is called
- Instead set a default SOC so that the compilation goes through by default
- User can always override the PDK_SOC variable if need to build for another SOC
in the same family
Signed-off-by: Sivaraj R <sivaraj@ti.com>
- Due to this the PDK_SOC variable is set to jacinto when the steenv script is called
- Instead set a default SOC so that the compilation goes through by default
- User can always override the PDK_SOC variable if need to build for another SOC
in the same family
Signed-off-by: Sivaraj R <sivaraj@ti.com>
packages/pdksetupenv.bat | patch | blob | history | |
packages/pdksetupenv.sh | patch | blob | history |
index 43ad1953fa6eced356f27073a22624696d25b02f..19bb1490f07f544b9eab6655a3911d078aa73dca 100644 (file)
--- a/packages/pdksetupenv.bat
+++ b/packages/pdksetupenv.bat
for /f "tokens=1,2,3,4,5 delims=/_" %%a in ("%pdkdir%") do set pdksoc=%%b&set v1=%%c&set v2=%%d&set v3=%%e\r
set pdkdir_ver=%v1%_%v2%_%v3%\r
\r
for /f "tokens=1,2,3,4,5 delims=/_" %%a in ("%pdkdir%") do set pdksoc=%%b&set v1=%%c&set v2=%%d&set v3=%%e\r
set pdkdir_ver=%v1%_%v2%_%v3%\r
\r
+@REM When pdk folder represents a device family, set a default SOC for that family\r
+if %pdksoc% == jacinto (\r
+ set pdksoc=am65xx\r
+)\r
+if %pdksoc% == sitara (\r
+ set pdksoc=am64x\r
+)\r
+\r
@REM Go to the SDK install directory\r
cd %PDK_INSTALL_PATH%\..\..\r
\r
@REM Go to the SDK install directory\r
cd %PDK_INSTALL_PATH%\..\..\r
\r
index 2912f2d3450542b4f97c0711db54bad23f4a335f..a3b831f13fc6fb2c025f6bb9c17bf6391a97b207 100755 (executable)
--- a/packages/pdksetupenv.sh
+++ b/packages/pdksetupenv.sh
CURDIR_LAST=${PWD##*/}
IFS='_' read -ra ADDR <<< "$CURDIR_LAST"
CURDIR_LAST=${PWD##*/}
IFS='_' read -ra ADDR <<< "$CURDIR_LAST"
+# When pdk folder represents a device family, set a default SOC for that family
+if [ ${ADDR[1]} == "jacinto" ]; then
+ ADDR[1]="am65xx"
+fi
+if [ ${ADDR[1]} == "sitara" ]; then
+ ADDR[1]="am64x"
+fi
if [ -z $PDK_SOC ]; then
export PDK_SOC=${ADDR[1]}
if [ -z $PDK_SOC ]; then
export PDK_SOC=${ADDR[1]}