]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - processor-sdk/pdk.git/commitdiff
PDK-6948: Board: Updated mmr config for am64x evm
authorM V Pratap Reddy <x0257344@ti.com>
Fri, 4 Dec 2020 12:52:36 +0000 (18:22 +0530)
committerSivaraj R <sivaraj@ti.com>
Mon, 7 Dec 2020 07:56:38 +0000 (01:56 -0600)
 - MMR config is failing during the pinmux configuration in release
   mode. Order of execution for setting kick0 and kick1 is done in reverse
   which is causing unlock/lock failure.
   Added volatile specifier for kick address variables to avoid the
   optimization.

packages/ti/board/src/am64x_evm/board_mmr.c

index 7e623dafc0aa4a4797c98f59020b88d679a4e1cc..26639a041fc0c096b5077dff4e90735ce9972f27 100644 (file)
@@ -145,7 +145,7 @@ typedef enum {
 #define MCU_PADCONFIG_MMR_BASE_ADDRESS CSL_MCU_PADCFG_CTRL0_CFG0_BASE\r
 #endif\r
 \r
 #define MCU_PADCONFIG_MMR_BASE_ADDRESS CSL_MCU_PADCFG_CTRL0_CFG0_BASE\r
 #endif\r
 \r
-uint32_t MMR_change_lock(mmr_lock_actions_t target_state, uint32_t * kick0);\r
+uint32_t MMR_change_lock(mmr_lock_actions_t target_state, volatile uint32_t * kick0);\r
 uint32_t generic_mmr_change_all_locks(mmr_lock_actions_t target_state, uint32_t base_addr, const  uint32_t * offset_array, uint32_t array_size);\r
 \r
 uint32_t MAIN_PADCONFIG_MMR_unlock_all();\r
 uint32_t generic_mmr_change_all_locks(mmr_lock_actions_t target_state, uint32_t base_addr, const  uint32_t * offset_array, uint32_t array_size);\r
 \r
 uint32_t MAIN_PADCONFIG_MMR_unlock_all();\r
@@ -173,8 +173,8 @@ uint32_t MCU_PLL_MMR_lock_all();
 uint32_t MCU_PLL_MMR_change_all_locks(mmr_lock_actions_t target_state);\r
 \r
 \r
 uint32_t MCU_PLL_MMR_change_all_locks(mmr_lock_actions_t target_state);\r
 \r
 \r
-    uint32_t MMR_change_lock(mmr_lock_actions_t target_state, uint32_t * kick0) {\r
-        uint32_t * kick1 = kick0 + 1;\r
+    uint32_t MMR_change_lock(mmr_lock_actions_t target_state, volatile uint32_t * kick0) {\r
+        volatile uint32_t * kick1 = kick0 + 1;\r
         uint32_t lock_state = (*kick0 & 0x1); //status is 1 if unlocked, 0 if locked\r
 \r
         //If lock state is not what we want, change it\r
         uint32_t lock_state = (*kick0 & 0x1); //status is 1 if unlocked, 0 if locked\r
 \r
         //If lock state is not what we want, change it\r
@@ -206,9 +206,9 @@ uint32_t MCU_PLL_MMR_change_all_locks(mmr_lock_actions_t target_state);
     uint32_t generic_mmr_change_all_locks(mmr_lock_actions_t target_state, uint32_t base_addr, const uint32_t * offset_array, uint32_t array_size) {\r
         uint32_t errors=0;\r
         uint32_t i=0;\r
     uint32_t generic_mmr_change_all_locks(mmr_lock_actions_t target_state, uint32_t base_addr, const uint32_t * offset_array, uint32_t array_size) {\r
         uint32_t errors=0;\r
         uint32_t i=0;\r
-        uint32_t * kick0_ptr;\r
+        volatile uint32_t * kick0_ptr;\r
         for(i=0;i<array_size;i++) {\r
         for(i=0;i<array_size;i++) {\r
-            kick0_ptr = (uint32_t *) (base_addr + offset_array[i]);\r
+            kick0_ptr = (volatile uint32_t *) (base_addr + offset_array[i]);\r
             if(MMR_change_lock(target_state, kick0_ptr) == AVV_FAIL){\r
                 errors++;\r
             }\r
             if(MMR_change_lock(target_state, kick0_ptr) == AVV_FAIL){\r
                 errors++;\r
             }\r