summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6579033)
raw | patch | inline | side by side (parent: 6579033)
author | Piyali Goswami <piyali_g@ti.com> | |
Sat, 2 Jan 2021 03:40:22 +0000 (09:10 +0530) | ||
committer | Sujith Shivalingappa <sujith.s@ti.com> | |
Mon, 18 Jan 2021 03:51:06 +0000 (21:51 -0600) |
Sciserver_UserProcessMsg has 2 flows:
1. Non-secure host --> Sciserver_UserProcessMsg (MCU1_0)
RM Process / PM Process
[RM forward to DMSC]
2. Secure Host --> DMSC --> Sciserver_UserProcessMsg (MCU1_0)
RM Process/ PM Process
Earlier logic was performing the following steps:
1. Check message type - based on that set RM, PM or forward flag.
2. If RM flag and forward flag is set the Process RM is called and the Forward message is called.
3. The effect is the local RM is called 2 times
4. If the local RM fails, we still end up calling the API 2 times.
5. If there is a fail in the Forward response function, the response is not sent back to the non-secure host.
So the logic has to be corrected to have only local RM processing when getting forwarded from a secure host and have non-secure processing call the Sciclient_service function which identifies the forward or non-forward message calls.
The earlier logic also has another issue where the value of return is checked for the setting of the ACK and NACK flag after the override finished for the ret value based on the fact that the ACK and NACK flag is already set in the response. So the net effect is the ACK / NACK flag is falsely set to ACK based on the ret value giving an incorrect response to the user.
The current logic does the following:
1. Checks if the message is from DMSC (forwarded) or not. Based on this it calls the full message processing or only the local to MCU1_0 RM message processing.
2. The Sciserver and the local RM message processing sets the ACK/NACK flag and the API does not overwrite this after the processing is complete.
Signed-off-by: Piyali Goswami <piyali_g@ti.com>
1. Non-secure host --> Sciserver_UserProcessMsg (MCU1_0)
RM Process / PM Process
[RM forward to DMSC]
2. Secure Host --> DMSC --> Sciserver_UserProcessMsg (MCU1_0)
RM Process/ PM Process
Earlier logic was performing the following steps:
1. Check message type - based on that set RM, PM or forward flag.
2. If RM flag and forward flag is set the Process RM is called and the Forward message is called.
3. The effect is the local RM is called 2 times
4. If the local RM fails, we still end up calling the API 2 times.
5. If there is a fail in the Forward response function, the response is not sent back to the non-secure host.
So the logic has to be corrected to have only local RM processing when getting forwarded from a secure host and have non-secure processing call the Sciclient_service function which identifies the forward or non-forward message calls.
The earlier logic also has another issue where the value of return is checked for the setting of the ACK and NACK flag after the override finished for the ret value based on the fact that the ACK and NACK flag is already set in the response. So the net effect is the ACK / NACK flag is falsely set to ACK based on the ret value giving an incorrect response to the user.
The current logic does the following:
1. Checks if the message is from DMSC (forwarded) or not. Based on this it calls the full message processing or only the local to MCU1_0 RM message processing.
2. The Sciserver and the local RM message processing sets the ACK/NACK flag and the API does not overwrite this after the processing is complete.
Signed-off-by: Piyali Goswami <piyali_g@ti.com>
diff --git a/packages/ti/drv/sciclient/src/sciclient/sciclient_direct.c b/packages/ti/drv/sciclient/src/sciclient/sciclient_direct.c
index 5c04bd2c7a65a7471b93f6224f303eb3fa97aad1..8173b0fac1da8a2dd87185be8cc9ea1e76aafdab 100644 (file)
hdr = (struct tisci_header *) &message;
pRespPrm->flags = hdr->flags;
- if (ret == CSL_PASS)
+ if ((ret == CSL_PASS) &&
+ ((pRespPrm->flags & TISCI_MSG_FLAG_ACK) == TISCI_MSG_FLAG_ACK))
{
/*
* This message is forwarded to DMSC for continued
*/
ret = boardcfg_RmAdjustReq((uint32_t *)pReqPrm->pReqPayload, adjSize);
}
- if (ret == CSL_PASS)
+ if ((ret == CSL_PASS) &&
+ ((pRespPrm->flags & TISCI_MSG_FLAG_ACK) == TISCI_MSG_FLAG_ACK))
{
memcpy(message, pReqPrm->pReqPayload, pReqPrm->reqPayloadSize);
diff --git a/packages/ti/drv/sciclient/src/sciserver/sciserver.c b/packages/ti/drv/sciclient/src/sciserver/sciserver.c
index 6a9c51426e26e0a10165a76f1fd04c1475f935e6..fb5f9d79c911b1523def2b6c4588ba116a8d7f73 100755 (executable)
#include <sciserver_secproxyTransfer.h>
#include <sciserver_hwiData.h>
#include <ti/drv/sciclient/src/sciclient/sciclient_priv.h>
+#include <ti/drv/uart/UART_stdio.h>
/* Set VERBOSE to 1 for trace information on message routing */
#define VERBOSE 0
#if VERBOSE
-#include <ti/drv/uart/UART_stdio.h>
#define Sciserver_printf UART_printf
#else
#define Sciserver_printf(...)
int32_t *pRespMsgSize,
uint8_t hw_host);
-static void Sciserver_TisciMsgClearFlags(struct tisci_header *hdr);
static int32_t Sciserver_TisciMsgResponse(uint8_t response_host,
uint32_t *response,
uint32_t size);
int32_t respMsgSize;
/* the response message pointer */
uint32_t *respMsg = NULL;
- /* the response message header pointer. Same as respMsg */
- struct tisci_header *respMsgHeader = NULL;
for (i = 0; i < SCISERVER_SECPROXY_INSTANCE_COUNT; i++)
{
&respMsgSize,
utd->user_msg_data[utd->state->current_buffer_idx]->host);
respMsg = utd->hw_msg_buffer_list[utd->state->current_buffer_idx];
- respMsgHeader = (struct tisci_header *) respMsg;
}
else
{
if (ret == CSL_PASS)
{
- if (ret == CSL_PASS)
- {
- Sciclient_TisciMsgSetAckResp(respMsgHeader);
- }
- else if ((respMsgHeader->flags & TISCI_MSG_FLAG_AOP) != 0)
- {
- Sciserver_TisciMsgClearFlags(respMsgHeader);
- Sciclient_TisciMsgSetNakResp(respMsgHeader);
- }
-
respHost = utd->user_msg_data[utd->state->current_buffer_idx]->host;
if (respHost == TISCI_HOST_ID_DMSC2DM)
{
}
-static void Sciserver_TisciMsgClearFlags(struct tisci_header *hdr)
-{
- hdr->flags = 0;
-}
-
static int32_t Sciserver_TisciMsgResponse(uint8_t response_host,
uint32_t *response,
uint32_t size)
hdr->host = hostId;
}
-int32_t Sciserver_ProcessForwardedMessage(uint32_t *msg_recv,
+int32_t Sciserver_ProcessFullMessage(uint32_t *msg_recv,
int32_t reqMsgSize,
int32_t respMsgSize)
{
ret = Sciclient_service(&reqPrm, &respPrm);
- if ((CSL_PASS == ret) && (respPrm.flags == TISCI_MSG_FLAG_ACK))
- {
- Sciserver_printf("Sciserver: forward success type=%d\n", hdr->type);
- memcpy(msg_recv, respMsgBuffer, respMsgSize);
+ memcpy(msg_recv, respMsgBuffer, respMsgSize);
- /* Must restore the seq field. When forwarded message is processed by
- * TIFS, the returned message would have incorrect sequence value */
- hdr->seq = reqSeq;
- }
- else
- {
- Sciserver_printf("Sciserver: forward failed type=%d, flag=%d\n",
- hdr->type, respPrm.flags);
- ret = CSL_EFAIL;
- }
+ /* Must restore the seq field. When forwarded message is processed by
+ * TIFS, the returned message would have incorrect sequence value */
+ hdr->seq = reqSeq;
return ret;
}
{
int32_t ret = CSL_PASS;
struct tisci_header *hdr = (struct tisci_header *) msg_recv;
- int32_t isRmMsg = 0, isPmMsg = 0, isFwdMsg = 0;
+ int32_t runLocalRmOnly = 0;
int32_t reqMsgSize;
int32_t respMsgSize;
switch (hdr->type)
{
case TISCI_MSG_VERSION:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_version_req);
respMsgSize = sizeof(struct tisci_msg_version_resp);
break;
/* Start of RM messages */
case TISCI_MSG_BOARD_CONFIG_RM:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_board_config_rm_req);
respMsgSize = sizeof(struct tisci_msg_board_config_rm_resp);
break;
case TISCI_MSG_RM_GET_RESOURCE_RANGE:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_rm_get_resource_range_req);
respMsgSize = sizeof(struct tisci_msg_rm_get_resource_range_resp);
break;
case TISCI_MSG_RM_IRQ_SET:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_irq_set_req);
respMsgSize = sizeof(struct tisci_msg_rm_irq_set_resp);
break;
case TISCI_MSG_RM_IRQ_RELEASE:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_irq_release_req);
respMsgSize = sizeof(struct tisci_msg_rm_irq_release_resp);
break;
case TISCI_MSG_RM_RING_CFG:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_ring_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_ring_cfg_resp);
break;
case TISCI_MSG_RM_RING_MON_CFG:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_ring_mon_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_ring_mon_cfg_resp);
break;
case TISCI_MSG_RM_UDMAP_TX_CH_CFG:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_udmap_tx_ch_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_tx_ch_cfg_resp);
break;
case TISCI_MSG_RM_UDMAP_RX_CH_CFG:
- isRmMsg = 1;
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_udmap_rx_ch_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_rx_ch_cfg_resp);
break;
case TISCI_MSG_RM_UDMAP_FLOW_CFG:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_cfg_resp);
break;
case TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_size_thresh_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_size_thresh_cfg_resp);
break;
case TISCI_MSG_RM_UDMAP_FLOW_DELEGATE:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_delegate_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_flow_delegate_resp);
break;
case TISCI_MSG_RM_UDMAP_GCFG_CFG:
- isRmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_rm_udmap_gcfg_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_udmap_gcfg_cfg_resp);
break;
case TISCI_MSG_RM_PSIL_PAIR:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_psil_pair_req);
respMsgSize = sizeof(struct tisci_msg_rm_psil_pair_resp);
break;
case TISCI_MSG_RM_PSIL_UNPAIR:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_psil_unpair_req);
respMsgSize = sizeof(struct tisci_msg_rm_psil_unpair_resp);
break;
case TISCI_MSG_RM_PSIL_READ:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_psil_read_req);
respMsgSize = sizeof(struct tisci_msg_rm_psil_read_resp);
break;
case TISCI_MSG_RM_PSIL_WRITE:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_psil_write_req);
respMsgSize = sizeof(struct tisci_msg_rm_psil_write_resp);
break;
case TISCI_MSG_RM_PROXY_CFG:
- isFwdMsg = 1;
reqMsgSize = sizeof(struct tisci_msg_rm_proxy_cfg_req);
respMsgSize = sizeof(struct tisci_msg_rm_proxy_cfg_resp);
break;
/* Start of PM messages */
case TISCI_MSG_BOARD_CONFIG_PM:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_board_config_pm_req);
respMsgSize = sizeof(struct tisci_msg_board_config_pm_resp);
break;
case TISCI_MSG_SET_CLOCK:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_set_clock_req);
respMsgSize = sizeof(struct tisci_msg_set_clock_resp);
break;
case TISCI_MSG_GET_CLOCK:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_get_clock_req);
respMsgSize = sizeof(struct tisci_msg_get_clock_resp);
break;
case TISCI_MSG_SET_CLOCK_PARENT:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_set_clock_parent_req);
respMsgSize = sizeof(struct tisci_msg_set_clock_parent_resp);
break;
case TISCI_MSG_GET_CLOCK_PARENT:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_get_clock_parent_req);
respMsgSize = sizeof(struct tisci_msg_get_clock_parent_resp);
break;
case TISCI_MSG_GET_NUM_CLOCK_PARENTS:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_get_num_clock_parents_req);
respMsgSize = sizeof(struct tisci_msg_get_num_clock_parents_resp);
break;
case TISCI_MSG_SET_FREQ:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_set_freq_req);
respMsgSize = sizeof(struct tisci_msg_set_freq_resp);
break;
case TISCI_MSG_QUERY_FREQ:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_query_freq_req);
respMsgSize = sizeof(struct tisci_msg_query_freq_resp);
break;
case TISCI_MSG_GET_FREQ:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_get_freq_req);
respMsgSize = sizeof(struct tisci_msg_get_freq_resp);
break;
case TISCI_MSG_SET_DEVICE:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_set_device_req);
respMsgSize = sizeof(struct tisci_msg_set_device_resp);
break;
case TISCI_MSG_GET_DEVICE:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_get_device_req);
respMsgSize = sizeof(struct tisci_msg_get_device_resp);
break;
case TISCI_MSG_SET_DEVICE_RESETS:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_set_device_resets_req);
respMsgSize = sizeof(struct tisci_msg_set_device_resets_resp);
break;
case TISCI_MSG_SYS_RESET:
- isPmMsg = 1;
+ reqMsgSize = sizeof(struct tisci_msg_sys_reset_req);
respMsgSize = sizeof(struct tisci_msg_sys_reset_resp);
break;
-
default:
- isRmMsg = 0;
- isPmMsg = 0;
- isFwdMsg = 1;
-
/* Forward the full message size */
reqMsgSize = SCISERVER_HW_QUEUE_SIZE;
respMsgSize = SCISERVER_HW_QUEUE_SIZE;
case TISCI_MSG_RM_PROXY_CFG:
if (hw_host_id == TISCI_HOST_ID_DMSC2DM)
{
- Sciserver_printf("Skip forward: type = %d\n", hdr->type);
- isFwdMsg = 0;
- isRmMsg = 1;
+ runLocalRmOnly = 1;
}
break;
}
- if (isRmMsg)
+ if (runLocalRmOnly == 1)
{
ret = Sciclient_ProcessRmMessage(msg_recv);
}
-
- if (isPmMsg)
- {
- ret = Sciclient_ProcessPmMessage(0, msg_recv);
- }
-
- if (isFwdMsg)
+ else
{
- ret = Sciserver_ProcessForwardedMessage(msg_recv,
- reqMsgSize, respMsgSize);
+ ret = Sciserver_ProcessFullMessage(msg_recv,
+ reqMsgSize, respMsgSize);
}
*pRespMsgSize = respMsgSize;
diff --git a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc
index 0f6656c3a08a88b9a43d6ba1b332ef4153c62a0a..5986e7fe42e61e2060b58db4f0c57466a077126e 100644 (file)
Binary files a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc and b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc differ
Binary files a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc and b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j7200/sciserver_testapp_mcu1_0_release.rprc differ
diff --git a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc
index 9856504a31210774edce94a4435a8f0369e314aa..3b09f2871fea1c484a10f53ef9c84753279665c8 100644 (file)
Binary files a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc and b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc differ
Binary files a/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc and b/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_mcu1_0_release.rprc differ