]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - processor-sdk/performance-audio-sr.git/blob - ipc_3_43_00_00_eng/packages/ti/ipc/HeapBufMP.h
Add IPC 3.34.00.00 eng release
[processor-sdk/performance-audio-sr.git] / ipc_3_43_00_00_eng / packages / ti / ipc / HeapBufMP.h
1 /*
2  * Copyright (c) 2012-2013, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * *  Redistributions of source code must retain the above copyright
10  *    notice, this list of conditions and the following disclaimer.
11  *
12  * *  Redistributions in binary form must reproduce the above copyright
13  *    notice, this list of conditions and the following disclaimer in the
14  *    documentation and/or other materials provided with the distribution.
15  *
16  * *  Neither the name of Texas Instruments Incorporated nor the names of
17  *    its contributors may be used to endorse or promote products derived
18  *    from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /**
33  *  @file       ti/ipc/HeapBufMP.h
34  *
35  *  @brief      Multi-processor fixed-size buffer heap implementation
36  *
37  *  @note       HeapBufMP is currently only available for SYS/BIOS.
38  *
39  *  Heap implementation that manages fixed size buffers that can be used
40  *  in a multiprocessor system with shared memory.
41  *
42  *  The HeapBufMP manager provides functions to allocate and free storage from a
43  *  heap of type HeapBufMP which inherits from IHeap. HeapBufMP manages a single
44  *  fixed-size buffer, split into equally sized allocatable blocks.
45  *
46  *  The HeapBufMP manager is intended as a very fast memory
47  *  manager which can only allocate blocks of a single size. It is ideal for
48  *  managing a heap that is only used for allocating a single type of object,
49  *  or for objects that have very similar sizes.
50  *
51  *  The HeapBufMP module uses a NameServer instance to
52  *  store instance information when an instance is created.  The name supplied
53  *  must be unique for all HeapBufMP instances.
54  *
55  *  HeapBufMP_create() initializes the shared memory as needed. Once an
56  *  instance is created, HeapBufMP_open() can be performed. The
57  *  open is used to gain access to the same HeapBufMP instance.
58  *  Generally an instance is created on one processor and opened on the
59  *  other processor(s).
60  *
61  *  The open returns a HeapBufMP instance handle like the create,
62  *  however the open does not modify the shared memory.
63  *
64  *  The HeapBufMP header should be included in an application as follows:
65  *  @code
66  *  #include <ti/ipc/HeapBufMP.h>
67  *  @endcode
68  */
70 #ifndef ti_ipc_HeapBufMP__include
71 #define ti_ipc_HeapBufMP__include
73 #if defined (__cplusplus)
74 extern "C" {
75 #endif
77 #include <ti/ipc/GateMP.h>
79 /* =============================================================================
80  *  All success and failure codes for the module
81  * =============================================================================
82  */
84 /*!
85  *  @brief  The resource is still in use
86  */
87 #define HeapBufMP_S_BUSY               2
89 /*!
90  *  @brief  The module has been already setup
91  */
92 #define HeapBufMP_S_ALREADYSETUP       1
94 /*!
95  *  @brief  Operation is successful.
96  */
97 #define HeapBufMP_S_SUCCESS            0
99 /*!
100  *  @brief  Generic failure.
101  */
102 #define HeapBufMP_E_FAIL              -1
104 /*!
105  *  @brief  Argument passed to function is invalid.
106  */
107 #define HeapBufMP_E_INVALIDARG        -2
109 /*!
110  *  @brief  Operation resulted in memory failure.
111  */
112 #define HeapBufMP_E_MEMORY            -3
114 /*!
115  *  @brief  The specified entity already exists.
116  */
117 #define HeapBufMP_E_ALREADYEXISTS     -4
119 /*!
120  *  @brief  Unable to find the specified entity.
121  */
122 #define HeapBufMP_E_NOTFOUND          -5
124 /*!
125  *  @brief  Operation timed out.
126  */
127 #define HeapBufMP_E_TIMEOUT           -6
129 /*!
130  *  @brief  Module is not initialized.
131  */
132 #define HeapBufMP_E_INVALIDSTATE      -7
134 /*!
135  *  @brief  A failure occurred in an OS-specific call
136  */
137 #define HeapBufMP_E_OSFAILURE         -8
139 /*!
140  *  @brief  Specified resource is not available
141  */
142 #define HeapBufMP_E_RESOURCE          -9
144 /*!
145  *  @brief  Operation was interrupted. Please restart the operation
146  */
147 #define HeapBufMP_E_RESTART           -10
149 /* =============================================================================
150  *  Structures & Enums
151  * =============================================================================
152  */
154 /*!
155  *  @brief  HeapBufMP_Handle type
156  */
157 typedef struct HeapBufMP_Object *HeapBufMP_Handle;
159 /*!
160  *  @brief  Structure defining parameters for the HeapBufMP module
161  *
162  *  @sa     HeapBufMP_create()
163  */
164 typedef struct HeapBufMP_Params {
165     String name;
166     /*!< @brief Name of this instance.
167      *
168      *  The name (if not NULL) must be unique among all HeapBufMP
169      *  instances in the entire system.  When creating a new
170      *  heap, it is necessary to supply an instance name.
171      *
172      *  The name does not have to be persistent.  The supplied string is copied
173      *  into persistent memory.
174      */
176     UInt16 regionId;
177     /*!< @brief Shared region ID
178      *
179      *  The index corresponding to the shared region from which shared memory
180      *  will be allocated.
181      */
183     /*! @cond */
184     Ptr sharedAddr;
185     /*!< @brief Physical address of the shared memory
186      *
187      *  This value can be left as 'null' unless it is required to place the
188      *  heap at a specific location in shared memory.  If sharedAddr is null,
189      *  then shared memory for a new instance will be allocated from the
190      *  heap belonging to the region identified by #HeapBufMP_Params.regionId.
191      */
192     /*! @endcond */
194     SizeT blockSize;
195     /*!< @brief Size (in MAUs) of each block.
196      *
197      *  HeapBufMP will round the blockSize up to the nearest multiple of the
198      *  alignment, so the actual blockSize may be larger. When creating a
199      *  HeapBufMP dynamically, this needs to be taken into account to determine
200      *  the proper buffer size to pass in.
201      *
202      *  Required parameter.
203      *
204      *  The default size of the blocks is 0 MAUs.
205      */
207     UInt numBlocks;
208     /*!< @brief Number of fixed-size blocks.
209      *
210      *  This is a required parameter for all new HeapBufMP instances.
211      */
213     SizeT align;
214     /*!< @brief Alignment (in MAUs) of each block.
215      *
216      *  The alignment must be a power of 2. If the value 0 is specified,
217      *  the value will be changed to meet minimum structure alignment
218      *  requirements and the cache alignment size of the region in which the
219      *  heap will be placed.  Therefore, the actual alignment may be larger.
220      *
221      *  The default alignment is 0.
222      */
224     Bool exact;
225     /*!< @brief Use exact matching
226      *
227      *  Setting this flag will allow allocation only if the requested size
228      *  is equal to (rather than less than or equal to) the buffer's block
229      *  size.
230      */
232     GateMP_Handle gate;
233     /*!< @brief GateMP used for critical region management of the shared memory
234      *
235      *  Using the default value of NULL will result in use of the GateMP
236      *  system gate for context protection.
237      */
239 } HeapBufMP_Params;
241 /*!
242  *  @brief  Stats structure for HeapBufMP_getExtendedStats()
243  *
244  *  @sa     HeapBufMP_getExtendedStats()
245  */
246 typedef struct HeapBufMP_ExtendedStats {
247     UInt maxAllocatedBlocks;
248     /*!< The maximum number of blocks allocated from this heap at any point in
249      *  time during the lifetime of this HeapBufMP instance.
250      */
252     UInt numAllocatedBlocks;
253     /*!< The total number of blocks currently allocated in this HeapBufMP
254      *  instance.
255      */
256 } HeapBufMP_ExtendedStats;
258 /* =============================================================================
259  *  HeapBufMP Module-wide Functions
260  * =============================================================================
261  */
263 /*!
264  *  @brief      Close a HeapBufMP instance
265  *
266  *  Closing an instance will free local memory consumed by the opened
267  *  instance. All opened instances should be closed before the instance
268  *  is deleted.
269  *
270  *  @param[in,out]  handlePtr   Pointer to handle returned from
271  *                              HeapBufMP_open()
272  *
273  *  @return     HeapBufMP status:
274  *              - #HeapBufMP_S_SUCCESS: Heap successfully closed
275  *
276  *  @sa         HeapBufMP_open()
277  */
278 Int HeapBufMP_close(HeapBufMP_Handle *handlePtr);
280 /*!
281  *  @brief      Create a HeapBufMP instance
282  *
283  *  @param[in]  params      HeapBufMP parameters
284  *
285  *  @return     HeapBufMP Handle
286  *
287  *  @sa         HeapBufMP_delete()
288  */
289 HeapBufMP_Handle HeapBufMP_create(const HeapBufMP_Params *params);
291 /*!
292  *  @brief      Delete a created HeapBufMP instance
293  *
294  *  @param[in,out]  handlePtr   Pointer to handle to delete.
295  *
296  *  @return     HeapBufMP status:
297  *              - #HeapBufMP_S_SUCCESS: Heap successfully deleted
298  *
299  *  @sa         HeapBufMP_create()
300  */
301 Int HeapBufMP_delete(HeapBufMP_Handle *handlePtr);
303 /*!
304  *  @brief      Open a created HeapBufMP instance
305  *
306  *  Once an instance is created, an open can be performed. The
307  *  open is used to gain access to the same HeapBufMP instance.
308  *  Generally an instance is created on one processor and opened on the
309  *  other processor.
310  *
311  *  The open returns a HeapBufMP instance handle like the create,
312  *  however the open does not initialize the shared memory. The supplied
313  *  name is used to identify the created instance.
314  *
315  *  Call #HeapBufMP_close when the opened instance is not longer needed.
316  *
317  *  @param[in]  name        Name of created HeapBufMP instance
318  *  @param[out] handlePtr   Pointer to HeapBufMP handle to be opened
319  *
320  *  @return     HeapBufMP status:
321  *              - #HeapBufMP_S_SUCCESS: Heap successfully opened
322  *              - #HeapBufMP_E_NOTFOUND: Heap is not yet ready to be opened.
323  *              - #HeapBufMP_E_FAIL: A general failure has occurred
324  *
325  *  @sa         HeapBufMP_close()
326  */
327 Int HeapBufMP_open(String name, HeapBufMP_Handle *handlePtr);
329 /*! @cond */
330 Int HeapBufMP_openByAddr(Ptr sharedAddr, HeapBufMP_Handle *handlePtr);
332 /*! @endcond */
334 /*!
335  *  @brief      Initialize a HeapBufMP parameters struct
336  *
337  *  @param[out] params      Pointer to creation parameters
338  *
339  *  @sa         HeapBufMP_create()
340  */
341 Void HeapBufMP_Params_init(HeapBufMP_Params *params);
343 /*! @cond */
344 /*!
345  *  @brief      Amount of shared memory required for creation of each instance
346  *
347  *  @param[in]  params      Pointer to the parameters that will be used in
348  *                          the create.
349  *
350  *  @return     Number of MAUs needed to create the instance.
351  */
352 SizeT HeapBufMP_sharedMemReq(const HeapBufMP_Params *params);
354 /*! @endcond */
356 /* =============================================================================
357  *  HeapBufMP Per-instance Functions
358  * =============================================================================
359  */
361 /*!
362  *  @brief      Allocate a block of memory of specified size and alignment
363  *
364  *  The actual block returned may be larger than requested to satisfy
365  *  alignment requirements. NULL is returned if the allocation fails.
366  *
367  *  HeapBufMP_alloc() will lock the heap using the HeapBufMP gate
368  *  while it traverses the list of free blocks to find a large enough block
369  *  for the request.
370  *
371  *  Guidelines for using large heaps and multiple alloc() calls.
372  *      - If possible, allocate larger blocks first. Previous allocations
373  *        of small memory blocks can reduce the size of the blocks
374  *        available for larger memory allocations.
375  *      - Realize that allocation can fail even if the heap contains a
376  *        sufficient absolute amount of unallocated space. This is
377  *        because the largest free memory block may be smaller than
378  *        total amount of unallocated memory.
379  *
380  *  @param[in]  handle    Handle to previously created/opened instance.
381  *  @param[in]  size      Size to be allocated (in MADUs)
382  *  @param[in]  align     Alignment for allocation (power of 2)
383  *
384  *  @sa         HeapBufMP_free()
385  */
386 Void *HeapBufMP_alloc(HeapBufMP_Handle handle, SizeT size, SizeT align);
388 /*!
389  *  @brief      Frees a block of memory.
390  *
391  *  HeapBufMP_free() places the memory block specified by addr and size back
392  *  into the free pool of the heap specified. The newly freed block is combined
393  *  with any adjacent free blocks. The space is then available for future
394  *  allocations.
395  *
396  *  HeapBufMP_free() will lock the heap using the HeapBufMP gate if one is
397  *  specified or the system GateMP if not.
398  *
399  *  @param[in]  handle    Handle to previously created/opened instance.
400  *  @param[in]  block     Block of memory to be freed.
401  *  @param[in]  size      Size to be freed (in MADUs)
402  *
403  *  @sa         HeapBufMP_alloc()
404  */
405 Void HeapBufMP_free(HeapBufMP_Handle handle, Ptr block, SizeT size);
407 /*!
408  *  @brief      Get extended memory statistics
409  *
410  *  This function retrieves extended statistics for a HeapBufMP
411  *  instance. Refer to #HeapBufMP_ExtendedStats for more information
412  *  regarding what information is returned.
413  *
414  *  In SYS/BIOS, HeapBufMP.trackAllocs needs to be set to 'true' in the
415  *  configuration to get meaningful extended stats.
416  *
417  *  @param[in]  handle    Handle to previously created/opened instance.
418  *  @param[out] stats     ExtendedStats structure
419  *
420  *  @sa     HeapBufMP_getStats()
421  */
422 Void HeapBufMP_getExtendedStats(HeapBufMP_Handle handle,
423                                 HeapBufMP_ExtendedStats *stats);
425 /*!
426  *  @brief      Get memory statistics
427  *
428  *  @param[in]  handle    Handle to previously created/opened instance.
429  *  @param[out] stats     Memory statistics structure
430  *
431  *  @sa     HeapBufMP_getExtendedStats()
432  */
433 Void HeapBufMP_getStats(HeapBufMP_Handle handle, Ptr stats);
435 #if defined (__cplusplus)
437 #endif /* defined (__cplusplus) */
438 #endif /* ti_ipc_HeapBufMP__include */