Merge branch 'dev_pasdk_pp_pasdk302' of ssh://git@bitbucket.itg.ti.com/pasdk/pasdk_sr...
[processor-sdk/performance-audio-sr.git] / psdk_cust / libarch_k2g_1_0_1_0 / examples / arm+dsp / test_app_arm.cpp
1 /******************************************************************************
2  * Copyright (c) 2015, Texas Instruments Incorporated - http://www.ti.com
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
29 ////////////////////////////////////////////////////////////////////////////////
30 //  This file shows an example of the host code of an application that uses an 
31 //  ARM+DSP library. 
32 //////////////////////////////////////////////////////////////////////////////// 
33 #include <cstdlib>
34 #include <cmath>
35 #include <cstring>
36 #include <iostream>
37 #include <fstream>
38 #define __CL_ENABLE_EXCEPTIONS
39 #include <CL/cl.hpp>
40 using namespace std;
41 using namespace cl;
42 // Both cl and std namespace define size_t, so we must be explicit.
43 #define size_t ::size_t
44 #ifndef TEST_FAT_BINARY
45 #include "ocl_util.h"
46 #endif
47 #include <pthread.h>
50 #define TEST_DEBUG_PRINT(...) {fprintf(stdout,"TEST DEBUG: ");fprintf(stdout,__VA_ARGS__);}
52 extern void lib_init_arm();
53 extern void lib_find_l2_start();
54 extern void lib_kernel_arm(double *in1_ptr, double *in2_ptr, double *out_ptr, int data_size);
56 void app_fill_memory(double *buf1, double *buf2, int num_elements);
57 double app_err_check(double *in1, double *in2, double *out, int num_elements);
59 #define TEST_DATA_SIZE     (1024)        //1K data points
61 /*==============================================================================
62  * Application code on the host which calls library functions to process data.
63  *============================================================================*/
64 int main()
65 {    
66     // Allocate input/output buffers using TI-OpenCL built-ins. 
67     TEST_DEBUG_PRINT("Allocating memory for input/output buffers.\n");   
68     double *in1_ptr  = (double *)__malloc_ddr(TEST_DATA_SIZE*sizeof(double));
69     double *in2_ptr  = (double *)__malloc_ddr(TEST_DATA_SIZE*sizeof(double));
70     double *out_ptr  = (double *)__malloc_ddr(TEST_DATA_SIZE*sizeof(double));
72     TEST_DEBUG_PRINT("in1_ptr  is: 0x%08x.\n", (unsigned int)in1_ptr);
73     TEST_DEBUG_PRINT("in2_ptr  is: 0x%08x.\n", (unsigned int)in2_ptr);
74     TEST_DEBUG_PRINT("out_ptr  is: 0x%08x.\n", (unsigned int)out_ptr);
76     if(in1_ptr==NULL || in2_ptr==NULL || out_ptr==NULL) {
77         TEST_DEBUG_PRINT("No memory!\n");
78         exit(0);
79     }
80     else {
81         TEST_DEBUG_PRINT("Memory allocated.\n");
82     }
84     // Fill memory with data for testing. 
85     app_fill_memory(in1_ptr, in2_ptr, TEST_DATA_SIZE);
87     // OpenCL initialization
88     lib_init_arm();
89         
90         // Testing - print L2 start address
91         lib_find_l2_start();
92         
93     // Pass input/output buffers to library function which sums two input buffers
94     // and return the sum in the output buffer. 
95     lib_kernel_arm(in1_ptr, in2_ptr, out_ptr, TEST_DATA_SIZE);
97     __free_ddr(in1_ptr); 
98     __free_ddr(in2_ptr); 
99     __free_ddr(out_ptr); 
101         double err = app_err_check(in1_ptr, in2_ptr, out_ptr, TEST_DATA_SIZE);
102         
103     TEST_DEBUG_PRINT("Error checking. Difference between ARM results and DSP results: %e\n", err);
104         
105         if(err != 0) {
106         TEST_DEBUG_PRINT("Failed!\n");          
107         }
108         else {
109         TEST_DEBUG_PRINT("Passed!\n");          
110         }
111         
112     return(0);
113 } /* main */
115 /*==============================================================================
116  * Filling memory with random data.
117  *============================================================================*/
118 void app_fill_memory(double *buf1, double *buf2, int num_elements)
120     for(int i=0; i<num_elements; i++)
121     {
122         buf1[i] = (double)rand()/RAND_MAX;
123         buf2[i] = (double)rand()/RAND_MAX;
124     }
126     for(int i=0;i<10;i++)
127     {
128       TEST_DEBUG_PRINT("ARM Input 1: %e, Input 2: %e\n", buf1[i],buf2[i]);
129     }
131 } /* app_fill_memory */
133 /*==============================================================================
134  * Error checking: check if buffer out is the sum of buffer in1 and buffer in2.
135  *============================================================================*/
136 double app_err_check(double *in1, double *in2, double *out, int num_elements)
138     double error = 0.0;
140     for(int i=0;i<10;i++)
141     {
142       TEST_DEBUG_PRINT("Output returned by DSP: %e\n", out[i]);
143     }
144   
145     for(int i=0; i<num_elements; i++)
146     {
147         error += out[i] - (in1[i]+in2[i]);
148     }
149    
150     return(error);
151 } /* app_err_check */
153 /* Nothing past this point */