PASDK-258:Merge remote-tracking branch 'origin/dev_pasdk_pp_pasdk242HigherSamplingRat...
[processor-sdk/performance-audio-sr.git] / psdk_cust / libarch_k2g_1_0_1_0 / examples / common / test_dsp_kernel.c
1 /******************************************************************************
2  * Copyright (c) 2015-2017, Texas Instruments Incorporated - http://www.ti.com
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <stdio.h>
29 #include <ti/libarch/libarch.h>
32 /*
33  * This file shows an example of a DSP library that uses the library framework API. 
34  */
36 /* Size requirement of each of the 4 memory types */
37 #ifdef SOC_K2H
38   #define TEST_MEM_SIZE_VFAST (28*1024UL) 
39   #define TEST_MEM_SIZE_FAST  (512*1024UL)
40   #define TEST_MEM_SIZE_MED   (4608*1024UL)  //4.5MB
41   #define TEST_MEM_SIZE_SLOW  (10240*1024UL) //10MB
42 #endif
43 #ifdef SOC_AM572x
44     #define TEST_MEM_SIZE_VFAST (28*1024UL)
45     #define TEST_MEM_SIZE_FAST  (20*1024UL)
46     #define TEST_MEM_SIZE_MED   (256*1024UL)  //256KB
47     #define TEST_MEM_SIZE_SLOW  (1024*1024UL) //1MB
48 #endif
49 #ifdef SOC_C6678
50     #define TEST_MEM_SIZE_VFAST (28*1024UL) 
51     #define TEST_MEM_SIZE_FAST  (20*1024UL)
52     #define TEST_MEM_SIZE_MED   (2048*1024UL)   //2MB 
53     #define TEST_MEM_SIZE_SLOW  (10240*1024UL)  //10MB        
54 #endif
55 #ifdef SOC_K2G
56     #define TEST_MEM_SIZE_VFAST (28*1024UL) 
57     #define TEST_MEM_SIZE_FAST  (20*1024UL)
58     #define TEST_MEM_SIZE_MED   (128*1024UL)   //128KB 
59     #define TEST_MEM_SIZE_SLOW  (1024*1024UL)  //1MB        
60 #endif
61 #define LIBFW_TEST_INIT_NOERR 0
62 #define LIBFW_TEST_INIT_ERROR 1
64 #define LIBFW_TEST_DATA_SIZE  256
66 /* Define memory descriptors for memory management */
67 lib_memdscr_t test_vfast_buf;
68 lib_memdscr_t test_fast_buf;
69 lib_memdscr_t test_med_buf;
70 lib_memdscr_t test_slow_buf;
72 /* Define a memory descriptor array */
73 lib_memdscr_t * test_memdscr_tab[LIB_MEMTYPE_N] = {
74     &test_vfast_buf,
75     &test_fast_buf,
76     &test_med_buf,
77     &test_slow_buf
78 };
80 #ifdef SOC_K2G
81 /* defined in src/ti/libarch/src/k2g/k2g_cfg.c */
82 extern signed char* getGlobalAddr(signed char* addr);
83 #else
84 void * getGlobalAddr(signed char* addr)
85 {
86     return ((void *)addr);
87 }
88 #endif
90 /*==============================================================================
91  * This function returns the address of the memory descriptor array
92  *============================================================================*/
93 void * testGetMemHandle()
94 {
95     return((void *)&test_memdscr_tab[0]);
96 } /* testGetMemHandle */
98 /*==============================================================================
99  * Example of library memory requirement query function
100  *   It returns the size requirement of each of the 4 memory types defined in 
101  *   the library framework. 
102  *============================================================================*/
103 void test_GetSizes(size_t *smem_size_vfast, size_t *smem_size_fast, 
104                    size_t *smem_size_med,   size_t *smem_size_slow)
106     *smem_size_vfast = TEST_MEM_SIZE_VFAST;  // very fast scratch memory
107     *smem_size_fast  = TEST_MEM_SIZE_FAST;   // fast scratch memory
108     *smem_size_med   = TEST_MEM_SIZE_MED;    // medium speed scratch memory
109     *smem_size_slow  = TEST_MEM_SIZE_SLOW;   // slow scratch memory
110 } /* test_GetSizes */
112 /*==============================================================================
113  * Example of library initialization function
114  *   It performs necessary initialization through library framework API in order
115  *   to do memory allocations.  
116  *============================================================================*/
117 int test_Init(void * svfast_buf_base, size_t svfast_buf_size,
118               void * sfast_buf_base,  size_t sfast_buf_size,
119               void * smed_buf_base,   size_t smed_buf_size,
120               void * sslow_buf_base,  size_t sslow_buf_size)
122     lib_memdscr_t **test_mem_handle = testGetMemHandle();
124     /* Verify supplied memories meet requirements */    
125     if(  (svfast_buf_base!=NULL) && (svfast_buf_size>=TEST_MEM_SIZE_VFAST)
126        &&(sfast_buf_base !=NULL) && (sfast_buf_size >=TEST_MEM_SIZE_FAST)
127        &&(smed_buf_base  !=NULL) && (smed_buf_size  >=TEST_MEM_SIZE_MED) 
128        &&(sslow_buf_base !=NULL) && (sslow_buf_size >=TEST_MEM_SIZE_MED) 
129       ) {
130         lib_smem_vinit(test_mem_handle, svfast_buf_base, svfast_buf_size);
131         lib_smem_finit(test_mem_handle, sfast_buf_base,  sfast_buf_size);
132         lib_smem_minit(test_mem_handle, smed_buf_base,   smed_buf_size);
133         lib_smem_sinit(test_mem_handle, sslow_buf_base,  sslow_buf_size);       
134         
135         return(LIBFW_TEST_INIT_NOERR);
136     }
137     else {
138         return(LIBFW_TEST_INIT_ERROR);
139     }
140 } /* test_Init */
143 /*==============================================================================
144  * Example of library processing function
145  *   It uses library framework API to do:
146  *      - scratch memory allocations
147  *      - memory transfers
148  *============================================================================*/
149 void lib_dsp_func(const double *in1, const double *in2, double *out,
150                    int num_elements)
152     double *vfast_buf, *fast_buf1, *fast_buf2, *med_buf, *slow_buf;
153     void *test_mem_handle;
154     lib_emt_Handle test_emt_handle;
155     int i;
156   
157     printf("DSP library kernel for LibArch testing:\n");
158   
159     /* Use memory allocation API to allocate memories. This can also be done in 
160        test_Init, but that would require usage of global variables.  */
161     test_mem_handle = testGetMemHandle();
162     vfast_buf = (double *)lib_smem_valloc(test_mem_handle, num_elements*sizeof(double), 3);
163     fast_buf1 = (double *)lib_smem_falloc(test_mem_handle, num_elements*sizeof(double), 3);
164     med_buf   = (double *)lib_smem_malloc(test_mem_handle, num_elements*sizeof(double), 3);
165     slow_buf  = (double *)lib_smem_salloc(test_mem_handle, num_elements*sizeof(double), 3);
166   
167     if(vfast_buf==NULL || fast_buf1==NULL || med_buf==NULL || slow_buf==NULL) {
168         printf("Scratch (shared) heap allocation error!\n");
169         return;
170     }
171   
172     /* Use external memory transfer API */
173     if((test_emt_handle=lib_emt_alloc(1))==NULL) {
174         printf("External memory transfer handle allocation error!\n");
175         return;    
176     } 
177   
178     printf("DSP library kernel: Transferring input 1 to very fast memory buffer (L1D).\n");
179     if(lib_emt_copy1D1D(test_emt_handle,
180                         (void *)getGlobalAddr((signed char *)in1),
181                         (void *)getGlobalAddr((signed char *)vfast_buf),
182                         num_elements*sizeof(double))) {
183         printf("External memory transfer error!\n");
184         return;    
185     }
186   
187     lib_emt_wait(test_emt_handle);
188   
189     printf("DSP library kernel: Transferring input 2 to fast memory buffer (L2).\n");
190     if(lib_emt_copy1D1D(test_emt_handle,
191                         (void *)getGlobalAddr((signed char *)in2),
192                         (void *)getGlobalAddr((signed char *)fast_buf1),
193                          num_elements*sizeof(double))){
194         printf("External memory transfer error!\n");
195         return;    
196     }
197   
198     lib_emt_wait(test_emt_handle);
199   
200     /*
201     for(i=0;i<10;i++)
202     {
203         printf("Input 1: %e, Input 2: %e\n", vfast_buf[i],fast_buf1[i]);
204     }
205     */  
207     /* Process input data */
208     printf("DSP library kernel: Processing data in very fast memory.\n");
209     for(i=0;i<num_elements;i++){
210         vfast_buf[i] += fast_buf1[i];
211     }
212   
213     /* Allocate another block of memory */
214     fast_buf2 = lib_smem_falloc(test_mem_handle, num_elements*sizeof(double), 3);
215   
216     /* Use internal memory transfer API */
217     printf("DSP library kernel: Transferring data from very fast memory to fast memory.\n");
218     lib_imt_copy((void *)vfast_buf, (void *)fast_buf2, num_elements*sizeof(double));
219     lib_imt_wait();
220     /*
221     for(i=0;i<10;i++)
222     {
223         printf("Output: %e\n", fast_buf2[i]);
224     }
225     */
227     printf("DSP library kernel: Transferring data from fast memory to output buffer.\n");
228     if(lib_emt_copy1D1D(test_emt_handle,
229                         (void *)getGlobalAddr((signed char *)fast_buf2),
230                         (void *)getGlobalAddr((signed char *)out),
231                         num_elements*sizeof(double))) {
232       printf("Memory transfer to output error!\n");
233       return;    
234     }
235   
236     lib_emt_wait(test_emt_handle);
237     
238     lib_emt_free(test_emt_handle);
239     
240     printf("DSP library kernel finished.\n");
241     
242 } /* lib_dsp_func */      
244 /* Nothing after this line */