[processor-sdk/performance-audio-sr.git] / psdk_cust / pdk_k2g_1_0_1_1_eng / packages / ti / csl / Settings.xdc
3 module Settings
4 {
5 /*! This is the CSL Version */
6 config string cslVersionString = "03.03.00.02";
8 /*! The flag is used to indicate if the CSL INTC Library needs to be built or not.
9 * This flag is FALSE by default since most operating systems provide INTC support and
10 * do not need to use this library.
11 * To ensure that the INTC library is also returned; add the following lines to the
12 * configuration file
13 *
14 * var cslSettings = xdc.useModule ('ti.csl.Settings');
15 * cslSettings.useCSLIntcLib = true;
16 *
17 */
18 config Bool useCSLIntcLib = false;
20 /*! This variable is to control the device type selection.
21 * By default this variable is set to NULL.
22 *
23 * To use CSL for the selected device, add the following lines to config
24 * file and set the deviceType correctly:
25 *
26 * var cslSettings = xdc.useModule ('ti.csl.Settings');
27 * cslSettings.deviceType = "k2k";
28 *
29 */
30 metaonly config string deviceType = "";
31 }