]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - processor-sdk/performance-audio-sr.git/blob - psdk_cust/pdk_k2g_1_0_1_2_eng/packages/pdkProjectCreate.bat
Changes for update to processor_audio_sdk_1_00_00_04 from processor_audio_sdk_1_00_00_03.
[processor-sdk/performance-audio-sr.git] / psdk_cust / pdk_k2g_1_0_1_2_eng / packages / pdkProjectCreate.bat
1 @REM ******************************************************************************
2 @REM * FILE PURPOSE: PDK Unit Test and Example Project Creator
3 @REM ******************************************************************************
4 @REM * FILE NAME: pdkProjectCreate.bat
5 @REM *
6 @REM * DESCRIPTION: 
7 @REM *  The script file is used to create the test and example projects of all
8 @REM *  components under PDK. These projects are available in the specified
9 @REM *  workspace.
10 @REM *
11 @REM * Syntax:
12 @REM *  pdkProjectCreate.bat [soc] [board] [endian] [module] [processor] [pdkDir]
13 @REM *
14 @REM * Description:     (first option is default)
15 @REM *  soc         -   AM335x / AM437x / AM571x / AM572x / K2E / K2G / K2K / K2H / K2L /
16 @REM *                  C6678 / C6657
17 @REM *  board       -   all (use "all" for K2X and C66X SOCs)
18 @REM *                  -or-
19 @REM *                  Refer to pdk_<soc>_<version>\packages\ti\board\lib
20 @REM *                  for valid board inputs for the soc
21 @REM *  endian      -   little / big
22 @REM *  module      -   all
23 @REM *                  -or-
24 @REM *                  aif2 / bcp / cppi / csl / dfe / emac / fatfs / fm / fftc / 
25 @REM *                  gpio / hyplnk / i2c / icss_emac / iqn2 / mcasp / mcbsp / mmcsd / nimu / 
26 @REM *                  nimu_icss / nwal / pa / pcie / pktlib / pruss / qmss / rm / sa /
27 @REM *                  serdes-diag / spi / srio / tcp3d / tfw / transportqmss /
28 @REM *                  transportsrio / tsip / uart / usb / wdtimer
29 @REM *  processor   -   arm / dsp / m4
30 @REM *  pdkDir      -   THIS FILE LOCATION / "C:\ti\pdk_<soc>_<version>\packages"
31 @REM *
32 @REM * Example:
33 @REM *  a) pdkProjectCreate.bat
34 @REM *              - Creates all module projects for the AM335x soc for arm little endian
35 @REM *  b) pdkProjectCreate.bat AM437x
36 @REM *              - Creates all module projects for the AM437x soc for arm little endian
37 @REM *  c) pdkProjectCreate.bat AM437x idkAM437x
38 @REM *              - Creates all module projects for idkAM437x device for arm little endian
39 @REM *  d) pdkProjectCreate.bat AM571x evmAM571x little
40 @REM *              - Creates all module projects for evmAM571x device for arm little endian
41 @REM *  e) pdkProjectCreate.bat AM571x evmAM571x little i2c dsp
42 @REM *              - Creates i2c module projects for evmAM571x device for dsp little endian
43 @REM *  f) pdkProjectCreate.bat K2H all little i2c arm
44 @REM *              - Creates i2c module projects for K2H device for arm little endian
45 @REM *  g) pdkProjectCreate.bat C6678 all little hyplnk dsp
46 @REM *              - Creates hyplnk module projects for C6678 device for dsp little endian
47 @REM *
48 @REM * Copyright (C) 2012-2016, Texas Instruments, Inc.
49 @REM *****************************************************************************
50 @echo OFF
52 REM Lists of valid input parameters - MUST be updated as new input parameters are added
53 REM *****************************************************************************
54 set soc_list=AM335x AM437x AM571x AM572x K2E K2K K2H K2L K2G C6678 C6657
55 set endian_list=little big
56 set module_list=all aif2 bcp cppi csl dfe emac fatfs fm fftc gpio hyplnk i2c icss_emac iqn2 mcasp mcbsp mmcsd nimu nimu_icss nwal pa pcie pktlib pruss qmss rm sa serdes_diag spi srio tcp3d tfw transportqmss transportsrio tsip uart usb wdtimer
57 set proc_list=arm dsp m4
59 REM Parameter Validation: Check if the argument was passed to the batch file.
60 REM *****************************************************************************
61 REM Argument [soc] is used to set SOC variable.
62 set tempVar1=%1
63 if not defined tempVar1 goto nosoc
64 set SOC=%tempVar1%
65 goto socdone
66 :nosoc
67 set SOC=AM335x
68 :socdone
70 REM Argument [board] is used to set BOARD variable.
71 REM This is the board type of the soc for which project are to be created.
72 set tempVar2=%2
73 if not defined tempVar2 goto noboard
74 set BOARD=%tempVar2%
75 goto boarddone
76 :noboard
77 set BOARD=all
78 :boarddone
80 REM Argument [endian] is used to set ENDIAN variable.
81 REM This is Endianess of the projects being created.
82 REM Valid Values are 'little' and 'big'. Defaults to 'little'.
83 set tempVar3=%3
84 if not defined tempVar3 goto littleendian
85 set ENDIAN=%tempVar3%
86 goto endiandone
87 :littleendian
88 set ENDIAN=little
89 :endiandone
91 REM Argument [module] is used to set MODULE variable.
92 REM This is specific module for which projects are created.
93 REM Valid Values are LLD name. Defaults to all LLD's.
94 set tempVar4=%4
95 if not defined tempVar4 goto nomodule
96 set MODULE=%tempVar4%
97 goto moduledone
98 :nomodule
99 set MODULE=all
100 :moduledone
102 REM Argument [processor] is used to set PROCESSOR variable.
103 REM This is specific processor type for which projects are created.
104 REM Valid Values are arm, dsp, or m4 . Defaults to arm.
105 set tempVar5=%5
106 if not defined tempVar5 goto noprocessor
107 set PROCESSOR=%tempVar5%
108 goto processordone
109 :noprocessor
110 set PROCESSOR=arm
111 :processordone
113 REM Argument [pdkDir] is used to set PDK_SHORT_NAME. This is PDK directory
114 REM where project description files are located. If there is no value passed,
115 REM it defaults to the file location directory. Then convert the variable to 
116 REM short name to avoid issues using batch file commands.
117 set tempVar6=%6
118 if not defined tempVar6 goto noparameter
119 set PDK_SHORT_NAME=%tempVar6%
120 goto done
121 :noparameter
122 set PDK_SHORT_NAME=%~sdp0
123 :done
125 REM *****************************************************************************
127 echo =========================================================================
128 echo Configuration:
129 echo.   SOC             :   %SOC%
130 echo    BOARD           :   %BOARD%
131 echo.   ENDIAN          :   %ENDIAN%
132 echo.   MODULE          :   %MODULE%
133 echo.   PROCESSOR       :   %PROCESSOR%
134 echo.   PDK_SHORT_NAME  :   %PDK_SHORT_NAME%
135 echo =========================================================================
136 echo Checking Configuration...
138 for %%a in (%soc_list%) do (
139     if %SOC% == %%a (
140         goto end_soc_check
141     )
143 echo ERROR: SOC (%SOC%) is invalid
144 goto CONFIG_ERR
145 :end_soc_check
147 if %BOARD% == all (
148     goto end_board_check
150 setlocal enabledelayedexpansion
151 set board_type=!BOARD:%SOC%=!
152 if not %board_type% == %BOARD% (
153     goto end_board_check
155 echo ERROR: Board (%BOARD%) is invalid for the specified SOC (%SOC%)
156 goto CONFIG_ERR
157 :end_board_check
159 for %%a in (%endian_list%) do (
160     if %ENDIAN% == %%a (
161         goto end_endian_check
162     )
164 echo ERROR: Endian (%ENDIAN%) is invalid
165 goto CONFIG_ERR
166 :end_endian_check
168 for %%a in (%module_list%) do (
169     if %MODULE% == %%a (
170         goto end_module_check
171     )
173 echo ERROR: Module (%MODULE%) is invalid
174 goto CONFIG_ERR
175 :end_module_check
177 for %%a in (%proc_list%) do (
178     if %PROCESSOR% == %%a (
179         goto end_proc_check
180     )
182 echo ERROR: Processor (%PROCESSOR%) is invalid
183 goto CONFIG_ERR
184 :end_proc_check
186 if %SOC% == AM335x (
187     if %PROCESSOR% == dsp (
188         echo ERROR: The AM335x soc does not contain a DSP processor
189         goto CONFIG_ERR
190     ) else if %PROCESSOR% == m4 (
191         echo ERROR: The AM335x soc does not contain a M4 processor
192         goto CONFIG_ERR
193     )
195     if %ENDIAN% == big (
196         echo ERROR: The AM335x soc's arm does not support big endian
197         goto CONFIG_ERR
198     )
199 ) else if %SOC% == AM437x (
200     if %PROCESSOR% == dsp (
201         echo ERROR: The AM437x soc does not contain a DSP processor
202         goto CONFIG_ERR
203     ) else if %PROCESSOR% == m4 (
204         echo ERROR: The AM437x soc does not contain a M4 processor
205         goto CONFIG_ERR
206     )
208     if %ENDIAN% == big (
209         echo ERROR: The AM437x soc's arm does not support big endian
210         goto CONFIG_ERR
211     )
212 ) else if %SOC% == AM571x (
213     if %ENDIAN% == big (
214         echo ERROR: The AM571x soc's processor's do not support big endian
215         goto CONFIG_ERR
216     )
217 ) else if %SOC% == AM572x (
218     if %ENDIAN% == big (
219         echo ERROR: The AM572x soc's processor's do not support big endian
220         goto CONFIG_ERR
221     )
222 )  else if %SOC% == K2K (
223     if %PROCESSOR% == m4 (
224         echo ERROR: The K2K soc does not contain a M4 processor
225         goto CONFIG_ERR
226     )
227     
228     if %PROCESSOR% == arm (
229         if %ENDIAN% == big (
230             echo ERROR: The K2K soc's arm does not support big endian
231             goto CONFIG_ERR
232         )
233     )
234 ) else if %SOC% == K2H (
235     if %PROCESSOR% == m4 (
236         echo ERROR: The K2H soc does not contain a M4 processor
237         goto CONFIG_ERR
238     )
239     
240     if %PROCESSOR% == arm (
241         if %ENDIAN% == big (
242             echo ERROR: The K2H soc's arm does not support big endian
243             goto CONFIG_ERR
244         )
245     )
246 ) else if %SOC% == K2E (
247     if %PROCESSOR% == m4 (
248         echo ERROR: The K2E soc does not contain a M4 processor
249         goto CONFIG_ERR
250     )
251     
252     if %PROCESSOR% == arm (
253         if %ENDIAN% == big (
254             echo ERROR: The K2E soc's arm does not support big endian
255             goto CONFIG_ERR
256         )
257     )
258 ) else if %SOC% == K2L (
259     if %PROCESSOR% == m4 (
260         echo ERROR: The K2L soc does not contain a M4 processor
261         goto CONFIG_ERR
262     )
263     
264     if %PROCESSOR% == arm (
265         if %ENDIAN% == big (
266             echo ERROR: The K2L soc's arm does not support big endian
267             goto CONFIG_ERR
268         )
269     )
270 ) else if %SOC% == K2G (
271     if %PROCESSOR% == m4 (
272         echo ERROR: The K2G soc does not contain a M4 processor
273         goto CONFIG_ERR
274     )
275     
276     if %PROCESSOR% == arm (
277         if %ENDIAN% == big (
278             echo ERROR: The K2G soc's arm does not support big endian
279             goto CONFIG_ERR
280         )
281     )
282 ) else if %SOC% == C6678 (
283     if %PROCESSOR% == m4 (
284         echo ERROR: The C6678 soc does not contain a M4 processor
285         goto CONFIG_ERR
286     )
287     
288     if %PROCESSOR% == arm (
289         echo ERROR: The C6678 soc does not contain an arm processor
290         goto CONFIG_ERR
291     )
292 ) else if %SOC% == C6657 (
293     if %PROCESSOR% == m4 (
294         echo ERROR: The C6657 soc does not contain a M4 processor
295         goto CONFIG_ERR
296     )
297     
298     if %PROCESSOR% == arm (
299         echo ERROR: The C6657 soc does not contain an arm processor
300         goto CONFIG_ERR
301     )
302 ) else (
303     echo ERROR: Invalid soc
304     goto CONFIG_ERR
307 goto CONFIG_COMPLETE
309 :CONFIG_ERR
310 echo Exiting...
311 echo =========================================================================
312 goto ENDSCRIPT
314 :CONFIG_COMPLETE
315 echo Complete
316 echo =========================================================================
318 REM *****************************************************************************
319 REM * Version Information of the various tools etc required to build the test
320 REM * projects. Customers are free to modify these to meet their requirements.
321 REM *****************************************************************************
323 REM This is to control the CCS version specific project create command
324 REM Set to 'no' when using CCSv5 and CCSv6 or set to 'yes' when using CCSv4
325 set IS_CCS_VERSION_4=no
327 REM Set to 'no' when using QT, EVM, VDB, or other hardware. Set to 'yes' only when using the simulator.
328 set IS_SIMULATOR_SUPPORT_NEEDED=no
330 REM Install Location for CCS
331 set CCS_INSTALL_PATH="C:\ti\ccsv6"
333 REM Workspace where the PDK projects will be created.
334 set MY_WORKSPACE=%PDK_SHORT_NAME%\MyExampleProjects
336 REM macros.ini location
337 set MACROS_FILE=%PDK_SHORT_NAME%\macros.ini
339 REM This is the format of the executable being created
340 REM Valid Values are 'ELF' and 'COFF'
341 set OUTPUT_FORMAT=ELF
343 REM Version of CG-Tools
344 set CGT_VERSION=8.1.0
346 REM Version of CG-ARM-Tools for M4
347 set CGT_M4_VERSION=5.2.5
349 REM Version of XDC
350 set XDC_VERSION=3.32.00.06
352 REM Version of BIOS
353 set BIOS_VERSION=6.45.01.29
355 REM Version of CG-Tools for ARM
356 set CGT_VERSION_ARM=GNU_4.8.4:Linaro
358 REM Version of the IPC
359 set IPC_VERSION=3.42.00.02
361 REM EDMA3 Version
362 set EDMA_VERSION=2.12.01.23
364 REM Version of the PDK
365 set PDK_VERSION=1.0.1
367 REM Version of the NDK
368 set NDK_VERSION=2.24.03.35
370 REM Version of UIA
371 set UIA_VERSION=2.00.03.43
373 REM PDK Part Number & Platform name
374 if %SOC% == K2K (
375     set PDK_PARTNO=TCI6638
376     set PDK_ECLIPSE_ID=com.ti.pdk.k2hk
377     set RTSC_PLATFORM_NAME=ti.platforms.evmTCI6638K2K
378     if %PROCESSOR% == arm (
379         set RTSC_TARGET=gnu.targets.arm.A15F
380         set CCS_DEVICE="Cortex A.TCI6638K2K"
381     )
382 ) else if  %SOC% == K2H (
383     set PDK_PARTNO=TCI6636
384     set PDK_ECLIPSE_ID=com.ti.pdk.k2hk
385     set RTSC_PLATFORM_NAME=ti.platforms.evmTCI6636K2H
386     if %PROCESSOR% == arm (
387         set RTSC_TARGET=gnu.targets.arm.A15F
388         set CCS_DEVICE="Cortex A.66AK2H12"
389     )
390 ) else if  %SOC% == K2L (
391     set PDK_PARTNO=TCI6630
392     set PDK_ECLIPSE_ID=com.ti.pdk.k2l
393     set RTSC_PLATFORM_NAME=ti.platforms.evmTCI6630K2L
394     if %PROCESSOR% == arm (
395         set RTSC_TARGET=gnu.targets.arm.A15F
396         set CCS_DEVICE="Cortex A.TCI6630K2L"
397     )
398 ) else if  %SOC% == K2E (
399     set PDK_PARTNO=66AK2E05
400     set PDK_ECLIPSE_ID=com.ti.pdk.k2e
401     set RTSC_PLATFORM_NAME=ti.platforms.evmC66AK2E
402     if %PROCESSOR% == arm (
403         set RTSC_TARGET=gnu.targets.arm.A15F
404         set CCS_DEVICE="Cortex A.66AK2E05"
405     )
406 ) else if  %SOC% == K2G (
407     set PDK_PARTNO=66AK2G02
408     set PDK_ECLIPSE_ID=com.ti.pdk.k2g
409     set RTSC_PLATFORM_NAME=ti.platforms.evmTCI66AK2G02
410     if %PROCESSOR% == arm (
411         set RTSC_TARGET=gnu.targets.arm.A15F
412         set CCS_DEVICE="Cortex A.66AK2G02"
413     )
414 ) else if  %SOC% == AM571x (
415     set PDK_PARTNO=AM571X
416     set PDK_ECLIPSE_ID=com.ti.pdk.am57xx
417     set RTSC_PLATFORM_NAME=ti.platforms.evmAM571X
418     if %PROCESSOR% == arm (
419         set RTSC_TARGET=gnu.targets.arm.A15F
420         set CCS_DEVICE="Cortex A.AM5728_RevA"
421     ) else if %PROCESSOR% == m4 (
422         set RTSC_TARGET=ti.targets.arm.elf.M4
423         set CCS_DEVICE="Cortex M.AM5728_RevA"
424     )
425 ) else if  %SOC% == AM572x (
426     set PDK_PARTNO=AM572X
427     set PDK_ECLIPSE_ID=com.ti.pdk.am57xx
428     set RTSC_PLATFORM_NAME=ti.platforms.evmAM572X
429     if %PROCESSOR% == arm (
430         set RTSC_TARGET=gnu.targets.arm.A15F
431         set CCS_DEVICE="Cortex A.AM5728_RevA"
432     ) else if %PROCESSOR% == m4 (
433         set RTSC_TARGET=ti.targets.arm.elf.M4
434         set CCS_DEVICE="Cortex M.AM5728_RevA"
435     )
436 ) else if  %SOC% == AM335x (
437     set PDK_PARTNO=AM335
438     set PDK_ECLIPSE_ID=com.ti.pdk.am335x
439     set RTSC_PLATFORM_NAME=ti.platforms.evmAM3359
440     set RTSC_TARGET=gnu.targets.arm.A8F
441     set CCS_DEVICE="Cortex A.AM3359.ICE_AM3359"
442 ) else if  %SOC% == AM437x (
443     set PDK_PARTNO=AM437
444     set PDK_ECLIPSE_ID=com.ti.pdk.am437x
445     set RTSC_PLATFORM_NAME=ti.platforms.evmAM437X
446     set RTSC_TARGET=gnu.targets.arm.A9F
447     set CCS_DEVICE="Cortex A.AM4379.IDK_AM437X"
448 ) else if  %SOC% == C6678 (
449     set PDK_PARTNO=C6678L
450     set PDK_ECLIPSE_ID=com.ti.pdk.c667x
451     set RTSC_PLATFORM_NAME=ti.platforms.evm6678
452 ) else if  %SOC% == C6657 (
453     set PDK_PARTNO=C6657
454     set PDK_ECLIPSE_ID=com.ti.pdk.c665x
455     set RTSC_PLATFORM_NAME=ti.platforms.evm6657
456 ) else (
457     REM Need to exit the batch script cleanly 
458     set PDK_PARTNO=TCI6634
459     set PDK_ECLIPSE_ID=ti.pdk
460     set RTSC_PLATFORM_NAME=ti.platforms.simKepler
463 REM RTSC Target 
464 REM - Please ensure that you select this taking into account the
465 REM   OUTPUT_FORMAT and the RTSC_PLATFORM_NAME 
466 if %PROCESSOR% == dsp (
467     if %ENDIAN% == big (
468         set RTSC_TARGET=ti.targets.elf.C66_big_endian
469         set CCS_DEVICE="com.ti.ccstudio.deviceModel.C6000.GenericC64xPlusDevice"
470     ) else ( 
471         set RTSC_TARGET=ti.targets.elf.C66
472         set CCS_DEVICE="com.ti.ccstudio.deviceModel.C6000.GenericC64xPlusDevice"
473     )
476 echo    PDK_PARTNO         : %PDK_PARTNO%
477 echo    PDK_ECLIPSE_ID     : %PDK_ECLIPSE_ID%
478 echo    RTSC_PLATFORM_NAME : %RTSC_PLATFORM_NAME%
479 echo.   RTSC_TARGET        : %RTSC_TARGET%
480 echo.   CCS_DEVICE         : %CCS_DEVICE%
481 REM *****************************************************************************
482 REM *****************************************************************************
483 REM                 Please do NOT change anything below this
484 REM *****************************************************************************
485 REM *****************************************************************************
487 REM Set auto create command by default for use with CCSv5 and CCSv6
488 set AUTO_CREATE_COMMAND=eclipse\eclipsec -noSplash
490 REM If is CCS version 4 then set auto create command for use with CCSv4
491 if .%IS_CCS_VERSION_4% == .yes set AUTO_CREATE_COMMAND=eclipse\jre\bin\java -jar %CCS_INSTALL_PATH%\eclipse\startup.jar
493 REM Set project for Silicon or QT by default
494 set SIMULATOR_SUPPORT_DEFINE=
496 REM If simulator support is needed then set the define
497 if .%IS_SIMULATOR_SUPPORT_NEEDED% == .yes set SIMULATOR_SUPPORT_DEFINE=-ccs.setCompilerOptions "--define SIMULATOR_SUPPORT"
499 REM Goto the PDK Installation Path.
501 pushd %PDK_SHORT_NAME%
503 echo *****************************************************************************
504 echo Detecting all projects in PDK and importing them in the workspace %MY_WORKSPACE%
506 REM Set BOARD to equal the SOC if BOARD is set to "all".  All projects for the
507 REM SOC will be picked up
508 if %BOARD% == all set BOARD=%SOC%
509 REM Set MODULE to null string so it picks up all projects of PROCESSOR
510 if %MODULE% == all set MODULE=""
512 if %PROCESSOR% == dsp (
513     REM Search for all the dsp test Project Files in the PDK.
514     for /F %%I IN ('dir /b /s *%MODULE%*%BOARD%*c66*roject.txt') do (
515         set project_detected = 1
517         echo Detected Test Project: %%~nI
519         REM Goto each directory where the test project file is located and create the projects.
520         pushd %%~dI%%~pI
522         REM Execute the command to create the project using the parameters specified above.
523         %CCS_INSTALL_PATH%\%AUTO_CREATE_COMMAND% -data %MY_WORKSPACE% -application com.ti.ccstudio.apps.projectCreate -ccs.name %%~nI -ccs.outputFormat %OUTPUT_FORMAT% -ccs.device %CCS_DEVICE% -ccs.endianness %ENDIAN% -ccs.kind executable -ccs.cgtVersion %CGT_VERSION% -rtsc.xdcVersion %XDC_VERSION% -rtsc.enableDspBios -rtsc.biosVersion %BIOS_VERSION% -rtsc.buildProfile "debug" -rtsc.products "com.ti.sdo.edma3:%EDMA_VERSION%;com.ti.rtsc.IPC:%IPC_VERSION%;com.ti.rtsc.SYSBIOS:%BIOS_VERSION%;%PDK_ECLIPSE_ID%:%PDK_VERSION%;com.ti.rtsc.NDK:%NDK_VERSION%;com.ti.uia:%UIA_VERSION%" -rtsc.platform "%RTSC_PLATFORM_NAME%" -rtsc.target %RTSC_TARGET% -ccs.rts libc.a -ccs.args %%~nI%%~xI %SIMULATOR_SUPPORT_DEFINE% -ccs.overwrite full
525         echo Copying macros.ini
526         copy %MACROS_FILE% %MY_WORKSPACE%\%%~nI\macros.ini
528         popd
529     )
532 if %PROCESSOR% == arm (
533     REM Search for all the arm test Project Files in the PDK.
534     for /F %%I IN ('dir /b /s *%MODULE%*%BOARD%*arm*roject.txt') do (
535         set project_detected = 1
536         
537         echo Detected Test Project: %%~nI
539         REM Goto each directory where the test project file is located and create the projects.
540         pushd %%~dI%%~pI
542         REM Execute the command to create the project using the parameters specified above.
543         %CCS_INSTALL_PATH%\%AUTO_CREATE_COMMAND% -data %MY_WORKSPACE% -application com.ti.ccstudio.apps.projectCreate -ccs.cmd "" -ccs.name %%~nI -ccs.outputFormat %OUTPUT_FORMAT% -ccs.setLinkerOptions "-L${BIOS_CG_ROOT}/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/lib/fpu" -ccs.device %CCS_DEVICE% -ccs.endianness %ENDIAN% -ccs.kind executable -ccs.cgtVersion "%CGT_VERSION_ARM%" -rtsc.xdcVersion %XDC_VERSION% -rtsc.enableDspBios -rtsc.biosVersion %BIOS_VERSION% -rtsc.buildProfile "debug" -rtsc.products "com.ti.sdo.edma3:%EDMA_VERSION%;com.ti.rtsc.SYSBIOS:%BIOS_VERSION%;%PDK_ECLIPSE_ID%:%PDK_VERSION%;com.ti.rtsc.NDK:%NDK_VERSION%" -rtsc.platform "%RTSC_PLATFORM_NAME%" -rtsc.target %RTSC_TARGET% -ccs.rts libc.a libgcc.a libuart.a libm.a libnosys.a -ccs.args %%~nI%%~xI %SIMULATOR_SUPPORT_DEFINE% -ccs.overwrite full
545         echo Copying macro.ini
546         copy %MACROS_FILE% %MY_WORKSPACE%\%%~nI\macros.ini
548         popd
549     )
552 if %PROCESSOR% == m4 (
553     REM Search for all the m4 test Project Files in the PDK.
554     for /F %%I IN ('dir /b /s *%MODULE%*%BOARD%*m4*roject.txt') do (
555         set project_detected = 1
556         
557         echo Detected Test Project: %%~nI
559         REM Goto each directory where the test project file is located and create the projects.
560         pushd %%~dI%%~pI
562         REM Execute the command to create the project using the parameters specified above.
563         %CCS_INSTALL_PATH%\%AUTO_CREATE_COMMAND% -data %MY_WORKSPACE% -application com.ti.ccstudio.apps.projectCreate -ccs.cmd "" -ccs.name %%~nI -ccs.outputFormat %OUTPUT_FORMAT% -ccs.device %CCS_DEVICE% -ccs.endianness %ENDIAN% -ccs.kind executable -ccs.cgtVersion "%CGT_M4_VERSION%" -rtsc.xdcVersion %XDC_VERSION% -rtsc.enableDspBios -rtsc.biosVersion %BIOS_VERSION% -rtsc.buildProfile "debug" -rtsc.products "com.ti.sdo.edma3:%EDMA_VERSION%;com.ti.rtsc.SYSBIOS:%BIOS_VERSION%;%PDK_ECLIPSE_ID%:%PDK_VERSION%" -rtsc.platform "%RTSC_PLATFORM_NAME%" -rtsc.target %RTSC_TARGET% -ccs.rts libc.a libgcc.a libuart.a libm.a libnosys.a -ccs.args %%~nI%%~xI %SIMULATOR_SUPPORT_DEFINE% -ccs.overwrite full
565         echo Copying macro.ini
566         copy %MACROS_FILE% %MY_WORKSPACE%\%%~nI\macros.ini
568         popd
569     )
571 popd
573 if not defined project_detected (
574     echo No projects detected
577 echo Project generation complete
578 echo *****************************************************************************
580 :ENDSCRIPT