]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - processor-sdk/performance-audio-sr.git/blob - tools/pyalpha/serial/rs485.py
Add Debug, Release, and SDF build profiles. This allows normal build all and SDF...
[processor-sdk/performance-audio-sr.git] / tools / pyalpha / serial / rs485.py
1 #!/usr/bin/env python
3 # RS485 support
4 #
5 # This file is part of pySerial. https://github.com/pyserial/pyserial
6 # (C) 2015 Chris Liechti <cliechti@gmx.net>
7 #
8 # SPDX-License-Identifier:    BSD-3-Clause
10 """\
11 The settings for RS485 are stored in a dedicated object that can be applied to
12 serial ports (where supported).
13 NOTE: Some implementations may only support a subset of the settings.
14 """
16 import time
17 import serial
20 class RS485Settings(object):
21     def __init__(
22             self,
23             rts_level_for_tx=True,
24             rts_level_for_rx=False,
25             loopback=False,
26             delay_before_tx=None,
27             delay_before_rx=None):
28         self.rts_level_for_tx = rts_level_for_tx
29         self.rts_level_for_rx = rts_level_for_rx
30         self.loopback = loopback
31         self.delay_before_tx = delay_before_tx
32         self.delay_before_rx = delay_before_rx
35 class RS485(serial.Serial):
36     """\
37     A subclass that replaces the write method with one that toggles RTS
38     according to the RS485 settings.
40     NOTE: This may work unreliably on some serial ports (control signals not
41           synchronized or delayed compared to data). Using delays may be
42           unreliable (varying times, larger than expected) as the OS may not
43           support very fine grained delays (no smaller than in the order of
44           tens of milliseconds).
46     NOTE: Some implementations support this natively. Better performance
47           can be expected when the native version is used.
49     NOTE: The loopback property is ignored by this implementation. The actual
50           behavior depends on the used hardware.
52     Usage:
54         ser = RS485(...)
55         ser.rs485_mode = RS485Settings(...)
56         ser.write(b'hello')
57     """
59     def __init__(self, *args, **kwargs):
60         super(RS485, self).__init__(*args, **kwargs)
61         self._alternate_rs485_settings = None
63     def write(self, b):
64         """Write to port, controlling RTS before and after transmitting."""
65         if self._alternate_rs485_settings is not None:
66             # apply level for TX and optional delay
67             self.setRTS(self._alternate_rs485_settings.rts_level_for_tx)
68             if self._alternate_rs485_settings.delay_before_tx is not None:
69                 time.sleep(self._alternate_rs485_settings.delay_before_tx)
70             # write and wait for data to be written
71             super(RS485, self).write(b)
72             super(RS485, self).flush()
73             # optional delay and apply level for RX
74             if self._alternate_rs485_settings.delay_before_rx is not None:
75                 time.sleep(self._alternate_rs485_settings.delay_before_rx)
76             self.setRTS(self._alternate_rs485_settings.rts_level_for_rx)
77         else:
78             super(RS485, self).write(b)
80     # redirect where the property stores the settings so that underlying Serial
81     # instance does not see them
82     @property
83     def rs485_mode(self):
84         """\
85         Enable RS485 mode and apply new settings, set to None to disable.
86         See serial.rs485.RS485Settings for more info about the value.
87         """
88         return self._alternate_rs485_settings
90     @rs485_mode.setter
91     def rs485_mode(self, rs485_settings):
92         self._alternate_rs485_settings = rs485_settings