[processor-sdk/performance-audio-sr.git] / psdk_cust / pdk_k2g_1_0_1_2_eng / packages / ti / board / diag / dcan / src / dcan.h
diff --git a/psdk_cust/pdk_k2g_1_0_1_2_eng/packages/ti/board/diag/dcan/src/dcan.h b/psdk_cust/pdk_k2g_1_0_1_2_eng/packages/ti/board/diag/dcan/src/dcan.h
+++ /dev/null
@@ -1,819 +0,0 @@
-/*
- * Copyright (C) 2013 Texas Instruments Incorporated - http://www.ti.com/
- *
- * Redistribution and use in source and binary forms, with or without
- * modification, are permitted provided that the following conditions
- * are met:
- *
- * Redistributions of source code must retain the above copyright
- * notice, this list of conditions and the following disclaimer.
- *
- * Redistributions in binary form must reproduce the above copyright
- * notice, this list of conditions and the following disclaimer in the
- * documentation and/or other materials provided with the
- * distribution.
- *
- * Neither the name of Texas Instruments Incorporated nor the names of
- * its contributors may be used to endorse or promote products derived
- * from this software without specific prior written permission.
- *
- * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
- * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
- * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
- * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
- * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
- * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
- * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
- * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
- * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
- * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
- * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
- *
- */
-/**
- * \file dcan.h
- *
- * \brief This file contains the function prototypes for the device
- * abstraction layer of DCAN. It also contains necessary
- * structure, enum and macro definitions
- * DCAN : Controller Area Network Controller module
- *
- */
-#ifndef DCAN_H_
-#define DCAN_H_
-
-#ifdef __cplusplus
-extern "C" {
-#endif
-
-/* ========================================================================== */
-/* Include Files */
-/* ========================================================================== */
-#include <ti/csl/cslr_dcan.h>
-
-#include "hw_dcan.h"
-
-/* ========================================================================== */
-/* Macros & Typedefs */
-/* ========================================================================== */
-/**
- * \brief Maximum message length in bytes that can be transmitted or received
- * in a single message object
- */
-#define DCAN_MAX_MSG_LENGTH (8U)
-
-/**
- * \brief Maximum message objects that can be stored in Message RAM
- */
-#define DCAN_MAX_MSG_OBJECTS (64U)
-
-/**
- * \brief Invalid Message Object
- */
-#define DCAN_INVALID_MSG_OBJECT (0U)
-
-/** \brief Message Object Size*/
-#define DCAN_MSG_OBJ_SIZE (0x20)
-
-/**
- * \brief Mask used to deduce whether single bit error is detected or not
- */
-#define DCAN_ECC_SB_ERR_STS (DCAN_ECC_CSR_SE_FLAG_MASK)
-
-/**
- * \brief Mask used to deduce whether double bit error is detected or not
- */
-#define DCAN_ECC_DB_ERR_STS (DCAN_ECC_CSR_DE_FLAG_MASK)
-
-/** \brief Error Status is updated*/
-#define DCAN_ERR_STS_UPDATED (0x8000U)
-
-/* ========================================================================== */
-/* Structures and Enums */
-/* ========================================================================== */
-
-/**
- * \brief Enumerates the values used to set the direction of message object
- */
-typedef enum dcanDirection
-{
- DCAN_DIR_RX = DCAN_IFARB_DIR_RECEIVE,
- /**< Direction of message object is receive */
- DCAN_DIR_TX = DCAN_IFARB_DIR_TRANSMIT
- /**< Direction of message object is transmit */
-} dcanDirection_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN error and status
- * values
- */
-typedef enum dcanErrStsMask
-{
- DCAN_ES_MASK_NO_ERR = DCAN_ES_LEC_EN_1_0X0,
- /**< LEC error code : No error */
- DCAN_ES_MASK_STUFF_ERR = DCAN_ES_LEC_EN_2_0X1,
- /**< LEC error code : Stuff error */
- DCAN_ES_MASK_FORM_ERR = DCAN_ES_LEC_EN_3_0X2,
- /**< LEC error code : Form error */
- DCAN_ES_MASK_ACK_ERR = DCAN_ES_LEC_EN_4_0X3,
- /**< LEC error code : Ack error */
- DCAN_ES_MASK_BIT1_ERR = DCAN_ES_LEC_EN_5_0X4,
- /**< LEC error code : Bit1 error */
- DCAN_ES_MASK_BIT0_ERR = DCAN_ES_LEC_EN_6_0X5,
- /**< LEC error code : Bit0 error */
- DCAN_ES_MASK_CRC_ERR = DCAN_ES_LEC_EN_7_0X6,
- /**< LEC error code : CRC error */
- DCAN_ES_MASK_NO_EVENT = DCAN_ES_LEC_EN_8_0X7,
- /**< LEC error code : No event detected */
- DCAN_ES_MASK_TX_OK = DCAN_ES_TXOK_MASK,
- /**< DCAN transmitted a message successfully */
- DCAN_ES_MASK_RX_OK = DCAN_ES_RXOK_MASK,
- /**< DCAN received a message successfully */
- DCAN_ES_MASK_ERR_PASSIVE = DCAN_ES_EPASS_MASK,
- /**< DCAN is in Error passive state */
- DCAN_ES_MASK_ERR_WARNING = DCAN_ES_EWARN_MASK,
- /**< DCAN has crossed the error warning limit */
- DCAN_ES_MASK_BUS_OFF = DCAN_ES_BOFF_MASK,
- /**< DCAN is in bus-off state */
- DCAN_ES_MASK_PARITY_ERR = DCAN_ES_PER_MASK,
- /**< Parity error is detected */
- DCAN_ES_MASK_WAKEUP_PENDING = DCAN_ES_WAKEUP_PND_MASK,
- /**< Wakeup pending */
- DCAN_ES_MASK_POWER_DOWN = DCAN_ES_PDA_MASK
- /**< DCAN is in local power down mode */
-} dcanErrStsMask_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN error counter
- * register values
- */
-typedef enum dcanErrCntrMask
-{
- DCAN_EC_MASK_TX_ERR = DCAN_ERRC_TEC_MASK,
- /**< DCAN transmit error counter */
- DCAN_EC_MASK_RX_ERR = DCAN_ERRC_REC_MASK,
- /**< DCAN receive error counter */
- DCAN_EC_MASK_RX_ERR_PASSIVE = DCAN_ERRC_RP_MASK
- /**< DCAN receive error passive */
-} dcanErrCntrMask_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN test modes
- */
-typedef enum dcanTestMode
-{
- DCAN_TEST_MODE_NONE,
- /**< All DCAN test mode is disabled. Use for normal operation. */
- DCAN_TEST_MODE_SILENT,
- /**< DCAN Silent test mode */
- DCAN_TEST_MODE_LPBACK,
- /**< DCAN loopback test mode */
- DCAN_TEST_MODE_LPBACK_SILENT,
- /**< DCAN loopback with silent test mode */
- DCAN_TEST_MODE_EXT_LPBACK
- /**< DCAN external loopback test mode */
-} dcanTestMode_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN interrupt lines
- */
-typedef enum dcanIntrLineNum
-{
- DCAN_INTR_LINE_NUM_0,
- /**< DCAN interrupt line 0 */
- DCAN_INTR_LINE_NUM_1
- /**< DCAN interrupt line 1 */
-} dcanIntrLineNum_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN interface
- * registers
- */
-typedef enum dcanIfRegNum
-{
- DCAN_IF_REG_NUM_1 = 1U,
- /**< DCAN interface register number 1 used for both read and write */
- DCAN_IF_REG_NUM_2 = 2U,
- /**< DCAN interface register number 2 used for both read and write */
- DCAN_IF_REG_NUM_3 = 3U
- /**< DCAN interface register number 3 used only for read
- */
-} dcanIfRegNum_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN Identifier Type
- */
-typedef enum dcanXidType
-{
- DCAN_XID_11_BIT,
- /**< 11bit DCAN Identifier */
- DCAN_XID_29_BIT
- /**< 29bit DCAN Identifier */
-} dcanXidType_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN mode of
- * operation
- */
-typedef enum dcanMode
-{
- DCAN_MODE_NORMAL,
- /**< DCAN normal mode */
- DCAN_MODE_INIT
- /**< DCAN initialization mode */
-} dcanMode_t;
-
-/**
- * \brief Enumerates the values used to represent the DCAN parity error
- * status
- */
-typedef enum dcanParityErrSts
-{
- DCAN_PARITY_ERR_STS_MSG_NUM = DCAN_PERR_MESSAGE_NUMBER_MASK,
- /**< Mask used to deduce the message number which caused the Parity error */
- DCAN_PARITY_ERR_STS_WORD_NUM = DCAN_PERR_WORD_NUMBER_MASK
- /**< Mask used to deduce the word number
- * which caused the Parity error */
-} dcanParityErrSts_t;
-
-#if defined (SOC_TDA3XX)
-/**
- * \brief Enumerates the values used to represent the DCAN ECC Diagnostic
- * status information
- */
-typedef enum dcanEccDiagErrStsMask
-{
- DCAN_ECC_DIAG_SB_ERR_STS = DCAN_ECC_DIAG_STATUS_SE_FLAG_MASK,
- /**< Mask used to deduce whether single bit error diagnostic is detected or
- *not */
- DCAN_ECC_DIAG_DB_ERR_STS = DCAN_ECC_DIAG_STATUS_DE_FLAG_MASK
- /**< Mask used to deduce whether double bit error
- * diagnostic is detected or not */
-} dcanEccDiagErrStsMask_t;
-#endif
-
-/* ========================================================================== */
-/* Structure Declarations */
-/* ========================================================================== */
-
-/** \brief Structure holding bit time parameters for DCAN
- */
-typedef struct dcanBitTimeParams
-{
- uint32_t baudRatePrescaler;
- /**< Baud rate prescaler
- * Value by which the CAN_CLK frequency is divided for generating the bit
- * time quanta. The bit time is built up from a multiple of this quanta
- * Valid programmed values are 0 to 63. The actual BRP value interpreted
- * for the bit timing will be programmed as BRP value + 1
- */
- uint32_t syncJumpWidth;
- /**< Synchronization Jump Width
- * Valid programmed values are 0 to 3. The actual SJW value interpreted
- * for the synchronization will be as programmed SJW value + 1
- */
- uint32_t timeSegment1;
- /**< Time segment before the sample point
- * Valid programmed values are 1 to 15. The actual TSeg1 value interpreted
- * for the bit timing will be programmed as TSeg1 value + 1
- */
- uint32_t timeSegment2;
- /**< Time segment after the sample point
- * Valid programmed values are 0 to 7. The actual TSeg2 value which is
- * interpreted for the bit timing will be the programmed as
- * TSeg2 value + 1
- */
- uint32_t baudRatePrescalerExt;
- /**< Baud rate prescaler extension
- * Valid programmed values are 0 to 15. By programming BRPE the baud rate
- * prescaler can be extended to values up to 1024
- */
-} dcanBitTimeParams_t;
-
-/** \brief Structure holding configuration parameters of DCAN module
- */
-typedef struct dcanCfgParams
-{
- uint32_t parityEnable;
- /**< Parity /ECC Enable or Disable for Tda2xx/Tda3xx
- * Valid values: TRUE or FALSE
- */
- uint32_t eccModeEnable;
- /**< Enable/disable SECDED single bit error correction
- * Valid values: TRUE or FALSE. This is used only for TDA3xx platform
- */
- uint32_t eccDiagModeEnable;
- /**< Enable/disable SECDED Diagnostic Mode
- * Valid values: TRUE or FALSE. This is used only for TDA3xx platform
- */
- uint32_t sbeEventEnable;
- /**< Enable/disable SECDED single bit error event
- * Valid values: TRUE or FALSE. This is used only for TDA3xx platform
- */
- uint32_t intrLine0Enable;
- /**< Interrupt line 0 enable/disable. Valid values: TRUE or FALSE */
- uint32_t intrLine1Enable;
- /**< Interrupt line 1 enable/disable. Valid values: TRUE or FALSE */
- uint32_t stsChangeIntrEnable;
- /**< Status Change Interrupt enable/disable. Valid values: TRUE or FALSE */
- uint32_t errIntrEnable;
- /**< Error Interrupt enable/disable. Valid values: TRUE or FALSE */
- uint32_t if1DmaEnable;
- /**< IF1 DMA enable/disable. Valid values: TRUE or FALSE */
- uint32_t if2DmaEnable;
- /**< IF2 DMA enable/disable. Valid values: TRUE or FALSE */
- uint32_t if3DmaEnable;
- /**< IF3 DMA enable/disable. Valid values: TRUE or FALSE */
- uint32_t autoRetransmitDisable;
- /**< Disable Automatic retransmission of failure messages :
- * Valid values: TRUE or FALSE
- */
- uint32_t autoBusOnEnable;
- /**< Auto Bus on enable/disable. Valid values: TRUE or FALSE */
- uint32_t autoBusOnTimerVal;
- /**< Auto Bus-On Timer Value in OCP clocks
- * Valid only when autoBusOnEnable is set
- */
- uint32_t testModeEnable;
- /**< Test Mode enable/disable. Valid values: TRUE or FALSE */
- uint32_t testMode;
- /**< Test mode. For valid values refer enum #dcanTestMode_t
- * Valid only when testModeEnable is set
- */
- uint32_t ramAccessEnable;
- /**< Direct access to the RAM is enabled/disabled while in test mode
- * Valid only when testModeEnable is set - Valid values: TRUE or FALSE
- */
-} dcanCfgParams_t;
-
-/** \brief Structure holding common configuration parameters of tx /rx of DCAN
- * module
- */
-typedef struct dcanMsgObjCfgParams
-{
- uint32_t direction;
- /**< Message object direction.For valid values refer
- * enum #dcanDirection_t
- */
- uint32_t xIdFlagMask;
- /**< Extended Identifier IDE bit Mask: Valid values: TRUE or FALSE */
- uint32_t dirMask;
- /**< Message Direction Mask: Valid values: TRUE or FALSE */
- uint32_t msgIdentifierMask;
- /**< Identifier Mask - [28:0] are valid bits */
- uint32_t xIdFlag;
- /**< Extended IDE Flag : Standard / Extended Identifier
- * For valid values refer enum # dcanXidType_t
- */
- uint32_t msgIdentifier;
- /**< Message Identifier - [28:0] are valid bits */
- uint32_t msgValid;
- /**< Valid or Invalid Message Objects.Valid values: TRUE or FALSE */
- uint32_t uMaskUsed;
- /**< Use mask (Msk[28:0], MXtd, and MDir) for acceptance filtering or not */
- uint32_t intEnable;
- /**< Interrupt Enable : IntPnd will be triggered or not after the
- * successful transmission/reception of a frame
- * Valid values: TRUE or FALSE
- */
- uint32_t remoteEnable;
- /**< At the reception of a remote frame, TxRqst is changed or not
- * Valid only for TX - Valid values: TRUE or FALSE
- */
- uint32_t fifoEOBFlag;
- /**< Message object is part of FIFO Buffer or not
- * Valid only for RX -Valid values: TRUE or FALSE
- */
-} dcanMsgObjCfgParams_t;
-
-/** \brief Structure holding transfer parameters of DCAN module
- */
-typedef struct dcanMsgParams
-{
- uint32_t dataLength;
- /**< Message object data length - Valid values: 1 to 8 */
- uint32_t msgLostFlag;
- /**< At the reception of a Message, Message is received or lost
- * Valid only for RX - Valid values: TRUE or FALSE
- */
- uint8_t msgData[DCAN_MAX_MSG_LENGTH];
- /**< Data Value to be transmitted */
-} dcanMsgParams_t;
-
-typedef dcanMsgParams_t dcanTxParams_t;
-typedef dcanMsgParams_t dcanRxParams_t;
-
-/** \brief Structure holding DCAN ECC Error status.
- */
-typedef struct dcanEccErrStatus
-{
- uint32_t singleBitErr;
- /**< DCAN ECC : When one bit Error occured on Message Ram */
- uint32_t doubleBitErr;
- /**< DCAN ECC : When two bits Error occured on Message Ram */
-} dcanEccErrStatus_t;
-
-/* ========================================================================== */
-/* Function Declarations */
-/* ========================================================================== */
-
-/**
- * \brief This API will reset the DCAN module and configure the DCAN TX/RX
- * IO Control register
- *
- * \param baseAddr Base Address of the DCAN module Register
- * \param timeOut Timeout value
- *
- * \return STW_SOK on success else STW_EFAIL when DCAN reset fails
- *
- * \note This API has to be called before the driver can be used
- */
-int32_t DCANReset(uint32_t baseAddr, uint32_t timeOut);
-
-/**
- * \brief This API will configure the operating mode of DCAN
- * In Init mode the communication on CAN bus is stopped and the
- * controller needs to be placed in Init mode for initialization
- * To start communication on CAN bus please keep the DCAN controller
- * in Normal mode of operation
- *
- * \param baseAddr Base Address of the DCAN module Register
- * \param mode DCAN mode to be configured
- * For valid values refer enum #dcanMode_t
- *
- * \return None
- */
-void DCANSetMode(uint32_t baseAddr, uint32_t mode);
-
-/**
- * \brief This API configures bit time parameters for DCAN module
- *
- * \param baseAddr Base Address of the DCAN module Register
- * \param pBitTimePrms Pointer which holds DCAN bit time parameters
- *
- * \return None
- */
-void DCANSetBitTime(uint32_t baseAddr, const dcanBitTimeParams_t *pBitTimePrms);
-
-/**
- * \brief This API configures DCAN controller
- *
- * \param baseAddr Base Address of the DCAN module Register
- * \param pDcanCfgPrms Pointer which holds DCAN controller config parameters
- *
- * \return None
- *
- * \note The API DCANReset has to be called before this API can
- * be used
- */
-void DCANConfig(uint32_t baseAddr, const dcanCfgParams_t *pDcanCfgPrms);
-
-/**
- * \brief This API configures DCAN TX/RX message object
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values: 1 to 64
- * \param ifRegNum DCAN interface register number
- * For valid value refer enum #dcanIfRegNum_t
- * \param pMsgObjCfgPrms Pointer which holds DCAN message object Config
- * parameters of TX/RX
- *
- * \return STW_SOK on success else STW_EFAIL when IF register busy flag is
- * set
- */
-int32_t DCANConfigMsgObj(uint32_t baseAddr,
- uint32_t msgObj,
- uint32_t ifRegNum,
- const dcanMsgObjCfgParams_t *pMsgObjCfgPrms);
-
-/**
- * \brief This API transmits a CAN message and writes a CAN message into a
- * CAN message object
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values: 1 to 64
- * \param ifRegNum DCAN interface register number
- * For valid values refer enum #dcanIfRegNum_t
- * \param pDcanTxPrms Pointer which holds DCAN transmit parameters
- * \param timeOut Timeout value
- *
- * \return STW_SOK on success else STW_EFAIL when IF register busy flag is
- * set
- */
-int32_t DCANTransmitData(uint32_t baseAddr,
- uint32_t msgObj,
- uint32_t ifRegNum,
- const dcanTxParams_t *pDcanTxPrms,
- uint32_t timeOut);
-
-/**
- * \brief This API gets received CAN message from message RAM
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values : 1 to 64
- *
- * \param ifRegNum DCAN interface register number
- * For valid values refer enum #dcanIfRegNum_t
- * \param pDcanRxPrms Pointer which holds DCAN receive parameters
- * \param timeOut Timeout value
- *
- * \return STW_SOK on success else STW_EFAIL when IF register busy flag is
- * set
- *
- * \note The API will receive valid data of size dataLength
- */
-int32_t DCANGetData(uint32_t baseAddr,
- uint32_t msgObj,
- uint32_t ifRegNum,
- dcanRxParams_t *pDcanRxPrms,
- uint32_t timeOut);
-
-/**
- * \brief This API returns Tx message object transmission status whether Tx
- * message object has a pending Tx request or not
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values: 1 to 64
- *
- * \return FALSE when data transmission is successful else TRUE when data
- * transmission is not successful
- */
-uint32_t DCANIsTxMsgPending(uint32_t baseAddr, uint32_t msgObj);
-
-/**
- * \brief This API returns Rx message object reception status whether Rx
- * message object has a pending Rx data or not
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values: 1 to 64
- *
- * \return TRUE when new data has arrived else FALSE when new data has not
- * arrived
- */
-uint32_t DCANHasRxMsgArrived(uint32_t baseAddr, uint32_t msgObj);
-
-/**
- * \brief This API checks for whether msgObj is valid or not
- *
- * \param baseAddr Base Address of the DCAN Module Registers.
- * \param msgObj Message object number whose message valid status
- * is to be returned.
- *
- * \return TRUE when message object is valid else FALSE when message object
- * is invalid
- */
-uint32_t DCANIsMsgValid(uint32_t baseAddr, uint32_t msgObj);
-
-/**
- * \brief This API checks for whether DCAN IF Register is busy or not
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param ifRegNum DCAN interface register number
- * For valid values refer enum #dcanIfRegNum_t
- *
- * \return TRUE when DCAN IF Register is busy else FALSE when DCAN IF
- * Register is not busy
- */
-uint32_t DCANIsIfRegBusy(uint32_t baseAddr, uint32_t ifRegNum);
-
-/**
- * \brief This API will configure which interrupt line is used to service
- * interrupts for message objects
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number
- * \param intrLineNum Interrupt line number to be configured
- * For valid values refer enum #dcanIntrLineNum_t
- *
- * \return None
- */
-void DCANConfigIntrMux(uint32_t baseAddr,
- uint32_t intrLineNum,
- uint32_t msgObj);
-
-/**
- * \brief This API returns interrupt line status of DCAN
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param intrLineNum DCAN interrupt line number
- * For valid values refer enum #dcanIntrLineNum_t
- *
- * \return message object number with highest pending interrupt or
- * number which indicates Source of the interrupt
- * 0x0000 : No interrupt is pending
- * 0x0001-0x0040 : Message object Number which caused the interrupt
- * 0x0041-0x7FFF : Unused
- * 0x8000 : DCAN_ES value is not 0x07.
- * 0x8001-0xFFFF : Unused
- */
-uint32_t DCANGetIntrStatus(uint32_t baseAddr, uint32_t intrLineNum);
-
-/**
- * \brief This API returns message object interrupt pending status
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values: 1 to 64
- *
- * \return TRUE when message object has pending interrupt else FALSE when
- * message object has no pending interrupt
- */
-uint32_t DCANIsMsgObjIntrPending(uint32_t baseAddr, uint32_t msgObj);
-
-/**
- * \brief This API will clear the interrupt pending status of received message
- * objects after a new message is received
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param msgObj Message object number of CAN node
- * Valid values : 1 to 64
- * \param ifRegNum DCAN interface register number
- * For valid values refer enum #dcanIfRegNum_t
- * \return None
- */
-void DCANIntrClearStatus(uint32_t baseAddr, uint32_t msgObj, uint32_t ifRegNum);
-
-/**
- * \brief This API will read the error and status information of DCAN
- * controller
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return Returns the error and status values.For valid values refer
- * enum #dcanErrStsMask_t
- *
- * \note Reading the error and status register will clear/set certain bits
- * in the error and status register. For more information please
- * refer the DCAN Technical Reference Manual(TRM). For debug support,
- * the auto clear functionality of error and status register is
- * disabled when in debug/suspend mode
- */
-uint32_t DCANGetErrStatus(uint32_t baseAddr);
-
-/**
- * \brief This API will read the error counter status of DCAN
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return Returns the error counter status values. For valid values refer
- * enum #dcanErrCntrMask_t
- */
-uint32_t DCANGetErrCntrStatus(uint32_t baseAddr);
-
-/**
- * \brief This API will read the DCAN parity error status
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return Returns the DCAN parity error status. For valid values refer
- * enum #dcanParityErrSts_t
- */
-uint32_t DCANGetParityErrStatus(uint32_t baseAddr);
-
-/**
- * \brief This API returns message object number where DCAN ECC Single
- * Bit Error is detected
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return retVal Returns the message object number where DCAN ECC Single
- * Bit Error is detected
- * For Tda2xx it returns DCAN_INVALID_MSG_OBJECT
- *
- * \note This API is valid only for Tda3xx
- */
-uint32_t DCANGetMsgObjBitErrDetected(uint32_t baseAddr);
-
-/**
- * \brief This API will read the ECC diagnostic status information of DCAN
- * controller
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return Returns the ECC disagnostic error status information.
- * For valid values refer enum #dcanEccDiagErrStsMask_t
- *
- * \note This API is valid only for Tda3xx
- */
-uint32_t DCANGetEccDiagErrStatus(uint32_t baseAddr);
-
-/**
- * \brief This API will read the ECC error status information of DCAN
- * controller
- *
- * \param baseAddr Base Address of the DCAN module register
- *
- * \return Returns the ECC error status information.
- *
- * \note This API is valid only for Tda3xx
- */
-uint32_t DCANGetEccErrStatus(uint32_t baseAddr);
-
-/**
- * \brief Enable/disable the DCAN parity/ECC
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param enablePMD Enable/Disable DCAN parity(for Tda2xx)/ECC(for Tda3xx)
- * Valid values: TRUE or FALSE
- *
- * \return None
- */
-void DCANParityEnable(uint32_t baseAddr, uint32_t enablePMD);
-
-/**
- * \brief Enable/ Disable the test mode of DCAN
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param enableTestMode Enable/Disable test mode of DCAN.
- * Valid values: TRUE or FALSE
- * \param testMode Select the DCAN test mode
- * For valid values refer enum # dcanTestMode_t
- *
- * \return None
- */
-void DCANTestModeEnable(uint32_t baseAddr,
- uint32_t enableTestMode,
- uint32_t testMode);
-
-/**
- * \brief Enable/disable the DCAN ECC Diagnostic Mode.
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param enableEccDiagMode Enable/Disable DCAN ECC Diagnostic Mode
- * Valid values: TRUE or FALSE
- *
- * \return None
- *
- * \note This API is valid only for Tda3xx
- */
-void DCANEccDiagModeEnable(uint32_t baseAddr, uint32_t enableEccDiagMode);
-
-/**
- * \brief This API is used to Enable/disable SECDED Single bit Error
- * correction and SECDED Single bit Error Event
- *
- * \param baseAddr Base Address of the DCAN module register
- * \param enableEccMode Enable/Disable SECDED Single bit Error
- * correction.
- * Valid values: TRUE or FALSE
- * \param enableSbeEvent Enable/Disable SECDED Single bit Error
- * Event.
- * Valid values: TRUE or FALSE
- *
- * \return None
- *
- * \note This API is valid only for Tda3xx
- */
-void DCANEccModeEnable(uint32_t baseAddr,
- uint32_t enableEccMode,
- uint32_t enableSbeEvent);
-
-/**
- * \brief This function clears the error status of DCAN ECC.
- *
- * \param errClr Holds the values of which error need to be cleared.
- * Refer #dcanEccErrStatus_t for more details.
- * A value of 1 is written to these fields that need to
- * be cleared and 0 for those that need not be cleared.
- *
- * \return STW_SOK on success else STW_EFAIL
- *
- * \note This API is valid only for Tda3xx
- */
-int32_t DCANClrEccErrStatus(uint32_t baseAddr,
- const dcanEccErrStatus_t *errClr);
-
-/**
- * \brief This function clears the error status of DCAN ECC Diagnostic.
- *
- * \param errClr Holds the values of which error need to be cleared.
- * Refer #dcanEccErrStatus_t for more details.
- * A value of 1 is written to these fields that need to
- * be cleared and 0 for those that need not be cleared.
- *
- * \return STW_SOK on success else STW_EFAIL
- *
- * \note This API is valid only for Tda3xx
- */
-int32_t DCANClrEccDiagErrStatus(uint32_t baseAddr,
- const dcanEccErrStatus_t *errClr);
-
-/**
- * \brief This function clears the status of parity error on
- * DCAN_PARITY interrupt line
- *
- * \return None
- */
-void DCANClrParityIntrStatus(uint32_t baseAddr);
-
-#ifdef __cplusplus
-}
-#endif
-
-#endif /* #ifndef DCAN_H_ */
-/********************************* End of file ******************************/