Change OS package name
Remove DEL3 from FD package
Add cygwin to path end instead of path start so git.exe found in git installation instead of cygwin
Update paf submodule
Small fixes for build profile
Remove unnecessary cd
Add Debug, Release, and SDF build profiles. This allows normal build all and SDF build all.
Add nul to directory existence check
Add OS package creation script
Move DH-IP package creation outside of CCS project build script
Add FD package creation script
Add ARM/DSP debug build profiles which use generated dolby ip packages
Save / restore path before / after PDK LLD libraries build
Remove unzip (git tools) from path since this disturbs PAF library builds
Update build scripts for package creation
Add brute force reset of environment after PDK LLD library builds
Update package creation script. Work in progress.
Update build scripts for auto build
Move build batch files to scripts folder
Change ENC channel map from for 7.1
Change DDP at-boot configuration to 7.1
Use already installed sed instead of cygwin sed for build. Update build instructions.
Add comment in at-boot for 12-speaker layout SYS channel config.
Update PAF and component build batch files.
ARM/DSP PAF libraries now built without manually modifying target.mk.
Note sed (cygwin) dependency introduced.
ARM/DSP PAF libraries now built without manually modifying target.mk.
Note sed (cygwin) dependency introduced.
Add BMDA configuration for at-boot DDP 5.1.2 speaker layout
Merge branch 'dev_pasdk_govind' into dev_pasdk_frank
Change at-boot configuration to DDP
Remove MAT-THD decoder at-boot commands for BMDA testing
Add at-boot testing configuration for MAT-THD decoder.
Add BMDA to DSP build
Remove debug SW_BREAKPOINT.
This allows more than single MAT-THD stream without hang on ARM.
However, need to make sure error returned by decode() is ok.
This allows more than single MAT-THD stream without hang on ARM.
However, need to make sure error returned by decode() is ok.
Update paf version. Required to run make_sw to generate updated .hdM files.
Update for DA10x checkIP (PASDK-140)
Add code missing from manual merge
Update PAF to MAT-THD integration version. Update DCS7 app-level parameters to avoid crash in DCS7_open.
Update CAR submodule
Revert at-boot input shortcut to execPAIInHDMIStereo
Update to test PASDK-80:DSP crashes when CAR dynamically enabled over UART w/ ADC&DAC I/O. Update CAR submodule.
Update to test PASDK-80:DSP crashes when CAR dynamically enabled over UART w/ ADC&DAC I/O. ADC Input & CAR in patches.
Remove SW breakpoint on afCbWrite
Merge remote-tracking branch 'remotes/origin/dev_pasdk_qin_pasdk111_fix' into dev_pasdk_frank
# Conflicts:
# pasdk/test_dsp/framework/itopo/patchs.c
# Conflicts:
# pasdk/test_dsp/framework/itopo/patchs.c
Update OARI submodule for PASDK-35 & PASDK-111 testing. This is version with OARI update only.
Re-order CAR and OAR in patches since OAR overwrites audio frame bitstream metadata mode to ch-based.
CAR will always execute if it follows OAR.
This follows DA8xx DH1.2 convention.
This PASDK-35 & PASDK-111 testing, before bug fix version of framework.
CAR will always execute if it follows OAR.
This follows DA8xx DH1.2 convention.
This PASDK-35 & PASDK-111 testing, before bug fix version of framework.
Update OARI submodule for PASDK-35 & PASDK-111 testing. This is before bug fix version of OARI.
Update for PASDK-79: DSP crashes on system initialization if CAR is enabled by default.
* Resolved Channel Swap Issue - for PASDK-101
* Added new 12 & 16 ch output shortcuts - for PASDK-49
* Added new 12 & 16 ch output shortcuts - for PASDK-49
Update for PASDK-64: DDP Baseline: alpha commands over UART cause muting. AFP task thread higher priority than ASIT/ASOT. This is a temporary fix.
Testing for PASDK-38:Verify ARM crash doesn't happen
Changes in generate mute frame - Use last audio frame configuration info to generate mute frame to avoid OAR/CAR re-initialization due to different channel configuration request
Included OAR in the ASP processing chain.
Fixed AF PCM buffers memory size calculation problem.
Update submodules.
Manual merge from dev_pasdk_qin_thdintegration, commitId=434f3e8
Moved AudioFrame buffers in DecodeInStruct/DecodeOutStruct to external
memory.
Moved AudioFrame buffers in DecodeInStruct/DecodeOutStruct to external
memory.
Update paf submodule
Update for UART/SPI/I2C LLD build instructions
Update paf submodule
Add build_pdk_libs.bat file
Update I2C and SPI LLD makefiles -- reduce build time
PDK: UART EDMA, Tx fifo fix in UART_close().
PDK: UART EDMA mode fixes updated.
SPI and I2C LLD slave support.
Add code build and install instructions
Update setup guide
Update include directories in test_dsp and test_arm CCS projects
Update paf submodule
Update paf submodule
Update Dolby IP submodules
Add paf as submodule
Update test_arm CCS project for Dolby IP submodules
Update test_arm and test_dsp CCS projects for Dolby IP submodules
Update submodules
Update submodules
Add submodules
Remove processor_audio_sdk_1_00_00_00 subfolder
Update test_arm and test_dsp projects for new locations of IPC and PDK eng
Move IPC 3.43.00.00 eng and PDK 1.0.1.0 eng to subfolders
Change directory names in eclipse folder for RTSC plugin -- missing feature.xml
Add batch file to build alg libs
Move components up one folder level
Remove IPC 3.43.00.00 eng .zip file
Update gitattributes & gitignore
Add IPC 3.34.00.00 eng release
Update DSP app to select pdk eng RTSC component
Update app builds for new pdk folder
Update files in eclipse folder for RTSC plugin
Change directory names in eclipse folder for RTSC plugin
Change pdk_k2g_1_0_1 directory name in preparation for updating RSTC plugin
Add alpha files for car
Fix typo
Initial CAR integration (256 kB L2).
Fix typo in comment
Remove DDPJOCDcodeModeDisable, change SYS ch cfg request to 7.1. Remove DAP, add OAR.
Increase at-boot master volume to 0 dB so no need to issue alpha command for volume increase at start up (convenient for development)
Add support for DDR shared heap. Note:algs use IALG_EXTERNAL_SHM, which is IALG_ESDATA.
Add comment for original nominal transfer size. Results in different type of failure for DDP streaming.
Reduce at-boot master volume to -40 dB for connection to amps