Update capIb to account for input buffer wrap. Add gCapIbAccBytes reset to capIbReset().
Update for PASDK150
Merge updates for PASDK-114
Update Debug_pkgs builds
Merge updates for PASDK-69
resolved merge issues.
Merge branch 'dev_pasdk_pp_pasdk69ArmDspCom' into 'dev_pasdk_pp_pasdk114matthdissue'
Conflicts:
build_paf_libs.bat
pasdk/test_arm/.cproject
pasdk/test_dsp/.cproject
pasdk/test_dsp/application/app.cmd
tools/alpha/thd_a.h
tools/alpha/thd_a.hdM
Conflicts:
build_paf_libs.bat
pasdk/test_arm/.cproject
pasdk/test_dsp/.cproject
pasdk/test_dsp/application/app.cmd
tools/alpha/thd_a.h
tools/alpha/thd_a.hdM
PASDK114: updated submodule.
PASDK150: Workaround for UART timeout due to Hwi_disable().
PASDK114: updated PAF and MAT-THD submodule.
PASDK114: Bug in Circular buffer fixed for MAT streams (observed when metadata size increased)
Fixed IPC init issue.
Updates for DCS7 (UART SWI implementation). Fixed IPC init issue.
Update dcs7_params.c for using the DCS7 code after review.
Took UART LLD cancel() improvement from Latest PDK code base.
Update dcs7_params.c for using the DCS7 code after review.
Took UART LLD cancel() improvement from Latest PDK code base.
PASDK150: Updated PAF submodule.
Merge branch 'dev_pasdk_pp_pasdk69ArmDspCom' into 'dev_pasdk_pp'.
Update PAF submodule
Add target platform and version number for generated packages.
Add date stamp to generated Dolby IP package names.
Dynamically determine Dolby IP package names in CCS project build.
Add date stamp to generated Dolby IP package names.
Dynamically determine Dolby IP package names in CCS project build.
PASDK69: Created task for idleAudioStream(). Added MAT-THD alpha header file.
PASDK69: Updated paf and MAT-THD submodule.
Fix merge changes to support MAT-THD.
Merge branch 'dev_pasdk_govind' into 'dev_pasdk_pp_pasdk69ArmDspCom'
Conflicts:
pasdk/paf
pasdk/test_arm/framework/audioStreamDecodeProc.c
pasdk/test_dsp/framework/audioStreamInpProc.c
Conflicts:
pasdk/paf
pasdk/test_arm/framework/audioStreamDecodeProc.c
pasdk/test_dsp/framework/audioStreamInpProc.c
Update PAF submodule
Update intrinsics submodule
Update DDP submodule
Add custom clean rule for mat-thd libraries
Add more build artifacts to gitignore
Remove original platform lib code -- can be obtained from Processor SDK 2.0.2.11
Remove SPI LLD build artifacts
Remove I2C LLD build artifacts
Remove UART LLD build artifacts
Single .gitignore for super repo
Add some build artifacts to gitignore
Add custom make rules for UART, SPI, and I2C LLDs
Update build scripts to remove check IP soure files (.c, .h) and makefile from OS package
Update ARM Debug_pkgs to use app_pkgs.cmd
Update setup guide to v0.3 for Alpha-2 release
Update submodules
Update processor audio sdk version number
Remove setup guide from OS package creation
PASDK69: updated ddp and paf submodules.
PASDK69: updated DCS7 params.
PASDK69: added support for NON_CACHE_STATUS.
Update FD package creation: pa parent folder and DOC folder name to docs
Update paf submodule
Remove checkIp.h header file from OS package
Update FD package generation to use existing component directory strcture
Retain stderr.h and bmerr.h in OS package
Fix scripts directory locatio
Update oar package include for dlb_buffer.h
Update alpha command files to not include dap
Fix DSP Debug_pkgs build
Reverse order of parameters to build_ccs_projects.bat
Change OS package name
Remove DEL3 from FD package
Add cygwin to path end instead of path start so git.exe found in git installation instead of cygwin
Update paf submodule
Small fixes for build profile
Remove unnecessary cd
Add Debug, Release, and SDF build profiles. This allows normal build all and SDF build all.
Add nul to directory existence check
Add OS package creation script
Move DH-IP package creation outside of CCS project build script
Add FD package creation script
PASDK69: Added support for Non-cacheable DDR memory.
Add ARM/DSP debug build profiles which use generated dolby ip packages
Save / restore path before / after PDK LLD libraries build
Remove unzip (git tools) from path since this disturbs PAF library builds
Update build scripts for package creation
Add brute force reset of environment after PDK LLD library builds
Update package creation script. Work in progress.
Update build scripts for auto build
Move build batch files to scripts folder
Change ENC channel map from for 7.1
Change DDP at-boot configuration to 7.1
Use already installed sed instead of cygwin sed for build. Update build instructions.
Add comment in at-boot for 12-speaker layout SYS channel config.
PASDK69: updated DDP and PAF submodule.
PASDK69: Created Non-Cacheable memory region.
Update PAF and component build batch files.
ARM/DSP PAF libraries now built without manually modifying target.mk.
Note sed (cygwin) dependency introduced.
ARM/DSP PAF libraries now built without manually modifying target.mk.
Note sed (cygwin) dependency introduced.
Add BMDA configuration for at-boot DDP 5.1.2 speaker layout
Merge branch 'dev_pasdk_govind' into dev_pasdk_frank
Change at-boot configuration to DDP
PASDK69: added common API to access shared status structures.
Remove MAT-THD decoder at-boot commands for BMDA testing
Add at-boot testing configuration for MAT-THD decoder.
Add BMDA to DSP build
Remove debug SW_BREAKPOINT.
This allows more than single MAT-THD stream without hang on ARM.
However, need to make sure error returned by decode() is ok.
This allows more than single MAT-THD stream without hang on ARM.
However, need to make sure error returned by decode() is ok.
Update paf version. Required to run make_sw to generate updated .hdM files.
Update for DA10x checkIP (PASDK-140)
merging from dev_pasdk_frank
Add code missing from manual merge
Update PAF to MAT-THD integration version. Update DCS7 app-level parameters to avoid crash in DCS7_open.
Update CAR submodule
Revert at-boot input shortcut to execPAIInHDMIStereo
Update to test PASDK-80:DSP crashes when CAR dynamically enabled over UART w/ ADC&DAC I/O. Update CAR submodule.
Update to test PASDK-80:DSP crashes when CAR dynamically enabled over UART w/ ADC&DAC I/O. ADC Input & CAR in patches.
Remove SW breakpoint on afCbWrite
Merge remote-tracking branch 'remotes/origin/dev_pasdk_qin_pasdk111_fix' into dev_pasdk_frank
# Conflicts:
# pasdk/test_dsp/framework/itopo/patchs.c
# Conflicts:
# pasdk/test_dsp/framework/itopo/patchs.c